MSP DSP Library
|
Cmsp_abs_iq31_params | Parameter structure for the IQ31 vector absolute value function |
Cmsp_abs_q15_params | Parameter structure for the Q15 vector absolute value function |
Cmsp_add_iq31_params | Parameter structure for the IQ31 vector add functions |
Cmsp_add_q15_params | Parameter structure for the Q15 vector add functions |
Cmsp_biquad_df1_q15_params | Parameter structure for Direct Form 1 biquad filter |
Cmsp_biquad_df2_q15_params | Parameter structure for Direct Form 2 biquad filter |
Cmsp_cmplx_add_iq31_params | Parameter structure for the IQ31 complex vector add functions |
Cmsp_cmplx_add_q15_params | Parameter structure for the Q15 complex vector add functions |
Cmsp_cmplx_bitrev_iq31_params | Parameter structure for IQ31 complex bit-reversal |
Cmsp_cmplx_bitrev_q15_params | Parameter structure for Q15 complex bit-reversal |
Cmsp_cmplx_conj_iq31_params | Parameter structure for the IQ31 complex vector conjugate function |
Cmsp_cmplx_conj_q15_params | Parameter structure for the Q15 complex vector conjugate function |
Cmsp_cmplx_fft_iq31_params | Parameter structure for IQ31 complex FFT functions |
Cmsp_cmplx_fft_q15_params | Parameter structure for Q15 complex FFT functions |
Cmsp_cmplx_fill_iq31_params | Parameters for IQ31 complex vector fill |
Cmsp_cmplx_fill_q15_params | Parameters for Q15 complex vector fill |
Cmsp_cmplx_fir_iq31_params | Parameter structure for complex FIR filter |
Cmsp_cmplx_fir_q15_params | Parameter structure for complex FIR filter |
Cmsp_cmplx_mac_iq31_params | Parameter structure for the IQ31 complex vector multiply and accumulate function |
Cmsp_cmplx_mac_q15_params | Parameter structure for the Q15 complex vector multiply and accumulate function |
Cmsp_cmplx_mpy_iq31_params | Parameter structure for the IQ31 complex vector multiply functions |
Cmsp_cmplx_mpy_q15_params | Parameter structure for the Q15 complex vector multiply functions |
Cmsp_cmplx_mpy_real_iq31_params | Parameter structure for the IQ31 complex vector multiply by real functions |
Cmsp_cmplx_mpy_real_q15_params | Parameter structure for the Q15 complex vector multiply by real functions |
Cmsp_cmplx_scale_iq31_params | Parameter structure for the IQ31 complex vector scale by real function |
Cmsp_cmplx_scale_q15_params | Parameter structure for the Q15 complex vector scale by real function |
Cmsp_cmplx_shift_iq31_params | Parameter structure for the IQ31 complex vector shift function |
Cmsp_cmplx_shift_q15_params | Parameter structure for the Q15 complex vector shift function |
Cmsp_cmplx_sub_iq31_params | Parameter structure for the IQ31 complex vector subtract functions |
Cmsp_cmplx_sub_q15_params | Parameter structure for the Q15 complex vector subtract functions |
Cmsp_copy_iq31_params | Parameters for IQ31 vector copy function |
Cmsp_copy_q15_params | Parameters for Q15 vector copy function |
Cmsp_deinterleave_iq31_params | Parameters for IQ31 vector deinterleave |
Cmsp_deinterleave_q15_params | Parameters for Q15 vector deinterleave |
Cmsp_fft_iq31_params | Parameter structure for IQ31 real FFT functions |
Cmsp_fft_q15_params | Parameter structure for Q15 real FFT functions |
Cmsp_fill_iq31_params | Parameters for IQ31 real vector fill |
Cmsp_fill_q15_params | Parameters for Q15 real vector fill |
Cmsp_fir_iq31_params | Parameter structure for FIR filter |
Cmsp_fir_q15_params | Parameter structure for FIR filter |
Cmsp_mac_iq31_params | Parameter structure for the IQ31 vector multiply and accumulate function |
Cmsp_mac_q15_params | Parameter structure for the Q15 vector multiply and accumulate function |
Cmsp_matrix_abs_iq31_params | Parameter structure for the real matrix absolute value function |
Cmsp_matrix_abs_q15_params | Parameter structure for the real matrix absolute value function |
Cmsp_matrix_add_iq31_params | Parameter structure for the matrix add function |
Cmsp_matrix_add_q15_params | Parameter structure for the matrix add function |
Cmsp_matrix_mpy_iq31_params | Parameter structure for the real matrix multiply function |
Cmsp_matrix_mpy_q15_params | Parameter structure for the real matrix multiply function |
Cmsp_matrix_neg_iq31_params | Parameter structure for the real matrix negate function |
Cmsp_matrix_neg_q15_params | Parameter structure for the real matrix negate function |
Cmsp_matrix_offset_iq31_params | Parameter structure for the real matrix offset function |
Cmsp_matrix_offset_q15_params | Parameter structure for the real matrix offset function |
Cmsp_matrix_scale_iq31_params | Parameter structure for the real matrix scale function |
Cmsp_matrix_scale_q15_params | Parameter structure for the real matrix scale function |
Cmsp_matrix_shift_iq31_params | Parameter structure for the real matrix shift function |
Cmsp_matrix_shift_q15_params | Parameter structure for the real matrix shift function |
Cmsp_matrix_sub_iq31_params | Parameter structure for the matrix subtract function |
Cmsp_matrix_sub_q15_params | Parameter structure for the matrix subtract function |
Cmsp_matrix_trans_iq31_params | Parameter structure for the matrix transpose function |
Cmsp_matrix_trans_q15_params | Parameter structure for the matrix transpose function |
Cmsp_max_iq31_params | Parameter structure for the IQ31 signed vector maximum function |
Cmsp_max_q15_params | Parameter structure for the Q15 signed vector maximum function |
Cmsp_max_uq15_params | Parameter structure for the Q15 unsigned vector maximum function |
Cmsp_max_uq31_params | Parameter structure for the IQ31 unsigned vector maximum function |
Cmsp_min_iq31_params | Parameter structure for the IQ31 signed vector minimum function |
Cmsp_min_q15_params | Parameter structure for the Q15 signed vector minimum function |
Cmsp_min_uq15_params | Parameter structure for the Q15 unsigned vector minimum function |
Cmsp_min_uq31_params | Parameter structure for the IQ31 unsigned vector minimum function |
Cmsp_mpy_iq31_params | Parameter structure for the IQ31 vector multiply functions |
Cmsp_mpy_q15_params | Parameter structure for the Q15 vector multiply functions |
Cmsp_neg_iq31_params | Parameter structure for the IQ31 vector negate function |
Cmsp_neg_q15_params | Parameter structure for the Q15 vector negate function |
Cmsp_offset_iq31_params | Parameter structure for the vector offset function |
Cmsp_offset_q15_params | Parameter structure for the Q15 vector offset function |
Cmsp_scale_iq31_params | Parameter structure for the IQ31 vector scale function |
Cmsp_scale_q15_params | Parameter structure for the Q15 vector scale function |
Cmsp_shift_iq31_params | Parameter structure for the IQ31 vector shift function |
Cmsp_shift_q15_params | Parameter structure for the Q15 vector shift function |
Cmsp_split_iq31_params | Parameter structure for IQ31 split operation |
Cmsp_split_q15_params | Parameter structure for Q15 split operation |
Cmsp_sub_iq31_params | Parameter structure for the IQ31 vector subtract functions |
Cmsp_sub_q15_params | Parameter structure for the Q15 vector subtract functions |