Logo
MSP DSP Library
msp_matrix_add_q15_params Struct Reference

Parameter structure for the matrix add function. More...

#include <DSPLib_matrix.h>

Data Fields

uint16_t rows
 Number of rows in the source matrices, must be a multiple of two.
 
uint16_t cols
 Number of columns in the source matrices, must be a multiple of two.
 

Detailed Description

Parameter structure for the matrix add function.


The documentation for this struct was generated from the following file: