MSP DSP Library
|
Parameter structure for Direct Form 1 biquad filter. More...
#include <DSPLib_filter.h>
Data Fields | |
uint16_t | length |
const _q15 * | coeffs |
_q15 * | stateBuffer |
Parameter structure for Direct Form 1 biquad filter.
const _q15* msp_biquad_df1_q15_params::coeffs |
Pointer to filter coefficients of length 5 in format b2, b1, b0, a2, a1.
uint16_t msp_biquad_df1_q15_params::length |
Length of the source data, must be a multiple of two.
_q15* msp_biquad_df1_q15_params::stateBuffer |
Pointer to an array of length four used to store the state of the biquad operation. When continuous operation is desired the previous state needs to be passed to the next biquad operation. This data block must be allocated in shared RAM when using LEASC.