1 #ifndef __DSPLIB_FILTER_H__
2 #define __DSPLIB_FILTER_H__
345 #endif //__DSPLIB_FILTER_H__
uint16_t length
Definition: DSPLib_filter.h:110
uint16_t length
Definition: DSPLib_filter.h:151
int32_t _iq31
Signed fixed point data type with 1 integer bit and 31 fractional bits.
Definition: DSPLib_types.h:59
msp_status msp_biquad_df2_q15(msp_biquad_df2_q15_params *params, const _q15 *src, _q15 *dst)
Single order direct form 2 biquad filter.
const _q15 * coeffs
Definition: DSPLib_filter.h:59
Parameter structure for FIR filter.
Definition: DSPLib_filter.h:69
_q15 sumMin
Definition: DSPLib_filter.h:161
uint16_t tapLength
Definition: DSPLib_filter.h:56
msp_status
Enumerated type to return the status of an operation.
Definition: DSPLib_types.h:78
_q15 Q1
Definition: DSPLib_filter.h:168
const _q15 * coeffs
Definition: DSPLib_filter.h:155
uint16_t tapLength
Definition: DSPLib_filter.h:94
uint16_t length
Definition: DSPLib_filter.h:72
Parameter structure for Direct Form 1 biquad filter.
Definition: DSPLib_filter.h:126
msp_status msp_cmplx_fir_iq31(const msp_cmplx_fir_iq31_params *params, const _iq31 *src, _iq31 *dst)
Discrete-time convolution of a complex source vector with complex coefficients to apply an FIR filter...
const _iq31 * coeffs
Definition: DSPLib_filter.h:78
const _iq31 * coeffs
Definition: DSPLib_filter.h:116
msp_status msp_biquad_df1_q15(const msp_biquad_df1_q15_params *params, const _q15 *src, _q15 *dst)
Single order direct form 1 biquad filter.
_q15 sumMax
Definition: DSPLib_filter.h:158
const _q15 * coeffs
Definition: DSPLib_filter.h:132
Parameter structure for FIR filter.
Definition: DSPLib_filter.h:50
uint16_t length
Definition: DSPLib_filter.h:91
int16_t _q15
Signed fixed point data type with 1 integer bit and 15 fractional bits.
Definition: DSPLib_types.h:38
const _q15 * coeffs
Definition: DSPLib_filter.h:97
msp_status msp_fir_q15(const msp_fir_q15_params *params, const _q15 *src, _q15 *dst)
Discrete-time convolution of a source vector with real coefficients to apply an FIR filter...
msp_status msp_cmplx_fir_q15(const msp_cmplx_fir_q15_params *params, const _q15 *src, _q15 *dst)
Discrete-time convolution of a complex source vector with complex coefficients to apply an FIR filter...
_q15 * stateBuffer
Definition: DSPLib_filter.h:138
Parameter structure for complex FIR filter.
Definition: DSPLib_filter.h:88
Parameter structure for Direct Form 2 biquad filter.
Definition: DSPLib_filter.h:148
_q15 Q2
Definition: DSPLib_filter.h:172
uint16_t tapLength
Definition: DSPLib_filter.h:75
_q15 bias
Definition: DSPLib_filter.h:164
uint16_t tapLength
Definition: DSPLib_filter.h:113
Parameter structure for complex FIR filter.
Definition: DSPLib_filter.h:107
uint16_t length
Definition: DSPLib_filter.h:129
msp_status msp_fir_iq31(const msp_fir_iq31_params *params, const _iq31 *src, _iq31 *dst)
Discrete-time convolution of a source vector with real coefficients to apply an FIR filter...
uint16_t length
Definition: DSPLib_filter.h:53