The CiA organization (CAN in Automation) pursues among other things the goal of creating order and exchangeability between devices of the same type by the standardization of device descriptions. For this purpose so-called CANopen profiles are defined, which conclusively describe the changeable and unchangeable parameters of a device.
Functions | |
| uint32_t | EC_API_SLV_CoE_getObject (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, EC_API_SLV_SCoE_Object_t **pObject_p) |
| This function returns an object of the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectData (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint32_t length_p, uint16_t *pData_p) |
| This function read the object data from the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_setObjectData (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint32_t length_p, uint16_t *pData_p) |
| This function writes Data to the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectEntryCount (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t *pCount_p) |
| This function returns the number of entries of a object. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectType (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t *pType_p) |
| This function returns the type flag of the object. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectEntry (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, uint8_t subIndex_p, EC_API_SLV_SCoE_ObjEntry_t **ppObjectEntry_p) |
| This function returns object entries from the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectEntryByObject (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t subIndex_p, EC_API_SLV_SCoE_ObjEntry_t **ppObjectEntry_p) |
| This function returns object entries from the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectEntryData (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_ObjEntry_t *pObjectEntry_p, uint32_t length_p, uint16_t *pData_p) |
| This function reads Data from the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_getObjectEntryDataByObject (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, EC_API_SLV_SCoE_ObjEntry_t *pObjectEntry_p, uint32_t length_p, uint16_t *pData_p) |
| This function reads Data from the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_setObjectEntryData (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_ObjEntry_t *pObjectEntry_p, uint32_t length_p, uint16_t *pData_p) |
| This function writes Data to the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_generateObjectDict (EC_API_SLV_SHandle_t *pEcSlaveApi_p) |
| Generate Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_odAddVariable (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, char *pName_p, uint16_t type_p, uint16_t bitLen_p, uint16_t flags_p, EC_API_SLV_CBObjRead_t cbRead_p, void *pReadCtxt_p, EC_API_SLV_CBObjWrite_t cbWrite_p, void *pWriteCtxt_p) |
| This function creates a Base Data Type Object for the Object Dictionary. More... | |
| uint32_t | EC_API_SLV_CoE_odAddArray (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, char *pName_p, uint8_t arrayLen_p, uint16_t type_p, uint16_t bitLen_p, uint16_t flags_p, EC_API_SLV_CBObjRead_t cbRead_p, void *pReadCtxt_p, EC_API_SLV_CBObjWrite_t cbWrite_p, void *pWriteCtxt_p) |
| uint32_t | EC_API_SLV_CoE_odAddRecord (EC_API_SLV_SHandle_t *pEcSlaveApi_p, uint16_t index_p, char *pName_p, EC_API_SLV_CBObjRead_t cbRead_p, void *pReadCtxt_p, EC_API_SLV_CBObjWrite_t cbWrite_p, void *pWriteCtxt_p, EC_API_SLV_SCoE_Object_t **pOutSdo_p) |
| This function creates a Record Object. More... | |
| uint32_t | EC_API_SLV_CoE_configRecordSubIndex (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, uint8_t subIndex_p, char *pName_p, uint16_t type_p, uint16_t bitLen_p, uint16_t flags_p) |
| This function creates a subIndex for the Record Object. More... | |
| uint32_t | EC_API_SLV_CoE_subIdx0WrFlag (EC_API_SLV_SHandle_t *pEcSlaveApi_p, EC_API_SLV_SCoE_Object_t *pObject_p, bool readWriteFlag_p) |
| Set write flag to SubIndex 0. More... | |