uint32_t EC_API_SLV_CoE_getObjectType | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p, |
EC_API_SLV_SCoE_Object_t * | pObject_p, | ||
uint8_t * | pType_p | ||
) |
This function returns the type flag of the object.
Returns the type flag of the object, VAR_TYPE, ARRAY_TYPE or RECORD_TYPE
[in] | pEcSlaveApi_p | The pointer to the EtherCAT API instance. |
[in] | pObject_p | pointer to the Object instance. |
[out] | pType_p | Object type flag. |