uint32_t EC_API_SLV_CoE_generateObjectDict | ( | EC_API_SLV_SHandle_t * | pEcSlaveApi_p | ) |
Generate Object Dictionary.
Configures the Application OBD based on the user configuration. Basic OBD is configured using the VendorID, Product Code and so on as well as the SyncManger PDO Assignment Objects (1C1X) and the objects defined by the user
[in] | pEcSlaveApi_p | pointer to API instance. |