AM62L FreeRTOS SDK  11.02.00

Introduction

This module contains APIs to program and use the SCMI module.

Sub Modules

 SCMI Clock IDs
 
 SCMI Clock protocol APIs
 
 SCMI DEVICE IDs
 
 SCMI base protocol APIs
 
 SCMI power domain protocol APIs
 
 SCMI transport APIs
 

Files

file  scp/scmi/v0/scmi.h
 SCMI Driver API/interface file. This is SCMI top level include for applications.
 

Data Structures

struct  SCMI_SharedMemory
 SCMI_SharedMemory - Description of a Shared memory buffer. More...
 
struct  SCMI_messageHeader
 
struct  SCMI_MessageData
 
struct  SCMI_AgentDataInfo
 
struct  SCMI_PowerDomainProtocol
 
struct  SCMI_ClockProtocol
 
struct  SCMI_Object
 
struct  SCMI_Config
 

Functions

void SCMI_init (void)
 SCMI initialization function. This function should be called before calling any driver APIs and only once. More...
 
void SCMI_deinit (void)
 This function de-initializes the SCMI module. More...
 
SCMI_Handle SCMI_open (uint32_t instanceIndex)
 This function opens a given SCMI instance. More...
 
void SCMI_close (SCMI_Handle handle)
 This function closes a given SCMI instance. More...
 
SCMI_Handle SCMI_getHandle (uint32_t driverInstanceIndex)
 This function returns the handle of an open SCMI Instance from the instance index. More...
 
int32_t SCMI_getSCMIProtocolErrorMapped (int32_t errorCode)
 This function translates the SCMI error codes to SystemP error codes. More...
 
void SCMI_getProtocolVersionLog (uint32_t instanceIndex)
 This function logs the SCMI version probed during init time. More...
 
uint32_t SCMI_getInitDriverIndex (void)
 This function returns the initialised instance index. More...
 

Typedefs

typedef void * SCMI_Handle
 A handle that is returned from a SCMI_open() call. More...
 

Macros

#define SCMI_MAX_POSSIBLE_PARENTS   (16U)
 

Macro Definition Documentation

◆ SCMI_MAX_POSSIBLE_PARENTS

#define SCMI_MAX_POSSIBLE_PARENTS   (16U)

< Maximum possible parents

Typedef Documentation

◆ SCMI_Handle

typedef void* SCMI_Handle

A handle that is returned from a SCMI_open() call.

Function Documentation

◆ SCMI_init()

void SCMI_init ( void  )

SCMI initialization function. This function should be called before calling any driver APIs and only once.

◆ SCMI_deinit()

void SCMI_deinit ( void  )

This function de-initializes the SCMI module.

◆ SCMI_open()

SCMI_Handle SCMI_open ( uint32_t  instanceIndex)

This function opens a given SCMI instance.

Parameters
instanceIndexIndex of config to use in the SCMI_Config array
Returns
A SCMI_Handle on success or a NULL on an error or if it has been opened already

◆ SCMI_close()

void SCMI_close ( SCMI_Handle  handle)

This function closes a given SCMI instance.

Precondition
SCMI_open() has to be called first
Parameters
handleSCMI_Handle returned from SCMI_open API.
See also
SCMI_open()

◆ SCMI_getHandle()

SCMI_Handle SCMI_getHandle ( uint32_t  driverInstanceIndex)

This function returns the handle of an open SCMI Instance from the instance index.

Parameters
driverInstanceIndexIndex of config to use in the SCMI_Config array
Returns
An SCMI_Handle if it has been opened already or NULL otherwise

◆ SCMI_getSCMIProtocolErrorMapped()

int32_t SCMI_getSCMIProtocolErrorMapped ( int32_t  errorCode)

This function translates the SCMI error codes to SystemP error codes.

Parameters
errorCodeError code returned from the SCMI message
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_getProtocolVersionLog()

void SCMI_getProtocolVersionLog ( uint32_t  instanceIndex)

This function logs the SCMI version probed during init time.

Parameters
instanceIndexInstance of SCMI that was opened in SCMI_open

◆ SCMI_getInitDriverIndex()

uint32_t SCMI_getInitDriverIndex ( void  )

This function returns the initialised instance index.

Returns
instanceIndex First instance which is open for SCMI driver