AM62L FreeRTOS SDK  11.02.00

Introduction

This module contains SCMI transport APIs.

Files

file  scmi_transport.h
 Header file containing scmi transport APIs.
 

Data Structures

struct  SCMI_TransportFxns
 
struct  SCMI_TransportObject
 

Functions

int32_t SCMITransport_processMessage (SCMI_Handle handle, SCMI_MessageData *message)
 Driver implementation to send a SCMI message. More...
 
int32_t SCMITransport_fetchResponse (SCMI_Handle handle, SCMI_MessageData *message)
 Driver implementation to receive a response for SCMI message. More...
 

Typedefs

typedef int32_t(* SCMI_TransportProcessMessage) (SCMI_Handle handle, SCMI_MessageData *message)
 Driver implementation to send a SCMI message. More...
 
typedef int32_t(* SCMI_TransportFetchResponse) (SCMI_Handle handle, SCMI_MessageData *message)
 Driver implementation to receive a response for SCMI message. More...
 

Typedef Documentation

◆ SCMI_TransportProcessMessage

typedef int32_t(* SCMI_TransportProcessMessage) (SCMI_Handle handle, SCMI_MessageData *message)

Driver implementation to send a SCMI message.

Typically this callback is hidden from the end application and is implemented when a new type of transport needs to be implemented.

Parameters
handle[in] SCMI driver handle
message[in] SCMI message structure
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

◆ SCMI_TransportFetchResponse

typedef int32_t(* SCMI_TransportFetchResponse) (SCMI_Handle handle, SCMI_MessageData *message)

Driver implementation to receive a response for SCMI message.

Typically this callback is hidden from the end application and is implemented when a new type of transport needs to be implemented.

Parameters
handle[in] SCMI driver handle
message[in] SCMI message structure
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

Function Documentation

◆ SCMITransport_processMessage()

int32_t SCMITransport_processMessage ( SCMI_Handle  handle,
SCMI_MessageData *  message 
)

Driver implementation to send a SCMI message.

Typically this callback is hidden from the end application and is implemented when a new type of transport needs to be implemented.

Parameters
handle[in] SCMI driver handle
message[in] SCMI message structure
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE

◆ SCMITransport_fetchResponse()

int32_t SCMITransport_fetchResponse ( SCMI_Handle  handle,
SCMI_MessageData *  message 
)

Driver implementation to receive a response for SCMI message.

Typically this callback is hidden from the end application and is implemented when a new type of transport needs to be implemented.

Parameters
handle[in] SCMI driver handle
message[in] SCMI message structure
Returns
SystemP_SUCCESS on success, else SystemP_FAILURE