AM62L FreeRTOS SDK  11.02.00
SCMI power domain protocol APIs

Introduction

This module contains SCMI power domain protocol APIs.

Files

file  scmi_power_domain.h
 Header file containing scmi power domain protocol APIs.
 

Functions

int32_t SCMI_powerDomainGetProtocolAttrs (SCMI_Handle handle, uint32_t *numPowerDomains, uint64_t *statsAddr, uint32_t *statsLen)
 API to get power domain protocol attributes using power domain SCMI protocol. More...
 
int32_t SCMI_powerDomainGetAttrs (SCMI_Handle handle, uint32_t domainId, uint32_t *attributes, uint8_t *name)
 API to get power domain attributes for a power domain Id. More...
 
int32_t SCMI_powerDomainStateSet (SCMI_Handle handle, uint32_t domainId, uint32_t flags, uint32_t pstate)
 API to set power domain to on or off state. More...
 
int32_t SCMI_powerDomainStateGet (SCMI_Handle handle, uint32_t domainId, uint32_t *pstate)
 API to get power domain state. More...
 
int32_t SCMI_powerDomainNameGet (SCMI_Handle handle, uint32_t domainId, uint8_t *name)
 API to get power domain extended name. More...
 
int32_t SCMI_powerDomainProtocolInit (SCMI_Handle handle)
 API to initialise power domain protocol. More...
 

Function Documentation

◆ SCMI_powerDomainGetProtocolAttrs()

int32_t SCMI_powerDomainGetProtocolAttrs ( SCMI_Handle  handle,
uint32_t *  numPowerDomains,
uint64_t *  statsAddr,
uint32_t *  statsLen 
)

API to get power domain protocol attributes using power domain SCMI protocol.

Parameters
handleSCMI_Handle handle returned from SCMI_open
numPowerDomainsPointer to get number of power domains
statsAddrPointer to get address for statistics shared memory
statsLenPointer to get length for statistics shared memory
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_powerDomainGetAttrs()

int32_t SCMI_powerDomainGetAttrs ( SCMI_Handle  handle,
uint32_t  domainId,
uint32_t *  attributes,
uint8_t *  name 
)

API to get power domain attributes for a power domain Id.

Parameters
handleSCMI_Handle handle returned from SCMI_open
domainIdPower domain Identifier
attributesPointer to power domain attributes
namePointer to name of power domain
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_powerDomainStateSet()

int32_t SCMI_powerDomainStateSet ( SCMI_Handle  handle,
uint32_t  domainId,
uint32_t  flags,
uint32_t  pstate 
)

API to set power domain to on or off state.

Parameters
handleSCMI_Handle handle returned from SCMI_open
domainIdPower domain Identifier
flagsParameter flags for the power domain
pstatePower state
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_powerDomainStateGet()

int32_t SCMI_powerDomainStateGet ( SCMI_Handle  handle,
uint32_t  domainId,
uint32_t *  pstate 
)

API to get power domain state.

Parameters
handleSCMI_Handle handle returned from SCMI_open
domainIdPower domain Identifier
pstatePower state pointer
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_powerDomainNameGet()

int32_t SCMI_powerDomainNameGet ( SCMI_Handle  handle,
uint32_t  domainId,
uint8_t *  name 
)

API to get power domain extended name.

Parameters
handleSCMI_Handle handle returned from SCMI_open
domainIdPower domain Identifier
namePointer to extended name
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_powerDomainProtocolInit()

int32_t SCMI_powerDomainProtocolInit ( SCMI_Handle  handle)

API to initialise power domain protocol.

Parameters
handleSCMI_Handle handle returned from SCMI_open
Returns
SystemP_SUCCESS or SystemP_FAILURE