AM62L FreeRTOS SDK  11.02.00
SCMI_AgentDataInfo Struct Reference

Data Fields

uint32_t version
 
uint32_t numAgents
 
uint32_t numProtocols
 
uint32_t implementationVersion
 
uint8_t protocols [SCMI_BASE_MAX_NUM_PROTOCOLS]
 
uint8_t vendor [SCMI_BASE_NAME_LENGTH_MAX]
 
uint8_t subVendor [SCMI_BASE_NAME_LENGTH_MAX]
 

Field Documentation

◆ version

uint32_t SCMI_AgentDataInfo::version

SCMI version

◆ numAgents

uint32_t SCMI_AgentDataInfo::numAgents

Number of agents in the system

◆ numProtocols

uint32_t SCMI_AgentDataInfo::numProtocols

Number of protocols supported by SCMI server

◆ implementationVersion

uint32_t SCMI_AgentDataInfo::implementationVersion

Implementation version

◆ protocols

uint8_t SCMI_AgentDataInfo::protocols[SCMI_BASE_MAX_NUM_PROTOCOLS]

List if protocols supported

◆ vendor

uint8_t SCMI_AgentDataInfo::vendor[SCMI_BASE_NAME_LENGTH_MAX]

Vendor name

◆ subVendor

uint8_t SCMI_AgentDataInfo::subVendor[SCMI_BASE_NAME_LENGTH_MAX]

SubVendor name