AM62L FreeRTOS SDK  11.02.00

Introduction

This module contains SCMI base protocol APIs.

Files

file  scmi_base.h
 Header file containing scmi base protocol APIs.
 

Functions

int32_t SCMI_baseGenericProtocolVersion (SCMI_Handle handle, SCMI_StandardProtocol protocolId, uint32_t *version)
 API to get generic protocol version. More...
 
int32_t SCMI_getBaseProtocolVersion (SCMI_Handle handle, uint32_t *version)
 API to get base protocol version. More...
 
int32_t SCMI_baseGetProtocolAttributes (SCMI_Handle handle, uint32_t *numAgents, uint32_t *numProtocols)
 API to get protocol attributes for base protocol. This gives number of agents and number of protocols supported in the platform. More...
 
int32_t SCMI_baseGetMessageAttributes (SCMI_Handle handle, uint32_t messageId, uint32_t *attributes)
 API to get message attributes for base protocol. More...
 
int32_t SCMI_baseDiscoverVendor (SCMI_Handle handle, uint8_t *vendor)
 API to get vendor name string. More...
 
int32_t SCMI_baseDiscoverSubVendor (SCMI_Handle handle, uint8_t *subVendor)
 API to get Sub-vendor name string. More...
 
int32_t SCMI_baseDiscoverImplementationVersion (SCMI_Handle handle, uint32_t *implVersion)
 API to get vendor implementation version. More...
 
int32_t SCMI_baseDiscoverListProtocols (SCMI_Handle handle, uint32_t *protocolCount, uint8_t *protocols)
 API to get supported protocols count and list by platform. More...
 

Function Documentation

◆ SCMI_baseGenericProtocolVersion()

int32_t SCMI_baseGenericProtocolVersion ( SCMI_Handle  handle,
SCMI_StandardProtocol  protocolId,
uint32_t *  version 
)

API to get generic protocol version.

Parameters
handleSCMI_Handle handle returned from SCMI_open
protocolIdSCMI standard protocol
versionPointer to version
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_getBaseProtocolVersion()

int32_t SCMI_getBaseProtocolVersion ( SCMI_Handle  handle,
uint32_t *  version 
)

API to get base protocol version.

Parameters
handleSCMI_Handle handle returned from SCMI_open
versionPointer to version
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseGetProtocolAttributes()

int32_t SCMI_baseGetProtocolAttributes ( SCMI_Handle  handle,
uint32_t *  numAgents,
uint32_t *  numProtocols 
)

API to get protocol attributes for base protocol. This gives number of agents and number of protocols supported in the platform.

Parameters
handleSCMI_Handle handle returned from SCMI_open
numAgentsNumber of agents
numProtocolsNumber of protocols
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseGetMessageAttributes()

int32_t SCMI_baseGetMessageAttributes ( SCMI_Handle  handle,
uint32_t  messageId,
uint32_t *  attributes 
)

API to get message attributes for base protocol.

Parameters
handleSCMI_Handle handle returned from SCMI_open
messageIdBase protocol message identifier
attributesAttributes for the message
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseDiscoverVendor()

int32_t SCMI_baseDiscoverVendor ( SCMI_Handle  handle,
uint8_t *  vendor 
)

API to get vendor name string.

Parameters
handleSCMI_Handle handle returned from SCMI_open
vendorArray to get vendor name
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseDiscoverSubVendor()

int32_t SCMI_baseDiscoverSubVendor ( SCMI_Handle  handle,
uint8_t *  subVendor 
)

API to get Sub-vendor name string.

Parameters
handleSCMI_Handle handle returned from SCMI_open
subVendorArray to get Sub-vendor name
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseDiscoverImplementationVersion()

int32_t SCMI_baseDiscoverImplementationVersion ( SCMI_Handle  handle,
uint32_t *  implVersion 
)

API to get vendor implementation version.

Parameters
handleSCMI_Handle handle returned from SCMI_open
implVersionPointer to implementation version.
Returns
SystemP_SUCCESS or SystemP_FAILURE

◆ SCMI_baseDiscoverListProtocols()

int32_t SCMI_baseDiscoverListProtocols ( SCMI_Handle  handle,
uint32_t *  protocolCount,
uint8_t *  protocols 
)

API to get supported protocols count and list by platform.

Parameters
handleSCMI_Handle handle returned from SCMI_open
protocolCountProtocols count.
protocolsArray for protocols list.
Returns
SystemP_SUCCESS or SystemP_FAILURE