This module contains APIs to program and use the GPADC module.
Files | |
file | gpadc/v0/gpadc.h |
This file contains the prototypes of the APIs present in the device abstraction layer file of GPADC. | |
Data Structures | |
struct | GPADC_ChannelConfigType |
GPADC Config Type data structure for the mode, trigger source and channel configuration for all the available external sources <0-8> More... | |
struct | GPADC_ConfigType |
GPADC Config Type data structure for the mode, trigger source and channel configuration for all the available external sources <0-8> More... | |
union | GPADC_ParamInfoType |
Configuration Parameters for GPADC in IFM mode ParamValue : Value to be programmed in one hot reg CollectSamples : Number of samples to collect @625KHz SkipSamples : Number of samples to skip @10MHz Time = Mantissa[3:0] * 2^(Exponent[6:4]) / 10M. More... | |
union | GPADC_channelsGroupSelectType |
Available <0-8> external sources/channels could be selected by using bitmap of 9 bits in LSB. Ex: 0x01F is the bitmap for conversion of <0-4> external sources. More... | |
struct | GPADC_DriverChannelConfigType |
GPADC Driver Channel configuration. More... | |
struct | GPADC_DriverObjectType |
GPADC Driver Object configuration. More... | |
struct | GPADC_EfuseTempTrimType |
The Temperature sensor trim parameters structure. More... | |
struct | GPADC_TempSensTrimType |
The Temperature sensor trim parameters structure. More... | |
struct | GPADC_TempSensMuxType |
Temperature sensors mux values. More... | |
struct | GPADC_TempSensValueType |
The Temperature sensor values structure. More... | |
struct | MSS_GPADC_RST_CTRL_REG |
GPADC Reset Control register. More... | |
struct | MSS_GPADC_CLK_DIV_VAL_REG |
GPADC Clock Divider Value register. More... | |
struct | MSS_GPADC_CLK_GATE_REG |
GPADC Clock Gate register. More... | |
struct | MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG |
Analog Mux Control Registers. More... | |
struct | MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG |
Analog Refsys spare Registers. More... | |
struct | U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG |
RCM Analog register TW Control Registers. More... | |
struct | GPADCREG_REG0 |
Register Offset 0x000. More... | |
struct | GPADCREG_REG1 |
Register1 Offset 0x004. More... | |
struct | GPADCREG_REG2 |
Register2 Offset 0x008. More... | |
union | U_GPADCREG_REG3 |
Register3 Offset 0x00C. More... | |
union | U_GPADCREG_REG4 |
Register4 Offset 0x010. More... | |
struct | GPADCREG_REG5 |
Register5 Offset 0x014. More... | |
struct | GPADCREG_REG6 |
Register6 Offset 0x018. More... | |
struct | GPADCREG_REG7 |
Register7 Offset 0x01C. More... | |
struct | GPADCREG_REG8 |
Register8 Offset 0x020. More... | |
struct | GPADCREG_REG9 |
Register9 Offset 0x024. More... | |
struct | GPADCREG_REG10 |
Register10 Offset 0x028. More... | |
struct | GPADCREG_REG11 |
Register11 Offset 0x02C. More... | |
struct | GPADCREG_REG12 |
Register12 Offset 0x030. More... | |
struct | GPADCREG_REG13 |
Register13 Offset 0x034. More... | |
struct | GPADCREG_REG14 |
Register14 Offset 0x038. More... | |
struct | GPADCREG_REG15 |
Register15 Offset 0x03C. More... | |
struct | GPADCREG_REG16 |
Register16 Offset 0x040. More... | |
struct | GPADCREG_REG17 |
Register17 Offset 0x044. More... | |
struct | GPADCREG_REG18 |
Register19 Offset 0x048. More... | |
struct | GPADCREG_REG19 |
Register20 Offset 0x04C. More... | |
struct | GPADCREG_REG20 |
Register21 Offset 0x050. More... | |
struct | GPADCREG_REG21 |
Register22 Offset 0x054. More... | |
struct | GPADCREG_REG22 |
Register22 Offset 0x058. More... | |
struct | T_GPADC_REGS |
MSS_GPADC_REG_REGS. More... | |
struct | MSS_CTRL_MSS_GPADC_MEM_INIT_REG |
GPADC Memory initialize registers. More... | |
struct | GPADC_CfgAndParamValuesType |
Configuration Parameters for GPADC LUT in IFM mode 32 bits: ConfigValue 32 bits: ParamInfo. More... | |
struct | GPADC_ResultType |
GPADC returning min, avg, max and sum. More... | |
Functions | |
void | GPADC_init (void) |
This function initializes the GPADC module. More... | |
void | GPADC_deinit (void) |
This function de-initializes the GPADC module. More... | |
int32_t | GPADC_open (GPADC_ConfigType *CfgPtr) |
Initializes the GPADC Driver with the channels configuration. More... | |
int32_t | GPADC_close (void) |
This function closes the GPADC module. More... | |
GPADC_ConvResultType | GPADC_startGroupConversion (GPADC_channelsGroupSelectType channels, uint8_t numChannels) |
Starts and triggers the multi channel ADC conversion. More... | |
GPADC_ConvResultType | GPADC_startSingleChannelConversion (GPADC_MeasExtSrcType channelID, uint16_t *gpadcValue) |
Starts and triggers the single channel conversion. Pass the channelID and result address to the driver and the result will be stored in the address passed. More... | |
int32_t | GPADC_stopConversion (void) |
Stops the GPADC conversion. More... | |
int32_t | GPADC_setupResultBuffer (uint16_t *ResBufferPtr) |
Initializes GPADC driver with the group specific result buffer start address where the conversion results will be stored. More... | |
int32_t | GPADC_readResultBuffer (uint16_t *ResBufferPtr) |
The function is used to read the result buffer from the GPADC Driver. More... | |
GPADC_StatusType | GPADC_getStatus (void) |
Gets the status of GPADC Driver HW unit. More... | |
int32_t | GPADC_readTemperature (uint8_t numAverages, uint8_t numChannels, GPADC_TempSensValueType *tempValuesPtr) |
Read the temperature sensor value. More... | |
void | GPADC_initTempMeasurement (void) |
Initialize GPADC efuse temperature parameters. More... | |
Macros | |
#define | MAX_CTM_GPADC_PARAMS (1U) |
Number of measurement parameters for GPADC in CTM mode More... | |
#define | GPADC_TIMEOUT_MAX (200000U) |
GPADC TIMEOUT Max Number of Sample collect : 256 Max Time for 256 samples collection : 256 * 16/10MHz = 409.6us Add 10 % margin : 450us Add 550us for skip samples Total timeout: 1ms Timout in terms of pmu count = 1ms/5ns = 200,000. More... | |
#define | EFUSE_TRIM_TEMPERATURE_CONST 523 |
Efuse Trime Constant Temperature. More... | |
#define | EFUSE_TRIM_TEMPERATURE_DIV_CONST 10 |
Efuse Trime Constant Temperature Divider. More... | |
#define | ZERO_PT_TRIM_FIXED_TRIM_TEMP 110 |
Zero point TRIM Fixed Temperature. More... | |
#define | ZERO_PT_TRIM_FIXED_DIG_TEMP_SENSOR_TRIM_30C 305U |
Zero point TRIM Fixed Digital Temperature. More... | |
#define | ZERO 0 |
Zero Value. More... | |
#define | ZERO_PT_TRIM_FIXED_SLOPE -1.05 |
Zero point TRIM Fixed Slope. More... | |
#define | ONE_PT_TRIM_FIXED_SLOPE -1.05 |
One point TRIM Fixed Slope. More... | |
#define | EFUSE1_ROW_14_FUSEROM_VER_START_BIT 20U |
Efuse Version Start Bit. More... | |
#define | EFUSE1_ROW_14_FUSEROM_VER_STOP_BIT 24U |
Efuse Version Stop Bit. More... | |
#define | EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_START_BIT 15U |
Efuse Trim Temperature 30C Start Bit. More... | |
#define | EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_STOP_BIT 25U |
Efuse Trim Temperature 30C Stop Bit. More... | |
#define | EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_START_BIT 0U |
Efuse Trim Temperature 125C Start Bit. More... | |
#define | EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_STOP_BIT 10U |
Efuse Trim Temperature 125C Stop Bit. More... | |
#define | EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_START_BIT 5U |
Efuse Digital DSP Temperature 30C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_STOP_BIT 14U |
Efuse Digital DSP Temperature 30C Sensor Stop Bit. More... | |
#define | EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_START_BIT 15U |
Efuse Digital HWA Temperature 30C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_STOP_BIT 24U |
Efuse Digital HWA Temperature 30C Sensor Stop Bit. More... | |
#define | EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_START_BIT 0U |
Efuse Digital HSM Temperature 30C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_STOP_BIT 9U |
Efuse Digital HSM Temperature 30C Sensor Stop Bit. More... | |
#define | EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_START_BIT 5U |
Efuse Digital DSP Temperature 125C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_STOP_BIT 14U |
Efuse Digital DSP Temperature 125C Sensor Stop Bit. More... | |
#define | EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_START_BIT 15U |
Efuse Digital HWA Temperature 125C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_STOP_BIT 24U |
Efuse Digital HWA Temperature 125C Sensor Stop Bit. More... | |
#define | EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_START_BIT 0U |
Efuse Digital HSM Temperature 125C Sensor Start Bit. More... | |
#define | EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_STOP_BIT 9U |
Efuse Digital HSM Temperature 125C Sensor Stop Bit. More... | |
#define | GPADC_REGS_PTR ((T_GPADC_REGS*)CSL_MSS_GPADC_REG_U_BASE) |
GPADC Register Base Address. More... | |
#define | GPADCPKTRAM_REGS_PTR ((T_GPADCPKTRAM_REGS*)CSL_MSS_GPADC_PKT_RAM_U_BASE) |
GPADCPKTRAM Register Base Address. More... | |
#define | GPADCOUT_RAM_PTR ((T_GPADCOUT_RAM*)CSL_MSS_GPADC_DATA_RAM_U_BASE) |
GPADCPKTRAM Data RAM Base Address. More... | |
#define | MSS_GPADC_RST_CTRL_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_RST_CTRL) |
GPADC Reset Control Address. More... | |
#define | MSS_GPADC_RST_CTRL_PTR ((MSS_GPADC_RST_CTRL_REG*)MSS_GPADC_RST_CTRL_ADDR) |
GPADC Reset Control Pointer. More... | |
#define | MSS_GPADC_CLK_DIV_VAL_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_DIV_VAL) |
GPADC Clock Divider value Address. More... | |
#define | MSS_GPADC_CLK_DIV_VAL_PTR ((MSS_GPADC_CLK_DIV_VAL_REG*)MSS_GPADC_CLK_DIV_VAL_ADDR) |
GPADC Clock Divider value pointer. More... | |
#define | MSS_GPADC_CLK_GATE_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_GATE) |
GPADC Clock Gate Address. More... | |
#define | MSS_GPADC_CLK_GATE_PTR ((MSS_GPADC_CLK_GATE_REG*)MSS_GPADC_CLK_GATE_ADDR) |
GPADC Clock Gate Pointer. More... | |
#define | MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV) |
RCM TW Analog TMUX Contol Address. More... | |
#define | MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_PTR ((MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR) |
RCM TW Analog TMUX Contol Poniter. More... | |
#define | MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV) |
RCM Analog Refsys Spare register Address. More... | |
#define | MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_PTR ((MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR) |
RCM Analog Refsys Spare register Pointer. More... | |
#define | MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV) |
RCM Analog TW Control register Address. More... | |
#define | MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_PTR ((U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR) |
RCM Analog TW Control register pointer. More... | |
#define | MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_MSS_GPADC_MEM_INIT) |
GPADC Memomory Init Address. More... | |
#define | MSS_CTRL_MSS_GPADC_MEM_INIT_PTR ((MSS_CTRL_MSS_GPADC_MEM_INIT_REG*)MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR) |
GPADC Memomory Init poniter. More... | |
#define | REG_STRUCT_SWRITE(w_hwRegStruct, w_regVal, w_regWrSts) |
Register Structure member write and compare macro. More... | |
#define | REG32_SCOMPARE(w_hwVal, w_swVal, w_regWrSts) |
32 bit register compare macro More... | |
#define | REG_STRUCT_SCLEAR(w_hwRegStruct, w_regVal, w_regWrSts) |
Register Structure member CLEAR and compare macro. More... | |
GPADC Macros | |
#define | GPADC_DISABLE (0U) |
Disable GPADC. More... | |
#define | GPADC_ENABLE (1U) |
Enable GPADC. More... | |
#define | GPADC_ASSERT_RESET (1U) |
Reset GPADC. More... | |
#define | GPADC_DEASSERT_RESET (0U) |
Release GPADC Reset. More... | |
#define | GPADC_FSM_ASSERT_RESET (0x7U) |
Reset GPADC for digital FSM. More... | |
#define | GPADC_FSM_DEASSERT_RESET (0U) |
Release Reset GPADC for digital FSM. More... | |
GPADC Modes | |
#define | GPADC_MODE_DISABLE (0U) |
GPADC Disable mode. More... | |
#define | GPADC_MODE_IFM (1U) |
GPADC IFM Operation mode. More... | |
#define | GPADC_MODE_CTM (2U) |
GPADC CTM Operation mode. More... | |
Instruction RAM Index | |
#define | GPADC_MON_INSTR_RAM_ST_IND (224U) |
GPADC RAM Instruction Index. More... | |
#define | GPADC_MAX_MON_INSTR_RAM (32U) |
GPADC MAX RAM Instruction. More... | |
#define GPADC_DISABLE (0U) |
Disable GPADC.
#define GPADC_ENABLE (1U) |
Enable GPADC.
#define GPADC_ASSERT_RESET (1U) |
Reset GPADC.
#define GPADC_DEASSERT_RESET (0U) |
Release GPADC Reset.
#define GPADC_FSM_ASSERT_RESET (0x7U) |
Reset GPADC for digital FSM.
#define GPADC_FSM_DEASSERT_RESET (0U) |
Release Reset GPADC for digital FSM.
#define GPADC_MODE_DISABLE (0U) |
GPADC Disable mode.
#define GPADC_MODE_IFM (1U) |
GPADC IFM Operation mode.
#define GPADC_MODE_CTM (2U) |
GPADC CTM Operation mode.
#define GPADC_MON_INSTR_RAM_ST_IND (224U) |
GPADC RAM Instruction Index.
#define GPADC_MAX_MON_INSTR_RAM (32U) |
GPADC MAX RAM Instruction.
#define MAX_CTM_GPADC_PARAMS (1U) |
Number of measurement parameters for GPADC in CTM mode
#define GPADC_TIMEOUT_MAX (200000U) |
GPADC TIMEOUT Max Number of Sample collect : 256 Max Time for 256 samples collection : 256 * 16/10MHz = 409.6us Add 10 % margin : 450us Add 550us for skip samples Total timeout: 1ms Timout in terms of pmu count = 1ms/5ns = 200,000.
#define EFUSE_TRIM_TEMPERATURE_CONST 523 |
Efuse Trime Constant Temperature.
#define EFUSE_TRIM_TEMPERATURE_DIV_CONST 10 |
Efuse Trime Constant Temperature Divider.
#define ZERO_PT_TRIM_FIXED_TRIM_TEMP 110 |
Zero point TRIM Fixed Temperature.
#define ZERO_PT_TRIM_FIXED_DIG_TEMP_SENSOR_TRIM_30C 305U |
Zero point TRIM Fixed Digital Temperature.
#define ZERO 0 |
Zero Value.
#define ZERO_PT_TRIM_FIXED_SLOPE -1.05 |
Zero point TRIM Fixed Slope.
#define ONE_PT_TRIM_FIXED_SLOPE -1.05 |
One point TRIM Fixed Slope.
#define EFUSE1_ROW_14_FUSEROM_VER_START_BIT 20U |
Efuse Version Start Bit.
#define EFUSE1_ROW_14_FUSEROM_VER_STOP_BIT 24U |
Efuse Version Stop Bit.
#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_START_BIT 15U |
Efuse Trim Temperature 30C Start Bit.
#define EFUSE1_ROW_36_TRIM_TEMPERATURE_30C_STOP_BIT 25U |
Efuse Trim Temperature 30C Stop Bit.
#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_START_BIT 0U |
Efuse Trim Temperature 125C Start Bit.
#define EFUSE1_ROW_33_TRIM_TEMPERATURE_125C_STOP_BIT 10U |
Efuse Trim Temperature 125C Stop Bit.
#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_START_BIT 5U |
Efuse Digital DSP Temperature 30C Sensor Start Bit.
#define EFUSE1_ROW_37_DIG_DSP_TEMP_SENSOR_TRIM0_30C_STOP_BIT 14U |
Efuse Digital DSP Temperature 30C Sensor Stop Bit.
#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_START_BIT 15U |
Efuse Digital HWA Temperature 30C Sensor Start Bit.
#define EFUSE1_ROW_37_DIG_HWA_TEMP_SENSOR_TRIM1_30C_STOP_BIT 24U |
Efuse Digital HWA Temperature 30C Sensor Stop Bit.
#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_START_BIT 0U |
Efuse Digital HSM Temperature 30C Sensor Start Bit.
#define EFUSE1_ROW_38_DIG_HSM_TEMP_SENSOR_TRIM2_30C_STOP_BIT 9U |
Efuse Digital HSM Temperature 30C Sensor Stop Bit.
#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_START_BIT 5U |
Efuse Digital DSP Temperature 125C Sensor Start Bit.
#define EFUSE1_ROW_34_DIG_DSP_TEMP_SENSOR_TRIM0_125C_STOP_BIT 14U |
Efuse Digital DSP Temperature 125C Sensor Stop Bit.
#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_START_BIT 15U |
Efuse Digital HWA Temperature 125C Sensor Start Bit.
#define EFUSE1_ROW_34_DIG_HWA_TEMP_SENSOR_TRIM1_125C_STOP_BIT 24U |
Efuse Digital HWA Temperature 125C Sensor Stop Bit.
#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_START_BIT 0U |
Efuse Digital HSM Temperature 125C Sensor Start Bit.
#define EFUSE1_ROW_35_DIG_HSM_TEMP_SENSOR_TRIM2_125C_STOP_BIT 9U |
Efuse Digital HSM Temperature 125C Sensor Stop Bit.
#define GPADC_REGS_PTR ((T_GPADC_REGS*)CSL_MSS_GPADC_REG_U_BASE) |
GPADC Register Base Address.
#define GPADCPKTRAM_REGS_PTR ((T_GPADCPKTRAM_REGS*)CSL_MSS_GPADC_PKT_RAM_U_BASE) |
GPADCPKTRAM Register Base Address.
#define GPADCOUT_RAM_PTR ((T_GPADCOUT_RAM*)CSL_MSS_GPADC_DATA_RAM_U_BASE) |
GPADCPKTRAM Data RAM Base Address.
#define MSS_GPADC_RST_CTRL_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_RST_CTRL) |
GPADC Reset Control Address.
#define MSS_GPADC_RST_CTRL_PTR ((MSS_GPADC_RST_CTRL_REG*)MSS_GPADC_RST_CTRL_ADDR) |
GPADC Reset Control Pointer.
#define MSS_GPADC_CLK_DIV_VAL_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_DIV_VAL) |
GPADC Clock Divider value Address.
#define MSS_GPADC_CLK_DIV_VAL_PTR ((MSS_GPADC_CLK_DIV_VAL_REG*)MSS_GPADC_CLK_DIV_VAL_ADDR) |
GPADC Clock Divider value pointer.
#define MSS_GPADC_CLK_GATE_ADDR (CSL_MSS_RCM_U_BASE + CSL_MSS_RCM_MSS_GPADC_CLK_GATE) |
GPADC Clock Gate Address.
#define MSS_GPADC_CLK_GATE_PTR ((MSS_GPADC_CLK_GATE_REG*)MSS_GPADC_CLK_GATE_ADDR) |
GPADC Clock Gate Pointer.
#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV) |
RCM TW Analog TMUX Contol Address.
#define MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_PTR ((MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_ANA_TMUX_CTRL_LOWV_ADDR) |
RCM TW Analog TMUX Contol Poniter.
#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV) |
RCM Analog Refsys Spare register Address.
#define MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_PTR ((MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_REFSYS_SPARE_REG_LOWV_ADDR) |
RCM Analog Refsys Spare register Pointer.
#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR (CSL_MSS_TOPRCM_U_BASE + CSL_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV) |
RCM Analog TW Control register Address.
#define MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_PTR ((U_MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_REG*)MSS_TOPRCM_ANA_REG_TW_CTRL_REG_LOWV_ADDR) |
RCM Analog TW Control register pointer.
#define MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR (CSL_MSS_CTRL_U_BASE + CSL_MSS_CTRL_MSS_GPADC_MEM_INIT) |
GPADC Memomory Init Address.
#define MSS_CTRL_MSS_GPADC_MEM_INIT_PTR ((MSS_CTRL_MSS_GPADC_MEM_INIT_REG*)MSS_CTRL_MSS_GPADC_MEM_INIT_ADDR) |
GPADC Memomory Init poniter.
#define REG_STRUCT_SWRITE | ( | w_hwRegStruct, | |
w_regVal, | |||
w_regWrSts | |||
) |
Register Structure member write and compare macro.
#define REG32_SCOMPARE | ( | w_hwVal, | |
w_swVal, | |||
w_regWrSts | |||
) |
32 bit register compare macro
#define REG_STRUCT_SCLEAR | ( | w_hwRegStruct, | |
w_regVal, | |||
w_regWrSts | |||
) |
Register Structure member CLEAR and compare macro.
enum GPADC_CtmTrigSrcType |
Enumeration which describes the trigger sources for GPADC CTM mode conversion.
Note: Only GPADC_TRIGG_SRC_SW is supported in the AM273x GPADC Driver. GPADC_TRIG_SRC_MMR_Based_SW_Trigger will be default trigger if CTM mode is configured
Enumeration which lists the conversion modes supported for AM273x GPADC conversion.
Note: Only GPADC_ONESHOT_CONV_MODE is supported in the AM273x GPADC Driver.
Enumerator | |
---|---|
GPADC_ONESHOT_CONV_MODE | 0x00 - IFM - Inter Frame Monitoring/One Shot Conversion Mode |
GPADC_CONTINUOUS_CONV_MODE | 0x01 - CTM - Continuous Time Monitoring/ Continuous conversion Mode |
enum GPADC_MeasExtSrcType |
Enumeration which describes the external sources available for GPADC conversion.
enum GPADC_ConvResultType |
enum GPADC_StatusType |
Current status of the conversion of the requested GPADC HW unit.
void GPADC_init | ( | void | ) |
This function initializes the GPADC module.
void GPADC_deinit | ( | void | ) |
This function de-initializes the GPADC module.
int32_t GPADC_open | ( | GPADC_ConfigType * | CfgPtr | ) |
Initializes the GPADC Driver with the channels configuration.
[in] | CfgPtr | Pointer to the GPADC configuration |
int32_t GPADC_close | ( | void | ) |
This function closes the GPADC module.
GPADC_ConvResultType GPADC_startGroupConversion | ( | GPADC_channelsGroupSelectType | channels, |
uint8_t | numChannels | ||
) |
Starts and triggers the multi channel ADC conversion.
Pass the channel selection bitmap for group conversion to the GPADC Driver and check the result buffer passed to the driver using GPADC_SetupResultBuffer() for conversion results of all configured channels. Conversion happens based on the parameters provided through GPADC_Init() for GPADC HW unit and each channel config like sampling parameters, buffered/ unbuffered. GPADC_Init() should be done before starting conversion Channel bitmap selected shouldn't be zero Result buffer should be setup before starting conversion using GPADC_SetupResultBuffer().
[in] | channels | Channel selection bitmap to start conversion together |
[in] | numChannels | number of channels |
GPADC_ConvResultType GPADC_startSingleChannelConversion | ( | GPADC_MeasExtSrcType | channelID, |
uint16_t * | gpadcValue | ||
) |
Starts and triggers the single channel conversion. Pass the channelID and result address to the driver and the result will be stored in the address passed.
[in] | channelID | Channel index from <0-8> available external sources |
[out] | gpadcValue | Pointer to the address where the result shall be stored. |
int32_t GPADC_stopConversion | ( | void | ) |
Stops the GPADC conversion.
This API should not be called before initialization.\n This API should not be called before starting group/single channel start conversion\n To be used when the mode of conversion is chosen as GPADC_CONTINUOUS_CONV_MODE.
return If stop conversion is successful returns SystemP_SUCCESS, else error on failure
int32_t GPADC_setupResultBuffer | ( | uint16_t * | ResBufferPtr | ) |
Initializes GPADC driver with the group specific result buffer start address where the conversion results will be stored.
The application has to ensure that the application buffer, where ResBufferPtr points to, can hold all the conversion results of the specified group. The initialization with GPADC_SetupResultBuffer is required after GPADC_Init(), before a group conversion can be started.
[in] | ResBufferPtr |
int32_t GPADC_readResultBuffer | ( | uint16_t * | ResBufferPtr | ) |
The function is used to read the result buffer from the GPADC Driver.
Reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the ResBufferPtr address.
[out] | ResBufferPtr |
GPADC_StatusType GPADC_getStatus | ( | void | ) |
Gets the status of GPADC Driver HW unit.
int32_t GPADC_readTemperature | ( | uint8_t | numAverages, |
uint8_t | numChannels, | ||
GPADC_TempSensValueType * | tempValuesPtr | ||
) |
Read the temperature sensor value.
[in] | numAverages | number of average samples |
[in] | numChannels | number of channels |
[out] | tempValuesPtr | Pointer to store the temperature values |
void GPADC_initTempMeasurement | ( | void | ) |
Initialize GPADC efuse temperature parameters.