ti | |
  ipc | |
   GateMP.h | Multiple processor gate that provides local and remote context protection |
   HeapBufMP.h | Multi-processor fixed-size buffer heap implementation |
   HeapMemMP.h | Multi-processor variable size buffer heap implementation |
   Ipc.h | Ipc Manager |
   ListMP.h | Multiple processor shared memory list |
   MessageQ.h | MessageQ Manager |
   MultiProc.h | Processor ID Manager |
   NameServer.h | NameServer Manager |
   Notify.h | Notification manager for IPC |
   SharedRegion.h | Shared memory manager and address translator |
  syslink | |
   utils | |
    Cache.h | Defines Cache API interface |
    Cfg.h | Configuration Helper Utilities |
    Dev.h | Defines Dev API interface |
    Gate.h | Critical section support |
    GateMonitor.h | Header file for Gate based on Monitor |
    GateMutex.h | Gate based on Mutex |
    GateProcess.h | Process level gate |
    GateSem.h | Header file for Gate based on Semaphore |
    GateSpinlock.h | Gate based on Spinlock |
    IGateProvider.h | Interface implemented by all gate providers |
    IHeap.h | Defines Heap based memory allocator |
    IpcMemMgr.h | IPC Memory Manager |
    List.h | Creates a doubly linked list. It works as utils for other modules |
    Memory.h | Memory manager interface definitions |
    MemoryDefs.h | Definitions for Memory module |
    MemoryOS.h | Memory abstraction APIs for local memory allocation |
    OsalPrint.h | Kernel utils Print interface definitions |
    OsalSemaphore.h | Kernel utils Semaphore interface definitions |
    ResTrack.h | Resource Tracker utility module |
    String.h | Defines for String manipulation library |
    SyslinkMemMgr.h | Header file implementing Memory manager. It is a wrapper implementation to support Shared memory allocation using heap address translations using shared region or Tiler buffer allocation using tiler buffer manager and address translations |
    Trace.h | Kernel Trace enabling/disabling/application interface |
   FrameQ.h | Defines for interfaces for FrameQ module. (Deprecated) |
   FrameQ_ShMem.h | Header file for FrameQ on SharedMemory interface. (Deprecated) |
   FrameQBufMgr.h | Defines for interfaces for FrameQBufMgr module. (Deprecated) |
   FrameQBufMgr_ShMem.h | Header file for FrameQBufMgr ShMem. (Deprecated) |
   FrameQBufMgrDefs.h | Defines configurable elements for FrameQBufMgr module |
   FrameQDefs.h | Defines configurable elements for FrameQ module. (Deprecated) |
   IpcHost.h | This file contains APIs and defines that are used by applications only on the host-side of the device |
   ProcMgr.h | The Processor Manager on a master processor provides control functionality for a slave device |
   RingIO.h | RingIO module |
   RingIOShm.h | RingIOShm shared memory based physical transport for communication with another client |
   Std.h | This will have definitions of standard data types for platform abstraction |
   SysLink.h | This module contains common definitions, types, structures and functions used by SysLink |