105 #ifndef HEAP_H_0x7033
106 #define HEAP_H_0x7033
114 #if defined (__cplusplus)
200 static inline Ptr IHeap_alloc (IHeap_Handle handle,
207 buffer = ((
IHeap_Object *) handle)->alloc (handle, size, align);
221 static inline Void IHeap_free (IHeap_Handle handle,
238 static inline Void IHeap_getStats (IHeap_Handle handle,
256 static inline Bool IHeap_isBlocking (IHeap_Handle handle)
260 isBlocking = ((
IHeap_Object *) handle)->isBlocking (handle);
276 static inline Ptr IHeap_getKnlHandle (IHeap_Handle handle)
280 knlHandle = ((
IHeap_Object *) handle)->getKnlHandle (handle);
285 #if defined (__cplusplus)