Files |
| file | FrameQ.h [code] |
| | Defines for interfaces for FrameQ module. (Deprecated)
|
| file | FrameQ_ShMem.h [code] |
| | Header file for FrameQ on SharedMemory interface. (Deprecated)
|
| file | FrameQBufMgr.h [code] |
| | Defines for interfaces for FrameQBufMgr module. (Deprecated)
|
| file | FrameQBufMgr_ShMem.h [code] |
| | Header file for FrameQBufMgr ShMem. (Deprecated)
|
| file | FrameQBufMgrDefs.h [code] |
| | Defines configurable elements for FrameQBufMgr module.
|
| file | FrameQDefs.h [code] |
| | Defines configurable elements for FrameQ module. (Deprecated)
|
| file | IpcHost.h [code] |
| | This file contains APIs and defines that are used by applications only on the host-side of the device.
|
| file | ProcMgr.h [code] |
| | The Processor Manager on a master processor provides control functionality for a slave device.
|
| file | RingIO.h [code] |
| | RingIO module.
|
| file | RingIOShm.h [code] |
| | RingIOShm shared memory based physical transport for communication with another client.
|
| file | Std.h [code] |
| | This will have definitions of standard data types for platform abstraction.
|
| file | SysLink.h [code] |
| | This module contains common definitions, types, structures and functions used by SysLink.
|