![]() |
![]() |
SysLink API Reference
2.21.03.11
|
Kernel utils Print interface definitions.
This will have the definitions for kernel side printf statements and also details of variable printfs supported in existing implementation.
Go to the source code of this file.
Macros | |
#define | OSALPRINT_MODULEID (UInt16) 0xC431 |
Module ID for OsalPrint OSAL module. |
Functions | |
Void | Osal_printf (char *format,...) |
#define OSALPRINT_MODULEID (UInt16) 0xC431 |
Module ID for OsalPrint OSAL module.
Void Osal_printf | ( | char * | format, |
... | |||
) |