5.10. WDG Module

5.10.1. Acronyms and Definitions

Abbreviation/Term

Explanation

AUTOSAR

Automotive Open System Architecture

RTE

Runtime Environment

BSW

Basic Software

MCU

Micro-Controller Unit

MCAL

Micro-Controller Abstraction Layer

API

Application Programming Interface

DET

Default Error Tracer

DEM

Diagnostics Event Manager

HW

Hardware

SW

Software

I/O

Input/Output

WDG

Watchdog

5.10.2. Introduction

The Wdg module provides services for initialization, changing the operation mode and setting the trigger condition (timeout).

WDG MCAL AUTOSAR

Fig. 5.53 WDG MCAL AUTOSAR

This document details AUTOSAR BSW WDG module implementation

Supported AUTOSAR Release

: 4.3.1

Supported Configuration Variants

: Pre-Compile, Link-Time & Post Build

Vendor ID

: WDG_VENDOR_ID (44)

Module ID

: WDG_MODULE_ID (102)

5.10.3. Functional Overview

The watchdog module generates an output pulse 512 watchdog-clocks (WDCLKs) wide whenever the 8-bit watchdog up counter has reached the maximum value. The watchdog clock source is INTOSC1 which is 10 MHz clock. Software must periodically write a 0x55 + 0xAA sequence into the watchdog key register to reset the watchdog counter. The counter can also be disabled.

WDG MCAL AUTOSAR

Fig. 5.54 WDG TIMER MODULE

5.10.4. Hardware Features

5.10.4.1. Hardware Features supported

The main features includes Servicing the Watchdog Timer, Minimum Window Check, Watchdog Reset or Watchdog Interrupt Mode and Watchdog Operation in Low-Power Modes. Details are explained in below sections.

5.10.4.1.1. Servicing the Watchdog Timer

The watchdog counter (WDCNTR) is reset when the proper sequence is written to the WDKEY register before the 8-bit watchdog counter overflows. The WDCNTR is reset-enabled when a value of 0x55 is written to the WDKEY. When the next value written to the WDKEY register is 0xAA, then the WDCNTR is reset. Any value written to the WDKEY other than 0x55 or 0xAA causes no action. Any sequence of 0x55 and 0xAA values can be written to the WDKEY without causing a system reset; only a write of 0x55 followed by a write of 0xAA to the WDKEY resets the WDCNTR.

5.10.4.1.2. Minimum Window Check

To complement the timeout mechanism, the watchdog also contains an optional “windowing” feature that requires a minimum delay between counter resets. To set the window minimum, write the desired minimum watchdog count to the WDWCR register. This value takes effect after the next WDKEY sequence. From then on, any attempt to service the watchdog when WDCNTR is less than WDWCR triggers a watchdog interrupt or reset. When WDCNTR is greater than or equal to WDWCR, the watchdog can be serviced normally.

5.10.4.1.3. Watchdog Reset or Watchdog Interrupt Mode

The watchdog can be configured in the SCSR register to either reset the device (WDRST) or assert an interrupt (WDINT), if the watchdog counter reaches the maximum value.

Reset mode: If the watchdog is configured to reset the device, then the WDRST signal pulls the device reset (XRS) pin low for 512 OSCCLK cycles when the watchdog counter reaches the maximum value.

Interrupt mode: When the watchdog counter expires, the watchdog asserts an interrupt by driving the WDINT signal low for 512 OSCCLK cycles. WDINT is mapped to the PIPE module to assert appropriate CPU interrupt line as configured.

5.10.4.1.4. Watchdog Operation in Low-Power Modes

IDLE mode: In IDLE mode, the watchdog interrupt (WDINT) signal can generate an interrupt to the CPU to take the CPU out of IDLE mode.

STANDBY mode:In STANDBY mode, clocks to the peripherals are turned off based on LPMCR, PCLKCRx and STANDBYEN registers. The CPU clock is gated when entering STANDBY mode based on LPMCR.LPM configuration but the watchdog remains functional since the module runs off the internal oscillator clock (INTOSC1). The WDINTsignal is applied to the Low Power Modes (LPM) block, so that the LPM block can be used to wake the CPU from STANDBY low-power mode.

5.10.4.2. Not supported Features

None

5.10.4.3. Non compliance

Below AUTOSAR design requirements are not supported for Wdg Driver:

SWS_Wdg_00136 : The function SetTriggerCondition shall reset the watchdog timeout counter according to the timeout value passed.

Rejection Reason : When user request non zero timeout value in Wdg_SetTriggerCondition API, it will be ignored. Due to hardware limitation, it is not possible to set the hardware watchdog counter value based on user provided timeout. Timeout value will always remain as per statically configured slow and fast mode timeout values.

SWS_Wdg_00034 : General design rule: configure Start address of trigger routine

Rejection Reason : Trigger routine information is not provided by hardware and not needed by the system.

SWS_Wdg_00076 : External Watchdog Driver

Rejection Reason : Internal watchdog is only supported, external watchdog support is not part of the current implementation.

For more details, Refer AUTOSAR_SWS_WdgDriver

5.10.5. Source files

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Can
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂hw_include
┃ ┣ 📂Mcal_Lib
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┃ ┗ 📂Wdg
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Wdg_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┗ 📜Wdg.h : Contains the API declarations of the Wdg driver to be used by upper layers.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Wdg_Priv.c : Contains Functions that support the API for Wdg driver
┃ ┃ ┃ ┗ 📜Wdg.c : Contains the implementation of the API for Wdg driver.
┃ ┃ ┗ 📜CMakeLists.txt
┣ 📂examples
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Wdg Header File Structure

Fig. 5.55 Wdg Header File Structure

5.10.6. Module requirements

5.10.6.1. Memory Mapping

The driver follows the AUTOSAR memory mapping strategy. All memory sections should be stored in memory as per AUTOSAR specifications, considering initialization policy, alignment requirements, safety classification, and core scope where applicable.

Reference memory map files can be found at:

{MCAL_INSTALL_PATH}\drivers\BSW_Stubs\MemMap\include

The memory sections are organized according to AUTOSAR specifications to ensure proper placement of code and data in different memory regions based on their usage and access patterns.

5.10.6.2. Scheduling

None

5.10.6.3. Error handling

5.10.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

5.10.6.3.2. Extended Production Error Reporting

Extended production errors are reported to the DEM using the service Dem_SetEventStatus(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

5.10.6.4. Error codes

Type of Error

Related Error code

Value (Hex)

API service used in wrong context:

WDG_E_DRIVER_STATE

0x10

API service called with wrong / inconsistent parameter(s):

WDG_E_PARAM_MODE

0x11

API service called with wrong / inconsistent parameter(s):

WDG_E_PARAM_CONFIG

0x12

The passed timeout value is higher than the maximum timeout value:

WDG_E_PARAM_TIMEOUT

0x13

API is called with wrong pointer value

WDG_E_PARAM_POINTER

0x14

Invalid configuration set selection

WDG_E_INIT_FAILED

0x15

5.10.7. Safety Mechanism

TI Diagnostic Unique Identifier

Summary

Description

CLK6

Internal Watchdog

Error detection are notified to user and Reported to DET & DEM

Note

More details of Safety Mechanisms can be found in Safety Manual.

5.10.8. Used resources

5.10.8.1. Interrupt Handling

There are no Interrupts in Wdg. The Watchdog module does not use any hardware interrupts; it operates by triggering a system reset upon timeout expiry.

5.10.8.2. Instance support

CPU instances

supported

CPU 1

YES

CPU 2

NO

CPU 3

NO

5.10.8.3. Hardware-Software Mapping

Below image shows Wdg driver Hardware-Software mapping. For more information related to HW/SW mapping, refer the F29 Reference Manual.

Wdg HW/SW Mapping

Fig. 5.56 Wdg HW/SW Mapping

5.10.9. Integration description

5.10.9.1. Dependent modules

5.10.9.1.1. DET

This implementation depends on the DET in order to report development errors. The detection of development errors is configurable (ON / OFF), The switch WDG_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

5.10.9.1.2. DEM

This implementation depends on the DEM in order to report Extended production errors and can be turned OFF. The switch WDG_DEM_ENABLE will activate or deactivate the detection of all extended production errors.

5.10.9.2. Multi-core and Resource allocator

The WDG module is not managed by the Resource Allocator. The Watchdog timer on F29H85x is a system-level peripheral that is exclusively controlled by CPU1 and cannot be allocated to other cores. Because the Watchdog is not a shareable, multi-core resource, it is not represented in the Resource Allocator configuration. No Resource Allocator instance allocation is needed for the WDG module.

5.10.10. Configuration

The Wdg Driver implementation supports multiple configuration variants, namely Wdg Post-Build config and Pre-Compile config. The driver expects generated Wdg_Cfg.h to be present as input file. The associated Wdg driver configuration generated source files are Wdg_Cfg.c or Wdg_Lcfg.c or Wdg_PBcfg.c

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

5.10.10.1. Configuration Parameters

5.10.10.1.1. WdgDemEventParameterRefs

Item

Name

WdgDemEventParameterRefs

Description

Container for the references to DemEventParameter elements which shall be invoked using the API Dem_SetEventStatus in case the corresponding error occurs. The EventId is taken from the referenced DemEventParameter’s DemEventId symbolic value. The standardized errors are provided in this container and can be extended by vendor-specific error references.

Post-build-variant-multiplicity

false

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.10.10.1.2. WdgGeneral

All general parameters of the watchdog driver are collected here.

5.10.10.1.2.1. WdgDevErrorDetect

Item

Name

WdgDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.10.10.1.2.2. WdgDisableAllowed

Item

Name

WdgDisableAllowed

Description

Compile switch to allow / forbid disabling the watchdog driver during runtime.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.10.10.1.2.3. WdgIndex

Item

Name

WdgIndex

Description

Specifies the InstanceId of this module instance. If only one instance is present it shall have the Id 0.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.10.10.1.2.4. WdgInitialTimeout

Item

Name

WdgInitialTimeout

Description

This is read only parameter just to display the initial timeout value based on the default mode. The initial timeout (sec) for the trigger condition to be initialized during Init function. It shall be not larger than WdgMaxTimeout. (click on auto calculate before generating)

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0.1

Max-value

0.1

Min-value

0.0

5.10.10.1.2.5. WdgMaxTimeout

Item

Name

WdgMaxTimeout

Description

This is read only parameter just to display the maximum timeout value based on the default mode. The maximum timeout (sec) to which the watchdog trigger condition can be initialized.Set the fast/slow mode timeout settings. (click on auto calculate before generating)

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

6.684672000000001

Max-value

7.0

Min-value

0.0

5.10.10.1.2.6. WdgRunArea

Item

Name

WdgRunArea

Description

Represents the watchdog driver execution area is either from ROM(Flash) or RAM as required with the particular microcontroller.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

RAM

Range

RAM
ROM

5.10.10.1.2.7. WdgTriggerLocation

Item

Name

WdgTriggerLocation

Description

Location (memory address) of the watchdog trigger routine.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.10.10.1.2.8. WdgVersionInfoApi

Item

Name

WdgVersionInfoApi

Description

Compile switch to enable / disable the version information API

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

true

Refer AUTOSAR_SWS_WDGDriver section: 10 Configuration specification for configuration parameters details

5.10.10.2. Steps To Configure Wdg Module

  1. Open EB Tresos configurator tool, load Wdg and Dem modules. Select the Config Variant ( Precompile/Post-Build/Link-Time)

  2. Open DEM module plugin and register DEM event “WDG_E_DISABLE_REJECTED” & “WDG_E_MODE_FAILED” to report extended production errors

  3. Open WDG module plugin and make sure that required parameters and mode settings are configured correctly

  4. Make sure that fastmode, slowmode configuration settings are provided

  5. Save the configuration and generate the configuration.

5.10.11. Examples

The example application demonstrates use of Wdg module, the list below identifies key steps performed the example.

5.10.11.1. Wdg_Example_Service

5.10.11.1.1. Overview of Wdg_Example_Service

  • Wdg_Example_Service

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes pins as GPIO Outputs and GPIO Inputs using Port_Init()

    • Verify the wdg servicing without expiry on configured timeouts

5.10.11.1.2. Setup required to run Wdg_Example_Service

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.10.11.1.3. How to run Wdg_Example_Service

  • Open CCS and Import Wdg_Example_Service example

  • Build project and start debug project

5.10.11.1.4. Sample Log of Wdg_Example_Service

Sample Application to test Wdg Interrupt & Servicing - STARTS !!!
Wdg GetVersionInfo API - STARTS !!!
WDG MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 102
SW Major Version    : 2
SW Minor Version    : 0
SW Patch Version    : 2
Wdg GetVersionInfo API - ENDS !!!
Wdg Initialization - STARTS !!!
Wdg Initialization - ENDS !!!
Wdg Max timeout duration in milliseconds is : 3342 !!!
Wdg servicing is called in loop, So interrupts will not be generated !!!
Wdg Example Service: Sample Application - Completes successfully !!!

5.10.11.2. Wdg_Example_Interrupt

5.10.11.2.1. Overview of Wdg_Example_Interrupt

  • Wdg_Example_Interrupt

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes pins as GPIO Outputs and GPIO Inputs using Port_Init()

    • Verify the wdg interrupts generation on timeout

5.10.11.2.2. Setup required to run Wdg_Example_Interrupt

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.10.11.2.3. How to run Wdg_Example_Interrupt

  • Open CCS and Import Wdg_Example_Interrupt example

  • Build project and start debug project

5.10.11.2.4. Sample Log of Wdg_Example_Interrupt

App_Utils Initialization is completed !!!
Sample Application to test Wdg Interrupt & Servicing - STARTS !!!
Wdg GetVersionInfo API - STARTS !!!
WDG MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 102
SW Major Version    : 2
SW Minor Version    : 0
SW Patch Version    : 2
Wdg GetVersionInfo API - ENDS !!!
Wdg Initialization - STARTS !!!
Wdg Initialization - ENDS !!!
Wdg Max timeout duration in milliseconds is : 3342 !!!
Wdg Interrupt is generated after timeout!!!
Wdg Example Interrupt: Sample Application - Completes successfully !!!

5.10.11.3. Wdg_Example_Reset

5.10.11.3.1. Overview of Wdg_Example_Reset

  • Wdg_Example_Reset

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes pins as GPIO Outputs and GPIO Inputs using Port_Init()

    • Demonstrates watchdog timer reset functionality when the watchdog is intentionally not serviced

    • Detects reset reason using Mcu_GetResetReason() API to identify MCU_WATCHDOG_RESET (value = 3)

    • Uses USER_REG1_PORESETN register to maintain a persistent counter across watchdog resets. This register retains data until PORESETn, so there should not be any other PORESETn in between.

    • Repeats the watchdog timeout cycle up to 20 times to verify reset behavior

    • After completion, disables the watchdog using Wdg_SetMode(WDGIF_OFF_MODE)

5.10.11.3.2. Setup required to run Wdg_Example_Reset

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.10.11.3.3. How to run Wdg_Example_Reset

  • Open CCS and Import Wdg_Example_Reset example

  • Build project and start debug project

5.10.11.3.4. Sample Log of Wdg_Example_Reset

------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #1
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #2
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #3
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #4
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #5
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #6
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #7
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #8
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #9
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #10
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #11
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #12
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #13
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #14
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #15
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #16
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #17
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #18
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #19
----------------------------------------------------- 
Waiting for watchdog to expire and trigger reset...
------------------------------- 
Wdg Reset Test Example !!!
------------------------------- 
Detected Reset Reason: 3
Reset Reasons: 0=POWER_ON, 1=EXTERNAL, 2=ESM_NMI_WD, 3=WATCHDOG, 4=SW, 5=ESM, 6=UNDEFINED
----------------------------------------------------- 
Restarted after a Watchdog Reset !!!
Wdg Example Reset: Sample Application - Watchdog Reset #20
----------------------------------------------------- 
----------------------------------------------------- 
Total watchdog resets performed: 20
Sample Application to test Wdg Reset  - COMPLETED !!!

5.10.11.4. File Structure

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┣ 📂examples
┃ ┣ 📂AppUtils
┃ ┣ 📂Can
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┃ ┣ 📂Wdg
┃ ┃ ┗ 📂 📂Wdg_Example_Service
┃ ┃ ┃ ┣ 📂CCS
┃ ┃ ┃ ┃ ┗ 📜📜Wdg_Example_Service.projectspec
┃ ┃ ┃ ┣ 📂📜Wdg_Service_Config
┃ ┃ ┃ ┃ ┣ 📂config
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Os.xdm
┃ ┃ ┃ ┃ ┃ ┗ 📜Wdg.xdm : Generated EB Tresos config file in .xdm format
┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.h
┃ ┃ ┃ ┃ ┃ ┗ 📜Wdg_Cfg.h : Contains the generated pre-compiler configuration header.
┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_PBcfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.c
┃ ┃ ┃ ┃ ┃ ┗ 📜Wdg_PBcfg.c : Contains the Post build configuration parameters.
┃ ┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜CMakeLists.txt
┃ ┃ ┗ ┗ 📜Wdg_Example_Service.c : Example application for Wdg
┃ ┗ 📜CMakeLists.txt
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Note

Either Wdg_PBcfg.c OR Wdg_Lcfg.c OR Wdg_Cfg.c will be present based on selected config variant by user