5.9. SPI Module

5.9.1. Acronyms and Definitions

Abbreviation/Term

Explanation

SPI

Serial peripheral Interface

AUTOSAR

AUTomotive Open System ARchitecture

BSW

Basic Software

RTE

Runtime Environment

MCAL

MicroController Abstraction Layer

API

Application Programming Interface

ECU

Electronic Control Unit

CS

Chip Select

MISO

Master Input Slave Output

MOSI

Master Output Slave Input

Master

A device controlling other devices (slaves)

Slave

A device being completely controlled by a master device

Channel

A Channel is a software exchange medium for data that are defined with the same criteria: Config. Parameters, Number of Data elements with same size and data pointers (Source & Destination) or location.

Job

A Job is composed of one or several Channels with the same Chip Select (is not released during the processing of Job). A Job is considered atomic and therefore cannot be interrupted by another Job. A Job has an assigned priority.

Sequence

A Sequence is a number of consecutive Jobs to transmit but it can be rescheduled between Jobs using a priority mechanism. A Sequence transmission is interruptible (by another Sequence transmission) or not depending on a static configuration

ID

Identification Number of an element (Channel, Job, Sequence)

EB

Externally buffered channels. Buffers containing data to transfer are outside the SPI Handler/Driver

IB

Internally buffered channels. Buffers containing data to transfer are inside the SPI Handler/Driver.

NMI

Non Maskable Interrupt

OS

Operating System

DET

Default Error Tracer

DEM

Diagnostic Event Manager – module to handle diagnostic relevant events.

DAR

Decision Analysis and Resolution

SoC

System on a Chip

5.9.2. Introduction

The SPI driver provides services for basic transmission and reception of SPI data using channels, Jobs and Sequences software components. These API’s and components can be used by an application.

SPI MCAL AUTOSAR

Fig. 5.48 SPI MCAL AUTOSAR

This document details AUTOSAR BSW SPI module implementation

Supported AUTOSAR Release

4.3.1

Supported Configuration Variants

Pre-Compile, Link-Time & Post Build

Vendor ID

SPI_VENDOR_ID (44)

Module ID

SPI_MODULE_ID (83)

5.9.3. Functional Overview

A SPI bus is a Controller-peripheral multi node bus system, the controller sets a Chip Select (CS) to select a peripheral for data communication. The SPI (Serial Peripheral Interface) has a 4-wire synchronous serial interface. Data communication is enabled with a Chip Select wire (CS). Data is transmitted with a 3-wire interface consisting of wires for serial data input (MOSI), serial data output (MISO) and Serial ClocK (SCK). The following SPI module provides channel based read, write and transfer access to different devices on SPI busses. A SPI channel represents data elements (8 to 16 data bits). These channels could be combined in sequence which shall not be interrupted (e.g. Daisy-Chain, EEPROM). Channels have a static configuration defining baud rate, chip select A SPI device is generally identified by the used SPI hardware unit and the associated chip select line. This module can operate only as SPI controller.

5.9.4. Hardware Features

5.9.4.1. Hardware Features supported

  • Two operational modes: Controller and Peripheral

  • Baud rate: 125 different programmable rates. The maximum baud rate that can be employed is limited by the maximum speed of the I/O buffers used on the SPI pins. See the device data sheet for more details.

  • Data word length: 1 to 16 data bits

  • Four clocking schemes (controlled by clock polarity and clock phase bits) include:

    • Falling edge without phase delay: SPICLK active-high. SPI transmits data on the falling edge of the SPICLK signal and receives data on the rising edge of the SPICLK signal.

    • Falling edge with phase delay: SPICLK active-high. SPI transmits data one half-cycle ahead of the falling edge of the SPICLK signal and receives data on the falling edge of the SPICLK signal.

    • Rising edge without phase delay: SPICLK inactive-low. SPI transmits data on the rising edge of the SPICLK signal and receives data on the falling edge of the SPICLK signal.

    • Rising edge with phase delay: SPICLK inactive-low. SPI transmits data one half-cycle ahead of the rising edge of the SPICLK signal and receives data on the rising edge of the SPICLK signal.

  • Simultaneous receive and transmit operation (transmit function can be disabled in software)

  • Transmitter and receiver operations are accomplished through either interrupt- driven or polled algorithm

  • Delayed transmit control

  • 16-level transmit/receive FIFO

  • High-speed mode

5.9.4.2. Not supported Features

  • The SPI Handler/Driver does not handle peripheral mode(slave mode).

  • The SPI Handler/Driver only supports full-duplex mode, and F29x SPI three-wire mode is a half-duplex communication, three-wire mode is not supported in SPI Handler/Driver as per AUTOSAR.

  • The LEVEL 2 SPI Handler/Driver is specified for microcontrollers that have to provide, at least, two SPI busses using separated hardware units. Otherwise, using this level of functionality does not make sense.

  • SPIPTE inversion for digital audio interface receive mode on devices with two SPI modules- since it requires SPI to be configured as peripheral mode, it is not handled in SPI Handler/Driver as per AUTOSAR

5.9.4.3. Non compliance

  • Since F29x SPI is 16 bit, SPI transfer/receive of word length greater than 16 bits are not supported.

SWS_BSW_00042 : Detection of Development Errors: The detection and reporting of Development errors shall be performed only if the configuration parameter for detection of Development errors is set

Partial Non Compliance Reason : Few Null pointer input parameter checks are needed irrespective of Development errors is set, to handle MISRA requirement.

SWS_Spi_00263 : Chip Select shall be handled during Job transmission and shall be released at the end of it. This Chip Select handling shall be done according to the Job configuration parameters.

Partial Non Compliance Reason : When peripheral engine is used, the CS might be pulled to idle state even in between channel transfer after every 8 bit or 16 bit transfer. This is a hardware limitation where the CS line cannot be controlled to stay at the active state throughout the job transfer. As a workaround, GPIO can be used as a CS so that the GPIO acts as a CS and remains in the active state throughout the job completion. This will be handled by the SPI driver and is configurable using the configuration parameter SpiCsSelection.

5.9.5. Source files

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┃ ┣ 📂BSW_Stubs
┃ ┣ 📂Can
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂hw_include
┃ ┣ 📂Mcal_Lib
┃ ┣ 📂Port
┃ ┣ 📂Mcu
┃ ┣ 📂Spi
┃ ┃ ┣ 📂include
┃ ┃ ┃ ┣ 📜Spi.h : Contains the API’s of the Spi driver to be used by upper layers.
┃ ┃ ┃ ┣ 📜Spi_Priv.h : Contains data structures and Internal function declarations.
┃ ┃ ┃ ┣ 📜Spi_Reg_Access.h : Contains the MACROs for Spi register access.
┃ ┃ ┃ ┗ 📜Spi_Utils.h : Contains Internal function declarations.
┃ ┃ ┣ 📂src
┃ ┃ ┃ ┣ 📜Spi.c : Contains the implementation of the API’s for Spi driver.
┃ ┃ ┃ ┣ 📜Spi_Irq.c : contains the implementation for Spi interrupts handlers.
┃ ┃ ┃ ┣ 📜Spi_Priv.c : Contains Functions that support the API’s for Spi driver
┃ ┃ ┃ ┗ 📜Spi_Utils.c : Contains Functions that support the API’s for Spi driver
┃ ┃ ┗ 📜CMakeLists.txt
┣ 📂examples
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Spi_Header_File_Structure

Fig. 5.49 Spi_Header_File_Structure

5.9.6. Module requirements

5.9.6.1. Memory Mapping

The driver follows the AUTOSAR memory mapping strategy. All memory sections should be stored in memory as per AUTOSAR specifications, considering initialization policy, alignment requirements, safety classification, and core scope where applicable.

Reference memory map files can be found at:

{MCAL_INSTALL_PATH}\drivers\BSW_Stubs\MemMap\include

The memory sections are organized according to AUTOSAR specifications to ensure proper placement of code and data in different memory regions based on their usage and access patterns.

5.9.6.2. Scheduling

Schedule Function API

Description

Spi_MainFunction_Handling

This function performs the polling of Rx interrupt flag and performs next transmission

5.9.6.3. Error handling

5.9.6.3.1. Development Error Reporting

Development errors are reported to the DET using the service Det_ReportError(),when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

Development RunTime errors are reported to the DET using the service Det_ReportRuntimeError().

5.9.6.3.1.1. Error codes

Type of Error

Related Error code

Value (Hex)

API SPI_Init service is called while the SPI the driver has already been initialized

SPI_E_ALREADY_INITIALIZED

0x4A

API service used without module initialization

SPI_E_UNINIT

0x1A

APIs called with a Null Pointer

SPI_E_PARAM_POINTER

0x10

API parameter checking: invalid channel

SPI_E_PARAM_CHANNEL

0x0A

API parameter checking: invalid job

SPI_E_PARAM_JOB

0x0B

API parameter checking: invalid sequence

SPI_E_PARAM_SEQ

0x0C

API parameter checking: invalid length

SPI_E_PARAM_LENGTH

0x0D

API parameter checking: invalid HWUnit

SPI_E_PARAM_UNIT

0x0E

Runtime Error - Services called in a wrong sequence

SPI_E_SEQ_PENDING

0x2A

Runtime Error - Synchronous transmission service

SPI_E_SEQ_IN_PROCESS

0x3A

5.9.6.3.2. Extended Production Error Reporting

Extended production errors are reported to the DEM using the service Dem_SetEventStatus(), when enabled. The driver interface contains the MACRO declaration of the error codes to be returned.

5.9.7. Safety Mechanism

TI Diagnostic Unique Identifier

Summary

Description

SPI6

SPI Data Overrun Detection

Error detection are notified to user and Reported to DEM

Note

More details of Safety Mechanisms can be found in Safety Manual.

5.9.8. Used resources

5.9.8.1. Interrupt Handling

AUTOSAR_SWS_SPIDriver section: 10 Configuration specification, details the expected behavior and control flow for ISR implementation, please refer the same.

The Driver doesn’t register any interrupts handler (ISR), it’s expected that consumer of this driver registers the required interrupt handler.

For every SPI Instance, an ISR requires to be registered. The Interrupt number associated with instance of the SPI is detailed in TRM (also, please refer the Example application). Interrupt type should be selected in SPI plugin.

SPI Instance

Interrupt Name

Interrupt handler

SPIA

SPIA_RXINT

Spi_A_RxISR

SPIB

SPIB_RXINT

Spi_B_RxISR

SPIC

SPIC_RXINT

Spi_C_RxISR

SPID

SPID_RXINT

Spi_D_RxISR

SPIE

SPIE_RXINT

Spi_E_RxISR

Note

Same Interrupt Category needs to be configured in both SPI and OS Modules. SPI Tx Interrupt is not used by SPI driver.

5.9.8.2. Instance support

CPU instances

supported

CPU 1

YES

CPU 2

NO

CPU 3

NO

5.9.8.3. Hardware-Software Mapping

Below image shows SPI driver Hardware-Software mapping. For more information related to HW, refer the F29x Reference Manual.

SPI HW/SW Mapping

Fig. 5.50 Spi HW/SW Mapping

5.9.9. Integration description

5.9.9.1. Dependent modules

5.9.9.1.1. DET

This implementation depends on the DET in order to report development errors The detection of development errors is configurable (ON / OFF), The switch SPI_CFG_DEV_ERROR_DETECT will activate or deactivate the detection of all development errors.

5.9.9.1.2. DEM

SPI Production errors are reported to DEM ( Diagnostic Event Manager ) Module.

5.9.9.1.3. SchM

If multiple AUTOSAR runnables have access to the same Data Store Memory block, the exported AUTOSAR specification enforces data consistency by using an AUTOSAR exclusive area. With this specification, the runnables have mutually exclusive access to the per-instance memory global data, which prevents data corruption. Beside the OS, the BSW Scheduler provides functions that SPI module calls at begin and end of critical sections. This implementation requires 1 level of exclusive access to guard critical sections.

The data consistency mechanism that has to be applied to an ExclusiveArea might be domain, ECU or even project specific. The decision which mechanism has to be applied by RTE / Basic Software Scheduler is taken during ECU integration by setting the Exclusive Area configuration parameter RteExclusiveAreaImplMechanism. This parameter is an input for RTE generator.

For SPI Module, data consistency and exclusive access to critical sections are required for the following sections as shown in the table below:

Exclusive Area Functions used

SPI Function calling Exclusive Area

Need for Exclusive Area

Recommended Exclusive Area Mapping

SPI_EXCLUSIVE_AREA_0

Spi_AsyncTransmit
Spi_Cancel
Spi_SyncTransmit
Spi_GetHWUnitStatus
Spi_WriteIB
Spi_ReadIB
Spi_SetupEB

To protect against multiple access for shared resources

OS_RESOURCE : If the SPI APIs are only called from pre-emptible task context, its recommended to use this mechanism as it takes care of resource access protection and task priority management.
None: If SPI APIs are only called from non pre-emptible task context or during init, its recommended to use this mechanism as multiple access protection to shared resource is not needed.

5.9.9.1.4. MCU

MCU Module is required to initialize all the clock to be used by different peripherals.

5.9.9.1.5. PORT

PORT Module is required to initialize Pin configurations and MUX mode for SPI Instances.

5.9.9.1.6. DIO

Dio Module is required to handle SPI chip select when GPIO is configured to use as chip select.

5.9.9.2. Resource Allocator

The SPI module uses the Resource Allocator to allocate SPI peripheral instances to CPU cores and configure their memory-mapped base addresses. Each allocation is placed inside a Context that maps to a CPU core (e.g. CPU1). The CurrentContext parameter in the Resource Allocator selects which Context is active for MCAL execution. See the Resource Allocator Module User Guide for details on configuring device-specific settings.

The Frame parameter (FRAME0–FRAME3) selects the memory-mapped frame for the instance, enabling simultaneous access from different initiators without arbitration stalls. The BaseAddr is auto-calculated based on the selected instance and frame. The DebugHaltEnabled and StandbyModeEnabled parameters control peripheral behaviour during CPU debug halt and standby low-power modes respectively.

5.9.9.2.1. Resource Allocator Usage Example

To allocate SPIA to CPU1 using FRAME0:

  1. In the Resource Allocator configuration, create a new Spi instance allocation under the CPU1 Context

  2. Set InstanceName to SPIA

  3. Set Frame to FRAME0

  4. The BaseAddr will be automatically calculated as SPIA_BASE_FRAME(0U)

  5. Optionally configure DebugHaltEnabled and StandbyModeEnabled

Resource Allocator Configuration:
├── Context (Core: CPU1)
│   └── SpiInstanceAllocation
│       ├── InstanceName: SPIA
│       ├── Frame: FRAME0
│       ├── BaseAddr: SPIA_BASE_FRAME(0U)  [auto-calculated]
│       ├── DebugHaltEnabled: true
│       └── StandbyModeEnabled: true

5.9.10. Configuration

The Spi Driver implementation supports multiple configuration variants The driver expects generated Spi_Cfg.h to be present as input file. The associated Spi driver configuration generated source files are Spi_LCfg.c if Link-Time variant is selected and Spi_PBcfg.c if Post-Build config variant is selected, only Spi_Cfg.c if Pre-Compile variant is selected

The generated configuration files should not be modified manually. The config tool Elektrobit Tresos should be used to modify the configuration files.

5.9.10.1. Configuration Parameters

5.9.10.1.1. SpiDemEventParameterRefs

Item

Name

SpiDemEventParameterRefs

Description

Container for the references to DemEventParameter elements which shall be invoked using the API Dem_SetEventStatus in case the corresponding error occurs. The EventId is taken from the referenced DemEventParameter’s DemEventId symbolic value. The standardized errors are provided in this container and can be extended by vendor-specific error references.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Post-build-variant-multiplicity

false

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.9.10.1.2. SpiDriver

This container contains the configuration parameters and sub containers of the AUTOSAR Spi module.

5.9.10.1.2.1. SpiMaxChannel

Item

Name

SpiMaxChannel

Description

This parameter contains the number of Channels configured. It will be gathered by tools during the configuration stage.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

1

Min-value

1

5.9.10.1.2.2. SpiMaxJob

Item

Name

SpiMaxJob

Description

Total number of Jobs configured.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

1

Max-value

65535

Min-value

1

5.9.10.1.2.3. SpiMaxSequence

Item

Name

SpiMaxSequence

Description

Total number of Sequences configured.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.9.10.1.2.4. SpiSequenceTimeOut

Item

Name

SpiSequenceTimeOut

Description

TimeOut value for sync transmission in seconds, if sync transmission didn’t happen within this time frame transmission will be aborted and DET runtime error is reported with SPI_E_SEQ_TIMEOUT error code

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

5.0E-5

Max-value

10.0

Min-value

1.0E-6

5.9.10.1.2.5. SpiCounterClockRef

Item

Name

SpiCounterClockRef

Description

This parameter references the SYSCLK to convert timeout values from milliseconds to clock ticks. Users should ensure the correct clock reference point is selected to achieve accurate timeout calculations.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

5.9.10.1.2.6. SpiChannel

All data needed to configure one SPI-channel

5.9.10.1.2.7. SpiChannelId

Item

Name

SpiChannelId

Description

SPI Channel ID, used as parameter in SPI API functions.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.9.10.1.2.8. SpiChannelType

Item

Name

SpiChannelType

Description

Buffer usage with EB/IB channel.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

IB

Range

EB
IB

5.9.10.1.2.9. SpiDataWidth

Item

Name

SpiDataWidth

Description

This parameter is the width of a transmitted data unit.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

8

Max-value

16

Min-value

1

5.9.10.1.2.10. SpiDefaultData

Item

Name

SpiDefaultData

Description

The default data to be transmitted when (for internal buffer or external buffer) the pointer passed to Spi_WriteIB (for internal buffer) or to Spi_SetupEB (for external buffer) is NULL. In case of SpiDataWidth is less than 16, only LSB bits are considered and MSB bits are ignored

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

65535

Max-value

65535

Min-value

0

5.9.10.1.2.11. SpiEbMaxLength

Item

Name

SpiEbMaxLength

Description

This parameter contains the maximum size (number of data elements) of data buffers in case of EB Channels and only.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

5.9.10.1.2.12. SpiIbNBuffers

Item

Name

SpiIbNBuffers

Description

This parameter contains the maximum number of data buffers in case of IB Channels and only.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

5.9.10.1.2.13. SpiTransferStart

Item

Name

SpiTransferStart

Description

This parameter defines the first starting bit for transmission.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

MSB

Range

LSB
MSB

5.9.10.1.2.14. SpiJob

All data needed to configure one SPI-Job, amongst others the connection between the internal SPI unit and the special settings for an external device is done.

5.9.10.1.2.15. SpiHwUnitSynchronous

Item

Name

SpiHwUnitSynchronous

Description

If SpiHwUnitSynchronous is set to “SYNCHRONOUS”, the SpiJob uses its containing SpiDriver in a synchronous manner. If it is set to “ASYNCHRONOUS”, it uses the driver in an asynchronous way. If the parameter is not set, the SpiChannel uses the driver also in an asynchronous way.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

SYNCHRONOUS

Range

ASYNCHRONOUS
SYNCHRONOUS

5.9.10.1.2.16. SpiJobEndNotification

Item

Name

SpiJobEndNotification

Description

This parameter is a reference to a notification function.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.9.10.1.2.17. SpiJobId

Item

Name

SpiJobId

Description

SPI Job ID, used as parameter in SPI API functions.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

5.9.10.1.2.18. SpiJobPriority

Item

Name

SpiJobPriority

Description

Priority set accordingly to SPI093: 0, lowest, 3, highest priority

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

3

Min-value

0

5.9.10.1.2.19. SpiDeviceAssignment

Item

Name

SpiDeviceAssignment

Description

Reference to the external device used by this job

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.9.10.1.2.20. SpiChannelList

References to SPI channels and their order within the Job.

5.9.10.1.2.21. SpiChannelIndex

Item

Name

SpiChannelIndex

Description

This parameter specifies the order of Channels within the Job.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.9.10.1.2.22. SpiChannelAssignment

Item

Name

SpiChannelAssignment

Description

A job reference to a SPI channel.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.9.10.1.2.23. SpiSequence

All data needed to configure one SPI-sequence

5.9.10.1.2.24. SpiInterruptibleSequence

Item

Name

SpiInterruptibleSequence

Description

This parameter allows or not this Sequence to be suspended by another one.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.2.25. SpiSeqEndNotification

Item

Name

SpiSeqEndNotification

Description

This parameter is a reference to a notification function.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

NULL_PTR

5.9.10.1.2.26. SpiSequenceId

Item

Name

SpiSequenceId

Description

SPI Sequence ID, used as parameter in SPI API functions.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.9.10.1.2.27. SpiJobAssignment

Item

Name

SpiJobAssignment

Description

A sequence references several jobs, which are executed during a communication sequence

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.9.10.1.2.28. SpiExternalDevice

The communication settings of an external device. Closely linked to SpiJob.

5.9.10.1.2.29. SpiExternalDeviceId

Item

Name

SpiExternalDeviceId

Description

The index of the corresponding external device config associated with job.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

65535

Min-value

0

5.9.10.1.2.30. SpiBaudrate

Item

Name

SpiBaudrate

Description

This parameter is the communication baudrate in bits per second (bps), Range is SYSCLK/128 to SYSCLK/4

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0.0

Max-value

5000000.0

Min-value

0.0

Note

SPI Baudrate field in the configurator is implemented as float due to AUTOSAR requirement. If a float value is configured as baud rate, the calculated clock divider value is rounded to an integer. Therefore, floating point values for baud rate are not supported.

5.9.10.1.2.31. SpiclkDivider

Item

Name

SpiclkDivider

Description

This parameter is the SPIBRR value

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

127

Min-value

0

5.9.10.1.2.32. SpiCsIdentifier

Item

Name

SpiCsIdentifier

Description

This parameter is the symbolic name to identify the Chip Select (CS) allocated to this Job.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

SPI_PERIPHERAL_CS_IDENTIFIER

5.9.10.1.2.33. SpiCsPolarity

Item

Name

SpiCsPolarity

Description

This parameter defines the active polarity of Chip Select.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LOW

Range

HIGH
LOW

5.9.10.1.2.34. SpiCsSelection

Item

Name

SpiCsSelection

Description

When the Chip select handling is enabled (see SpiEnableCs), then this parameter specifies if the chip select is handled automatically by Peripheral HW engine or via general purpose IO by Spi driver.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

true

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

CS_VIA_PERIPHERAL_ENGINE

Range

CS_VIA_GPIO
CS_VIA_PERIPHERAL_ENGINE

5.9.10.1.2.35. SpiDataShiftEdge

Item

Name

SpiDataShiftEdge

Description

This parameter defines the SPI data shift edge.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

TRAILING

Range

LEADING
TRAILING

5.9.10.1.2.36. SpiEnableCs

Item

Name

SpiEnableCs

Description

This parameter enables or not the Chip Select handling functions. If this parameter is enabled then parameter SpiCsSelection further details the type of chip selection.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.2.37. SpiHwUnit

Item

Name

SpiHwUnit

Description

This parameter is the symbolic name to identify the HW SPI Hardware

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

SPIA

Range

SPIA
SPIB
SPIC
SPID
SPIE

5.9.10.1.2.38. SpiShiftClockIdleLevel

Item

Name

SpiShiftClockIdleLevel

Description

This parameter defines the SPI shift clock idle level.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

LOW

Range

HIGH
LOW

5.9.10.1.2.39. SpiDataWordDelay

Item

Name

SpiDataWordDelay

Description

This parameter defines the SPI delay between every transfer from FIFO transmit buffer to transmit shift register, work only in FIFO mode

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

255

Min-value

0

5.9.10.1.2.40. SpiSysClockRef

Item

Name

SpiSysClockRef

Description

Reference to the SPI clock source configuration, which is set in the MCU driver configuration.

Origin

Texas Instruments

Post-Build-Variant-Value

true

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

5.9.10.1.2.41. SpiCsGpioRef

Item

Name

SpiCsGpioRef

Description

Reference to the Dio channel configuration to get symbolic name from Dio, which is set in the DIO driver configuration

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

Texas Instruments

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

5.9.10.1.2.42. SpiHwUnitConfig

HW Unit configurations

5.9.10.1.2.43. SpiHighSpeedMode

Item

Name

SpiHighSpeedMode

Description

Enables High speed mode for SPI instance, Note: Since only selected pins support HS mode, to enable high speed communication apropriate HS pins shall be configured for SPI in port configration, please check c29x TRM and data sheet for HS mode supported pins

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

5.9.10.1.2.44. SpiLoopBackMode

Item

Name

SpiLoopBackMode

Description

Enables Loop Back mode for SPI instance

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Default-value

false

5.9.10.1.2.45. SpiFifoModeEnable

Item

Name

SpiFifoModeEnable

Description

Enables FIFO mode for SPI instance

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Pre-Compile-Time

VARIANT-PRE-COMPILE

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Default-value

true

5.9.10.1.2.46. SpiIrqType

Item

Name

SpiIrqType

Description

Type of Isr function: CAT1 realtime interrupt or CAT1 : interrupt void func(void) or CAT2 : ISR(func)

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

SPI_ISR_CAT2

Range

SPI_ISR_CAT1_RTINT
SPI_ISR_CAT1_INT
SPI_ISR_CAT2

5.9.10.1.2.47. SpiHwUnitType

Item

Name

SpiHwUnitType

Description

Reference to the SPI Instance.

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

5.9.10.1.3. SpiGeneral

General configuration settings for SPI-Handler

5.9.10.1.3.1. SpiCancelApi

Item

Name

SpiCancelApi

Description

Switches the Spi_Cancel function ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.3.2. SpiChannelBuffersAllowed

Item

Name

SpiChannelBuffersAllowed

Description

Selects the SPI Handler/Driver Channel Buffers usage allowed and delivered, IB = 0; EB = 1; IB/EB = 2;

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

2

Max-value

2

Min-value

0

5.9.10.1.3.3. SpiChannelInternalBufferMaxLength

Item

Name

SpiChannelInternalBufferMaxLength

Description

Internal Buffer length in bytes - applicable for SpiChannelBuffer type - SPI_IB. This is the maximum length that can be allocated by each channel and it is fixed.Can vary buffer length per channel by configuring SpiIbNBuffers and SpiDataWidth. Refer MCAL-24874 and MCAL-25127

Origin

Texas Instruments

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Pre-Compile-Time

VARIANT-PRE-COMPILE

Post-Build-Time

VARIANT-POST-BUILD

Default-value

64

Max-value

131070

Min-value

1

5.9.10.1.3.4. SpiDevErrorDetect

Item

Name

SpiDevErrorDetect

Description

Switches the development error detection and notification on or off.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.3.5. SpiHwStatusApi

Item

Name

SpiHwStatusApi

Description

Switches the Spi_GetHWUnitStatus function ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.3.6. SpiInterruptibleSeqAllowed

Item

Name

SpiInterruptibleSeqAllowed

Description

Switches the Interruptible Sequences handling functionality ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.3.7. SpiLevelDelivered

Item

Name

SpiLevelDelivered

Description

Selects the SPI Handler/Driver level of scalable functionality that is available and delivered.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0

Max-value

2

Min-value

0

5.9.10.1.3.8. SpiMainFunctionPeriod

Item

Name

SpiMainFunctionPeriod

Description

This parameter defines the cycle time of the function Spi_MainFunction_Handling in seconds. The parameter is not used by the driver it self, but it is used by upper layer.

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

0.01

Max-value

INF

Min-value

0.0

5.9.10.1.3.9. SpiSupportConcurrentSyncTransmit

Item

Name

SpiSupportConcurrentSyncTransmit

Description

Specifies whether concurrent Spi_SyncTransmit() calls for different sequences shall be configurable.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

5.9.10.1.3.10. SpiUserCallbackHeaderFile

Item

Name

SpiUserCallbackHeaderFile

Description

Header file name which will be included by the Spi. The value of this parameter shall be used as h-char-sequence or q-char-sequence according to ISO C90 section 6.10.2 “source file inclusion”. The parameter value MUST NOT represent a path, since ISO C90 does not specify how such a path is treated (i.e., this is implementation defined (and additionally depends on the operating system and the underlying file system)).

Multiplicity-Configuration-Class

–

Link Time

VARIANT-LINK-TIME

Post-Build Time

VARIANT-POST-BUILD

Pre-Compile Time

VARIANT-PRE-COMPILE

Origin

AUTOSAR_ECUC

Post-build-variant-multiplicity

false

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

HeaderFileName

5.9.10.1.3.11. SpiVersionInfoApi

Item

Name

SpiVersionInfoApi

Description

Switches the Spi_GetVersionInfo function ON or OFF.

Origin

AUTOSAR_ECUC

Post-Build-Variant-Value

false

Value-Configuration-Class

–

Link-Time

VARIANT-LINK-TIME

Post-Build-Time

VARIANT-POST-BUILD

Pre-Compile-Time

VARIANT-PRE-COMPILE

Default-value

false

Refer AUTOSAR_SWS_SPIDriver section: 10 Configuration specification for configuration parameters details

5.9.10.2. Steps To Configure Spi Module

  1. Open EB Tresos configurator tool and load Port, Mcu, Ecum, Os, Dem and Spi modules

  2. Open PORT module plugin and configure required pins as MISO, MOSI, CLK, CS.

  3. Open SPI module plugin, Select the Config Variant (Pre-compile or Link-Time or Post-Build)

  4. In SPI module plugin configure required parameters.

  5. Save the configuration and generate the configuration.

5.9.11. Examples

The example application demonstrates use of Spi module, the list below identifies key steps performed the example.

5.9.11.1. Spi_Example_Sync_AsyncTransfer

5.9.11.1.1. Overview of Spi_Example_Sync_AsyncTransfer

  • Spi_Example_Sync_AsyncTransfer

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes required port pins for SPI.

    • Spi_Init()

    • Write the data into channels if channel buffer type is IB,setup buffer if channel buffer type is EB.

    • Transmit One sequence Synchronously.

    • Transmit another sequence Asynchronously.

    • Check for HWUnit, Job, Sequence status.

    • Read the data from channels.

    • Validate the received data with pre-defined transmit data.

5.9.11.1.2. Setup required to run Spi_Example_Sync_AsyncTransfer

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.9.11.1.3. How to run Spi_Example_Sync_AsyncTransfer

  • Open CCS and Import Spi_Example_Sync_AsyncTransfer

  • Build project and start debug project

5.9.11.1.4. Sample Log of Spi_Example_Sync_AsyncTransfer

Sample Application - STARTS !!!
SPI MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 83
SW Major Version    : 3
SW Minor Version    : 1
SW Patch Version    : 3
Writing to internal buffer channel0.
Writing to internal buffer channel1.
Writing to external buffer channel2.
Transmitting data in asynchronous mode.
AsyncTransmit status is 0
Transmitting data in synchronous mode.
SyncTransmit status is 0
Getting hardware unit status.
Getting job status.
Called Sequence end notification function
Called Sequence end notification function
Getting sequence status.
Result of sequence_1 is SPI_SEQ_OK.
De-initializing SPI.
Spi_Example_Sync_AsyncTransfer : Sample Application success

5.9.11.2. Spi_Example_AsyncTransfer_Interrupt

5.9.11.2.1. Overview of Spi_Example_AsyncTransfer_Interrupt

  • Spi_Example_AsyncTransfer_Interrupt

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes required port pins for SPI.

    • Spi_Init()

    • Write the data into channels if channel buffer type is IB,setup buffer if channel buffer type is EB.

    • Transmit data asynchronously.

    • Check for HWUnit, Job, Sequence status.

    • Read the data from channels.

    • Validate the received data with pre-defined transmit data.

5.9.11.2.2. Setup required to run Spi_Example_AsyncTransfer_Interrupt

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.9.11.2.3. How to run Spi_Example_AsyncTransfer_Interrupt

  • Open CCS and Import Spi_Example_AsyncTransfer_Interrupt

  • Build project and start debug project

5.9.11.2.4. Sample Log of Spi_Example_AsyncTransfer_Interrupt

Sample Application - STARTS !!!
SPI MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 83
SW Major Version    : 3
SW Minor Version    : 1
SW Patch Version    : 3
Writing to internal buffer channel0.
Writing to internal buffer channel1.
Writing to external buffer channel2.
Transmitting data in asynchronous mode.
Called Sequence end notification function
Called Sequence end notification function
AsyncTransmit status is 0
Getting hardware unit status.
Result of Hardware unit is not SPI_BUSY.
Getting job status.
Getting sequence status.
Result of sequence_1 is SPI_SEQ_OK.
De-initializing SPI.
Spi_Example_AsyncTransfer_Interrupt : Sample Application success

5.9.11.3. Spi_Example_SyncTransfer

5.9.11.3.1. Overview of Spi_Example_SyncTransfer

  • Spi_Example_SyncTransfer

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes required port pins for SPI.

    • Spi_Init()

    • Write the data into channels if channel buffer type is IB,setup buffer if channel buffer type is EB.

    • Transmit data synchronously.

    • Check for HWUnit, Job, Sequence status.

    • Read the data from channels.

    • Validate the received data with pre-defined transmit data.

5.9.11.3.2. Setup required to run Spi_Example_SyncTransfer

  • Connect the hardware and power up

  • Connect the uart set up to check the log on serial console

5.9.11.3.3. How to run Spi_Example_SyncTransfer

  • Open CCS and Import Spi_Example_SyncTransfer

  • Build project and start debug project

5.9.11.3.4. Sample Log of Spi_Example_SyncTransfer

Sample Application - STARTS !!!
SPI MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 83
SW Major Version    : 3
SW Minor Version    : 1
SW Patch Version    : 3
Writing to internal buffer channel0.
Writing to internal buffer channel1.
Writing to external buffer channel2.
Getting hardware unit status.
Transmitting data in synchronous mode.
SyncTransmit status is 0
Getting sequence status.
Deinitializing SPI.
Spi_Example_SyncTransfer : Sample Application success

5.9.11.4. Spi_Example_External_Loopback

5.9.11.4.1. Overview of Spi_Example_External_Loopback

  • Spi_Example_External_Loopback

    • EcuM_Init()

      • Initializes clock to 200 MHz using Mcu_Init()

      • Initializes required port pins for SPI.

    • Call Spi_Init() to initialize SPI Driver

    • Initialize Internal and External Buffers.

    • Transmit data synchronously.

    • Read the data from channels.

    • Received data can be seen in Spi_DestBuf0

    • Validate the received data with pre-defined transmit data.

5.9.11.4.2. Setup required to run Spi_Example_External_Loopback

  • Connect the hardware and power up

  • Makes sure to disable the S2 POCI switch on the XDS110 to OFF (Only when used with SOM EVM) as shown below:

S2 POCI Switch on XDS110 Debugger

Fig. 5.51 S2 POCI Switch on XDS110 Debugger

  • Place the SOM on Bank Mode 2 and disable FOTA.

  • Make necessary connections between SPI A and SPI D as shown in the figure below:

SPI Example External Loopback Connections

Fig. 5.52 SPI Example External Loopback Connections

  • Connect the uart set up to check the log on serial console

5.9.11.4.3. How to run Spi_Example_External_Loopback

  • Build the example to generate .out.

  • Connect to CPU1 and load only the *_c29x1.out.

  • After the program is loaded, run CPU1.

  • CPU1 configures and releases CPU3 out of reset.

  • CPU1 pauses due to software breakpoint (EMUSTOP0).

  • Connect to CPU3 target now. C29x3.out would have started execution as soon as it is released from reset.

  • Resume CPU1 after CPU3 starts running.

Note

Note: To visualize the CPU3 source file (in debug mode), load the CPU3.out by clicking on the “Load Symbols” option.

5.9.11.4.4. Sample Log of Spi_Example_External_Loopback

Sample Application - STARTS !!!
SPI MCAL Version Info
---------------------
Vendor ID           : 44
Module ID           : 83
SW Major Version    : 3
SW Minor Version    : 1
SW Patch Version    : 3
Writing to internal buffer channel0.
Getting hardware unit status.
Transmitting data in asynchronous mode.
SyncTransmit status is 0
Getting sequence status.
Deinitializing SPI.
Spi_Example_External_Loopback : Sample Application success

5.9.11.5. File Structure

📦f29h85x_mcal
┣ 📂build
┣ 📂docs
┣ 📂drivers
┣ 📂examples
┃ ┣ 📂AppUtils
┃ ┣ 📂Can
┃ ┣ 📂DeviceSupport
┃ ┣ 📂Dio
┃ ┣ 📂Gpt
┃ ┣ 📂Mcu
┃ ┣ 📂Port
┃ ┣ 📂Spi
┃ ┃ ┣ 📂 Spi_Example_Sync_AsyncTransfer
┃ ┃ ┃ ┣ 📂CCS
┃ ┃ ┃ ┃ ┗ 📜Spi_Example_Sync_AsyncTransfer.projectspec
┃ ┃ ┃ ┣ 📂F29H85x_Config
┃ ┃ ┃ ┃ ┣ 📂config
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Os.xdm
┃ ┃ ┃ ┃ ┃ ┣ 📜Port.xdm
┃ ┃ ┃ ┃ ┃ ┗ 📜Spi.xdm : Generated EB Tresos config file in .xdm format
┃ ┃ ┃ ┃ ┣ 📂include
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.h
┃ ┃ ┃ ┃ ┃ ┣ 📜Port_Cfg.h
┃ ┃ ┃ ┃ ┃ ┗ 📜Spi_Cfg.h : Contains the generated pre-compiler configuration header.
┃ ┃ ┃ ┃ ┣ 📂src
┃ ┃ ┃ ┃ ┃ ┣ 📜Dem_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜EcuM_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Mcu_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Os_Cfg.c
┃ ┃ ┃ ┃ ┃ ┣ 📜Port_PBcfg.c
┃ ┃ ┃ ┃ ┃ ┗ 📜Spi_PBcfg.c : Contains the Post build configuration parameters.
┃ ┃ ┃ ┃ ┗ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜CMakeLists.txt
┃ ┃ ┃ ┣ 📜Spi_Example_Sync_AsyncTransfer.c : Example application for Spi
┃ ┃ ┃ ┗ 📜Spi_Example_Sync_AsyncTransfer.h : Example application for Spi
┃ ┃ ┣ 📂 Spi_Example_AsyncTransfer_Interrupt
┃ ┃ ┗ 📂 Spi_Example_SyncTransfer
┃ ┗ 📜CMakeLists.txt
┣ 📂plugins
┣ 📜CMakeLists.txt
┗ 📜CMakePresets.json

Note

Spi_PBcfg.c will be present if Post-Build config variant is selected, only Spi_Cfg.c will be present if Pre-Compile variant is selected and only Spi_Lcfg.c will be present if Link-Time variant is selected