5.1. CAN

5.1.1. Types

Base type

Type Name

Brief

enum

Can_ProcessingType

Can Tx/Rx Processing.

enum

Can_ReturnType

Values that can be returned by CAN Driver APIs.

enum

Can_HandleType

Can Handle Type FULL/BASIC.

enum

Can_ControllerInstance

Can Controller Instance ID.

enum

Can_MailboxDirectionType

Can Mailbox direction enum.

enum

Can_Icom_signal_operation_type

Icom signal operation type.

enum

Can_DrvState

Can Driver state.

enum

Can_ControllerOperationMode

Enum to represent the MCAN mode of operation.

enum

Can_ClockStopAckMode

Enum to represent the MCAN mode of operation.

enum

Can_MailboxElemSizeType

Enum to represent FIFO/Buffer element Size.

enum

Can_MemType

Enum to represent the CAN Message RAM type.

enum

Can_RxFifoNumType

Enum to represent the MCAN Rx FIFO number.

enum

Can_EventPin

Enum for the event pin.

enum

Can_StandardFilterType

Enum for the Can standard filter selection.

5.1.1.1. enum Can_ProcessingType

Enumerator

Value

Description

CAN_INTERRUPT

0x0U

Interrupt.

CAN_MIXED

0x1U

Mixed

CAN_POLLING

0x2U

Polling.

Brief: Can Tx/Rx Processing.

5.1.1.2. enum Can_ReturnType

Enumerator

Value

Description

CAN_BUSY

2U

Transmit request could not be processed because no transmit object was available.

Brief: Values that can be returned by CAN Driver APIs.

5.1.1.3. enum Can_HandleType

Enumerator

Value

Description

CAN_FULL

0x0U

Full

CAN_BASIC

Basic

Brief: Can Handle Type FULL/BASIC.

5.1.1.4. enum Can_ControllerInstance

Enumerator

Value

Description

CAN_CONTROLLER_INSTANCE_MCAN1

0x0U

MCANA Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN2

0x1U

MCANB Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN3

0x2U

MCANC Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN4

0x3U

MCAND Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN5

0x4U

MCANE Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN6

0x5U

MCANF Controller Instance.

Brief: Can Controller Instance ID.

5.1.1.5. enum Can_MailboxDirectionType

Enumerator

Value

Description

CAN_RECEIVE

0x0U

Mailbox is for receive.

CAN_TRANSMIT

Mailbox is for transmit.

Brief: Can Mailbox direction enum.

5.1.1.6. enum Can_Icom_signal_operation_type

Enumerator

Value

Description

AND

0U

AND.

EQUAL

1U

EQUAL.

GREATER

2U

GREATER.

SMALLER

3U

SMALLER.

XOR

4U

XOR.

Brief: Icom signal operation type.

5.1.1.7. enum Can_DrvState

Enumerator

Value

Description

CAN_UNINIT

0U

Can module state when reset/power-up.

CAN_READY

1U

Can module state after initialization.

Brief: Can Driver state.

5.1.1.8. enum Can_ControllerOperationMode

Enumerator

Value

Description

CAN_CONTROLLER_OPERATION_MODE_NORMAL

0U

CAN normal mode.

CAN_CONTROLLER_OPERATION_MODE_SW_INIT

1U

CAN SW initialization mode.

Brief: Enum to represent the MCAN mode of operation.

5.1.1.9. enum Can_ClockStopAckMode

Enumerator

Value

Description

CAN_CLOCK_STOP_NO_ACK

0U

No clock stop acknowledged.

CAN_CLOCK_STOP_ACK

1U

MCAN may be set in power down

Brief: Enum to represent the MCAN mode of operation.

5.1.1.10. enum Can_MailboxElemSizeType

Enumerator

Value

Description

CAN_ELEM_SIZE_8BYTES

0U

8 byte data field

CAN_ELEM_SIZE_12BYTES

1U

12 byte data field

CAN_ELEM_SIZE_16BYTES

2U

16 byte data field

CAN_ELEM_SIZE_20BYTES

3U

20 byte data field

CAN_ELEM_SIZE_24BYTES

4U

24 byte data field

CAN_ELEM_SIZE_32BYTES

5U

32 byte data field

CAN_ELEM_SIZE_48BYTES

6U

48 byte data field

CAN_ELEM_SIZE_64BYTES

7U

64 byte data field

Brief: Enum to represent FIFO/Buffer element Size.

5.1.1.11. enum Can_MemType

Enumerator

Value

Description

CAN_MEM_TYPE_BUF

0U

MCAN Msg RAM buffersss.

CAN_MEM_TYPE_FIFO

1U

MCAN Msg RAM FIFO/Queue.

Brief: Enum to represent the CAN Message RAM type.

5.1.1.12. enum Can_RxFifoNumType

Enumerator

Value

Description

CAN_RX_FIFO_NUM_0

0U

MCAN Rx FIFO 0.

CAN_RX_FIFO_NUM_1

1U

MCAN Rx FIFO 1.

Brief: Enum to represent the MCAN Rx FIFO number.

5.1.1.13. enum Can_EventPin

Enumerator

Value

Description

CAN_EVENT_PIN_0

0x0U

EVENT PIN0.

CAN_EVENT_PIN_1

0x1U

EVENT PIN1.

CAN_EVENT_PIN_NONE

0x2U

EVENT NONE.

Brief: Enum for the event pin.

5.1.1.14. enum Can_StandardFilterType

Enumerator

Value

Description

CAN_RANGE_FILTER

0x0U

Range filter from SFID1 to SFID2 (SFID2 ≥ SFID1)

CAN_DUAL_ID_FILTER

0x1U

Dual ID filter for SFID1 or SFID2.

CAN_CLASSIC_FILTER

0x2U

Classic filter: SFID1 = filter; SFID2 = mask.

CAN_FILTER_DISABLED

0x03

Filter element disabled.

Brief: Enum for the Can standard filter selection.

5.1.2. Structures

Name

Brief

Can_MainFunctionRWPeriodRefType

Can Main Function RW Period Ref Type Identifier.

Can_MaskType

Structure defining the filter mask to be used.

Can_CanConfigType

MCan Controller Specific Configuration.

Can_FdBaudConfigType

Structure defining the CAN FD data phase baud rate configuration.

Can_BaudConfigType

Can Controller Baud Rate Configuration definition.

Can_ControllerType

Can Controller Configuration definition.

Can_MailboxType

Can mailbox configuration definition.

Can_IcomSignalConfigType

Icom signal config data structure.

Can_IcomRxMessageType

Icom Rx message data structure.

Can_IcomConfigType

Icom data structure containing the overall ICOM configuration data.

Can_ConfigType

External data structure containing the overall initialization data for the CAN driver and SFR settings affecting all controllers.

Can_PeriodicReadBackDataType

Can periodic readback register definition.

Can_CanIfIndicationType

Can State Transition indication done to CanIf module.

Can_MsgRAMConfigParams

Structure for MCAN Message RAM Configuration Parameters Message RAM can contain following sections: Standard ID filters, Extended ID filters, TX FIFO(or TX Q), TX Buffers, TX EventFIFO, RX FIFO0, RX FIFO1, RX Buffer. Note: If particular section in the RAM is not used then it’s size should be initialized to ‘0’ (Number of buffers in case of Tx/Rx buffer).

Can_StdMsgIDFilterElement

Structure for MCAN Standard Message ID Filter Element.

Can_ExtMsgIDFilterElement

Structure for MCAN Extended Message ID Filter Element.

Can_FdMsgRAMConfigObjType

Can FD controller Message RAM Configuration object structure.

Can_ControllerObjType

Can controller object structure.

Can_MailboxObjType

Can Mailbox type strucuture.

Can_DriverObjType

Can Driver object type structure.

Can_TxBufElementType

Structure for CAN Tx Buffer element.

Can_RxBufElementType

Structure for CAN Rx Buffer element.

Can_RxFIFOStatusType

Structure for CAN Rx FIFO Status.

Can_RxNewDataStatusType

Structure for Can new data flag for Rx buffer.

5.1.3. Defines

Name

Brief

CAN_SW_MAJOR_VERSION

Driver Implementation Major Version.

CAN_SW_MINOR_VERSION

Driver Implementation Minor Version.

CAN_SW_PATCH_VERSION

Driver Implementation Patch Version.

CAN_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CAN Driver.

CAN_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CAN Driver.

CAN_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CAN Driver.

CAN_VENDOR_ID

CAN Driver ID Info.

CAN_MODULE_ID

CAN Driver Module ID.

CAN_INSTANCE_ID

CAN Instance ID.

CAN_SID_INIT

The Service Id is one of the argument to Det_ReportError function and is used to identify the source of the error.

CAN_SID_MAINFUNC_WRITE

Service ID - Can_MainFunction_Write().

CAN_SID_SETCTR

Service ID - Can_SetControllerMode().

CAN_SID_DIINT

Service ID - Can_DisableControllerInterrupts().

CAN_SID_ENINT

Service ID - Can_EnableControllerInterrupts().

CAN_SID_WRITE

Service ID - Can_Write().

CAN_SID_GET_VERSION_INFO

Service ID - Can_GetVersionInfo().

CAN_SID_MAINFUNC_READ

Service ID - Can_MainFunction_Read().

CAN_SID_MAINFUNC_BO

Service ID - Can_MainFunction_BusOff().

CAN_SID_MAINFUNC_WU

Service ID - Can_MainFunction_Wakeup().

CAN_SID_CKWAKEUP

Service ID - Can_CheckWakeup().

CAN_SID_MAINFUNC_MODE

Service ID - Can_MainFunction_Mode().

CAN_SID_CHNGBAUDRATE

Service ID - Can_ChangeBaudrate().

CAN_SID_CHKBAUDRATE

Service ID - Can_CheckBaudrate().

CAN_SID_SETBAUDRATE

Service ID - Can_SetBaudRate().

CAN_SID_DEINIT

Service ID - Can_DeInit().

CAN_SID_GETCNTRERRSTATE

Service ID - Can_GetControllerErrorState().

CAN_SID_GETCNTRMODE

Service ID - Can_GetControllerMode().

CAN_SID_PROCESSISR

Service ID - Can_ProcessISR().

CAN_SID_ICOMCONFIG

Service ID - Can_SetIcomConfiguration().

CAN_SID_READBACK

Service ID - Can_PeriodicReadback().

CAN_E_PARAM_POINTER

Error codes returned by Can functions - Development Errors.

CAN_E_PARAM_HANDLE

Invalid Controller Handle.

CAN_E_PARAM_DATA_LENGTH

Invalid length of msg.

CAN_E_PARAM_CONTROLLER

Invalid controller id.

CAN_E_UNINIT

Error due to API invoked without performing Can_Init().

CAN_E_TRANSITION

Error during Controller state transition.

CAN_E_PARAM_BAUDRATE

Invalid Baudrate configuration.

CAN_E_ICOM_CONFIG_INVALID

Invalid ICOM configuration Id.

CAN_E_DATALOST

Error codes returned by Can functions - Run Time Errors.

CAN_ICOM_CONFIG_DISABLE

Icom config disable.

CAN_EXTENDED_ID

Extended id.

CAN_STANDARD_ID

Standard id.

CAN_MIXED_ID

Mixed id.

CAN_CLASSIC_PAYLOAD_MAX_BYTES

Can classic payload max bytes.

CAN_FD_PAYLOAD_MAX_BYTES

Can FD payload max bytes.

CAN_MAX_CONTROLLER_SUPPORTED

Can max controller supported.

CAN_TDCR_TDCF_MAX

Can TDCR and TDCF max

CAN_TDCR_TDCO_MAX

Can TDCR and TDCO max

CAN_ID_STD

Can id STD

CAN_ID_XTD

Can id XTD

CAN_ID_MIXED

Can id MIXED

CAN_XTD_MSGID_MASK

Can XID MSGID mask

CAN_STD_MSGID_MASK

Can STD MSGID mask

CAN_STD_MSGID_SHIFT

Can STD MSGID shift

CAN_ID_CAN_CONTROLLER_TYPE_MASK

Can id can controller type mask

CAN_MSG_TYPE_MASK

Can msg type mask

CAN_MSG_ID_TYPE_EXT

Can msg type mask

CAN_MSG_TYPE_CLASSIC_CAN

Can msg type classic can

CAN_MSG_TYPE_CAN_FD

Can msg type can id

MCAN_MSG_RAM_STD_ELEM_SIZE

Standard ID Filter Element Size.

MCAN_MSG_RAM_EXT_ELEM_SIZE

Extended ID Filter Element Size.

MCAN_MSG_RAM_TX_RX_ELEM_SIZE

Tx/Rx Mailbox Size.

MCAN_TX_BUFFER_MAX_NUM

MCAN IP TX buffer max number.

MCAN_RX_BUFFER_MAX_NUM

MCAN IP RX buffer max number.

MCAN_RX_FIFO_0_MAX_NUM

MCAN rx FIFO_0 max number.

MCAN_RX_FIFO_1_MAX_NUM

MCAN rx FIFO_1 max number.

MCAN_TX_MB_MAX_NUM

MCAN TX_MB max number.

MCAN_RX_MB_MAX_NUM

MCAN RX_MB max number.

CAN_INTR_MASK_ALL

Macro defines mask for all the interrupts status for MCAN.

MCAN_INT_LINE_0

MCAN Interrupt line 0.

MCAN_INT_LINE_1

MCAN Interrupt line 0.

5.1.4. Functions

Return type

Function Name

Brief

void

Can_GetVersionInfo(Std_VersionInfoType * versioninfo)

Function returns the version information of this module.

void

Can_Init(const Can_ConfigType * Config_Ptr)

This function initializes the configuration.

void

Can_DeInit(void )

This function deinitializes the module.

Std_ReturnType

Can_SetBaudrate(uint8 Controller, const uint16 BaudRateConfigID)

This service shall set the baud rate configuration of the CAN Controller.

Std_ReturnType

Can_SetControllerMode(uint8 Controller, Can_ControllerStateType Transition)

This service performs software triggered state transitions of the CAN controller State machine.

void

Can_DisableControllerInterrupts(uint8 Controller)

This service disables all interrupts.

void

Can_EnableControllerInterrupts(uint8 Controller)

This service enables all allowed interrupts.

Std_ReturnType

Can_CheckWakeup(uint8 Controller)

This service checks if a wakeup has occurred for the given controller.

Std_ReturnType

Can_GetControllerErrorState(uint8 Controller, Can_ErrorStateType * ErrorStatePtr)

This service obtains the error state of the CAN controller.

Std_ReturnType

Can_GetControllerMode(uint8 Controller, Can_ControllerStateType * ControllerModePtr)

This service reports about the current status of the requested CAN controller.

Std_ReturnType

Can_Write(uint8 Hth, const Can_PduType * PduInfo)

This service is called by CanIf to pass a CAN message to CanDrv for transmission.

void

Can_MainFunction_Write(uint16 RWFuncID)

This service performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

void

Can_MainFunction_Read(uint16 RWFuncID)

This service performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

void

Can_MainFunction_BusOff(void )

This service performs the polling of bus-off events that are configured statically as ‘to be polled’.

void

Can_MainFunction_Wakeup(void )

This function performs the polling of wake-up events that are configured statically as ‘to be polled’.

void

Can_MainFunction_Mode(void )

This function performs the polling of CAN controller mode transitions.

Std_ReturnType

Can_SetIcomConfiguration(uint8 Controller, IcomConfigIdType ConfigurationId)

This service shall change the Icom Configuration of a CAN controller to the requested one.

void

Can_PeriodicReadback(uint8 Controller, Can_PeriodicReadBackDataType * ReadBackRegisterdata)

This service shall read all the statically configured registers.

void

Can_ResetDrvObjPriv(Can_DriverObjType * drvObj)

This function will reset default Config structure.

void

Can_InitDrvObjPriv(Can_DriverObjType * drvObj, const Can_ConfigType * ConfigPtr)

This function will initialize Driver Config structure.

void

Can_HwUnitConfigPriv(Can_ControllerObjType * canController, const Can_MailboxObjType * canMailbox, uint8 maxMbCnt, uint8 * canHtrhMbMap)

This function will initialize Can HW Unit.

void

Can_MsgRamConfigPriv(uint32 baseAddr, Can_FdMsgRAMConfigObjType * canFDMsgRamConfig)

This API will configure the Message RAM.

void

Can_HWSetBaudRatePriv(uint32 baseAddr, const Can_BaudConfigType * baudConfig)

This API will configure a bit timings for MCAN module.

void

Can_DisableInterruptsPriv(const Can_ControllerType * configParam)

This function will disable MCAN interrupts as per config.

void

Can_EnableInterruptsPriv(const Can_ControllerType * configParam)

This function will enable MCAN interrupts as per config.

void

Can_HwDeInitPriv(const Can_ControllerType * configParam)

This function will de-initialize Can HW Unit.

Can_ErrorStateType

Can_GetProtocolStatusPriv(const Can_ControllerObjType * canController)

This function will fetch Protocol Errors detected by CAN HW Unit.

Std_ReturnType

Can_HWCheckWakeupPriv(const Can_ControllerType * configParam)

This function will fetch Wakeup Status for CAN HW Unit.

Std_ReturnType

Can_HwUnitStartPriv(Can_ControllerObjType * controllerObj, Can_CanIfIndicationType * canIfIndication)

This function will start Can HW Unit.

void

Can_HwUnitStopPriv(Can_ControllerObjType * controllerObj, Can_CanIfIndicationType * canIfIndication)

This function will stop Can HW Unit.

Std_ReturnType

Can_HwUnitSleepPriv(Can_ControllerObjType * controllerObj, Can_CanIfIndicationType * canIfIndication)

This function will sleep Can HW Unit.

Std_ReturnType

Can_HwUnitWakeupPriv(Can_ControllerObjType * controllerObj, Can_CanIfIndicationType * canIfIndication)

This function will wakeup Can HW Unit.

Std_ReturnType

Can_GetFreeTxMsgObjPriv(const Can_MailboxType * mailboxCfg, const Can_ControllerObjType * canController, Can_HwHandleType * msgObj, uint8 htrh)

This function will check if desired Tx mailbox is free.

void

Can_WriteTxMailboxPriv(const Can_MailboxType * mailboxCfg, Can_ControllerObjType * controllerObj, uint8 hth, uint32 messageBox, const Can_PduType * pduInfo)

This function will write into the Transmit Mailbox.

void

Can_HwUnitTxDonePollingPriv(Can_ControllerObjType * canController, const Can_MailboxObjType * canMailbox, uint8 htrh)

This function will poll for Tx confirmation.

void

Can_ReadRxMailboxPriv(Can_ControllerObjType * controllerObj, const Can_MailboxObjType * canMailbox, uint8 maxMbCnt)

This function will read Rx messages from Mailbox.

void

Can_BusOffProcessPriv(Can_ControllerObjType * controllerObj)

This function will inform CanIf if bus off is detected.

void

Can_WakeupProcessPriv(Can_ControllerObjType * controllerObj)

This function will inform EcuM if Wakeup is detected.

void

Can_ModeProcessPriv(Can_ControllerObjType * controllerObj, Can_CanIfIndicationType * indication)

This function will inform CanIf if any mode changes are detected.

void

Can_ProcessLine0ISR(Can_ControllerInstance canInstance, uint32 lineSelect)

void

Can_ProcessLine1ISR(Can_ControllerInstance canInstance, uint32 lineSelect)

void

Can_ProcessWakeUpISR(Can_ControllerInstance instance)

Can_ProcessWakeUpISR: Invoked by the respective CAN controller ISR.

void

Can_PollingCheck(Can_DriverObjType * drvObj, uint8 Controller)

This service disables all interrupts.

void

Can_InterruptCounterCheckPriv(Can_DriverObjType * drvObj, uint8 Controller)

This service enables all allowed interrupts.

void

Can_HwMsgRamConfigPriv(uint32 baseAddr, const Can_MsgRAMConfigParams * msgRAMConfigParams)

This API will configure the Message RAM.

void

Can_AddPdgValFindStdDtlen(const Can_PduType * pduInfo, Can_TxBufElementType * elemPtr, const Can_MailboxType * mailboxCfg)

This function will add padding value to unused to data in payload and find standard data length .

void

Can_CallRxIndication(const boolean RxIndicationStatus, const uint8 htrh, const uint32 canIdentifier, const uint8 canDataLength, Can_ControllerObjType * controllerObj)

This function will Call Receive Indication .

void

Can_CanSetBaudRatePriv(uint32 baseAddr, const Can_BaudConfigType * baudConfig)

This function will configure a bit timings for MCAN module.

Std_ReturnType

Can_ValidateIcomConfigPriv(uint16 loopCnt, const Can_IcomConfigType * icomConfigPtr, uint64 sduData, uint16 rxMessageConfigId)

This function will validate the icom configuration critiria based on rx message configs.

void

Can_CheckTxDelayCompEnablePriv(uint32 baseAddress, const Can_BaudConfigType * baudConfig)

This function will Configure Transceiver Delay Compensation.

void

Can_WriteRxFIFOAckPriv(uint32 baseAddr, uint32 idx)

This API will write acknowledgment for read of Rx FIFO.

Std_ReturnType

Can_IcomSignalOp(const Can_IcomSignalConfigType * signalData, uint64 sduData)

This function will validate the icom configuration critiria based on rx message configs.

void

Can_HwUnitTxConfirmationPriv(uint32 loopCnt, uint32 buffNum, uint8 htrh, Can_ControllerObjType * canController, const Can_MailboxObjType * canMailbox)

This API will Call Tx Confirmation.

uint8

Can_CheckCtrltypeActstMaildir(uint8 maxMbCnt, Can_ControllerObjType * controllerObj, const Can_MailboxObjType * canMailbox, uint8 elemxtd, uint32 canIdentifier)

This function will Check for Controller type and Active state as well as MailBox Direction.

uint8

Can_CheckControllerType(uint8 maxMbCount, Can_RxBufElementType * elm, Can_ControllerObjType * controllerObject, const Can_MailboxObjType * canMailboxObject)

This function will Check for Controller type and Active state as well as MailBox Direction.

void

Can_WriteMsgRamPriv(uint32 baseAddr, uint32 bufNum, const Can_TxBufElementType * elem, const Can_PduType * pdu_Info, const Can_MailboxType * mailBoxConfig)

This API will update data in the Message RAM.

void

Can_ReadMsgRamPriv(uint32 baseAddr, uint32 memType, uint32 bufNum, Can_RxBufElementType * elem)

This API will read data from Message Ram of Can Hw Unit.

void

Can_PeriodicReadbackPrv(uint8 Controller, Can_PeriodicReadBackDataType * ReadBackRegisterdata)

This service shall read all the statically configured registers.

void

Can_EccLoadRegister(uint32 baseAddr, uint32 regOffset)

This service shall load the specific ECC register based on the parameters.

5.1.4.1. function Can_GetVersionInfo

void Can_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: Function returns the version information of this module.

This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported.

Parameters:

  • versioninfo Pointer to where to store the version information of this module.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.2. function Can_Init

void Can_Init(
    const Can_ConfigType * Config_Ptr
)

Brief: This function initializes the configuration.

This function initializes the message RAM, which also clears all the message objects, and places the CAN controller in an init state. Write access to the configuration registers is available as a result, allowing the bit timing and message objects to be setup.

Parameters:

  • ConfigPtr Pointer to post-build configuration data.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.3. function Can_DeInit

void Can_DeInit(
    void 
)

Brief: This function deinitializes the module.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.4. function Can_SetBaudrate

Std_ReturnType Can_SetBaudrate(
    uint8 Controller,
    const uint16 BaudRateConfigID
)

Brief: This service shall set the baud rate configuration of the CAN Controller.

This function sets the baud rate configuration of the CAN controller. Depending on necessary baud rate modifications the controller might have to reset.

Parameters:

  • Controller CAN controller, whose baud rate shall be set.

  • BaudRateConfigID references a baud rate configuration by ID.

Returns:

  • E_OK - Service request accepted, setting of (new) baud rate started.

  • E_NOT_OK - Service request not accepted.

Return: Setting the Baudrate successful or failure.

Precondition: None

Postcondition: None

5.1.4.5. function Can_SetControllerMode

Std_ReturnType Can_SetControllerMode(
    uint8 Controller,
    Can_ControllerStateType Transition
)

Brief: This service performs software triggered state transitions of the CAN controller State machine.

The function perfroms the transition of the CAN controller state machine which is software triggered.

Parameters:

  • Controller CAN controller for which the status shall be changed.

  • Transition Transition value to request new CAN controller state.

Returns:

  • E_OK Request accepted.

  • E_NOT_OK Request not accepted i.e. an error occured while requesting an incorrect from one state to other or an incorrect transition.

Return: Setting the controller mode successful/failure.

Precondition: None

Postcondition: None

5.1.4.6. function Can_DisableControllerInterrupts

void Can_DisableControllerInterrupts(
    uint8 Controller
)

Brief: This service disables all interrupts.

This function checks if there is a DET Error and then disables all the interrupts for the controller.

Parameters:

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.7. function Can_EnableControllerInterrupts

void Can_EnableControllerInterrupts(
    uint8 Controller
)

Brief: This service enables all allowed interrupts.

This function checks the total number of interrupts and enables all the interrupts allowed for the controller.

Parameters:

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.8. function Can_CheckWakeup

Std_ReturnType Can_CheckWakeup(
    uint8 Controller
)

Brief: This service checks if a wakeup has occurred for the given controller.

This function checks if the Init is done and checks if wakeup has occured and returns value accordingly for the given controller.

Parameters:

  • Controller to be checked for a wakeup.

Returns:

  • E_OK API call has been accepted.

  • E_NOT_OK API call has not been accepted.

Return: Wakeup occurred or not for a controller

Precondition: None

Postcondition: None

5.1.4.9. function Can_GetControllerErrorState

Std_ReturnType Can_GetControllerErrorState(
    uint8 Controller,
    Can_ErrorStateType * ErrorStatePtr
)

Brief: This service obtains the error state of the CAN controller.

This function gets the error state of the CAN controller.

Parameters:

  • Controller CAN controller, which is requested for ErrorState.

  • ErrorStatePtr Pointer to a memory location, where the error state of the CAN controller will be stored.

Returns:

  • E_OK - Error state request has been accepted.

  • E_NOT_OK - Error state request has not been accepted..

Return: Error state obtained successfully/failed to obtain error state.

Precondition: None

Postcondition: None

5.1.4.10. function Can_GetControllerMode

Std_ReturnType Can_GetControllerMode(
    uint8 Controller,
    Can_ControllerStateType * ControllerModePtr
)

Brief: This service reports about the current status of the requested CAN controller.

This function gets the current status of the CAN controller.

Parameters:

  • Controller CAN controller, which is requested for ErrorState.

  • ControllerModePtr Pointer to a memory location, where the current mode of the CAN controller will be stored.

Returns:

  • E_OK - Controller mode request has been accepted.

  • E_NOT_OK - Controller mode request has not been accepted.

Return: Able/unable to fetch current status of the controller.

Precondition: None

Postcondition: None

5.1.4.11. function Can_Write

Std_ReturnType Can_Write(
    uint8 Hth,
    const Can_PduType * PduInfo
)

Brief: This service is called by CanIf to pass a CAN message to CanDrv for transmission.

The function Can_Write first checks if the hardware transmit object is identified and is free. It passes the CAN message to CanDrv for transmission.

Parameters:

  • Hth information which HW-transmit handle shall be used for transmit. Implicitly this is also the information about the controller to use because the Hth numbers are unique inside one hardware unit.

  • PduInfo Pointer to SDU user memory, DLC and Identifier.

Returns:

  • E_OK Write command has been accepted.

  • E_NOT_OK Development error occurred.

  • CAN_BUSY No TX hardware buffer available or pre-emptive call of Can_Write that can’t be implemented re-entrant

Return: Can write command is accepted (or) resulted in an error (or) Controller is busy

Precondition: None

Postcondition: None

5.1.4.12. function Can_MainFunction_Write

void Can_MainFunction_Write(
    uint16 RWFuncID
)

Brief: This service performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. For a TX Mailbox if the controller is active polling of TX confirmation is done.

Parameters:

  • RWFuncID Read/Write period ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.13. function Can_MainFunction_Read

void Can_MainFunction_Read(
    uint16 RWFuncID
)

Brief: This service performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. For a Rx Mailbox if the controller is active polling of Rx indications is done.

Parameters:

  • RWFuncID Read/Write period ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.14. function Can_MainFunction_BusOff

void Can_MainFunction_BusOff(
    void 
)

Brief: This service performs the polling of bus-off events that are configured statically as ‘to be polled’.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. If the controller is active the polling of bus-off events that are configured statically as ‘to be polled’.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.15. function Can_MainFunction_Wakeup

void Can_MainFunction_Wakeup(
    void 
)

Brief: This function performs the polling of wake-up events that are configured statically as ‘to be polled’.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. The polling of wake-up events is done.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.16. function Can_MainFunction_Mode

void Can_MainFunction_Mode(
    void 
)

Brief: This function performs the polling of CAN controller mode transitions.

This function checks if Can Initialisation is done to check for error if DET error detect is enabled. The polling of CAN controller mode transitions is done.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.17. function Can_SetIcomConfiguration

Std_ReturnType Can_SetIcomConfiguration(
    uint8 Controller,
    IcomConfigIdType ConfigurationId
)

Brief: This service shall change the Icom Configuration of a CAN controller to the requested one.

Parameters:

  • Controller CAN controller for which the status shall be changed

  • ConfigurationId Requested Configuration

Returns:

  • E_OK CAN driver succeeded in setting a configuration with a valid Configuration id.

  • E_NOT_OK CAN driver failed to set a configuration with a valid Configuration id.

Return: Std_ReturnType

Precondition: None

Postcondition: None

5.1.4.18. function Can_PeriodicReadback

void Can_PeriodicReadback(
    uint8 Controller,
    Can_PeriodicReadBackDataType * ReadBackRegisterdata
)

Brief: This service shall read all the statically configured registers.

Parameters:

  • Controller CAN controller for which the configured registers shall be read

  • ReadBackRegisterdata pointer for the read back registers

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.19. function Can_ResetDrvObjPriv

void Can_ResetDrvObjPriv(
    Can_DriverObjType * drvObj
)

Brief: This function will reset default Config structure.

Parameters:

  • drvObj Pointer to post-build configuration data.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.20. function Can_InitDrvObjPriv

void Can_InitDrvObjPriv(
    Can_DriverObjType * drvObj,
    const Can_ConfigType * ConfigPtr
)

Brief: This function will initialize Driver Config structure.

Parameters:

  • drvObj Pointer to post-build configuration data.

  • ConfigPtr Pointer to Can controllers Config structure.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.21. function Can_HwUnitConfigPriv

void Can_HwUnitConfigPriv(
    Can_ControllerObjType * canController,
    const Can_MailboxObjType * canMailbox,
    uint8 maxMbCnt,
    uint8 * canHtrhMbMap
)

Brief: This function will initialize Can HW Unit.

Parameters:

  • canController Pointer to Can controller Config structure.

  • canMailbox Pointer to Mailbox structure.

  • maxMbCnt Maximum number of mailbox configured.

  • canHtrhMbMap Pointer to Htrh to mailbox mapping.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.22. function Can_MsgRamConfigPriv

void Can_MsgRamConfigPriv(
    uint32 baseAddr,
    Can_FdMsgRAMConfigObjType * canFDMsgRamConfig
)

Brief: This API will configure the Message RAM.

Parameters:

  • baseAddr Base Address of controller.

  • canFDMsgRamConfig Message RAM Configuration parameters.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.23. function Can_HWSetBaudRatePriv

void Can_HWSetBaudRatePriv(
    uint32 baseAddr,
    const Can_BaudConfigType * baudConfig
)

Brief: This API will configure a bit timings for MCAN module.

Parameters:

  • baseAddr Base Address of the MCAN Registers.

  • baudConfig Configuration parameters for MCAN bit timing.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.24. function Can_DisableInterruptsPriv

void Can_DisableInterruptsPriv(
    const Can_ControllerType * configParam
)

Brief: This function will disable MCAN interrupts as per config.

Parameters:

  • configParam Pointer to CAN Controller config parameters.

Returns:

  • None

Return: None

Precondition: Can module must be initialized

Postcondition: None

5.1.4.25. function Can_EnableInterruptsPriv

void Can_EnableInterruptsPriv(
    const Can_ControllerType * configParam
)

Brief: This function will enable MCAN interrupts as per config.

Parameters:

  • configParam Pointer to CAN Controller config parameters.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.26. function Can_HwDeInitPriv

void Can_HwDeInitPriv(
    const Can_ControllerType * configParam
)

Brief: This function will de-initialize Can HW Unit.

Parameters:

  • configParam Pointer to CAN Controller config parameters.

Returns:

  • None

Return: None

Precondition: Can module must be initialized

Postcondition: None

5.1.4.27. function Can_GetProtocolStatusPriv

Can_ErrorStateType Can_GetProtocolStatusPriv(
    const Can_ControllerObjType * canController
)

Brief: This function will fetch Protocol Errors detected by CAN HW Unit.

Parameters:

  • canController Pointer to Can controller Config structure.

Returns:

  • CAN_ERRORSTATE_ACTIVE - If no protocol errors are present.

  • CAN_ERRORSTATE_PASSIVE - If CAN controller is in passive state due to protocol errors.

  • CAN_ERRORSTATE_BUSOFF - If bus off error is detected.

Return: The Can error state when controller is ACTIVE/PASSIVE/BUS-OFF

Precondition: None

Postcondition: None

5.1.4.28. function Can_HWCheckWakeupPriv

Std_ReturnType Can_HWCheckWakeupPriv(
    const Can_ControllerType * configParam
)

Brief: This function will fetch Wakeup Status for CAN HW Unit.

Parameters:

  • configParam Pointer to CAN Controller config parameters.

Returns:

  • TRUE - If CAN HW Unit is in Wakeup.

  • FALSE - If CAN HW Unit is still sleeping.

Return: The status of whether CAN HW Unit is Wakeup/Sleeping

Precondition: Can module must be initialized

Postcondition: None

5.1.4.29. function Can_HwUnitStartPriv

Std_ReturnType Can_HwUnitStartPriv(
    Can_ControllerObjType * controllerObj,
    Can_CanIfIndicationType * canIfIndication
)

Brief: This function will start Can HW Unit.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • canIfIndication Pointer to a struct containing Start/Stop/Sleep/Wakeup controller status to update, CanIf module indication done information

  • canIfIndication Updates, Start successful status to the pointer

Returns:

  • E_OK - If startup is successful.

  • E_NOT_OK - If startup is unsuccessful.

Return: The status of whether starting of Can HW Unit is successful

Precondition: Can module must be initialized

Postcondition: None

5.1.4.30. function Can_HwUnitStopPriv

void Can_HwUnitStopPriv(
    Can_ControllerObjType * controllerObj,
    Can_CanIfIndicationType * canIfIndication
)

Brief: This function will stop Can HW Unit.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • canIfIndication Pointer to a struct containing Start/Stop/Sleep/Wakeup controller status to update, CanIf module indication done information

  • canIfIndication Updates, Stop successful status to the pointer

Returns:

  • None

Return: The status of whether stopping of Can HW Unit is successful

Precondition: Can module must be initialized

Postcondition: None

5.1.4.31. function Can_HwUnitSleepPriv

Std_ReturnType Can_HwUnitSleepPriv(
    Can_ControllerObjType * controllerObj,
    Can_CanIfIndicationType * canIfIndication
)

Brief: This function will sleep Can HW Unit.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • canIfIndication Pointer to a struct containing Start/Stop/Sleep/Wakeup controller status to update, CanIf module indication done information

  • canIfIndication Updates, Sleep successful status to the pointer

Returns:

  • E_OK - If sleep is successful.

  • E_NOT_OK - If sleep is unsuccessful.

Return: The status of whether sleep of Can HW Unit is successful

Precondition: Can module must be initialized

Postcondition: None

5.1.4.32. function Can_HwUnitWakeupPriv

Std_ReturnType Can_HwUnitWakeupPriv(
    Can_ControllerObjType * controllerObj,
    Can_CanIfIndicationType * canIfIndication
)

Brief: This function will wakeup Can HW Unit.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • canIfIndication Pointer to a struct containing Start/Stop/Sleep/Wakeup controller status to update, CanIf module indication done information

  • canIfIndication Updates, Wakeup successful status to the pointer

Returns:

  • E_OK - If wakeup is successful.

  • E_NOT_OK - If wakeup is unsuccessful.

Return: The status of whether wakeup of Can HW Unit is successful

Precondition: Can module must be initialized

Postcondition: None

5.1.4.33. function Can_GetFreeTxMsgObjPriv

Std_ReturnType Can_GetFreeTxMsgObjPriv(
    const Can_MailboxType * mailboxCfg,
    const Can_ControllerObjType * canController,
    Can_HwHandleType * msgObj,
    uint8 htrh
)

Brief: This function will check if desired Tx mailbox is free.

Parameters:

  • mailboxCfg Pointer to Mailbox structure.

  • canController Pointer to Can controller Config structure.

  • msgObj HW object in the controller.

  • htrh HW object in the configuration.

Returns:

  • E_OK - If free message object is found.

  • E_NOT_OK - If free message object is not found.

  • CAN_BUSY - If message is already pending.

Return: The status of Tx mailbox free/busy/not-found

Precondition: Can module must be initialized

Postcondition: None

5.1.4.34. function Can_WriteTxMailboxPriv

void Can_WriteTxMailboxPriv(
    const Can_MailboxType * mailboxCfg,
    Can_ControllerObjType * controllerObj,
    uint8 hth,
    uint32 messageBox,
    const Can_PduType * pduInfo
)

Brief: This function will write into the Transmit Mailbox.

Parameters:

  • mailboxCfg Pointer to Mailbox structure.

  • controllerObj Pointer to Can controller Config structure.

  • hth HW object in the configuration.

  • messageBox HW object in the controller.

  • pduInfo Pointer to SDU user memory, DLC and Identifier.

Returns:

  • None

Return: None

Precondition: Can module must be initialized

Postcondition: None

5.1.4.35. function Can_HwUnitTxDonePollingPriv

void Can_HwUnitTxDonePollingPriv(
    Can_ControllerObjType * canController,
    const Can_MailboxObjType * canMailbox,
    uint8 htrh
)

Brief: This function will poll for Tx confirmation.

Parameters:

  • canController Pointer to Can controller Config structure.

  • mailboxCfg Pointer to Mailbox structure.

  • htrh HW object in the configuration.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.36. function Can_ReadRxMailboxPriv

void Can_ReadRxMailboxPriv(
    Can_ControllerObjType * controllerObj,
    const Can_MailboxObjType * canMailbox,
    uint8 maxMbCnt
)

Brief: This function will read Rx messages from Mailbox.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • canMailbox Pointer to Mailbox structure.

  • maxMbCnt Maximum number of mailbox configured.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.37. function Can_BusOffProcessPriv

void Can_BusOffProcessPriv(
    Can_ControllerObjType * controllerObj
)

Brief: This function will inform CanIf if bus off is detected.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.38. function Can_WakeupProcessPriv

void Can_WakeupProcessPriv(
    Can_ControllerObjType * controllerObj
)

Brief: This function will inform EcuM if Wakeup is detected.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.39. function Can_ModeProcessPriv

void Can_ModeProcessPriv(
    Can_ControllerObjType * controllerObj,
    Can_CanIfIndicationType * indication
)

Brief: This function will inform CanIf if any mode changes are detected.

Parameters:

  • controllerObj Pointer to Can controller Config structure.

  • indication Pointer to a struct containing Start/Stop/Sleep/Wakeup controller status indication done to CanIf module

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.40. function Can_ProcessLine0ISR

void Can_ProcessLine0ISR(
    Can_ControllerInstance canInstance,
    uint32 lineSelect
)

5.1.4.41. function Can_ProcessLine1ISR

void Can_ProcessLine1ISR(
    Can_ControllerInstance canInstance,
    uint32 lineSelect
)

5.1.4.42. function Can_ProcessWakeUpISR

void Can_ProcessWakeUpISR(
    Can_ControllerInstance instance
)

Brief: Can_ProcessWakeUpISR: Invoked by the respective CAN controller ISR.

This Interrupt function is invoked when CAN wakeup event occur for a controller, inside the respective Controller ISR, when the interrupts for the controller are enabled.

Parameters:

  • instance the Can Controller Instance ID

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.43. function Can_PollingCheck

void Can_PollingCheck(
    Can_DriverObjType * drvObj,
    uint8 Controller
)

Brief: This service disables all interrupts.

This function checks if there is a DET Error and then disables all the interrupts for the controller.

Parameters:

  • drvObj Pointer to Can controller Config structure.

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.44. function Can_InterruptCounterCheckPriv

void Can_InterruptCounterCheckPriv(
    Can_DriverObjType * drvObj,
    uint8 Controller
)

Brief: This service enables all allowed interrupts.

This function checks the total number of interrupts and enables all the interrupts allowed for the controller.

Parameters:

  • drvObj Pointer to Can controller Config structure.

  • Controller CAN controller for which interrupts shall be re-enabled.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.45. function Can_HwMsgRamConfigPriv

void Can_HwMsgRamConfigPriv(
    uint32 baseAddr,
    const Can_MsgRAMConfigParams * msgRAMConfigParams
)

Brief: This API will configure the Message RAM.

Parameters:

  • baseAddr Base Address of controller.

  • msgRAMConfigParams Message RAM Configuration parameters.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.46. function Can_AddPdgValFindStdDtlen

void Can_AddPdgValFindStdDtlen(
    const Can_PduType * pduInfo,
    Can_TxBufElementType * elemPtr,
    const Can_MailboxType * mailboxCfg
)

Brief: This function will add padding value to unused to data in payload and find standard data length .

Parameters:

  • pduInfo Base Address of controller.

  • elemPtr Pointer to location to store value read.

  • mailboxCfg Mailbox Configuration parameters.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.47. function Can_CallRxIndication

void Can_CallRxIndication(
    const boolean RxIndicationStatus,
    const uint8 htrh,
    const uint32 canIdentifier,
    const uint8 canDataLength,
    Can_ControllerObjType * controllerObj
)

Brief: This function will Call Receive Indication .

Parameters:

  • RxIndicationStatus Receive indication status.

  • controllerObj Pointer to Can controller config parameters.

  • canIdentifier Holds Can Identifier value.

  • htrh Handle ID of HTH.

  • canDataLength Frame length of msg.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.48. function Can_CanSetBaudRatePriv

void Can_CanSetBaudRatePriv(
    uint32 baseAddr,
    const Can_BaudConfigType * baudConfig
)

Brief: This function will configure a bit timings for MCAN module.

Parameters:

  • baseAddr Base Address of controller.

  • baudConfig Configuration parameters for MCAN bit timing.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.49. function Can_ValidateIcomConfigPriv

Std_ReturnType Can_ValidateIcomConfigPriv(
    uint16 loopCnt,
    const Can_IcomConfigType * icomConfigPtr,
    uint64 sduData,
    uint16 rxMessageConfigId
)

Brief: This function will validate the icom configuration critiria based on rx message configs.

Parameters:

  • loopCnt Signal Count.

  • icomConfigPtr Pointer to Icom data structure containing the overall ICOM configuration data.

  • sduData Hold sdu data.

  • rxMessageConfigId Indidicates Receive Message Id.

Returns:

  • E_OK - If icom configuration matched.

  • E_NOT_OK - If icom configuration not matched.

Return: The status of whether the icom configuration critiria matched or not

Precondition: None

Postcondition: None

5.1.4.50. function Can_CheckTxDelayCompEnablePriv

void Can_CheckTxDelayCompEnablePriv(
    uint32 baseAddress,
    const Can_BaudConfigType * baudConfig
)

Brief: This function will Configure Transceiver Delay Compensation.

Parameters:

  • baseAddr Base Address of controller.

  • baudConfig Configuration parameters for MCAN bit timing.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.51. function Can_WriteRxFIFOAckPriv

void Can_WriteRxFIFOAckPriv(
    uint32 baseAddr,
    uint32 idx
)

Brief: This API will write acknowledgment for read of Rx FIFO.

Parameters:

  • baseAddr Base Address of controller.

  • idx FIFO element ID.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.52. function Can_IcomSignalOp

Std_ReturnType Can_IcomSignalOp(
    const Can_IcomSignalConfigType * signalData,
    uint64 sduData
)

Brief: This function will validate the icom configuration critiria based on rx message configs.

Parameters:

  • signalData Hold Icom signal config data

  • sduData Hold sdu data.

Returns:

  • E_OK - If icom Signal Operation configuration matched.

  • E_NOT_OK - If icom Signal Operation configuration not matched.

Return: The status of whether the icom configuration critiria matched or not

Precondition: None

Postcondition: None

5.1.4.53. function Can_HwUnitTxConfirmationPriv

void Can_HwUnitTxConfirmationPriv(
    uint32 loopCnt,
    uint32 buffNum,
    uint8 htrh,
    Can_ControllerObjType * canController,
    const Can_MailboxObjType * canMailbox
)

Brief: This API will Call Tx Confirmation.

Parameters:

  • loopCnt Tx number of buffer elements.

  • buffNum Tx number of buffer and FIFO elements.

  • canController Pointer to Can controller config parameters.

  • canMailbox Message RAM Configuration parameters.

  • htrh Handle ID of HTH.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.54. function Can_CheckCtrltypeActstMaildir

uint8 Can_CheckCtrltypeActstMaildir(
    uint8 maxMbCnt,
    Can_ControllerObjType * controllerObj,
    const Can_MailboxObjType * canMailbox,
    uint8 elemxtd,
    uint32 canIdentifier
)

Brief: This function will Check for Controller type and Active state as well as MailBox Direction.

Parameters:

  • maxMbCnt Maximum number of Mailbox to be configured.

  • controllerObj Pointer to Can controller config parameters.

  • canMailbox Message RAM Configuration parameters..

  • elemxtd Extended Identifier of CAN Rx Buffer element

  • canIdentifier Holds Can Identifier value

Returns:

  • returns the value of type uint8

Return: returns the value of uint8

Precondition: None

Postcondition: None

5.1.4.55. function Can_CheckControllerType

uint8 Can_CheckControllerType(
    uint8 maxMbCount,
    Can_RxBufElementType * elm,
    Can_ControllerObjType * controllerObject,
    const Can_MailboxObjType * canMailboxObject
)

Brief: This function will Check for Controller type and Active state as well as MailBox Direction.

Parameters:

  • maxMbCount Maximum number of Mailbox to be configured.

  • elm Pointer to location to store value read.

  • controllerObject Pointer to Can controller config parameters.

  • canMailboxObject Message RAM Configuration parameters.

Returns:

  • returns the value of type uint8

Return: returns htrh value

Precondition: None

Postcondition: None

5.1.4.56. function Can_WriteMsgRamPriv

void Can_WriteMsgRamPriv(
    uint32 baseAddr,
    uint32 bufNum,
    const Can_TxBufElementType * elem,
    const Can_PduType * pdu_Info,
    const Can_MailboxType * mailBoxConfig
)

Brief: This API will update data in the Message RAM.

Parameters:

  • baseAddr Base Address of controller.

  • buffNum Transmit Buffer number.

  • elem Pointer to the data to be written in Message RAM.

Returns:

  • None

Return: None

Precondition: Can module must be initialized

Postcondition: None

5.1.4.57. function Can_ReadMsgRamPriv

void Can_ReadMsgRamPriv(
    uint32 baseAddr,
    uint32 memType,
    uint32 bufNum,
    Can_RxBufElementType * elem
)

Brief: This API will read data from Message Ram of Can Hw Unit.

Parameters:

  • baseAddr Base Address of controller.

  • memType Base Address of controller.

  • bufNum Transmit Buffer number.

  • elem Pointer to location to store value read.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.58. function Can_PeriodicReadbackPrv

void Can_PeriodicReadbackPrv(
    uint8 Controller,
    Can_PeriodicReadBackDataType * ReadBackRegisterdata
)

Brief: This service shall read all the statically configured registers.

Parameters:

  • Controller CAN controller for which the configured registers shall be read

  • ReadBackRegisterdata pointer for the read back registers

Returns:

  • None

Return: None

Precondition: None

Postcondition: None

5.1.4.59. function Can_EccLoadRegister

void Can_EccLoadRegister(
    uint32 baseAddr,
    uint32 regOffset
)

Brief: This service shall load the specific ECC register based on the parameters.

Parameters:

  • baseAddr CAN controller base address.

  • regOffset regOffset for the register to load.

Returns:

  • None

Return: None

Precondition: None

Postcondition: None