5.7. PORT
5.7.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Enum of Port Direction. |
|
enum |
Enum of Port Pin Level. |
|
enum |
Enum of Port Pin Pad, Up/Down Type selection. |
|
enum |
Values that can be passed to set qualification parameter to initialize MCU module. |
|
enum |
Values that can be passed to select master core for MCU module. |
|
enum |
Values that can be passed to set the mode in which Pin should operate. |
|
typedef uint32 |
Type for symbolic name of Port pins. |
|
typedef uint32 |
Pin Mode type structure. |
|
typedef uint8 |
Type for Pin Config Flag. Pin config flags Bit 0 - Is Pin configurable? Bit 1 - Does Pin support Analog Mode? Bit 2 - Does Pin operate in AGPIO mode? Bit 3 - Does Pin operate in AIO mode? Bit 4 - Does Pin operate in GPIO mode? |
5.7.1.1. enum Port_PinDirectionType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_IN |
Direction IN. |
|
PORT_PIN_OUT |
Direction OUT. |
|
PORT_PIN_NA |
NA Direction. |
Brief: Enum of Port Direction.
5.7.1.2. enum Port_PinLevelValueType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_LEVEL_HIGH |
Pin Level HIGH. |
|
PORT_PIN_LEVEL_LOW |
Pin Level LOW. |
|
PORT_PIN_LEVEL_NA |
Pin Level NA. |
Brief: Enum of Port Pin Level.
5.7.1.3. enum Port_PinPadConfigType
Enumerator |
Value |
Description |
|---|---|---|
PORT_PIN_TYPE_STD |
1U |
Standard pad configuration with pull up disable. |
PORT_PIN_TYPE_PULLUP |
2U |
Enable pull up for the pin. |
PORT_PIN_TYPE_STD_PULLUP |
3U |
Standard pad configuration with pull up enable. |
PORT_PIN_TYPE_OPEN_DRAIN |
4U |
Open Drain pad configuration with pull up disable. |
PORT_PIN_TYPE_OPEN_DRAIN_PULLUP |
6U |
Open Drain pad configuration with pull up enable. |
PORT_PIN_TYPE_NA |
255U |
No pad configuration. |
Brief: Enum of Port Pin Pad, Up/Down Type selection.
5.7.1.4. enum Port_PinQualificationMode
Enumerator |
Value |
Description |
|---|---|---|
PORT_QUAL_SYNC |
Synchronization to SYSCLKOUT. |
|
PORT_QUAL_3SAMPLE |
Qualified with 3 samples. |
|
PORT_QUAL_6SAMPLE |
Qualified with 6 samples. |
|
PORT_QUAL_ASYNC |
No synchronization. |
|
PORT_QUAL_NA |
Invalid synchronization. |
Brief: Values that can be passed to set qualification parameter to initialize MCU module.
5.7.1.5. enum Port_PinCoreSelect
Enumerator |
Value |
Description |
|---|---|---|
PORT_CORE_CPU1 |
CPU1 selected as master core. |
|
PORT_CORE_CPU2 |
CPU2 selected as master core. |
|
PORT_CORE_CPU3 |
CPU3 selected as master core. |
Brief: Values that can be passed to select master core for MCU module.
5.7.1.6. enum Port_AnalogModeType
Enumerator |
Value |
Description |
|---|---|---|
PORT_ANALOG_DISABLED |
Pin is in digital mode. |
|
PORT_ANALOG_ENABLED |
Pin is in analog mode. |
Brief: Values that can be passed to set the mode in which Pin should operate.
5.7.1.7. typedef Port_PinType
typedef uint32 Port_PinType;
Brief: Type for symbolic name of Port pins.
5.7.1.8. typedef Port_PinModeType
typedef uint32 Port_PinModeType;
Brief: Pin Mode type structure.
5.7.1.9. typedef Port_PinConfigFlagType
typedef uint8 Port_PinConfigFlagType;
Brief: Type for Pin Config Flag. Pin config flags Bit 0 - Is Pin configurable? Bit 1 - Does Pin support Analog Mode? Bit 2 - Does Pin operate in AGPIO mode? Bit 3 - Does Pin operate in AIO mode? Bit 4 - Does Pin operate in GPIO mode?
5.7.2. Structures
Name |
Brief |
|---|---|
Pin Mux Mode Config type structure. |
|
Pin Configuration structure. |
|
PORT Module ROOT configuration. |
|
Controller Specific structure. |
5.7.3. Defines
Name |
Brief |
|---|---|
PORT_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
PORT_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
PORT_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
PORT_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by PORT Driver. |
PORT_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by PORT Driver. |
PORT_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by PORT Driver. |
PORT_VENDOR_ID |
Texas Instruments Vendor ID. |
PORT_MODULE_ID |
PORT Driver Module ID. |
PORT_INSTANCE_ID |
PORT Driver Instance ID. |
PORT_E_PARAM_PIN |
Invalid Port Pin ID requested. |
PORT_E_DIRECTION_UNCHANGEABLE |
Port Pin not configured as changeable. |
PORT_E_INIT_FAILED |
API Port_Init service called with wrong parameter. |
PORT_E_PARAM_INVALID_MODE |
API Port_SetPinMode service called when mode is unchangeable. |
PORT_E_MODE_UNCHANGEABLE |
API Port_SetPinMode service called when mode is unchangeable. |
PORT_E_UNINIT |
API service called without module initialization. |
PORT_E_PARAM_POINTER |
APIs called with a Null pointer. |
PORT_SID_INIT |
Service ID - Port_Init(). |
PORT_SID_SET_PIN_DIR |
Service ID - Port_SetPinDirection(). |
PORT_SID_REFRESH_PORT_DIR |
Service ID - Port_RefreshPortDirection() |
PORT_SID_GET_VERSION_INFO |
Service ID - Port_GetVersionInfo(). |
PORT_SID_SET_PIN_MODE |
Service ID - Port_SetPinMode(). |
PORT_SID_COMMIT_CONFIGURATION |
Service ID - Port_CommitConfiguration(). |
PORT_IS_PIN_CONFIGURABLE (x) |
Pin configuration check. |
PORT_IS_ANALOG_MODE_SUPPORTED (x) |
Pin Analog Support check. |
PORT_IS_PIN_AGPIO (x) |
AGPIO Pin check. |
PORT_IS_PIN_AIO (x) |
AIO Pin check. |
PORT_IS_PIN_GPIO (x) |
GPIO Pin check. |
PORT_WIDTH |
Port Width : 32. |
PORT_WIDTH_HALF |
Half of Port Width. |
PORT_WIDTH_QUARTER |
Quarter of Port Width. |
ONE_BIT_MASK |
One bit mask value. |
TWO_BIT_MASK |
Two bit mask value. |
AGPIO_PINS_START_VALUE |
AGPIO Pin start Value. |
PORT_CTRL_REGS_STEP |
Port Control register step size. |
PORT_DATA_REGS_STEP |
Port Data register step size. |
PORT_DATA_READ_REGS_STEP |
Port Data read register step size. |
PORT_CTRL_REGS_INDEX |
Port Control register Index value. |
PORT_QSEL_REGS_INDEX |
Port Q-Select register Index value. |
PORT_MUX_REGS_INDEX |
Port MUX register Index value. |
PORT_PUD_REGS_INDEX |
Port Pull up disable register Index value. |
PORT_INV_REGS_INDEX |
Port Invert polarity register Index value. |
PORT_ODR_REGS_INDEX |
Port Open drain register Index value. |
PORT_AMSEL_REGS_INDEX |
Port AM Select register Index value. |
PORT_GMUX_REGS_INDEX |
Port GMUX register Index value. |
PORT_CSEL_REGS_INDEX |
Port Core Select register Index value. |
PORT_LOCK_REGS_INDEX |
Port Lock configuration register Index value. |
PORT_CR_REGS_INDEX |
Port lock commit register Index value. |
PORT_DAT_REGS_INDEX |
Port Data register Index value. |
PORT_SET_REGS_INDEX |
Port Data Set register Index value. |
PORT_CLEAR_REGS_INDEX |
Port Data Clear register Index value. |
PORT_TOGGLE_REGS_INDEX |
Port Data Toggle register Index value. |
PORT_DIR_REGS_INDEX |
Port Data Direction Set register Index value. |
GPIO_DAT_R_REGS_INDEX |
Port Data read register Index value. |
PORT_MUX_TO_GMUX |
Port MUX to GMUX difference value. |
5.7.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Port_Init(const Port_ConfigType * CfgPtr) |
Initializes the Port Driver module. |
void |
Port_SetPinDirection(Port_PinType Pin, Port_PinDirectionType Direction) |
Sets the port pin direction. |
void |
Port_RefreshPortDirection(void ) |
Refreshes port direction. |
void |
Port_GetVersionInfo(Std_VersionInfoType * versioninfo) |
Service to get the version information of the module. |
void |
Port_SetPinMode(Port_PinType Pin, Port_PinModeType Mode) |
Sets the port pin mode. |
void |
Port_CommitConfiguration(void ) |
Commits the locked Critical Configuration registers for the current Configuration. |
Std_ReturnType |
Port_SetCntSpConfig(const Port_PinConfigType * PinConfigPtr) |
Sets the pad/pull configuration for the specified pin. |
Std_ReturnType |
Port_SetPinLevel(const Port_PinConfigType * PinConfigPtr, Port_PinLevelValueType PinLevel) |
Writes the level value to the specified pin. |
Std_ReturnType |
Port_EnableLPMWakeUpPin(const Port_PinConfigType * PinConfig) |
Set pins as Low Power wakeup modes GPIO pins. |
void |
Port_SetPinModeConfig(uint32 PinMode) |
Configures the Pin Mode function of a PORT pin. |
Std_ReturnType |
Port_SetDirectionMode(const Port_PinConfigType * PinConfigPtr, Port_PinDirectionType PinDirection) |
Sets the direction of the specified pin. |
Std_ReturnType |
Port_IsPinNumberValid(Port_PinType PinNumber) |
Checks if the provided pin number is Valid or Not. |
Std_ReturnType |
Port_ValidateSetPinMode(Port_PinModeType Mode, const Port_PinConfigType * pinConfig, uint8 * errorIdPtr) |
Validates the pin Mode provided. |
void |
Port_LockConfiguration(const Port_PinConfigType * pinConfig) |
Locks the Critical Configuration registers for the passed Pin. |
void |
Port_UnlockConfiguration(const Port_PinConfigType * pinConfig) |
Unlocks the Critical Configuration registers for the passed Pin. |
void |
Port_CommitConfigurationProcess(Port_PinType pinNumber) |
Locks and Commit the Critical Configuration registers for the passed Pin. |
5.7.4.1. function Port_Init
void Port_Init(
const Port_ConfigType * CfgPtr
)
Brief: Initializes the Port Driver module.
This function is called by user to initialize the Port pins of the microcontroller
Parameters:
CfgPtr is the configuration pointer for Port module.
None
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.7.4.2. function Port_SetPinDirection
void Port_SetPinDirection(
Port_PinType Pin,
Port_PinDirectionType Direction
)
Brief: Sets the port pin direction.
This function is used to change the direction of the pin during runtime.
Parameters:
Pin is the symbolic name of the pin.
Direction is the direction to which pin is to be set.
None
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.3. function Port_RefreshPortDirection
void Port_RefreshPortDirection(
void
)
Brief: Refreshes port direction.
This function refreshes the Port pins to their initial direction. Pins whose direction can be changed during runtime are excluded from this action.
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.4. function Port_GetVersionInfo
void Port_GetVersionInfo(
Std_VersionInfoType * versioninfo
)
Brief: Service to get the version information of the module.
This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter PORT_CFG_GET_VERSION_INFO_API is enabled.
Parameters:
Versioninfo structure that contains the version information parameters.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.7.4.5. function Port_SetPinMode
void Port_SetPinMode(
Port_PinType Pin,
Port_PinModeType Mode
)
Brief: Sets the port pin mode.
This function is used to change the Mode of the pin during runtime.
Parameters:
Pin is the symbolic name of the pin.
Mode is desired functionality of the Pin e.g. PORT_PIN_MODE_ADC, PORT_PIN_MODE_DIO etc.
Returns:
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.6. function Port_CommitConfiguration
void Port_CommitConfiguration(
void
)
Brief: Commits the locked Critical Configuration registers for the current Configuration.
This function Commits the locked Critical Configuration registers for the current Configuration
Parameters:
None
Returns:
None
None
Return: None
Precondition: Port_Init should be called before calling this function
Postcondition: None
5.7.4.7. function Port_SetCntSpConfig
Std_ReturnType Port_SetCntSpConfig(
const Port_PinConfigType * PinConfigPtr
)
Brief: Sets the pad/pull configuration for the specified pin.
This function sets the controller specific parameters for the specified pin. The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as PinNumber.
Parameters:
PinConfigPtr is the pointer to the pin config structure.
returnvalue
Returns:
E_OK if pad configuration is success
E_NOT_OK if pad configuration Fails
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.8. function Port_SetPinLevel
Std_ReturnType Port_SetPinLevel(
const Port_PinConfigType * PinConfigPtr,
Port_PinLevelValueType PinLevel
)
Brief: Writes the level value to the specified pin.
Writes the corresponding bit values to the output pin specified by PinNumber. Writing to a pin configured as an input pin has no effect.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as PinNumber.
Parameters:
PinConfigPtr is the pointer to the pin config structure.
PinLevel is the value to write to the pin.
returnvalue
Returns:
E_OK if Level Set success
E_NOT_OK if Level Set Fails
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.9. function Port_EnableLPMWakeUpPin
Std_ReturnType Port_EnableLPMWakeUpPin(
const Port_PinConfigType * PinConfig
)
Brief: Set pins as Low Power wakeup modes GPIO pins.
This function Writes the corresponding bit values to the LPM registers.
Parameters:
controllerSpecificPtr is the structure containing LPM details.
returnvalue
Returns:
E_OK if Wakeup Enable is success
E_NOT_OK if Wakeup Enable is failure
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.10. function Port_SetPinModeConfig
void Port_SetPinModeConfig(
uint32 PinMode
)
Brief: Configures the Pin Mode function of a PORT pin.
This function configures the pin mux that selects the peripheral function associated with a particular PORT pin. Only one peripheral function at a time can be associated with a PORT pin, and each peripheral function should only be associated with a single PORT pin at a time (despite the fact that many of them can be associated with more than one PORT pin).
The available mappings are supplied in Port_Pin_Map.h
Parameters:
PinMode is the pin configuration value for pin
returnvalue
Returns:
None
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.11. function Port_SetDirectionMode
Std_ReturnType Port_SetDirectionMode(
const Port_PinConfigType * PinConfigPtr,
Port_PinDirectionType PinDirection
)
Brief: Sets the direction of the specified pin.
This function configures the specified pin on the selected GPIO port as either input or output.
The parameter PinDirection is an enumerated data type that can be one of the following values:
PORT_PIN_IN
PORT_PIN_OUT
where PORT_PIN_IN specifies that the pin is programmed as an input and PORT_PIN_OUT specifies that the pin is programmed as an output.
The pin is specified by its numerical value. For example, GPIO34 is specified by passing 34 as pin.
Parameters:
PinConfigPtr is the pointer to the pin config structure.
PinDirection is the pin direction mode.
Returns:
E_OK if pin direction is set successfully.
E_NOT_OK if pin direction is Not set successfully.
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.12. function Port_IsPinNumberValid
Std_ReturnType Port_IsPinNumberValid(
Port_PinType PinNumber
)
Brief: Checks if the provided pin number is Valid or Not.
This function Checks if the pin number provided in the configuration is valid or not.
Parameters:
PinNumber is the pin num value provided in the pin configuration
returnvalue
Returns:
E_OK if pin number is valid.
E_NOT_OK if pin number is not valid.
Return: returnValue
Precondition: None
Postcondition: None
5.7.4.13. function Port_ValidateSetPinMode
Std_ReturnType Port_ValidateSetPinMode(
Port_PinModeType Mode,
const Port_PinConfigType * pinConfig,
uint8 * errorIdPtr
)
Brief: Validates the pin Mode provided.
This function checks with the Pin mode provided for the particular pin config is valid mode or not
Parameters:
Mode is the Mode passed to Pin
pinConfig is the Pointer having pin config
errorIdPtr is the error pointer
retVal
Returns:
E_OK if valid mode is provided
E_NOT_OK if mode provided is not valid
Return: retVal
Precondition: None
Postcondition: None
5.7.4.14. function Port_LockConfiguration
void Port_LockConfiguration(
const Port_PinConfigType * pinConfig
)
Brief: Locks the Critical Configuration registers for the passed Pin.
This function Locks the Critical Configuration registers for the passed Pin
Parameters:
pinConfig is the Pointer having pin config
Returns:
None
None
Return: None
Precondition: None
Postcondition: None
5.7.4.15. function Port_UnlockConfiguration
void Port_UnlockConfiguration(
const Port_PinConfigType * pinConfig
)
Brief: Unlocks the Critical Configuration registers for the passed Pin.
This function Unlocks the Critical Configuration registers for the passed Pin
Parameters:
pinConfig is the Pointer having pin config
Returns:
None
None
Return: None
Precondition: None
Postcondition: None
5.7.4.16. function Port_CommitConfigurationProcess
void Port_CommitConfigurationProcess(
Port_PinType pinNumber
)
Brief: Locks and Commit the Critical Configuration registers for the passed Pin.
This function Locks and Commit the Critical Configuration registers for the passed Pin
Parameters:
pinNumber Pin Number
Returns:
None
None
Return: None
Precondition: None
Postcondition: None