5.2. DIO
5.2.1. Types
Base type |
Type Name |
Brief |
|---|---|---|
typedef uint32 |
Numeric ID of a DIO channel. |
|
typedef uint32 |
Numeric ID of a DIO port. |
|
typedef uint8 |
These are the possible levels a DIO channel can have (input or output). |
|
typedef uint32 |
If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port. |
5.2.1.1. typedef Dio_ChannelType
typedef uint32 Dio_ChannelType;
Brief: Numeric ID of a DIO channel.
5.2.1.2. typedef Dio_PortType
typedef uint32 Dio_PortType;
Brief: Numeric ID of a DIO port.
5.2.1.3. typedef Dio_LevelType
typedef uint8 Dio_LevelType;
Brief: These are the possible levels a DIO channel can have (input or output).
5.2.1.4. typedef Dio_PortLevelType
typedef uint32 Dio_PortLevelType;
Brief: If the uC owns ports of different port widths Dio_PortLevelType inherits the size of the largest port.
5.2.2. Structures
Name |
Brief |
|---|---|
Type definition for identifying channel groups (meaning a set of pins in one port). |
5.2.3. Defines
Name |
Brief |
|---|---|
DIO_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
DIO_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
DIO_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
DIO_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by DIO Driver. |
DIO_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by DIO Driver. |
DIO_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by DIO Driver. |
DIO_VENDOR_ID |
Texas Instruments Vendor ID. |
DIO_MODULE_ID |
DIO Driver Module ID. |
DIO_INSTANCE_ID |
DIO Driver Instance ID. |
DIO_E_PARAM_INVALID_CHANNEL_ID |
API service called with invalid channel ID. |
DIO_E_PARAM_INVALID_PORT_ID |
API service called with invalid port ID. |
DIO_E_PARAM_INVALID_GROUP |
API service called with invalid channel group ID. |
DIO_E_PARAM_POINTER |
Dio_GetVersionInfo() called with NULL_PTR as parameter. |
DIO_SID_READ_CHANNEL |
Dio_ReadChannel() |
DIO_SID_WRITE_CHANNEL |
Dio_WriteChannel() |
DIO_SID_READ_PORT |
Dio_ReadPort() |
DIO_SID_WRITE_PORT |
Dio_WritePort() |
DIO_SID_READ_CHANNEL_GROUP |
Dio_ReadChannelGroup() |
DIO_SID_WRITE_CHANNEL_GROUP |
Dio_WriteChannelGroup() |
DIO_SID_FLIP_CHANNEL |
Dio_FlipChannel() |
DIO_SID_GET_VERSION_INFO |
Dio_GetVersionInfo() |
GPIO_DATA_INDEX |
Index of GPIO_DATA register for a port registers set. |
GPIO_TOGGLE_INDEX |
Index of GPIO_TOGGLE register for a port registers set. |
GPIO_CLEAR_INDEX |
Index of GPIO_CLEAR register for a port registers set. |
GPIO_SET_INDEX |
Index of GPIO_SET register for a port registers set. |
GPIO_DATA_REGS_STEP |
Port Data register step size. |
DIO_PORT_WIDTH |
Width of GPIO register in this platform. |
GPIO_PORT_A |
GPIO PORT A identifier. |
GPIO_PORT_B |
GPIO PORT B identifier. |
GPIO_PORT_C |
GPIO PORT C identifier. |
GPIO_PORT_D |
GPIO PORT D identifier. |
GPIO_PORT_E |
GPIO PORT E identifier. |
GPIO_PORT_F |
GPIO PORT F identifier. |
GPIO_PORT_G |
GPIO PORT G identifier. |
GPIO_PORT_H |
GPIO PORT H identifier. |
5.2.4. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Dio_GetVersionInfo(Std_VersionInfoType * Versioninfo) |
Service to get the version information of the module. |
Dio_ReadChannel(Dio_ChannelType ChannelId) |
Returns the value of the specified DIO channel. |
|
void |
Dio_WriteChannel(Dio_ChannelType ChannelId, Dio_LevelType Level) |
Service to set a level of a channel. |
Dio_ReadPort(Dio_PortType PortId) |
Returns the level of all channels of that port. |
|
void |
Dio_WritePort(Dio_PortType PortId, Dio_PortLevelType Level) |
Service to set a value of the port. |
Dio_ReadChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr) |
This Service reads a subset of the adjoining bits of a port. |
|
void |
Dio_WriteChannelGroup(const Dio_ChannelGroupType * ChannelGroupIdPtr, Dio_PortLevelType Level) |
Service to set a subset of the adjoining bits of a port to a specified level. |
Dio_FlipChannel(Dio_ChannelType ChannelId) |
Service to flip the value of a DIO channel. |
|
Std_ReturnType |
Dio_IsChannelValid(Dio_ChannelType ChannelId) |
Checks if the channel ID is valid. |
Std_ReturnType |
Dio_IsChannelGroupValid(const Dio_ChannelGroupType * ChannelGroupIdPtr) |
Checks if the channel group is valid. |
Dio_PinReadPriv(Dio_ChannelType channelId) |
Reads the value present on the specified pin. |
|
void |
Dio_PinWritePriv(Dio_ChannelType channelId, Dio_LevelType channelVal) |
Writes a value to the specified pin. |
void |
Dio_WritePortDataPriv(Dio_PortType portId, Dio_PortLevelType portValue) |
Writes a value to the specified port. |
void |
Dio_WriteChannelGroupPriv(const Dio_ChannelGroupType * ChannelGroupIdPtr, Dio_PortLevelType PortValue) |
Writes a subset of the adjoining bits of a port to a specified level. |
void |
Dio_ReadPortDataPriv(Dio_PortType PortId, Dio_PortLevelType * PortValue) |
Reads the data on the specified port. |
void |
Dio_PinFlipVal(Dio_ChannelType ChannelId) |
Toggles the present value of the specified channel. |
5.2.4.1. function Dio_GetVersionInfo
void Dio_GetVersionInfo(
Std_VersionInfoType * Versioninfo
)
Brief: Service to get the version information of the module.
This service writes the version information of this module into the data structure referenced by the parameter. If this parameter references NULL_PTR, a development error is reported to Det. This service is only available if the pre-compile configuration parameter DIO_VERSION_INFO_API is enabled.
Parameters:
Versioninfo
Versioninfo structure that contains the version information parameters.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.2. function Dio_ReadChannel
Dio_LevelType Dio_ReadChannel(
Dio_ChannelType ChannelId
)
Brief: Returns the value of the specified DIO channel.
This service is to read from a specified DIO channel. If the channel specified is not valid, a development error is reported to Det. The value for the DIO channel is read and returned.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Returns:
STD_HIGH logic level 1
STD_LOW logic level 0
Return: Returns the logic level(value) on a specified DIO pin of type Dio_LevelType.
Precondition: None
Postcondition: None
5.2.4.3. function Dio_WriteChannel
void Dio_WriteChannel(
Dio_ChannelType ChannelId,
Dio_LevelType Level
)
Brief: Service to set a level of a channel.
This service is to set a specified level of a particular DIO channel. If the channel specified is not valid, a development error is reported to Det. The value is written to the specified DIO channel.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Level specifies the value to be written to the channel. Value can be STD_HIGH or STD_LOW.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.4. function Dio_ReadPort
Dio_PortLevelType Dio_ReadPort(
Dio_PortType PortId
)
Brief: Returns the level of all channels of that port.
This service reads the value of a DIO port. If the port is not enabled, a development error is reported to Det. The value of the port of which the ID is specified is read and returned.
Parameters:
PortId specifies the ID of the grouped Input/Output channels.
Returns:
Value of type Dio_PortLevelType
Return: level of all the channels of the specified port
Precondition: None
Postcondition: None
5.2.4.5. function Dio_WritePort
void Dio_WritePort(
Dio_PortType PortId,
Dio_PortLevelType Level
)
Brief: Service to set a value of the port.
This service sets a specified value of a DIO port. If the port is not enabled, a development error is reported to Det. The value is written to the specified DIO port.
Parameters:
PortId specifies the ID of the grouped Input/Output channels.
Level Value consisting of level of all the channels of the specified port.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.6. function Dio_ReadChannelGroup
Dio_PortLevelType Dio_ReadChannelGroup(
const Dio_ChannelGroupType * ChannelGroupIdPtr
)
Brief: This Service reads a subset of the adjoining bits of a port.
This service reads the value of the subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The value of the level of the channel group is read and returned.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
Returns:
value of type Dio_PortLevelType
Return: levels of the specified channel group.
Precondition: None
Postcondition: None
5.2.4.7. function Dio_WriteChannelGroup
void Dio_WriteChannelGroup(
const Dio_ChannelGroupType * ChannelGroupIdPtr,
Dio_PortLevelType Level
)
Brief: Service to set a subset of the adjoining bits of a port to a specified level.
This service writes the specified value to a subset of the bits of a port. If this parameter references NULL_PTR, a development error is reported to Det. The information of the channel group is in the referenced channel group structure.The data is then written to the port.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
Level Value consisting of levels of the specified channel group.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.8. function Dio_FlipChannel
Dio_LevelType Dio_FlipChannel(
Dio_ChannelType ChannelId
)
Brief: Service to flip the value of a DIO channel.
This service is to change the value of the corresponding DIO channel.If the channel specified is not valid, a development error is reported to Det. The value of the specified channel is flipped.This service is only available if the pre-compile configuration parameter DIO_FLIP_CHANNEL_API is enabled.
Parameters:
ChannelId specifies the ID of the general-purpose digital input/output pin.
Returns:
STD_HIGH logic level 1 STD_LOW: logic level 0
Return: Value consisting of level of the specified channel after flip of type Dio_LevelType.
Precondition: None
Postcondition: None
5.2.4.9. function Dio_IsChannelValid
Std_ReturnType Dio_IsChannelValid(
Dio_ChannelType ChannelId
)
Brief: Checks if the channel ID is valid.
Checks if the channel_id passed to the API is valid or not by calculating the Port of the Channel and checking if the port is enabled.
Parameters:
ChannelId specifies the ID of the general-purpose digital
Returns:
value E_OK: ChannelId is valid. E_NOT_OK: ChannelId is Invalid.
Return: This function returns Std_ReturnType
Precondition: None
Postcondition: None
5.2.4.10. function Dio_IsChannelGroupValid
Std_ReturnType Dio_IsChannelGroupValid(
const Dio_ChannelGroupType * ChannelGroupIdPtr
)
Brief: Checks if the channel group is valid.
Checks if the channelgroup_id_ptr passed to the API is valid or not by comparing it with the structure pointers of the current configuration.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
Returns:
E_OK ChannelGroupIdPtr is valid. E_NOT_OK: ChannelGroupIdPtr is Invalid.
Return: This function returns Std_ReturnType
Precondition: None
Postcondition: None
5.2.4.11. function Dio_PinReadPriv
Dio_LevelType Dio_PinReadPriv(
Dio_ChannelType channelId
)
Brief: Reads the value present on the specified pin.
The value at the specified channel is read, as specified by channelId and returned
Parameters:
channelId is the identifying number of the pin.
Returns:
STD_HIGH logic level 1 STD_LOW: logic level 0
Return: Returns the logic level(value) on a specified DIO pin of type Dio_LevelType.
Precondition: None
Postcondition: None
5.2.4.12. function Dio_PinWritePriv
void Dio_PinWritePriv(
Dio_ChannelType channelId,
Dio_LevelType channelVal
)
Brief: Writes a value to the specified pin.
Writes the corresponding bit values to the pin specified by channelId. Writing to a channel configured as an input pin has no effect.
Parameters:
channelId is the identifying number of the pin.
channelVal is the value to write to the channel.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.13. function Dio_WritePortDataPriv
void Dio_WritePortDataPriv(
Dio_PortType portId,
Dio_PortLevelType portValue
)
Brief: Writes a value to the specified port.
This function writes the value port_value to the port specified by the portId parameter.
Parameters:
portId is the DIO port being accessed.
portValue is the value to write to the port.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.14. function Dio_WriteChannelGroupPriv
void Dio_WriteChannelGroupPriv(
const Dio_ChannelGroupType * ChannelGroupIdPtr,
Dio_PortLevelType PortValue
)
Brief: Writes a subset of the adjoining bits of a port to a specified level.
This function compute the port value based on the received level, group mask and offset. Then write the computed port value to the specified port based on the portId received in channelGroupPtr.
Parameters:
ChannelGroupIdPtr for referencing channel group structures.
PortValue is the value to write to the port.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.15. function Dio_ReadPortDataPriv
void Dio_ReadPortDataPriv(
Dio_PortType PortId,
Dio_PortLevelType * PortValue
)
Brief: Reads the data on the specified port.
The value at the specified port is read, as specified by PortId and writes into the PortValue parameter.
Parameters:
PortId is the DIO port being accessed.
PortValue stores the value of the corresponding port being referred.
Returns:
None
Return: None
Precondition: None
Postcondition: None
5.2.4.16. function Dio_PinFlipVal
void Dio_PinFlipVal(
Dio_ChannelType ChannelId
)
Brief: Toggles the present value of the specified channel.
Toggles the corresponding bit values to the pin specified by ChannelId.
Parameters:
ChannelId is the identifying number of the pin.
Returns:
None
Return: None
Precondition: None
Postcondition: None