![]() |
![]() |
| C_NoRTOS_Config | NoRTOS framework global configuration |
| CADC_Config_ | ADC Global configuration |
| CADC_FxnTable_ | The definition of a ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params_ | ADC Parameters |
| CADCBuf_Config_ | ADCBuf Global configuration |
| CADCBuf_Conversion_ | An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK |
| CADCBuf_FxnTable_ | The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation |
| CADCBuf_Params_ | ADC Parameters |
| CADCBufMSP432E4_Channels | ADCBufMSP432E4 Channel Settings |
| CADCBufMSP432E4_HWAttrsV1 | ADCBufMSP432E4 Hardware attributes |
| CADCBufMSP432E4_Object | |
| CADCBufMSP432E4_ParamsExtension | MSP432E4 ADCBuf_Params Parameter Extensions |
| CADCMSP432E4_HWAttrsV1 | ADCMSP432E4 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For SimpleLink these definitions are found in: |
| CADCMSP432E4_Object | ADCMSP432 Object |
| CAESCBC_Config_ | AESCBC Global configuration |
| CAESCBC_Operation_ | Struct containing the parameters required for encrypting/decrypting a message |
| CAESCBC_Params_ | CBC Parameters |
| CAESCBCMSP432E4_HWAttrs | Hardware-specific configuration attributes |
| CAESCCM_Config_ | AESCCM Global configuration |
| CAESCCM_Operation_ | Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message |
| CAESCCM_Params_ | CCM Parameters |
| CAESCCMMSP432E4_HWAttrs | Hardware-specific configuration attributes |
| CAESCTR_Config | AESCTR Global configuration |
| CAESCTR_Operation | Struct containing the parameters required for encrypting/decrypting a message |
| CAESCTR_Params | CTR Parameters |
| CAESCTRMSP432E4_HWAttrs | Hardware-specific configuration attributes |
| CAESGCM_Config_ | AESGCM Global configuration |
| CAESGCM_Operation_ | Struct containing the parameters required for encrypting/decrypting and authenticating/verifying a message |
| CAESGCM_Params_ | GCM Parameters |
| CAESGCMMSP432E4_HWAttrs | Hardware-specific configuration attributes |
| CCAN_Config_ | CAN Global configuration |
| Ccan_frame | CAN frame structure |
| CCAN_FxnTable_ | The definition of a CAN function table that contains the required set of functions to control a specific CAN driver implementation |
| CCAN_Params_ | CAN Parameters |
| CCANMSP432E4_HWAttrs | CANMSP432E4 Hardware attributes |
| CCANMSP432E4_Object | CANMSP432E4 Object |
| CCryptoKey_ | CryptoKey datastructure |
| CCryptoKey_KeyBlob_ | Keyblob CryptoKey datastructure |
| CCryptoKey_KeyStore_ | Key store CryptoKey datastructure |
| CCryptoKey_Plaintext_ | Plaintext CryptoKey datastructure |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayGrLib_Object | |
| CDisplayHost_HWAttrs | DisplayHost Attributes |
| CDisplayHost_Object | DisplayHost Object |
| CDisplaySharp_HWAttrsV1 | |
| CDisplaySharp_Object | |
| CDisplaySharpColor_t | Foreground and background color struct, compatible with GrLib |
| CDisplayUart_HWAttrs | DisplayUart Attributes |
| CDisplayUart_Object | DisplayUart Object |
| CEMACMSP432E4_HWAttrs | EMACMSP432E4 Hardware attributes |
| CGPIOMSP432E4_Config | GPIO device specific driver configuration structure |
| CI2C_Config_ | I2C global configuration |
| CI2C_FxnTable_ | The definition of an I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params_ | I2C Parameters |
| CI2C_Transaction_ | Structure used to perform I2C bus transfers |
| CI2CMSP432E4_HWAttrs_ | I2CMSP432E4 Hardware attributes |
| CI2CMSP432E4_Object_ | I2CMSP432E4 Object |
| CList_Elem | |
| CList_List | |
| CNVS_Attrs | NVS attributes |
| CNVS_Config_ | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CNVSMSP432E4_HWAttrs | NVSMSP432E4 attributes |
| CNVSMSP432E4_Object | |
| CNVSRAM_HWAttrs | NVSRAM Hardware Attributes |
| CNVSRAM_Object | |
| CNVSSPI25X_HWAttrs | NVSSPI25X attributes |
| CNVSSPI25X_Object | |
| CPower_NotifyObj_ | Power notify object structure |
| CPowerMSP432E4_Config | Power global configuration structure |
| CPWM_Config_ | PWM Global configuration |
| CPWM_FxnTable_ | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params_ | PWM Parameters |
| CPWMMSP432E4_HWAttrs | PWMMSP432E4 Hardware attributes |
| CPWMMSP432E4_Object | PWMMSP432E4 Object |
| CPWMMSP432E4_Status | PWMMSP432E4_Status |
| CRingBuf_Object | |
| CSD_Config_ | SD Global configuration |
| CSD_FxnTable_ | The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation |
| CSD_Params_ | SD Parameters |
| CSDFatFS_Config_ | SDFatFS Global configuration |
| CSDFatFS_Object_ | SDFatFS Object The application must not access any member variables of this structure! |
| CSDSPI_HWAttrs | SDSPI Hardware attributes |
| CSDSPI_HWAttrs_ | |
| CSDSPI_Object_ | SDSPI Object |
| CSHA2_Config | SHA2 Global configuration |
| CSHA2_Params | SHA2 Parameters |
| CSHA2MSP432E4_HWAttrs | Hardware-specific configuration attributes |
| CSPI_Config_ | SPI Global configuration |
| CSPI_FxnTable_ | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params_ | SPI Parameters |
| CSPI_Transaction_ | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| Cspiffs_config | |
| Cspiffs_DIR | |
| Cspiffs_dirent | |
| Cspiffs_stat | |
| Cspiffs_t | |
| CSPIFFSNVS_Data_ | SPIFFSNVS data object |
| CSPIFFSNVS_Lock_ | SPIFFSNVS Lock |
| CSPIMSP432E4DMA_HWAttrs | SPIMSP432E4DMA Hardware attributes |
| CSPIMSP432E4DMA_Object | SPIMSP432E4DMA Object |
| CStructRingBuf_Object | |
| CTimer_Config_ | Timer Global configuration |
| CTimer_FxnTable_ | The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation |
| CTimer_Params_ | Timer Parameters |
| CTimerMSP432E4_HWAttrs_ | TimerMSP432E4 Hardware Attributes |
| CTimerMSP432E4_Object_ | TimerMSP432E4_Object |
| CUART_Config_ | UART Global configuration |
| CUART_FxnTable_ | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params_ | UART Parameters |
| CUARTMSP432E4_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432E4_read(). Internal use only |
| CUARTMSP432E4_HWAttrs | UARTMSP432E4 Hardware attributes |
| CUARTMSP432E4_Object | UARTMSP432E4 Object |
| CUDMAMSP432E4_Config | UDMAMSP432E4 Global configuration |
| CUDMAMSP432E4_HWAttrs | UDMAMSP432E4 Hardware attributes |
| CUDMAMSP432E4_Object | UDMAMSP432E4 object |
| CWatchdog_Config_ | Watchdog Global configuration |
| CWatchdog_FxnTable_ | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params_ | Watchdog Parameters |
| CWatchdogMSP432E4_HWAttrs | Watchdog hardware attributes for MSP432E4 |
| CWatchdogMSP432E4_Object | Watchdog Object for MSP432E4 |