Data Fields
ADCBufMSP432E4_ParamsExtension Struct Reference

MSP432E4 ADCBuf_Params Parameter Extensions. More...

#include <ADCBufMSP432E4.h>

Data Fields

ADCBufMSP432E4_SamplingDuration samplingDuration
 

Detailed Description

MSP432E4 ADCBuf_Params Parameter Extensions.

To use non-default MSP432E4 specific parameters when calling ADCBuf_open(), a pointer to an instance of this structure must be specified in ADCBuf_Params.custom. Alternatively, these values can be set using the ADCBuf_control() function after calling ADCBuf_open().

Field Documentation

§ samplingDuration

ADCBufMSP432E4_SamplingDuration ADCBufMSP432E4_ParamsExtension::samplingDuration

ADC sampling duration, ADCBufMSP432E4_SamplingDuration


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale