Data Fields
UDMAMSP432E4_Config Struct Reference

UDMAMSP432E4 Global configuration. More...

#include <UDMAMSP432E4.h>

Data Fields

void * object
 
void const * hwAttrs
 

Detailed Description

UDMAMSP432E4 Global configuration.

The UDMAMSP432E4_Config structure contains pointers used by the UDMAMSP432E4 driver.

This structure needs to be defined before calling UDMAMSP432E4_init() and it must not be changed thereafter.

Field Documentation

§ object

void* UDMAMSP432E4_Config::object

Pointer to UDMAMSP432E4 object

§ hwAttrs

void const* UDMAMSP432E4_Config::hwAttrs

Pointer to hardware attributes


The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale