Data Fields
PWMMSP432E4_Object Struct Reference

PWMMSP432E4 Object. More...

#include <PWMMSP432E4.h>

Collaboration diagram for PWMMSP432E4_Object:
Collaboration graph
[legend]

Data Fields

PWMMSP432E4_StatuspwmStatusStruct
 
PWM_Duty_Units dutyUnits
 
PWM_Period_Units periodUnits
 
PWM_IdleLevel idleLevel
 
uint8_t pwmOutputNum
 
uint8_t pwmOutputBit
 
bool isOpen
 
bool isRunning
 

Detailed Description

PWMMSP432E4 Object.

The application must not access any member variables of this structure!

Field Documentation

§ pwmStatusStruct

PWMMSP432E4_Status* PWMMSP432E4_Object::pwmStatusStruct

§ dutyUnits

PWM_Duty_Units PWMMSP432E4_Object::dutyUnits

§ periodUnits

PWM_Period_Units PWMMSP432E4_Object::periodUnits

§ idleLevel

PWM_IdleLevel PWMMSP432E4_Object::idleLevel

§ pwmOutputNum

uint8_t PWMMSP432E4_Object::pwmOutputNum

§ pwmOutputBit

uint8_t PWMMSP432E4_Object::pwmOutputBit

§ isOpen

bool PWMMSP432E4_Object::isOpen

§ isRunning

bool PWMMSP432E4_Object::isRunning

The documentation for this struct was generated from the following file:
© Copyright 1995-2018, Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy policy | Terms of use | Terms of sale