Macros | Functions
debug.h File Reference

Go to the source code of this file.

Macros

#define ASSERT(expr)
 
#define assert(expr)
 

Functions

void __error__ (char *pcFilename, unsigned long line)
 

Macro Definition Documentation

#define ASSERT (   expr)

Referenced by ADC14_configureMultiSequenceMode(), ADC14_configureSingleSampleMode(), ADC14_getResultArray(), ADC14_initModule(), ADC14_setComparatorWindowValue(), ADC14_setPowerMode(), ADC14_setResolution(), ADC14_setResultFormat(), ADC14_setSampleHoldTime(), ADC14_setSampleHoldTrigger(), COMP_E_disableInputBuffer(), COMP_E_enableInputBuffer(), COMP_E_initModule(), COMP_E_registerInterrupt(), COMP_E_setInterruptEdgeDirection(), COMP_E_setReferenceAccuracy(), COMP_E_setReferenceVoltage(), COMP_E_unregisterInterrupt(), CRC32_getResult(), CRC32_getResultReversed(), CRC32_set16BitData(), CRC32_set16BitDataReversed(), CRC32_set8BitData(), CRC32_set8BitDataReversed(), CRC32_setSeed(), CS_disableClockRequest(), CS_disableFaultCounter(), CS_enableClockRequest(), CS_enableFaultCounter(), CS_initClockSignal(), CS_resetFaultCounter(), CS_setDCOCenteredFrequency(), CS_setDCOFrequency(), CS_setReferenceOscillatorFrequency(), CS_startFaultCounter(), CS_startLFXTWithTimeout(), DMA_assignChannel(), DMA_assignInterrupt(), DMA_disableChannel(), DMA_disableChannelAttribute(), DMA_disableInterrupt(), DMA_enableChannel(), DMA_enableChannelAttribute(), DMA_enableInterrupt(), DMA_getChannelAttribute(), DMA_getChannelMode(), DMA_getChannelSize(), DMA_isChannelEnabled(), DMA_registerInterrupt(), DMA_requestChannel(), DMA_setChannelControl(), DMA_setChannelScatterGather(), DMA_setChannelTransfer(), DMA_setControlBase(), DMA_unregisterInterrupt(), EUSCI_A_SPI_changeClockPhasePolarity(), EUSCI_A_SPI_clearInterruptFlag(), EUSCI_A_SPI_disableInterrupt(), EUSCI_A_SPI_enableInterrupt(), EUSCI_A_SPI_getInterruptStatus(), EUSCI_A_SPI_select4PinFunctionality(), EUSCI_A_SPI_slaveInit(), EUSCI_B_SPI_changeClockPhasePolarity(), EUSCI_B_SPI_clearInterruptFlag(), EUSCI_B_SPI_disableInterrupt(), EUSCI_B_SPI_enableInterrupt(), EUSCI_B_SPI_getInterruptStatus(), EUSCI_B_SPI_select4PinFunctionality(), EUSCI_B_SPI_slaveInit(), FlashCtl_A_disableReadBuffering(), FlashCtl_A_enableReadBuffering(), FlashCtl_A_getReadMode(), FlashCtl_A_getWaitState(), FlashCtl_A_setReadMode(), FlashCtl_A_setWaitState(), FlashCtl_A_verifyMemory(), FlashCtl_disableReadBuffering(), FlashCtl_enableReadBuffering(), FlashCtl_getReadMode(), FlashCtl_getWaitState(), FlashCtl_isSectorProtected(), FlashCtl_protectSector(), FlashCtl_setReadMode(), FlashCtl_setWaitState(), FlashCtl_unprotectSector(), FlashCtl_verifyMemory(), GPIO_getEnabledInterruptStatus(), I2C_clearInterruptFlag(), I2C_disableInterrupt(), I2C_enableInterrupt(), I2C_getInterruptStatus(), I2C_initMaster(), I2C_initSlave(), I2C_masterReceiveMultiByteFinishWithTimeout(), I2C_masterSendMultiByteFinishWithTimeout(), I2C_masterSendMultiByteNextWithTimeout(), I2C_masterSendMultiByteStartWithTimeout(), I2C_masterSendMultiByteStopWithTimeout(), I2C_masterSendSingleByteWithTimeout(), I2C_registerInterrupt(), I2C_setMode(), I2C_setTimeout(), I2C_unregisterInterrupt(), Interrupt_disableInterrupt(), Interrupt_enableInterrupt(), Interrupt_getPriority(), Interrupt_isEnabled(), Interrupt_pendInterrupt(), Interrupt_registerInterrupt(), Interrupt_setPriority(), Interrupt_setPriorityGrouping(), Interrupt_unpendInterrupt(), Interrupt_unregisterInterrupt(), MPU_disableRegion(), MPU_enableModule(), MPU_enableRegion(), MPU_getRegion(), MPU_registerInterrupt(), MPU_setRegion(), PCM_getCoreVoltageLevel(), PCM_getPowerMode(), PCM_shutdownDevice(), PMAP_configurePorts(), PSS_setHighSideVoltageTrigger(), REF_A_setReferenceVoltage(), SPI_initMaster(), SPI_initSlave(), SPI_registerInterrupt(), SPI_unregisterInterrupt(), SysCtl_disablePeripheralAtCPUHalt(), SysCtl_disableSRAMBank(), SysCtl_disableSRAMBankRetention(), SysCtl_enablePeripheralAtCPUHalt(), SysCtl_enableSRAMBank(), SysCtl_enableSRAMBankRetention(), SysCtl_setWDTPasswordViolationResetType(), SysTick_setPeriod(), Timer32_haltTimer(), Timer32_initModule(), Timer32_startTimer(), Timer_A_clearCaptureCompareInterrupt(), Timer_A_configureContinuousMode(), Timer_A_configureUpDownMode(), Timer_A_configureUpMode(), Timer_A_disableCaptureCompareInterrupt(), Timer_A_enableCaptureCompareInterrupt(), Timer_A_generatePWM(), Timer_A_getCaptureCompareCount(), Timer_A_getOutputForOutputModeOutBitValue(), Timer_A_getSynchronizedCaptureCompareInput(), Timer_A_initCapture(), Timer_A_initCompare(), Timer_A_registerInterrupt(), Timer_A_setCompareValue(), Timer_A_startCounter(), Timer_A_unregisterInterrupt(), UART_clearInterruptFlag(), UART_disableInterrupt(), UART_enableInterrupt(), UART_getInterruptStatus(), UART_initModule(), UART_queryStatusFlags(), UART_registerInterrupt(), UART_selectDeglitchTime(), and UART_unregisterInterrupt().

#define assert (   expr)

Function Documentation

void __error__ ( char *  pcFilename,
unsigned long  line 
)

Copyright 2018, Texas Instruments Incorporated