![]() |
![]() |
eUSCI Universal Asynchronous Receiver/Transmitter (UART) serial communication module. More...
Data Structures | |
struct | _eUSCI_eUSCI_UART_Config |
Type definition for _eUSCI_UART_Config structure. More... | |
Typedefs | |
typedef struct _eUSCI_eUSCI_UART_Config | eUSCI_UART_Config |
Functions | |
bool | UART_initModule (uint32_t moduleInstance, const eUSCI_UART_Config *config) |
void | UART_transmitData (uint32_t moduleInstance, uint_fast8_t transmitData) |
uint8_t | UART_receiveData (uint32_t moduleInstance) |
void | UART_enableModule (uint32_t moduleInstance) |
void | UART_disableModule (uint32_t moduleInstance) |
uint_fast8_t | UART_queryStatusFlags (uint32_t moduleInstance, uint_fast8_t mask) |
void | UART_setDormant (uint32_t moduleInstance) |
void | UART_resetDormant (uint32_t moduleInstance) |
void | UART_transmitAddress (uint32_t moduleInstance, uint_fast8_t transmitAddress) |
void | UART_transmitBreak (uint32_t moduleInstance) |
uint32_t | UART_getReceiveBufferAddressForDMA (uint32_t moduleInstance) |
uint32_t | UART_getTransmitBufferAddressForDMA (uint32_t moduleInstance) |
void | UART_selectDeglitchTime (uint32_t moduleInstance, uint32_t deglitchTime) |
void | UART_enableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
void | UART_disableInterrupt (uint32_t moduleInstance, uint_fast8_t mask) |
uint_fast8_t | UART_getInterruptStatus (uint32_t moduleInstance, uint8_t mask) |
uint_fast8_t | UART_getEnabledInterruptStatus (uint32_t moduleInstance) |
void | UART_clearInterruptFlag (uint32_t moduleInstance, uint_fast8_t mask) |
void | UART_registerInterrupt (uint32_t moduleInstance, void(*intHandler)(void)) |
void | UART_unregisterInterrupt (uint32_t moduleInstance) |
eUSCI Universal Asynchronous Receiver/Transmitter (UART) serial communication module.
The modes of operations supported by the UART and the library include
In UART mode, the USCI transmits and receives characters at a bit rate asynchronous to another device. Timing for each character is based on the selected baud rate of the USCI. The transmit and receive functions use the same baud-rate frequency.
Below is a very brief code example showing how to configure and enable the UART module. In the case of this example, we assume the MCLK is operating off of the DCO and the DCO is tuned to 12MHz. This makes the configuration parameters so that the baud rate is 9600.
Below is an example of the UART configuration parameter:
This code snippet is the actual configuration of the UART module using the DriverLib APIs:
#define DEFAULT_SYNC 0x00 |
Referenced by UART_transmitBreak().
#define EUSCI_A_UART_AUTOMATICBAUDRATE_SYNC 0x55 |
Referenced by UART_transmitBreak().
#define EUSCI_A_UART_NO_PARITY 0x00 |
Referenced by UART_initModule().
#define EUSCI_A_UART_ODD_PARITY 0x01 |
Referenced by UART_initModule().
#define EUSCI_A_UART_EVEN_PARITY 0x02 |
Referenced by UART_initModule().
#define EUSCI_A_UART_MSB_FIRST EUSCI_A_CTLW0_MSB |
Referenced by UART_initModule().
#define EUSCI_A_UART_LSB_FIRST 0x00 |
Referenced by UART_initModule().
#define EUSCI_A_UART_MODE EUSCI_A_CTLW0_MODE_0 |
Referenced by UART_initModule().
#define EUSCI_A_UART_IDLE_LINE_MULTI_PROCESSOR_MODE EUSCI_A_CTLW0_MODE_1 |
Referenced by UART_initModule().
#define EUSCI_A_UART_ADDRESS_BIT_MULTI_PROCESSOR_MODE EUSCI_A_CTLW0_MODE_2 |
Referenced by UART_initModule().
#define EUSCI_A_UART_AUTOMATIC_BAUDRATE_DETECTION_MODE EUSCI_A_CTLW0_MODE_3 |
Referenced by UART_initModule(), and UART_transmitBreak().
#define EUSCI_A_UART_CLOCKSOURCE_SMCLK EUSCI_A_CTLW0_SSEL__SMCLK |
Referenced by UART_initModule().
#define EUSCI_A_UART_CLOCKSOURCE_ACLK EUSCI_A_CTLW0_SSEL__ACLK |
Referenced by UART_initModule().
#define EUSCI_A_UART_ONE_STOP_BIT 0x00 |
Referenced by UART_initModule().
#define EUSCI_A_UART_TWO_STOP_BITS EUSCI_A_CTLW0_SPB |
Referenced by UART_initModule().
#define EUSCI_A_UART_OVERSAMPLING_BAUDRATE_GENERATION 0x01 |
#define EUSCI_A_UART_LOW_FREQUENCY_BAUDRATE_GENERATION 0x00 |
#define EUSCI_A_UART_RECEIVE_INTERRUPT EUSCI_A_IE_RXIE |
Referenced by UART_disableInterrupt(), UART_enableInterrupt(), and UART_getEnabledInterruptStatus().
#define EUSCI_A_UART_TRANSMIT_INTERRUPT EUSCI_A_IE_TXIE |
Referenced by UART_disableInterrupt(), UART_enableInterrupt(), and UART_getEnabledInterruptStatus().
#define EUSCI_A_UART_RECEIVE_ERRONEOUSCHAR_INTERRUPT EUSCI_A_CTLW0_RXEIE |
Referenced by UART_disableInterrupt(), UART_enableInterrupt(), and UART_getEnabledInterruptStatus().
#define EUSCI_A_UART_BREAKCHAR_INTERRUPT EUSCI_A_CTLW0_BRKIE |
Referenced by UART_disableInterrupt(), UART_enableInterrupt(), and UART_getEnabledInterruptStatus().
#define EUSCI_A_UART_STARTBIT_INTERRUPT EUSCI_A_IE_STTIE |
Referenced by UART_disableInterrupt(), and UART_enableInterrupt().
#define EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT EUSCI_B_IE_STPIE |
Referenced by UART_disableInterrupt(), and UART_enableInterrupt().
#define EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG EUSCI_A_IFG_RXIFG |
Referenced by UART_clearInterruptFlag(), UART_getEnabledInterruptStatus(), and UART_getInterruptStatus().
#define EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG EUSCI_A_IFG_TXIFG |
Referenced by UART_clearInterruptFlag(), UART_getEnabledInterruptStatus(), and UART_getInterruptStatus().
#define EUSCI_A_UART_STARTBIT_INTERRUPT_FLAG EUSCI_A_IFG_STTIFG |
Referenced by UART_clearInterruptFlag(), and UART_getInterruptStatus().
#define EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT_FLAG EUSCI_A_IFG_TXCPTIFG |
Referenced by UART_clearInterruptFlag(), and UART_getInterruptStatus().
#define EUSCI_A_UART_LISTEN_ENABLE EUSCI_A_STATW_LISTEN |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_FRAMING_ERROR EUSCI_A_STATW_FE |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_OVERRUN_ERROR EUSCI_A_STATW_OE |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_PARITY_ERROR EUSCI_A_STATW_PE |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_BREAK_DETECT EUSCI_A_STATW_BRK |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_RECEIVE_ERROR EUSCI_A_STATW_RXERR |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_ADDRESS_RECEIVED EUSCI_A_STATW_ADDR_IDLE |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_IDLELINE EUSCI_A_STATW_ADDR_IDLE |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_BUSY EUSCI_A_STATW_BUSY |
Referenced by UART_queryStatusFlags().
#define EUSCI_A_UART_DEGLITCH_TIME_2ns 0x00 |
Referenced by UART_selectDeglitchTime().
#define EUSCI_A_UART_DEGLITCH_TIME_50ns 0x0001 |
Referenced by UART_selectDeglitchTime().
#define EUSCI_A_UART_DEGLITCH_TIME_100ns 0x0002 |
Referenced by UART_selectDeglitchTime().
#define EUSCI_A_UART_DEGLITCH_TIME_200ns (0x0001 + 0x0002) |
Referenced by UART_selectDeglitchTime().
#define EUSCI_A_UART_transmitData UART_transmitData |
#define EUSCI_A_UART_receiveData UART_receiveData |
#define EUSCI_A_UART_enableInterrupt UART_enableInterrupt |
#define EUSCI_A_UART_disableInterrupt UART_disableInterrupt |
#define EUSCI_A_UART_getInterruptStatus UART_getInterruptStatus |
#define EUSCI_A_UART_clearInterruptFlag UART_clearInterruptFlag |
#define EUSCI_A_UART_enable UART_enableModule |
#define EUSCI_A_UART_disable UART_disableModule |
#define EUSCI_A_UART_queryStatusFlags UART_queryStatusFlags |
#define EUSCI_A_UART_setDormant UART_setDormant |
#define EUSCI_A_UART_resetDormant UART_resetDormant |
#define EUSCI_A_UART_transmitAddress UART_transmitAddress |
#define EUSCI_A_UART_transmitBreak UART_transmitBreak |
#define EUSCI_A_UART_getReceiveBufferAddressForDMA UART_getReceiveBufferAddressForDMA |
#define EUSCI_A_UART_getTransmitBufferAddressForDMA UART_getTransmitBufferAddressForDMA |
#define EUSCI_A_UART_selectDeglitchTime UART_selectDeglitchTime |
typedef struct _eUSCI_eUSCI_UART_Config eUSCI_UART_Config |
bool UART_initModule | ( | uint32_t | moduleInstance, |
const eUSCI_UART_Config * | config | ||
) |
Initialization routine for the UART block. The values to be written into the UCAxBRW and UCAxMCTLW registers should be pre-computed and passed into the initialization function
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
config | Configuration structure for the UART module |
Configuration options for eUSCI_UART_Config structure.
It is important to note that for eUSCI modules, only "A" modules such as EUSCI_A0 can be used. "B" modules such as EUSCI_B0 do not support the UART mode.
selectClockSource | selects Clock source. Valid values are
|
clockPrescalar | is the value to be written into UCBRx bits |
firstModReg | is First modulation stage register setting. This value is a pre-calculated value which can be obtained from the Device User Guide.This value is written into UCBRFx bits of UCAxMCTLW. |
secondModReg | is Second modulation stage register setting. This value is a pre-calculated value which can be obtained from the Device User Guide. This value is written into UCBRSx bits of UCAxMCTLW. |
parity | is the desired parity. Valid values are
|
msborLsbFirst | controls direction of receive and transmit shift register. Valid values are
|
numberofStopBits | indicates one/two STOP bits Valid values are
|
uartMode | selects the mode of operation Valid values are
|
overSampling | indicates low frequency or oversampling baud generation Valid values are
|
Upon successful initialization of the UART block, this function will have initialized the module, but the UART block still remains disabled and must be enabled with UART_enableModule()
Refer to this calculator for help on calculating values for the parameters.
Modified bits are UCPEN, UCPAR, UCMSB, UC7BIT, UCSPB, UCMODEx, UCSYNC bits of UCAxCTL0 and UCSSELx, UCSWRST bits of UCAxCTL1
References ASSERT, _eUSCI_eUSCI_UART_Config::clockPrescalar, EUSCI_A_CMSIS, EUSCI_A_UART_ADDRESS_BIT_MULTI_PROCESSOR_MODE, EUSCI_A_UART_AUTOMATIC_BAUDRATE_DETECTION_MODE, EUSCI_A_UART_CLOCKSOURCE_ACLK, EUSCI_A_UART_CLOCKSOURCE_SMCLK, EUSCI_A_UART_EVEN_PARITY, EUSCI_A_UART_IDLE_LINE_MULTI_PROCESSOR_MODE, EUSCI_A_UART_LSB_FIRST, EUSCI_A_UART_MODE, EUSCI_A_UART_MSB_FIRST, EUSCI_A_UART_NO_PARITY, EUSCI_A_UART_ODD_PARITY, EUSCI_A_UART_ONE_STOP_BIT, EUSCI_A_UART_TWO_STOP_BITS, _eUSCI_eUSCI_UART_Config::firstModReg, _eUSCI_eUSCI_UART_Config::msborLsbFirst, _eUSCI_eUSCI_UART_Config::numberofStopBits, _eUSCI_eUSCI_UART_Config::overSampling, _eUSCI_eUSCI_UART_Config::parity, _eUSCI_eUSCI_UART_Config::secondModReg, _eUSCI_eUSCI_UART_Config::selectClockSource, and _eUSCI_eUSCI_UART_Config::uartMode.
void UART_transmitData | ( | uint32_t | moduleInstance, |
uint_fast8_t | transmitData | ||
) |
Transmits a byte from the UART Module.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
transmitData | data to be transmitted from the UART module |
This function will place the supplied data into UART transmit data register to start transmission
Modified register is UCAxTXBUF
References EUSCI_A_CMSIS.
uint8_t UART_receiveData | ( | uint32_t | moduleInstance | ) |
Receives a byte that has been sent to the UART Module.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
This function reads a byte of data from the UART receive data Register.
Modified register is UCAxRXBUF
References EUSCI_A_CMSIS.
void UART_enableModule | ( | uint32_t | moduleInstance | ) |
Enables the UART block.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
This will enable operation of the UART block.
Modified register is UCAxCTL1
References EUSCI_A_CMSIS.
void UART_disableModule | ( | uint32_t | moduleInstance | ) |
Disables the UART block.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
This will disable operation of the UART block.
Modified register is UCAxCTL1
References EUSCI_A_CMSIS.
uint_fast8_t UART_queryStatusFlags | ( | uint32_t | moduleInstance, |
uint_fast8_t | mask | ||
) |
Gets the current UART status flags.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
mask | is the masked interrupt flag status to be returned. |
This returns the status for the UART module based on which flag is passed. mask parameter can be either any of the following selection.
Modified register is UCAxSTAT
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_ADDRESS_RECEIVED, EUSCI_A_UART_BREAK_DETECT, EUSCI_A_UART_BUSY, EUSCI_A_UART_FRAMING_ERROR, EUSCI_A_UART_IDLELINE, EUSCI_A_UART_LISTEN_ENABLE, EUSCI_A_UART_OVERRUN_ERROR, EUSCI_A_UART_PARITY_ERROR, and EUSCI_A_UART_RECEIVE_ERROR.
void UART_setDormant | ( | uint32_t | moduleInstance | ) |
Sets the UART module in dormant mode
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
Puts USCI in sleep mode Only characters that are preceded by an idle-line or with address bit set UCRXIFG. In UART mode with automatic baud-rate detection, only the combination of a break and synch field sets UCRXIFG.
Modified register is UCAxCTL1
References EUSCI_A_CMSIS.
void UART_resetDormant | ( | uint32_t | moduleInstance | ) |
Re-enables UART module from dormant mode
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
Not dormant. All received characters set UCRXIFG.
Modified bits are UCDORM of UCAxCTL1 register.
References EUSCI_A_CMSIS.
void UART_transmitAddress | ( | uint32_t | moduleInstance, |
uint_fast8_t | transmitAddress | ||
) |
Transmits the next byte to be transmitted marked as address depending on selected multiprocessor mode
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
transmitAddress | is the next byte to be transmitted |
Modified register is UCAxCTL1, UCAxTXBUF
References EUSCI_A_CMSIS.
void UART_transmitBreak | ( | uint32_t | moduleInstance | ) |
Transmit break. Transmits a break with the next write to the transmit buffer. In UART mode with automatic baud-rate detection, EUSCI_A_UART_AUTOMATICBAUDRATE_SYNC(0x55) must be written into UCAxTXBUF to generate the required break/synch fields. Otherwise, DEFAULT_SYNC(0x00) must be written into the transmit buffer. Also ensures module is ready for transmitting the next data
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
Modified register is UCAxCTL1, UCAxTXBUF
References DEFAULT_SYNC, EUSCI_A_CMSIS, EUSCI_A_UART_AUTOMATIC_BAUDRATE_DETECTION_MODE, and EUSCI_A_UART_AUTOMATICBAUDRATE_SYNC.
uint32_t UART_getReceiveBufferAddressForDMA | ( | uint32_t | moduleInstance | ) |
Returns the address of the RX Buffer of the UART for the DMA module.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
Returns the address of the UART RX Buffer. This can be used in conjunction with the DMA to store the received data directly to memory.
References EUSCI_A_CMSIS.
uint32_t UART_getTransmitBufferAddressForDMA | ( | uint32_t | moduleInstance | ) |
Returns the address of the TX Buffer of the UART for the DMA module.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
Returns the address of the UART TX Buffer. This can be used in conjunction with the DMA to obtain transmitted data directly from memory.
References EUSCI_B_CMSIS.
void UART_selectDeglitchTime | ( | uint32_t | moduleInstance, |
uint32_t | deglitchTime | ||
) |
Sets the deglitch time
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
deglitchTime | is the selected deglitch time Valid values are
|
Returns the address of the UART TX Buffer. This can be used in conjunction with the DMA to obtain transmitted data directly from memory.
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_DEGLITCH_TIME_100ns, EUSCI_A_UART_DEGLITCH_TIME_200ns, EUSCI_A_UART_DEGLITCH_TIME_2ns, and EUSCI_A_UART_DEGLITCH_TIME_50ns.
void UART_enableInterrupt | ( | uint32_t | moduleInstance, |
uint_fast8_t | mask | ||
) |
Enables individual UART interrupt sources.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
mask | is the bit mask of the interrupt sources to be enabled. |
Enables the indicated UART interrupt sources. The interrupt flag is first and then the corresponding interrupt is enabled. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The mask parameter is the logical OR of any of the following:
Modified register is UCAxIFG, UCAxIE and UCAxCTL1
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_BREAKCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_ERRONEOUSCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_INTERRUPT, EUSCI_A_UART_STARTBIT_INTERRUPT, EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT, and EUSCI_A_UART_TRANSMIT_INTERRUPT.
void UART_disableInterrupt | ( | uint32_t | moduleInstance, |
uint_fast8_t | mask | ||
) |
Disables individual UART interrupt sources.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
mask | is the bit mask of the interrupt sources to be disabled. |
Disables the indicated UART interrupt sources. Only the sources that are enabled can be reflected to the processor interrupt; disabled sources have no effect on the processor.
The mask parameter is the logical OR of any of the following:
Modified register is UCAxIFG, UCAxIE and UCAxCTL1
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_BREAKCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_ERRONEOUSCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_INTERRUPT, EUSCI_A_UART_STARTBIT_INTERRUPT, EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT, and EUSCI_A_UART_TRANSMIT_INTERRUPT.
uint_fast8_t UART_getInterruptStatus | ( | uint32_t | moduleInstance, |
uint8_t | mask | ||
) |
Gets the current UART interrupt status.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
mask | is the masked interrupt flag status to be returned. Mask value is the logical OR of any of the following:
|
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG, EUSCI_A_UART_STARTBIT_INTERRUPT_FLAG, EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT_FLAG, and EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG.
Referenced by UART_getEnabledInterruptStatus().
uint_fast8_t UART_getEnabledInterruptStatus | ( | uint32_t | moduleInstance | ) |
Gets the current UART interrupt status masked with the enabled interrupts. This function is useful to call in ISRs to get a list of pending interrupts that are actually enabled and could have caused the ISR.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
References EUSCI_A_CMSIS, EUSCI_A_UART_BREAKCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_ERRONEOUSCHAR_INTERRUPT, EUSCI_A_UART_RECEIVE_INTERRUPT, EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG, EUSCI_A_UART_TRANSMIT_INTERRUPT, EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG, and UART_getInterruptStatus().
void UART_clearInterruptFlag | ( | uint32_t | moduleInstance, |
uint_fast8_t | mask | ||
) |
Clears UART interrupt sources.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
mask | is a bit mask of the interrupt sources to be cleared. |
The UART interrupt source is cleared, so that it no longer asserts. The highest interrupt flag is automatically cleared when an interrupt vector generator is used.
The mask parameter has the same definition as the mask parameter to EUSCI_A_UART_enableInterrupt().
Modified register is UCAxIFG
References ASSERT, EUSCI_A_CMSIS, EUSCI_A_UART_RECEIVE_INTERRUPT_FLAG, EUSCI_A_UART_STARTBIT_INTERRUPT_FLAG, EUSCI_A_UART_TRANSMIT_COMPLETE_INTERRUPT_FLAG, and EUSCI_A_UART_TRANSMIT_INTERRUPT_FLAG.
void UART_registerInterrupt | ( | uint32_t | moduleInstance, |
void(*)(void) | intHandler | ||
) |
Registers an interrupt handler for UART interrupts.
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
intHandler | is a pointer to the function to be called when the timer capture compare interrupt occurs. |
This function registers the handler to be called when an UART interrupt occurs. This function enables the global interrupt in the interrupt controller; specific UART interrupts must be enabled via UART_enableInterrupt(). It is the interrupt handler's responsibility to clear the interrupt source via UART_clearInterruptFlag().
References ASSERT, INT_EUSCIA0, INT_EUSCIA1, INT_EUSCIA2, INT_EUSCIA3, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().
void UART_unregisterInterrupt | ( | uint32_t | moduleInstance | ) |
Unregisters the interrupt handler for the UART module
moduleInstance | is the instance of the eUSCI A (UART) module. Valid parameters vary from part to part, but can include:
|
This function unregisters the handler to be called when timer interrupt occurs. This function also masks off the interrupt in the interrupt controller so that the interrupt handler no longer is called.
References ASSERT, INT_EUSCIA0, INT_EUSCIA1, INT_EUSCIA2, INT_EUSCIA3, Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().