![]() |
![]() |
Configures and controls MSP432's DMA controller which is built around ARM's uDMA controller. More...
Data Structures | |
struct | _DMA_ControlTable |
Macros | |
#define | DMA_TaskStructEntry(transferCount,itemSize,srcIncrement,srcAddr,dstIncrement,dstAddr,arbSize,mode) |
#define | UDMA_ATTR_USEBURST 0x00000001 |
#define | UDMA_ATTR_ALTSELECT 0x00000002 |
#define | UDMA_ATTR_HIGH_PRIORITY 0x00000004 |
#define | UDMA_ATTR_REQMASK 0x00000008 |
#define | UDMA_ATTR_ALL 0x0000000F |
#define | UDMA_MODE_STOP 0x00000000 |
#define | UDMA_MODE_BASIC 0x00000001 |
#define | UDMA_MODE_AUTO 0x00000002 |
#define | UDMA_MODE_PINGPONG 0x00000003 |
#define | UDMA_MODE_MEM_SCATTER_GATHER 0x00000004 |
#define | UDMA_MODE_PER_SCATTER_GATHER 0x00000006 |
#define | UDMA_MODE_ALT_SELECT 0x00000001 |
#define | UDMA_DST_INC_8 0x00000000 |
#define | UDMA_DST_INC_16 0x40000000 |
#define | UDMA_DST_INC_32 0x80000000 |
#define | UDMA_DST_INC_NONE 0xc0000000 |
#define | UDMA_SRC_INC_8 0x00000000 |
#define | UDMA_SRC_INC_16 0x04000000 |
#define | UDMA_SRC_INC_32 0x08000000 |
#define | UDMA_SRC_INC_NONE 0x0c000000 |
#define | UDMA_SIZE_8 0x00000000 |
#define | UDMA_SIZE_16 0x11000000 |
#define | UDMA_SIZE_32 0x22000000 |
#define | UDMA_DST_PROT_PRIV 0x00200000 |
#define | UDMA_SRC_PROT_PRIV 0x00040000 |
#define | UDMA_ARB_1 0x00000000 |
#define | UDMA_ARB_2 0x00004000 |
#define | UDMA_ARB_4 0x00008000 |
#define | UDMA_ARB_8 0x0000c000 |
#define | UDMA_ARB_16 0x00010000 |
#define | UDMA_ARB_32 0x00014000 |
#define | UDMA_ARB_64 0x00018000 |
#define | UDMA_ARB_128 0x0001c000 |
#define | UDMA_ARB_256 0x00020000 |
#define | UDMA_ARB_512 0x00024000 |
#define | UDMA_ARB_1024 0x00028000 |
#define | UDMA_NEXT_USEBURST 0x00000008 |
#define | UDMA_PRI_SELECT 0x00000000 |
#define | UDMA_ALT_SELECT 0x00000008 |
#define | DMA_CH0_RESERVED0 0x00000000 |
#define | DMA_CH0_EUSCIA0TX 0x01000000 |
#define | DMA_CH0_EUSCIB0TX0 0x02000000 |
#define | DMA_CH0_EUSCIB3TX1 0x03000000 |
#define | DMA_CH0_EUSCIB2TX2 0x04000000 |
#define | DMA_CH0_EUSCIB1TX3 0x05000000 |
#define | DMA_CH0_TIMERA0CCR0 0x06000000 |
#define | DMA_CH0_AESTRIGGER0 0x07000000 |
#define | DMA_CH1_RESERVED0 0x00000001 |
#define | DMA_CH1_EUSCIA0RX 0x01000001 |
#define | DMA_CH1_EUSCIB0RX0 0x02000001 |
#define | DMA_CH1_EUSCIB3RX1 0x03000001 |
#define | DMA_CH1_EUSCIB2RX2 0x04000001 |
#define | DMA_CH1_EUSCIB1RX3 0x05000001 |
#define | DMA_CH1_TIMERA0CCR2 0x06000001 |
#define | DMA_CH1_AESTRIGGER1 0x07000001 |
#define | DMA_CH2_RESERVED0 0x00000002 |
#define | DMA_CH2_EUSCIA1TX 0x01000002 |
#define | DMA_CH2_EUSCIB1TX0 0x02000002 |
#define | DMA_CH2_EUSCIB0TX1 0x03000002 |
#define | DMA_CH2_EUSCIB3TX2 0x04000002 |
#define | DMA_CH2_EUSCIB2TX3 0x05000002 |
#define | DMA_CH2_TIMERA1CCR0 0x06000002 |
#define | DMA_CH2_AESTRIGGER2 0x07000002 |
#define | DMA_CH3_RESERVED0 0x00000003 |
#define | DMA_CH3_EUSCIA1RX 0x01000003 |
#define | DMA_CH3_EUSCIB1RX0 0x02000003 |
#define | DMA_CH3_EUSCIB0RX1 0x03000003 |
#define | DMA_CH3_EUSCIB3RX2 0x04000003 |
#define | DMA_CH3_EUSCIB2RX3 0x05000003 |
#define | DMA_CH3_TIMERA1CCR2 0x06000003 |
#define | DMA_CH3_RESERVED1 0x07000003 |
#define | DMA_CH4_RESERVED0 0x00000004 |
#define | DMA_CH4_EUSCIA2TX 0x01000004 |
#define | DMA_CH4_EUSCIB2TX0 0x02000004 |
#define | DMA_CH4_EUSCIB1TX1 0x03000004 |
#define | DMA_CH4_EUSCIB0TX2 0x04000004 |
#define | DMA_CH4_EUSCIB3TX3 0x05000004 |
#define | DMA_CH4_TIMERA2CCR0 0x06000004 |
#define | DMA_CH4_RESERVED1 0x07000004 |
#define | DMA_CH5_RESERVED0 0x00000005 |
#define | DMA_CH5_EUSCIA2RX 0x01000005 |
#define | DMA_CH5_EUSCIB2RX0 0x02000005 |
#define | DMA_CH5_EUSCIB1RX1 0x03000005 |
#define | DMA_CH5_EUSCIB0RX2 0x04000005 |
#define | DMA_CH5_EUSCIB3RX3 0x05000005 |
#define | DMA_CH5_TIMERA2CCR2 0x06000005 |
#define | DMA_CH5_RESERVED1 0x07000005 |
#define | DMA_CH6_RESERVED0 0x00000006 |
#define | DMA_CH6_EUSCIA3TX 0x01000006 |
#define | DMA_CH6_EUSCIB3TX0 0x02000006 |
#define | DMA_CH6_EUSCIB2TX1 0x03000006 |
#define | DMA_CH6_EUSCIB1TX2 0x04000006 |
#define | DMA_CH6_EUSCIB0TX3 0x05000006 |
#define | DMA_CH6_TIMERA3CCR0 0x06000006 |
#define | DMA_CH6_EXTERNALPIN 0x07000006 |
#define | DMA_CH7_RESERVED0 0x00000007 |
#define | DMA_CH7_EUSCIA3RX 0x01000007 |
#define | DMA_CH7_EUSCIB3RX0 0x02000007 |
#define | DMA_CH7_EUSCIB2RX1 0x03000007 |
#define | DMA_CH7_EUSCIB1RX2 0x04000007 |
#define | DMA_CH7_EUSCIB0RX3 0x05000007 |
#define | DMA_CH7_TIMERA3CCR2 0x06000007 |
#define | DMA_CH7_ADC14 0x07000007 |
#define | DMA_INT0 INT_DMA_INT0 |
#define | DMA_INT1 INT_DMA_INT1 |
#define | DMA_INT2 INT_DMA_INT2 |
#define | DMA_INT3 INT_DMA_INT3 |
#define | DMA_INTERR INT_DMA_ERR |
#define | DMA_CHANNEL_0 0 |
#define | DMA_CHANNEL_1 1 |
#define | DMA_CHANNEL_2 2 |
#define | DMA_CHANNEL_3 3 |
#define | DMA_CHANNEL_4 4 |
#define | DMA_CHANNEL_5 5 |
#define | DMA_CHANNEL_6 6 |
#define | DMA_CHANNEL_7 7 |
Typedefs | |
typedef struct _DMA_ControlTable | DMA_ControlTable |
Functions | |
void | DMA_enableModule (void) |
void | DMA_disableModule (void) |
uint32_t | DMA_getErrorStatus (void) |
void | DMA_clearErrorStatus (void) |
void | DMA_enableChannel (uint32_t channelNum) |
void | DMA_disableChannel (uint32_t channelNum) |
bool | DMA_isChannelEnabled (uint32_t channelNum) |
void | DMA_setControlBase (void *controlTable) |
void * | DMA_getControlBase (void) |
void * | DMA_getControlAlternateBase (void) |
void | DMA_requestChannel (uint32_t channelNum) |
void | DMA_enableChannelAttribute (uint32_t channelNum, uint32_t attr) |
void | DMA_disableChannelAttribute (uint32_t channelNum, uint32_t attr) |
uint32_t | DMA_getChannelAttribute (uint32_t channelNum) |
void | DMA_setChannelControl (uint32_t channelStructIndex, uint32_t control) |
void | DMA_setChannelTransfer (uint32_t channelStructIndex, uint32_t mode, void *srcAddr, void *dstAddr, uint32_t transferSize) |
void | DMA_setChannelScatterGather (uint32_t channelNum, uint32_t taskCount, void *taskList, uint32_t isPeriphSG) |
uint32_t | DMA_getChannelSize (uint32_t channelStructIndex) |
uint32_t | DMA_getChannelMode (uint32_t channelStructIndex) |
void | DMA_assignChannel (uint32_t mapping) |
void | DMA_requestSoftwareTransfer (uint32_t channel) |
void | DMA_assignInterrupt (uint32_t interruptNumber, uint32_t channel) |
void | DMA_enableInterrupt (uint32_t interruptNumber) |
void | DMA_disableInterrupt (uint32_t interruptNumber) |
uint32_t | DMA_getInterruptStatus (void) |
void | DMA_clearInterruptFlag (uint32_t channel) |
void | DMA_registerInterrupt (uint32_t interruptNumber, void(*intHandler)(void)) |
void | DMA_unregisterInterrupt (uint32_t interruptNumber) |
Configures and controls MSP432's DMA controller which is built around ARM's uDMA controller.
The DMA controller has the following features:
The uDMA controller supports several different transfer modes, allowing for complex transfer schemes. The following transfer modes are provided:
Detailed explanation of the various transfer modes is beyond the scope of this document. Please refer to the device data sheet for more information on the operation of the uDMA controller.
Below is a very brief example of how to configure the DMA controller to transfer from a data array (data_array) to the EUSCI I2C module to be sent over the I2C line. This is useful in the sense that the EUSCI module does not constantly have to wake up the CPU in order to load the next byte into the buffer.
#define DMA_TaskStructEntry | ( | transferCount, | |
itemSize, | |||
srcIncrement, | |||
srcAddr, | |||
dstIncrement, | |||
dstAddr, | |||
arbSize, | |||
mode | |||
) |
A helper macro for building scatter-gather task table entries.
This macro is intended to be used to help populate a table of DMA tasks for a scatter-gather transfer. This macro will calculate the values for the fields of a task structure entry based on the input parameters.
There are specific requirements for the values of each parameter. No checking is done so it is up to the caller to ensure that correct values are used for the parameters.
The transferCount parameter is the number of items that will be transferred by this task. It must be in the range 1-1024.
The itemSize parameter is the bit size of the transfer data. It must be one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32.
The srcIncrement parameter is the increment size for the source data. It must be one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE.
The srcAddr parameter is a void pointer to the beginning of the source data.
The dstIncrement parameter is the increment size for the destination data. It must be one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_DST_INC_NONE.
The dstAddr parameter is a void pointer to the beginning of the location where the data will be transferred.
The arbSize parameter is the arbitration size for the transfer, and must be one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, and so on up to UDMA_ARB_1024. This is used to select the arbitration size in powers of 2, from 1 to 1024.
The mode parameter is the mode to use for this transfer task. It must be one of UDMA_MODE_BASIC, UDMA_MODE_AUTO, UDMA_MODE_MEM_SCATTER_GATHER, or UDMA_MODE_PER_SCATTER_GATHER. Note that normally all tasks will be one of the scatter-gather modes while the last task is a task list will be AUTO or BASIC.
This macro is intended to be used to initialize individual entries of a structure of DMA_ControlTable type, like this:
transferCount | is the count of items to transfer for this task. |
itemSize | is the bit size of the items to transfer for this task. |
srcIncrement | is the bit size increment for source data. |
srcAddr | is the starting address of the data to transfer. |
dstIncrement | is the bit size increment for destination data. |
dstAddr | is the starting address of the destination data. |
arbSize | is the arbitration size to use for the transfer task. |
mode | is the transfer mode for this task. |
#define UDMA_ATTR_USEBURST 0x00000001 |
Referenced by DMA_disableChannelAttribute(), DMA_enableChannelAttribute(), and DMA_getChannelAttribute().
#define UDMA_ATTR_ALTSELECT 0x00000002 |
Referenced by DMA_disableChannelAttribute(), DMA_enableChannelAttribute(), and DMA_getChannelAttribute().
#define UDMA_ATTR_HIGH_PRIORITY 0x00000004 |
Referenced by DMA_disableChannelAttribute(), DMA_enableChannelAttribute(), and DMA_getChannelAttribute().
#define UDMA_ATTR_REQMASK 0x00000008 |
Referenced by DMA_disableChannelAttribute(), DMA_enableChannelAttribute(), and DMA_getChannelAttribute().
#define UDMA_ATTR_ALL 0x0000000F |
#define UDMA_MODE_STOP 0x00000000 |
#define UDMA_MODE_BASIC 0x00000001 |
#define UDMA_MODE_AUTO 0x00000002 |
#define UDMA_MODE_PINGPONG 0x00000003 |
#define UDMA_MODE_MEM_SCATTER_GATHER 0x00000004 |
Referenced by DMA_getChannelMode(), and DMA_setChannelTransfer().
#define UDMA_MODE_PER_SCATTER_GATHER 0x00000006 |
Referenced by DMA_getChannelMode(), and DMA_setChannelTransfer().
#define UDMA_MODE_ALT_SELECT 0x00000001 |
Referenced by DMA_getChannelMode(), and DMA_setChannelTransfer().
#define UDMA_DST_INC_8 0x00000000 |
#define UDMA_DST_INC_16 0x40000000 |
#define UDMA_DST_INC_32 0x80000000 |
#define UDMA_DST_INC_NONE 0xc0000000 |
Referenced by DMA_setChannelTransfer().
#define UDMA_SRC_INC_8 0x00000000 |
#define UDMA_SRC_INC_16 0x04000000 |
#define UDMA_SRC_INC_32 0x08000000 |
#define UDMA_SRC_INC_NONE 0x0c000000 |
Referenced by DMA_setChannelTransfer().
#define UDMA_SIZE_8 0x00000000 |
#define UDMA_SIZE_16 0x11000000 |
#define UDMA_SIZE_32 0x22000000 |
#define UDMA_DST_PROT_PRIV 0x00200000 |
#define UDMA_SRC_PROT_PRIV 0x00040000 |
#define UDMA_ARB_1 0x00000000 |
#define UDMA_ARB_2 0x00004000 |
#define UDMA_ARB_4 0x00008000 |
#define UDMA_ARB_8 0x0000c000 |
#define UDMA_ARB_16 0x00010000 |
#define UDMA_ARB_32 0x00014000 |
#define UDMA_ARB_64 0x00018000 |
#define UDMA_ARB_128 0x0001c000 |
#define UDMA_ARB_256 0x00020000 |
#define UDMA_ARB_512 0x00024000 |
#define UDMA_ARB_1024 0x00028000 |
#define UDMA_NEXT_USEBURST 0x00000008 |
#define UDMA_PRI_SELECT 0x00000000 |
#define UDMA_ALT_SELECT 0x00000008 |
Referenced by DMA_setChannelScatterGather(), and DMA_setChannelTransfer().
#define DMA_CH0_RESERVED0 0x00000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_EUSCIA0TX 0x01000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_EUSCIB0TX0 0x02000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_EUSCIB3TX1 0x03000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_EUSCIB2TX2 0x04000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_EUSCIB1TX3 0x05000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_TIMERA0CCR0 0x06000000 |
Referenced by DMA_assignChannel().
#define DMA_CH0_AESTRIGGER0 0x07000000 |
Referenced by DMA_assignChannel().
#define DMA_CH1_RESERVED0 0x00000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_EUSCIA0RX 0x01000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_EUSCIB0RX0 0x02000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_EUSCIB3RX1 0x03000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_EUSCIB2RX2 0x04000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_EUSCIB1RX3 0x05000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_TIMERA0CCR2 0x06000001 |
Referenced by DMA_assignChannel().
#define DMA_CH1_AESTRIGGER1 0x07000001 |
Referenced by DMA_assignChannel().
#define DMA_CH2_RESERVED0 0x00000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_EUSCIA1TX 0x01000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_EUSCIB1TX0 0x02000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_EUSCIB0TX1 0x03000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_EUSCIB3TX2 0x04000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_EUSCIB2TX3 0x05000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_TIMERA1CCR0 0x06000002 |
Referenced by DMA_assignChannel().
#define DMA_CH2_AESTRIGGER2 0x07000002 |
Referenced by DMA_assignChannel().
#define DMA_CH3_RESERVED0 0x00000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_EUSCIA1RX 0x01000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_EUSCIB1RX0 0x02000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_EUSCIB0RX1 0x03000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_EUSCIB3RX2 0x04000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_EUSCIB2RX3 0x05000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_TIMERA1CCR2 0x06000003 |
Referenced by DMA_assignChannel().
#define DMA_CH3_RESERVED1 0x07000003 |
Referenced by DMA_assignChannel().
#define DMA_CH4_RESERVED0 0x00000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_EUSCIA2TX 0x01000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_EUSCIB2TX0 0x02000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_EUSCIB1TX1 0x03000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_EUSCIB0TX2 0x04000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_EUSCIB3TX3 0x05000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_TIMERA2CCR0 0x06000004 |
Referenced by DMA_assignChannel().
#define DMA_CH4_RESERVED1 0x07000004 |
Referenced by DMA_assignChannel().
#define DMA_CH5_RESERVED0 0x00000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_EUSCIA2RX 0x01000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_EUSCIB2RX0 0x02000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_EUSCIB1RX1 0x03000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_EUSCIB0RX2 0x04000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_EUSCIB3RX3 0x05000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_TIMERA2CCR2 0x06000005 |
Referenced by DMA_assignChannel().
#define DMA_CH5_RESERVED1 0x07000005 |
Referenced by DMA_assignChannel().
#define DMA_CH6_RESERVED0 0x00000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EUSCIA3TX 0x01000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EUSCIB3TX0 0x02000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EUSCIB2TX1 0x03000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EUSCIB1TX2 0x04000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EUSCIB0TX3 0x05000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_TIMERA3CCR0 0x06000006 |
Referenced by DMA_assignChannel().
#define DMA_CH6_EXTERNALPIN 0x07000006 |
Referenced by DMA_assignChannel().
#define DMA_CH7_RESERVED0 0x00000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_EUSCIA3RX 0x01000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_EUSCIB3RX0 0x02000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_EUSCIB2RX1 0x03000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_EUSCIB1RX2 0x04000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_EUSCIB0RX3 0x05000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_TIMERA3CCR2 0x06000007 |
Referenced by DMA_assignChannel().
#define DMA_CH7_ADC14 0x07000007 |
Referenced by DMA_assignChannel().
#define DMA_INT0 INT_DMA_INT0 |
Referenced by DMA_registerInterrupt(), and DMA_unregisterInterrupt().
#define DMA_INT1 INT_DMA_INT1 |
#define DMA_INT2 INT_DMA_INT2 |
#define DMA_INT3 INT_DMA_INT3 |
#define DMA_INTERR INT_DMA_ERR |
Referenced by DMA_registerInterrupt(), and DMA_unregisterInterrupt().
#define DMA_CHANNEL_0 0 |
#define DMA_CHANNEL_1 1 |
#define DMA_CHANNEL_2 2 |
#define DMA_CHANNEL_3 3 |
#define DMA_CHANNEL_4 4 |
#define DMA_CHANNEL_5 5 |
#define DMA_CHANNEL_6 6 |
#define DMA_CHANNEL_7 7 |
typedef struct _DMA_ControlTable DMA_ControlTable |
void DMA_enableModule | ( | void | ) |
Enables the DMA controller for use.
This function enables the DMA controller. The DMA controller must be enabled before it can be configured and used.
void DMA_disableModule | ( | void | ) |
Disables the DMA controller for use.
This function disables the DMA controller. Once disabled, the DMA controller cannot operate until re-enabled with DMA_enableModule().
uint32_t DMA_getErrorStatus | ( | void | ) |
Gets the DMA error status.
This function returns the DMA error status. It should be called from within the DMA error interrupt handler to determine if a DMA error occurred.
void DMA_clearErrorStatus | ( | void | ) |
Clears the DMA error interrupt.
This function clears a pending DMA error interrupt. This function should be called from within the DMA error interrupt handler to clear the interrupt.
void DMA_enableChannel | ( | uint32_t | channelNum | ) |
Enables a DMA channel for operation.
channelNum | is the channel number to enable. |
When a DMA transfer is completed, the channel is automatically disabled by the DMA controller. Therefore, this function should be called prior to starting up any new transfer.
References ASSERT.
void DMA_disableChannel | ( | uint32_t | channelNum | ) |
Disables a DMA channel for operation.
channelNum | is the channel number to disable. |
This function disables a specific DMA channel. Once disabled, a channel cannot respond to DMA transfer requests until re-enabled via DMA_enableChannel().
References ASSERT.
bool DMA_isChannelEnabled | ( | uint32_t | channelNum | ) |
Checks if a DMA channel is enabled for operation.
channelNum | is the channel number to check. |
This function checks to see if a specific DMA channel is enabled. This function can be used to check the status of a transfer, as the channel is automatically disabled at the end of a transfer.
References ASSERT.
void DMA_setControlBase | ( | void * | controlTable | ) |
Sets the base address for the channel control table.
controlTable | is a pointer to the 1024-byte-aligned base address of the DMA channel control table. |
This function configures the base address of the channel control table. This table resides in system memory and holds control information for each DMA channel. The table must be aligned on a 1024-byte boundary. The base address must be configured before any of the channel functions can be used.
The size of the channel control table depends on the number of DMA channels and the transfer modes that are used. Refer to the introductory text and the microcontroller datasheet for more information about the channel control table.
References ASSERT.
void* DMA_getControlBase | ( | void | ) |
Gets the base address for the channel control table.
This function gets the base address of the channel control table. This table resides in system memory and holds control information for each DMA channel.
void* DMA_getControlAlternateBase | ( | void | ) |
Gets the base address for the channel control table alternate structures.
This function gets the base address of the second half of the channel control table that holds the alternate control structures for each channel.
void DMA_requestChannel | ( | uint32_t | channelNum | ) |
Requests a DMA channel to start a transfer.
channelNum | is the channel number on which to request a DMA transfer. |
This function allows software to request a DMA channel to begin a transfer. This function could be used for performing a memory-to-memory transfer, or if for some reason a transfer needs to be initiated by software instead of the peripheral associated with that channel.
References ASSERT.
void DMA_enableChannelAttribute | ( | uint32_t | channelNum, |
uint32_t | attr | ||
) |
Enables attributes of a DMA channel.
channelNum | is the channel to configure. |
attr | is a combination of attributes for the channel. |
This function is used to enable attributes of a DMA channel.
The attr parameter is the logical OR of any of the following:
References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
void DMA_disableChannelAttribute | ( | uint32_t | channelNum, |
uint32_t | attr | ||
) |
Disables attributes of a DMA channel.
channelNum | is the channel to configure. |
attr | is a combination of attributes for the channel. |
This function is used to disable attributes of a DMA channel.
The attr parameter is the logical OR of any of the following:
References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
uint32_t DMA_getChannelAttribute | ( | uint32_t | channelNum | ) |
Gets the enabled attributes of a DMA channel.
channelNum | is the channel to configure. |
This function returns a combination of flags representing the attributes of the DMA channel.
References ASSERT, UDMA_ATTR_ALTSELECT, UDMA_ATTR_HIGH_PRIORITY, UDMA_ATTR_REQMASK, and UDMA_ATTR_USEBURST.
void DMA_setChannelControl | ( | uint32_t | channelStructIndex, |
uint32_t | control | ||
) |
Sets the control parameters for a DMA channel control structure.
channelStructIndex | is the logical OR of the DMA channel number with UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
control | is logical OR of several control values to set the control parameters for the channel. |
This function is used to set control parameters for a DMA transfer. These parameters are typically not changed often.
The channelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.
The control parameter is the logical OR of five values: the data size, the source address increment, the destination address increment, the arbitration size, and the use burst flag. The choices available for each of these values is described below.
Choose the data size from one of UDMA_SIZE_8, UDMA_SIZE_16, or UDMA_SIZE_32 to select a data size of 8, 16, or 32 bits.
Choose the source address increment from one of UDMA_SRC_INC_8, UDMA_SRC_INC_16, UDMA_SRC_INC_32, or UDMA_SRC_INC_NONE to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.
Choose the destination address increment from one of UDMA_DST_INC_8, UDMA_DST_INC_16, UDMA_DST_INC_32, or UDMA_SRC_INC_8 to select an address increment of 8-bit bytes, 16-bit half-words, 32-bit words, or to select non-incrementing.
The arbitration size determines how many items are transferred before the DMA controller re-arbitrates for the bus. Choose the arbitration size from one of UDMA_ARB_1, UDMA_ARB_2, UDMA_ARB_4, UDMA_ARB_8, through UDMA_ARB_1024 to select the arbitration size from 1 to 1024 items, in powers of 2.
The value UDMA_NEXT_USEBURST is used to force the channel to only respond to burst requests at the tail end of a scatter-gather transfer.
References ASSERT, and _DMA_ControlTable::control.
void DMA_setChannelTransfer | ( | uint32_t | channelStructIndex, |
uint32_t | mode, | ||
void * | srcAddr, | ||
void * | dstAddr, | ||
uint32_t | transferSize | ||
) |
Sets the transfer parameters for a DMA channel control structure.
channelStructIndex | is the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
mode | is the type of DMA transfer. |
srcAddr | is the source address for the transfer. |
dstAddr | is the destination address for the transfer. |
transferSize | is the number of data items to transfer. |
This function is used to configure the parameters for a DMA transfer. These parameters are typically changed often. The function DMA_setChannelControl() MUST be called at least once for this channel prior to calling this function.
The channelStructIndex parameter should be the logical OR of the channel number with one of UDMA_PRI_SELECT or UDMA_ALT_SELECT to choose whether the primary or alternate data structure is used.
The mode parameter should be one of the following values:
The srcAddr and dstAddr parameters are pointers to the first location of the data to be transferred. These addresses should be aligned according to the item size. The compiler takes care of this alignment if the pointers are pointing to storage of the appropriate data type.
The transferSize parameter is the number of data items, not the number of bytes.
The two scatter-gather modes, memory and peripheral, are actually different depending on whether the primary or alternate control structure is selected. This function looks for the UDMA_PRI_SELECT and UDMA_ALT_SELECT flag along with the channel number and sets the scatter-gather mode as appropriate for the primary or alternate control structure.
The channel must also be enabled using DMA_enableChannel() after calling this function. The transfer does not begin until the channel has been configured and enabled. Note that the channel is automatically disabled after the transfer is completed, meaning that DMA_enableChannel() must be called again after setting up the next transfer.
References ASSERT, _DMA_ControlTable::control, _DMA_ControlTable::dstEndAddr, _DMA_ControlTable::srcEndAddr, UDMA_ALT_SELECT, UDMA_DST_INC_NONE, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, UDMA_MODE_PER_SCATTER_GATHER, and UDMA_SRC_INC_NONE.
void DMA_setChannelScatterGather | ( | uint32_t | channelNum, |
uint32_t | taskCount, | ||
void * | taskList, | ||
uint32_t | isPeriphSG | ||
) |
Configures a DMA channel for scatter-gather mode.
channelNum | is the DMA channel number. |
taskCount | is the number of scatter-gather tasks to execute. |
taskList | is a pointer to the beginning of the scatter-gather task list. |
isPeriphSG | is a flag to indicate it is a peripheral scatter-gather transfer (else it is memory scatter-gather transfer) |
This function is used to configure a channel for scatter-gather mode. The caller must have already set up a task list and must pass a pointer to the start of the task list as the taskList parameter. The taskCount parameter is the count of tasks in the task list, not the size of the task list. The flag bIsPeriphSG should be used to indicate if scatter-gather should be configured for peripheral or memory operation.
References ASSERT, _DMA_ControlTable::control, _DMA_ControlTable::dstEndAddr, _DMA_ControlTable::spare, _DMA_ControlTable::srcEndAddr, and UDMA_ALT_SELECT.
uint32_t DMA_getChannelSize | ( | uint32_t | channelStructIndex | ) |
Gets the current transfer size for a DMA channel control structure.
channelStructIndex | is the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
This function is used to get the DMA transfer size for a channel. The transfer size is the number of items to transfer, where the size of an item might be 8, 16, or 32 bits. If a partial transfer has already occurred, then the number of remaining items is returned. If the transfer is complete, then 0 is returned.
References ASSERT, and _DMA_ControlTable::control.
uint32_t DMA_getChannelMode | ( | uint32_t | channelStructIndex | ) |
Gets the transfer mode for a DMA channel control structure.
channelStructIndex | is the logical OR of the DMA channel number with either UDMA_PRI_SELECT or UDMA_ALT_SELECT. |
This function is used to get the transfer mode for the DMA channel and to query the status of a transfer on a channel. When the transfer is complete the mode is UDMA_MODE_STOP.
References ASSERT, _DMA_ControlTable::control, UDMA_MODE_ALT_SELECT, UDMA_MODE_MEM_SCATTER_GATHER, and UDMA_MODE_PER_SCATTER_GATHER.
void DMA_assignChannel | ( | uint32_t | mapping | ) |
Assigns a peripheral mapping for a DMA channel.
mapping | is a macro specifying the peripheral assignment for a channel. |
This function assigns a peripheral mapping to a DMA channel. It is used to select which peripheral is used for a DMA channel. The parameter mapping should be one of the macros named UDMA_CHn_tttt from the header file dma.h. For example, to assign DMA channel 0 to the eUSCI AO RX channel, the parameter should be the macro UDMA_CH1_EUSCIA0RX.
Please consult the data sheet for a table showing all the possible peripheral assignments for the DMA channels for a particular device.
References ASSERT, DMA_CH0_AESTRIGGER0, DMA_CH0_EUSCIA0TX, DMA_CH0_EUSCIB0TX0, DMA_CH0_EUSCIB1TX3, DMA_CH0_EUSCIB2TX2, DMA_CH0_EUSCIB3TX1, DMA_CH0_RESERVED0, DMA_CH0_TIMERA0CCR0, DMA_CH1_AESTRIGGER1, DMA_CH1_EUSCIA0RX, DMA_CH1_EUSCIB0RX0, DMA_CH1_EUSCIB1RX3, DMA_CH1_EUSCIB2RX2, DMA_CH1_EUSCIB3RX1, DMA_CH1_RESERVED0, DMA_CH1_TIMERA0CCR2, DMA_CH2_AESTRIGGER2, DMA_CH2_EUSCIA1TX, DMA_CH2_EUSCIB0TX1, DMA_CH2_EUSCIB1TX0, DMA_CH2_EUSCIB2TX3, DMA_CH2_EUSCIB3TX2, DMA_CH2_RESERVED0, DMA_CH2_TIMERA1CCR0, DMA_CH3_EUSCIA1RX, DMA_CH3_EUSCIB0RX1, DMA_CH3_EUSCIB1RX0, DMA_CH3_EUSCIB2RX3, DMA_CH3_EUSCIB3RX2, DMA_CH3_RESERVED0, DMA_CH3_RESERVED1, DMA_CH3_TIMERA1CCR2, DMA_CH4_EUSCIA2TX, DMA_CH4_EUSCIB0TX2, DMA_CH4_EUSCIB1TX1, DMA_CH4_EUSCIB2TX0, DMA_CH4_EUSCIB3TX3, DMA_CH4_RESERVED0, DMA_CH4_RESERVED1, DMA_CH4_TIMERA2CCR0, DMA_CH5_EUSCIA2RX, DMA_CH5_EUSCIB0RX2, DMA_CH5_EUSCIB1RX1, DMA_CH5_EUSCIB2RX0, DMA_CH5_EUSCIB3RX3, DMA_CH5_RESERVED0, DMA_CH5_RESERVED1, DMA_CH5_TIMERA2CCR2, DMA_CH6_EUSCIA3TX, DMA_CH6_EUSCIB0TX3, DMA_CH6_EUSCIB1TX2, DMA_CH6_EUSCIB2TX1, DMA_CH6_EUSCIB3TX0, DMA_CH6_EXTERNALPIN, DMA_CH6_RESERVED0, DMA_CH6_TIMERA3CCR0, DMA_CH7_ADC14, DMA_CH7_EUSCIA3RX, DMA_CH7_EUSCIB0RX3, DMA_CH7_EUSCIB1RX2, DMA_CH7_EUSCIB2RX1, DMA_CH7_EUSCIB3RX0, DMA_CH7_RESERVED0, and DMA_CH7_TIMERA3CCR2.
void DMA_requestSoftwareTransfer | ( | uint32_t | channel | ) |
Initializes a software transfer of the corresponding DMA channel. This is done if the user wants to force a DMA on the specified channel without the hardware precondition. Specific channels can be configured using the DMA_assignChannel function.
channel | is the channel to trigger the interrupt |
void DMA_assignInterrupt | ( | uint32_t | interruptNumber, |
uint32_t | channel | ||
) |
Assigns a specific DMA channel to the corresponding interrupt handler. For MSP432 devices, there are three configurable interrupts, and one master interrupt. This function will assign a specific DMA channel to the provided configurable DMA interrupt.
Note that once a channel is assigned to a configurable interrupt, it will be masked in hardware from the master DMA interrupt (interruptNumber zero). This function can also be used in conjunction with the DMAIntTrigger function to provide the feature to software trigger specific channel interrupts.
interruptNumber | is the configurable interrupt to assign the given channel. Valid values are:
|
channel | is the channel to assign the interrupt |
References ASSERT, DMA_enableInterrupt(), DMA_INT1, DMA_INT2, and DMA_INT3.
void DMA_enableInterrupt | ( | uint32_t | interruptNumber | ) |
Enables the specified interrupt for the DMA controller. Note for interrupts one through three, specific channels have to be mapped to the interrupt using the DMA_assignInterrupt function.
interruptNumber | identifies which DMA interrupt is to be enabled. This interrupt should be one of the following: |
References ASSERT, DMA_INT1, DMA_INT2, and DMA_INT3.
Referenced by DMA_assignInterrupt().
void DMA_disableInterrupt | ( | uint32_t | interruptNumber | ) |
Disables the specified interrupt for the DMA controller.
interruptNumber | identifies which DMA interrupt is to be disabled. This interrupt should be one of the following: |
DMA_INT3 the third configurable DMA interrupt handler
Note for interrupts that are associated with a specific DMA channel (DMA_INT1 - DMA_INT3), this function will also enable that specific channel for interrupts.
uint32_t DMA_getInterruptStatus | ( | void | ) |
Gets the DMA controller channel interrupt status for interrupt zero.
This function is used to get the interrupt status of the DMA controller. The returned value is a 32-bit bit mask that indicates which channels are requesting an interrupt. This function can be used from within an interrupt handler to determine or confirm which DMA channel has requested an interrupt.
Note that this will only apply to interrupt zero for the DMA controller as only one interrupt can be associated with interrupts one through three. If an interrupt is assigned to an interrupt other than interrupt zero, it will be masked by this function.
void DMA_clearInterruptFlag | ( | uint32_t | channel | ) |
Clears the DMA controller channel interrupt mask for interrupt zero.
channel | is the channel interrupt to clear. |
This function is used to clear the interrupt status of the DMA controller. Note that only interrupts that weren't assigned to DMA interrupts one through three using the DMA_assignInterrupt function will be affected by this function. For other DMA interrupts, only one channel can be associated and therefore clearing is unnecessary.
void DMA_registerInterrupt | ( | uint32_t | interruptNumber, |
void(*)(void) | intHandler | ||
) |
Registers an interrupt handler for the DMA controller.
interruptNumber | identifies which DMA interrupt is to be registered. |
intHandler | is a pointer to the function to be called when the interrupt is called. |
This function registers and enables the handler to be called when the DMA controller generates an interrupt. The interrupt parameter should be one of the following:
References ASSERT, DMA_INT0, DMA_INT1, DMA_INT2, DMA_INT3, DMA_INTERR, Interrupt_enableInterrupt(), and Interrupt_registerInterrupt().
void DMA_unregisterInterrupt | ( | uint32_t | interruptNumber | ) |
Unregisters an interrupt handler for the DMA controller.
interruptNumber | identifies which DMA interrupt to unregister. |
This function disables and unregisters the handler to be called for the specified DMA interrupt. The interrupt parameter should be one of the parameters as documented for the function DMA_registerInterrupt().
Note for interrupts that are associated with a specific DMA channel (DMA_INT1 - DMA_INT3), this function will also disable that specific channel for interrupts.
References ASSERT, DMA_INT0, DMA_INT1, DMA_INT2, DMA_INT3, DMA_INTERR, Interrupt_disableInterrupt(), and Interrupt_unregisterInterrupt().