File List
Here is a list of all files with brief descriptions:
 ADC.hADC driver interface
 ADCBuf.hADCBuf driver interface
 ADCBufMSP432.hADC driver implementation for a MSP432 analog-to-digital converter
 ADCMSP432.hADC driver implementation for the ADC peripheral on MSP432
 Camera.hCamera driver interface
 Capture.hCapture driver interface
 CaptureMSP432.hCapture driver interface for MSP432 devices
 Display.hGeneric interface for text output
 DisplayHost.hDisplay driver for printf-like output
 DisplayUart.hDisplay.h implementation for UART output
 GPIO.hGPIO driver
 GPIOMSP432.hGPIO driver implementation for MSP432 devices
 I2C.hI2C driver interface
 I2CMSP432.hI2C driver implementation for the EUSCI controller on MSP432
 I2CSlave.hI2CSlave driver interface
 I2CSlaveMSP432.hI2CSlave driver implementation for the EUSCI controller on MSP432
 I2S.hI2S driver interface
 List.hLinked List interface for use in drivers
 NVS.hNon-Volatile Storage driver interface
 NVSMSP432.h
 NVSSPI25X.hNon-Volatile Storage driver implementation for SPI flash peripherals
 PIN.hGeneric PIN & GPIO driver
 Power.hPower manager interface
 PowerMSP432.hPower manager interface for the MSP432
 PWM.hPWM driver interface
 PWMTimerMSP432.hPWM driver implementation using the MSP432 Timer_A peripherals
 RingBuf.h
 SD.hSD driver interface
 SDFatFS.hFATFS driver interface
 SDSPI.hSDSPI driver interface
 SDSPIMSP432.hSDSPI driver implementation using an EUSCI SPI peripheral for MSP432
 SPI.hSPI driver interface
 SPIMSP432DMA.hSPI driver implementation for a EUSCI peripheral on MSP432 using the micro DMA controller
 Timer.hTimer driver interface
 TimerMSP432.hTimer driver interface for MSP432 devices
 UART.hUART driver interface
 UARTMSP432.hUART driver implementation for a EUSCIA peripheral for MSP432
 UDMAMSP432.hUDMA driver implementation for MSP432
 Watchdog.hWatchdog driver interface
 WatchdogMSP432.hWatchdog driver implementation for MSP432
Copyright 2017, Texas Instruments Incorporated