![]() |
![]() |
| C_TimerMSP432_HWAttr | TimerMSP432 Hardware Attributes |
| CADC_Config_ | ADC Global configuration |
| CADC_FxnTable_ | The definition of a ADC function table that contains the required set of functions to control a specific ADC driver implementation |
| CADC_Params_ | ADC Parameters |
| CADCBuf_Config_ | ADCBuf Global configuration |
| CADCBuf_Conversion_ | An ADCBuf_Conversion data structure is used with ADCBuf_convert(). It indicates which channel to perform the ADC conversion on, how many conversions to make, and where to put them. The arg variable is an user-definable argument which gets passed to the ADCBuf_Callback when the ADC driver is in ADCBuf_RETURN_MODE_CALLBACK |
| CADCBuf_FxnTable_ | The definition of an ADCBuf function table that contains the required set of functions to control a specific ADC driver implementation |
| CADCBuf_Params_ | ADC Parameters |
| CADCBufMSP432_Channels | ADCMSP432 Channel setting These fields define channel-specific settings: GPIO and reference voltage. These settings happen when ADCBuf_convert() is called |
| CADCBufMSP432_HWAttrs | ADCBufMSP432 Hardware attributes These fields are populated by PinMux tool but user is allowed to change for different channels setting |
| CADCBufMSP432_Object | ADCBufMSP432 Object |
| CADCBufMSP432_ParamsExtension | MSP432 specfic extension to ADCBuf_Params |
| CADCMSP432_HWAttrsV1 | ADCMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSPWare these definitions are found in: |
| CADCMSP432_Object | ADCMSP432 Object |
| CCamera_Config_ | Camera Global configuration |
| CCamera_FxnTable_ | The definition of a Camera function table that contains the required set of functions to control a specific Camera driver implementation |
| CCamera_Params_ | Camera Parameters |
| CCapture_Config_ | Capture Global configuration |
| CCapture_FxnTable_ | The definition of a capture function table that contains the required set of functions to control a specific capture driver implementation |
| CCapture_Params_ | Capture Parameters |
| CCaptureMSP432_HWAttrs | CaptureMSP432 Hardware Attributes |
| CCaptureMSP432_Object | CaptureMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure |
| CDisplay_Config | Display Global configuration |
| CDisplay_FxnTable | The definition of a Display function table that contains the required set of functions to control a specific Display driver implementation |
| CDisplay_Params | Display Parameters |
| CDisplayHost_HWAttrs | DisplayHost Attributes |
| CDisplayHost_Object | DisplayHost Object |
| CDisplayUart_HWAttrs | DisplayUart Attributes |
| CDisplayUart_Object | DisplayUart Object |
| CGPIOMSP432_Config | GPIO device specific driver configuration structure |
| CI2C_Config_ | I2C global configuration |
| CI2C_FxnTable_ | The definition of an I2C function table that contains the required set of functions to control a specific I2C driver implementation |
| CI2C_Params_ | I2C Parameters |
| CI2C_Transaction_ | I2C transaction |
| CI2CMSP432_HWAttrsV1 | I2CMSP432 Hardware attributes |
| CI2CSlave_Config_ | I2CSlave Global configuration |
| CI2CSlave_FxnTable_ | The definition of a I2CSlave function table that contains the required set of functions to control a specific I2CSlave driver implementation |
| CI2CSlave_Params_ | I2CSlave Parameters |
| CI2CSlaveMSP432_HWAttrs | I2CSlaveMSP432 Hardware attributes These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in: |
| CI2CSlaveMSP432_Object | I2CSlaveMSP432 Object |
| CI2S_BufDesc_ | I2S buffer descriptor for issue/reclaim mode |
| CI2S_Config_ | I2S Global configuration |
| CI2S_FxnTable_ | The definition of a I2S function table that contains the required set of functions to control a specific I2S driver implementation |
| CI2S_Params_ | Basic I2S Parameters |
| CList_Elem | |
| CList_List | |
| CNVS_Attrs | NVS attributes |
| CNVS_Config_ | NVS Global configuration |
| CNVS_FxnTable | The definition of an NVS function table that contains the required set of functions to control a specific NVS driver implementation |
| CNVS_Params | NVS Parameters |
| CNVSMSP432_HWAttrs | NVSMSP432 attributes |
| CNVSMSP432_Object | |
| CNVSSPI25X_HWAttrs | NVSSPI25X attributes |
| CNVSSPI25X_Object | |
| CPIN_State_s | Underlying data structure for type PIN_State |
| CPower_NotifyObj_ | Power notify object structure |
| CPowerMSP432_ConfigV1 | Power global configuration (MSP432-specific) |
| CPowerMSP432_Freqs | Structure holding device frequencies (in Hz) |
| CPowerMSP432_PerfLevel | Structure defining a performance level |
| CPWM_Config_ | PWM Global configuration |
| CPWM_FxnTable_ | The definition of a PWM function table that contains the required set of functions to control a specific PWM driver implementation |
| CPWM_Params_ | PWM Parameters |
| CPWMTimerMSP432_HWAttrsV2 | PWMTimerMSP432 Hardware attributes |
| CPWMTimerMSP432_Object | PWMTimerMSP432 Object |
| CPWMTimerMSP432_Status | PWMTimerMSP432_Status |
| CRingBuf_Object | |
| CSD_Config_ | SD Global configuration |
| CSD_FxnTable_ | The definition of a SD function table that contains the required set of functions to control a specific SD driver implementation |
| CSD_Params_ | SD Parameters |
| CSDFatFS_Config_ | SDFatFS Global configuration |
| CSDFatFS_Object_ | SDFatFS Object The application must not access any member variables of this structure! |
| CSDSPI_Config_ | SDSPI Global configuration |
| CSDSPI_FxnTable_ | The definition of a SDSPI function table that contains the required set of functions to control a specific SDSPI driver implementation |
| CSDSPI_Params_ | SDSPI Parameters |
| CSDSPIMSP432_HWAttrs | SDSPIMSP432 Hardware attributes |
| CSDSPIMSP432_HWAttrsV1 | |
| CSDSPIMSP432_Object | SDSPIMSP432 Object |
| CSPI_Config_ | SPI Global configuration |
| CSPI_FxnTable_ | The definition of a SPI function table that contains the required set of functions to control a specific SPI driver implementation |
| CSPI_Params_ | SPI Parameters |
| CSPI_Transaction_ | A SPI_Transaction data structure is used with SPI_transfer(). It indicates how many SPI_FrameFormat frames are sent and received from the buffers pointed to txBuf and rxBuf. The arg variable is an user-definable argument which gets passed to the SPI_CallbackFxn when the SPI driver is in SPI_MODE_CALLBACK |
| CSPIMSP432DMA_HWAttrsV1 | SPIMSP432DMA Hardware attributes These fields, with the exception of intPriority, are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432 driverlib these definitions are found in: |
| CSPIMSP432DMA_Object | SPIMSP432DMA Object |
| CTimer_Config_ | Timer Global configuration |
| CTimer_FxnTable_ | The definition of a timer function table that contains the required set of functions to control a specific timer driver implementation |
| CTimer_Params_ | Timer Parameters |
| CTimerMSP432_Object | TimerMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure |
| CUART_Config_ | UART Global configuration |
| CUART_FxnTable_ | The definition of a UART function table that contains the required set of functions to control a specific UART driver implementation |
| CUART_Params_ | UART Parameters |
| CUARTMSP432_BaudrateConfig | UARTMSP432 Baudrate configuration |
| CUARTMSP432_FxnSet | Complement set of read functions to be used by the UART ISR and UARTMSP432_read(). Internal use only |
| CUARTMSP432_HWAttrsV1 | UARTMSP432 Hardware attributes |
| CUARTMSP432_Object | UARTMSP432 Object |
| CUDMAMSP432_Config | UDMAMSP432 Global configuration |
| CUDMAMSP432_HWAttrs | UDMAMSP432 Hardware attributes |
| CUDMAMSP432_Object | UDMAMSP432 object |
| CWatchdog_Config_ | Watchdog Global configuration |
| CWatchdog_FxnTable_ | The definition of a Watchdog function table that contains the required set of functions to control a specific Watchdog driver implementation |
| CWatchdog_Params_ | Watchdog Parameters |
| CWatchdogMSP432_HWAttrs | Watchdog hardware attributes for MSP432 These fields are used by driverlib APIs and therefore must be populated by driverlib macro definitions. For MSP432Ware these definitions are found in: |
| CWatchdogMSP432_Object | Watchdog Object for MSP432 |