CaptureMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure. More...
#include <CaptureMSP432.h>
Data Fields | |
Capture_Config * | config |
HwiP_Params | hwiParams |
HwiP_Handle | hwiHandle |
Capture_CallBackFxn | callBack |
Capture_Period_Unit | periodUnits |
uint32_t | captureCount |
uint32_t | ccrRegister |
uint32_t | intNum |
bool | isRunning |
CaptureMSP432 Object Driver specific structure that takes care of various driver parameters such as hardware interrupts and callbacks. The application should not modify any members of this structure.
Capture_Config* CaptureMSP432_Object::config |
HwiP_Params CaptureMSP432_Object::hwiParams |
HwiP_Handle CaptureMSP432_Object::hwiHandle |
Capture_CallBackFxn CaptureMSP432_Object::callBack |
Capture_Period_Unit CaptureMSP432_Object::periodUnits |
uint32_t CaptureMSP432_Object::captureCount |
uint32_t CaptureMSP432_Object::ccrRegister |
uint32_t CaptureMSP432_Object::intNum |
bool CaptureMSP432_Object::isRunning |