TI BLE Stack API Documentation
2.03.10
|
Macros | |
#define | GAP_DEVICE_INIT_DONE_EVENT 0x00 |
Sent when the Device Initialization is complete. This event is sent as an OSAL message defined as gapDeviceInitDoneEvent_t. | |
#define | GAP_DEVICE_DISCOVERY_EVENT 0x01 |
Sent when the Device Discovery Process is complete. This event is sent as an OSAL message defined as gapDevDiscEvent_t. | |
#define | GAP_ADV_DATA_UPDATE_DONE_EVENT 0x02 |
Sent when the Advertising Data or SCAN_RSP Data has been updated. This event is sent as an OSAL message defined as gapAdvDataUpdateEvent_t. | |
#define | GAP_MAKE_DISCOVERABLE_DONE_EVENT 0x03 |
Sent when the Make Discoverable Request is complete. This event is sent as an OSAL message defined as gapMakeDiscoverableRspEvent_t. | |
#define | GAP_END_DISCOVERABLE_DONE_EVENT 0x04 |
Sent when the Advertising has ended. This event is sent as an OSAL message defined as gapEndDiscoverableRspEvent_t. | |
#define | GAP_LINK_ESTABLISHED_EVENT 0x05 |
Sent when the Establish Link Request is complete. This event is sent as an OSAL message defined as gapEstLinkReqEvent_t. | |
#define | GAP_LINK_TERMINATED_EVENT 0x06 |
Sent when a connection was terminated. This event is sent as an OSAL message defined as gapTerminateLinkEvent_t. | |
#define | GAP_LINK_PARAM_UPDATE_EVENT 0x07 |
Sent when an Update Parameters Event is received. This event is sent as an OSAL message defined as gapLinkUpdateEvent_t. | |
#define | GAP_RANDOM_ADDR_CHANGED_EVENT 0x08 |
Sent when a random address was changed. This event is sent as an OSAL message defined as gapRandomAddrEvent_t. | |
#define | GAP_SIGNATURE_UPDATED_EVENT 0x09 |
Sent when the device's signature counter is updated. This event is sent as an OSAL message defined as gapSignUpdateEvent_t. | |
#define | GAP_AUTHENTICATION_COMPLETE_EVENT 0x0A |
Sent when the Authentication (pairing) process is complete. This event is sent as an OSAL message defined as gapAuthCompleteEvent_t. | |
#define | GAP_PASSKEY_NEEDED_EVENT 0x0B |
Sent when a Passkey is needed. This is part of the pairing process. This event is sent as an OSAL message defined as gapPasskeyNeededEvent_t. | |
#define | GAP_SLAVE_REQUESTED_SECURITY_EVENT 0x0C |
Sent when a Slave Security Request is received. This event is sent as an OSAL message defined as gapSlaveSecurityReqEvent_t. | |
#define | GAP_DEVICE_INFO_EVENT 0x0D |
Sent during the Device Discovery Process when a device is discovered. This event is sent as an OSAL message defined as gapDeviceInfoEvent_t. | |
#define | GAP_BOND_COMPLETE_EVENT 0x0E |
Sent when the bonding(bound) process is complete. This event is sent as an OSAL message defined as gapBondCompleteEvent_t. | |
#define | GAP_PAIRING_REQ_EVENT 0x0F |
Sent when an unexpected Pairing Request is received. This event is sent as an OSAL message defined as gapPairingReqEvent_t. | |
#define | GAP_AUTHENTICATION_FAILURE_EVT 0x10 |
Sent when pairing fails, no GAP_AUTHENTICATION_COMPLETE_EVENT is sent and GBM_QUEUE_PAIRINGS. This event is sent as an OSAL message defined as osal_event_hdr_t. | |
#define | GAP_UPDATE_LINK_PARAM_REQ_EVENT 0x11 |
Sent when during a Connection Parameter Update Procedure. This event is sent as an OSAL message defined as gapConnParamUpdate_t. | |