TI BLE Stack API Documentation
2.03.10
|
#include <gap.h>
Public Attributes | |
osal_event_hdr_t | hdr |
GAP_MSG_EVENT and status. | |
uint8 | opcode |
GAP_LINK_PARAM_UPDATE_EVENT. | |
uint8 | status |
bStatus_t | |
uint16 | connectionHandle |
Connection handle of the update. | |
uint16 | connInterval |
Requested connection interval. | |
uint16 | connLatency |
Requested connection latency. | |
uint16 | connTimeout |
Requested connection timeout. | |
GAP_LINK_PARAM_UPDATE_EVENT message format. This message is sent to the app when the connection parameters update request is complete.