TI BLE Stack API Documentation
2.03.10
|
#include <gap.h>
Public Attributes | |
osal_event_hdr_t | hdr |
GAP_MSG_EVENT and status. | |
uint8 | opcode |
GAP_PASSKEY_NEEDED_EVENT. | |
uint8 | deviceAddr [6] |
address of device to pair with, and could be either public or random. | |
uint16 | connectionHandle |
Connection handle. | |
uint8 | uiInputs |
Pairing User Interface Inputs - Ask user to input passcode. | |
uint8 | uiOutputs |
Pairing User Interface Outputs - Display passcode. | |
uint32 | numComparison |
Numeric Comparison value to be displayed. | |
GAP_PASSKEY_NEEDED_EVENT message format. This message is sent to the app when a Passkey is needed from the app's user interface.