3.1.2.3. SD, eMMC and USB
Warning
There is important information on multimedia card (MMC) support for AM62x device, go here for more information.
3.1.2.3.1. Overview
The following guide shows how to flash and boot from storage media such as the embedded multimedia card (eMMC), secure digital (SD) card, and USB storage devices. While this is a step-by-step guide, it is in no way extensive and does not cover all the per-platform corner-cases. For any issues or questions on this guide, reach out to: Help e2e.
3.1.2.3.2. MMC
3.1.2.3.2.1. Listing MMC devices
Usually in all the platforms there will be two multimedia card (MMC) instances of which one would be SD and the other would be eMMC. The device index of them can vary from one class of platforms to the other. For a given platform, the device index can be found in the following way:
=> mmc list
sdhci@fa10000: 0 (eMMC)
sdhci@fa00000: 1 (SD)
The device index “0” for eMMC will be used when flashing to the eMMC device here using mmc dev command.
In u-boot environment, usually mmcdev=n is used to select which MMC device to boot Linux from, where n is the device index.
3.1.2.3.2.2. MMC HW partitions
This sections includes a summary of MMC hardware partitions.
eMMC
Normally eMMC is divided into 4 areas (also known as HW partitions):
User data area (UDA): Used to store user data such as a file system. This partition can divided into disk partitions
Boot0/1: Used to store firmware and data needed during boot
Replay protected memory block (RPMB) : Used to store secure data
SD
SD card memory is not divided into sections such as eMMC, but acts like UDA in eMMC where user can create disk partitions in software allowing to divide the storage space into multiple sections.
3.1.2.3.2.3. Selecting MMC device and partitions
To select an MMC device in u-boot, the command: mmc dev could be used. The general syntax is:
=> mmc dev [dev] [partition]
Where [dev] is the MMC device index.
The following lists examples and their explanation for each MMC device and partitions according to the example here.
=> mmc dev 0 0 # select eMMC UDA
=> mmc dev 0 1 # select eMMC Boot0
=> mmc dev 0 2 # select eMMC Boot1
=> mmc dev 1 # select SD
3.1.2.3.2.4. View MMC partition contents
This section assumes an SD card or eMMC was prepared previously to boot the device.
Note
For eMMC, typically, the device ships without a partition table If there is a need to create a partition in UDA, go here and to format the partition go here before proceeding.
To list disk partitions for any MMC device from u-boot prompt, use the command: mmc part.
=> mmc dev 0
switch to partitions #0, OK
mmc0(part 0) is current device
=> mmc part
Partition Map for MMC device 0  --   Partition Type: DOS
Part   Start Sector    Num Sectors     UUID           Type
 1     2048            31078400        8ece5cfe-01    83
If the partitions are formatted with a file system type that is supported by u-boot, you can view the contents of the MMC partition as show below:
=> ls mmc 0:1
<DIR>       4096 .
<DIR>       4096 ..
<SYM>          7 bin
<DIR>       4096 boot
<DIR>       4096 dev
<DIR>       4096 etc
<DIR>       4096 home
<SYM>          7 lib
<DIR>       4096 media
<DIR>       4096 mnt
<DIR>       4096 opt
<DIR>       4096 proc
<DIR>       4096 root
<DIR>       4096 run
<SYM>          8 sbin
<DIR>       4096 srv
<DIR>       4096 sys
<DIR>       4096 tmp
<DIR>       4096 usr
<DIR>       4096 var
=> ls mmc 0:1 boot/dtb/ti
<DIR>       4096 .
<DIR>       4096 ..
           60319 k3-am625-sk.dtb
Where the general syntax is:
$ ls <interface> [<dev[:partition]> [directory]]
3.1.2.3.2.5. MMC supported boot modes
The K3 based processors support and recommends using eMMC boot from Boot0 or Boot1. For complete
information on the MMC boot modes supported by ROM, refer to the device specific TRM,
under: Initialization/Boot Mode Pins. ROM supports the following two MMC boot modes:
eMMC boot
This boot mode is a special boot mode specific to eMMC device. In this boot mode, ROM cannot boot from SD and can only boot from Boot0 or Boot1 in eMMC. Go here for a step-by-step guide to boot with this boot mode.
MMCSD boot
This boot mode allows to boot from either eMMC or SD device. With this boot mode, ROM can only boot from SD card or UDA in eMMC. ROM allows to boot in raw or filesystem (FS) mode, FS mode being the recommended option and therefore will have a subsequent guide to boot using this mode. Configuration for selecting MMC device and raw/FS mode, is done with boot mode pins, refer to TRM for this setup. To boot from eMMC UDA in FS mode, go here.
3.1.2.3.2.6. Flashing an MMC device using USB-DFU
To flash the eMMC device (Boot0) using USB-DFU, the device should be booted to u-boot prompt and a USB cable connected from the host machine to the device USB port configured to USB peripheral mode.
From u-boot prompt enter the following:
=> setenv dfu_alt_info ${dfu_alt_info_emmc}
=> dfu 0 mmc 0
This command assumes eMMC device exists and is MMC device 0.
On the host machine have the boot loader binaries ready to flash to eMMC Boot0. Run the dfu-util to transfer files to the device. The general syntax for dfu-util command is:
$ sudo dfu-util -R -a <dfu-target> -D <binary>
To see what are the dfu-targets, on the host machine run: sudo dfu-util -l
$ sudo dfu-util -l
dfu-util 0.9
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=6, name="sysfw.itb.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=5, name="u-env.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=4, name="u-boot.img.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=3, name="tispl.bin.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=2, name="tiboot3.bin.raw", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=1, name="rootfs", serial="0000000000000591"
Found DFU: [0451:6165] ver=0223, devnum=32, cfg=1, intf=0, path="1-10", alt=0, name="rawemmc", serial="0000000000000591"
Then transfer each binary from the host to the device:
- Host: - $ sudo dfu-util -R -a tiboot3.bin.raw -D tiboot3.bin $ sudo dfu-util -R -a tispl.bin.raw -D tispl.bin $ sudo dfu-util -R -a u-boot.img.raw -D u-boot.img 
- Device: - ##DOWNLOAD ... OK Ctrl+C to exit ... ##DOWNLOAD ... OK Ctrl+C to exit ... ##DOWNLOAD ... OK Ctrl+C to exit ... 
3.1.2.3.2.7. Flashing an SD card from a host PC
This section assumes that you have flashed an SD card by using the script “create-sdcard.sh” packaged in the installation program or have made a compatible layout manually. In this case, you will need to copy the boot images:
- tiboot3.bin
- tispl.bin
- u-boot.img
to the SD card boot partition. At this point, the device can boot to u-boot prompt.
3.1.2.3.3. USB
3.1.2.3.3.1. Configuring USB in Host Mode
Note
There are two instances of USB on AM62 SoC. On the SK board, zeroth instance is brought out through a Type C port and the first instance is brought through a Type A port. By default, USB0 port is configured to be in peripheral mode. Since U-Boot does not support dynamic switching of USB roles, below DT fragment needs to be applied and U-Boot image needs to be rebuilt to make USB0 port to be USB 2.0 host port.
diff --git a/arch/arm/dts/k3-am625-sk-u-boot.dtsi b/arch/arm/dts/k3-am625-sk-u-boot.dtsi
index 20c24d2fa7a4..2b662653023f 100644
--- a/arch/arm/dts/k3-am625-sk-u-boot.dtsi
+++ b/arch/arm/dts/k3-am625-sk-u-boot.dtsi
@@ -117,5 +117,5 @@
 };
 &usb0 {
-       dr_mode = "peripheral";
+       dr_mode = "host";
        u-boot,dm-spl;
3.1.2.3. Loading images from USB storage
For loading images from a FAT partition on a different media than MMC, replace the mmc command with the required media. For example, to load images from a FAT partition on a USB storage device connected to the zeroth instance of USB:
=> fatload usb 0 ${loadaddr} <file name>
3.1.2.3.3.2. Flash and boot SPL from USB storage
Boot SPL from USB storage documentation is pending for AM62x reach out to: Help e2e for additional information.
3.1.2.3.3.3. Boot Linux from USB storage
To load the Linux kernel, Device Tree and the Root file system from USB Mass storage device, the following changes are required to be done:
- U-Boot - In U-Boot the USB controller can be used in either host or peripheral mode. For booting to Linux kernel from USB storage device, the USB port is to be set as host. 
- By default, on AM625-SK board the zero instance of USB connected to the Type C port, is set to peripheral mode and the first instance of USB connected to the Type A port is set to host mode. 
- Therefore, USB controller needs to be set host mode and custom boot loader images are required to be built, if zeroth instance is used. Refer to note in section Configuring USB in Host Mode 
 
- Linux - In Linux, by default the USB subsystem is built as modules. For booting from USB mass storage device, USB subsytem is required to be built into the image. This can be done by making the following changes in the configuration used for building kernel: 
 - CONFIG_USB_COMMON=y CONFIG_USB=y CONFIG_USB_XHCI_HCD=y CONFIG_USB_XHCI_PCI=y CONFIG_USB_XHCI_PLATFORM=y CONFIG_USB_STORAGE=y CONFIG_USB_DWC3=y CONFIG_USB_DWC3_AM62=y CONFIG_USB_GADGET=y CONFIG_TYPEC=y CONFIG_TYPEC_TPS6598X=y CONFIG_USB_ROLE_SWITCH=y 
Copying the images to USB storage device
After making the required changes mentioned above, build the kernel, device tree file and modules.
The USB Mass storage device should have the rootfs as the second partition with ext4 file system. The following images should be in /boot/ directory:
Linux kernel Image
Device tree (dtb) file
Run usbboot
During boot, cancel the autoboot at U-Boot and run the following command at u-boot prompt:
=> run usbboot
3.1.2.3.3.4. MMC support in u-boot
Missing eMMC support
Support for eMMC is missing for AM62SIP SK in Processor SDK 11.01. Therefore, eMMC boot, reading/writting/accessing the eMMC will not work on AM62SIP SK. If eMMC support is required, apply the following diff to k3-am6254xxl-sk.dts:
diff --git a/dts/upstream/src/arm64/ti/k3-am6254xxl-sk.dts b/dts/upstream/src/arm64/ti/k3-am6254xxl-sk.dts
index 060df318b3f..d2c9f226b73 100644
--- a/dts/upstream/src/arm64/ti/k3-am6254xxl-sk.dts
+++ b/dts/upstream/src/arm64/ti/k3-am6254xxl-sk.dts
@@ -42,6 +42,22 @@
};
&main_pmx0 {
+       main_mmc0_pins_default: main-mmc0-default-pins {
+               bootph-all;
+               pinctrl-single,pins = <
+                       AM62X_IOPAD(0x220, PIN_INPUT, 0) /* (Y3) MMC0_CMD */
+                       AM62X_IOPAD(0x218, PIN_INPUT, 0) /* (AB1) MMC0_CLK */
+                       AM62X_IOPAD(0x214, PIN_INPUT, 0) /* (AA2) MMC0_DAT0 */
+                       AM62X_IOPAD(0x210, PIN_INPUT_PULLUP, 0) /* (AA1) MMC0_DAT1 */
+                       AM62X_IOPAD(0x20c, PIN_INPUT_PULLUP, 0) /* (AA3) MMC0_DAT2 */
+                       AM62X_IOPAD(0x208, PIN_INPUT_PULLUP, 0) /* (Y4) MMC0_DAT3 */
+                       AM62X_IOPAD(0x204, PIN_INPUT_PULLUP, 0) /* (AB2) MMC0_DAT4 */
+                       AM62X_IOPAD(0x200, PIN_INPUT_PULLUP, 0) /* (AC1) MMC0_DAT5 */
+                       AM62X_IOPAD(0x1fc, PIN_INPUT_PULLUP, 0) /* (AD2) MMC0_DAT6 */
+                       AM62X_IOPAD(0x1f8, PIN_INPUT_PULLUP, 0) /* (AC2) MMC0_DAT7 */
+               >;
+       };
+
      main_rgmii2_pins_default: main-rgmii2-default-pins {
               bootph-all;
               pinctrl-single,pins = <
@@ -147,6 +163,14 @@
      };
};
+&sdhci0 {
+       bootph-all;
+       status = "okay";
+       pinctrl-names = "default";
+       pinctrl-0 = <&main_mmc0_pins_default>;
+};
+
&sdhci1 {
      vmmc-supply = <&vdd_mmc1>;
      vqmmc-supply = <&vdd_sd_dv>;
3.1.2.3.3.5. Steps for working around SD card issues in u-boot
In some cases, issues can be seen while using some SD cards, such as:
- Error while trying to initialize: - U-Boot SPL 2021.01-g74fc69c889 (May 19 2022 - 02:44:29 +0000) SYSFW ABI: 3.1 (firmware rev 0x0008 '8.3.2--v08.03.02 (Jolly Jellyfi') Trying to boot from MMC2 spl: mmc init failed with error: -110 SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ### 
Given below are the list of various workarounds that can be done in the device tree MMC node to get SD card working. The workarounds are ordered in increasing order of reducing performance.
Note
All the mentioned below, are to be done in the MMC device tree node corresponding to the SD instance. This is usually the first (index starting from zero) instance.
- Restricting to a given speed mode - By default the U-Boot driver tries to enumerate a SD card in the highest supported speed mode. Given below is the order in which the driver tries to enumerate a SD card: - SDR104 
- SDR50 
- DDR50 
- SD HS 
- SD legacy 
 - The sdhci-caps-mask can be added to the DT node to cap at a specific mode: - Limit to DDR50: - sdhci-caps-mask = <0x00000003 0x00000000>
- Limit to SD HS: - sdhci-caps-mask = <0x00000007 0x00000000>
- Limit to SD legacy: - sdhci-caps-mask = <0x00000007 0x00200000>
 - &sdhci1 { /* SD/MMC */ vmmc-supply = <&vdd_mmc1>; vqmmc-supply = <&vdd_sd_dv>; pinctrl-names = "default"; pinctrl-0 = <&main_mmc1_pins_default>; ti,driver-strength-ohm = <50>; disable-wp; sdhci-caps-mask = <0x00000003 0x00000000>; /* Limiting to DDR50 speed mode */ }; 
- Increase power cycle period - Increasing the delay while power cycling the SD card. This can be done by increasing the delay value in the diff indicated below, - diff --git a/drivers/mmc/mmc.c b/drivers/mmc/mmc.c index f486e2a2c364..38cc956b3d53 100644 --- a/drivers/mmc/mmc.c +++ b/drivers/mmc/mmc.c @@ -2761,7 +2761,7 @@ static int mmc_power_cycle(struct mmc *mmc) * SD spec recommends at least 1ms of delay. Let's wait for 2ms * to be on the safer side. */ - udelay(2000); + udelay(4000); return mmc_power_on(mmc); } 
- Reduce the bus width - The SD interface supports a bus width of 4. It can be reduced to 1 by changing the bus-width device tree property from 4 to 1. - diff --git a/arch/arm/dts/k3-am62-main.dtsi b/arch/arm/dts/k3-am62-main.dtsi index c06ec7355035..4ab29b6aa4b7 100644 --- a/arch/arm/dts/k3-am62-main.dtsi +++ b/arch/arm/dts/k3-am62-main.dtsi @@ -373,7 +373,7 @@ ti,itap-del-sel-sdr12 = <0x0>; ti,itap-del-sel-sdr25 = <0x0>; ti,clkbuf-sel = <0x7>; - bus-width = <4>; + bus-width = <1>; }; sdhci2: mmc@fa20000 {