3.14. OP-TEE

OP-TEE is a Trusted Execution Environment (TEE) designed as a companion to a non-secure Linux kernel running on Arm Cortex-A cores using the TrustZone technology.

  1. Furthur information about it can be found at: https://optee.readthedocs.io/en/latest/general/about.html

  2. Official OP-TEE documentation: https://optee.readthedocs.io/en/latest

  3. OP-TEE advisory listing: https://github.com/OP-TEE/optee_os/security/advisories

The OP-TEE binary (bl32.bin/tee-pager_v2.bin) is bundled into tispl.bin and the following are the instructions to build:


3.14.1. Getting the OP-TEE Source Code

The pre-built OPTEE binary should be packaged in TI Processor SDK: <path-to-processor-sdk>/board-support/prebuilt-images/<optional-build-machine-name>/bl32.bin. Use this binary since it has been tested with TI Processor SDK.

If it is not possible to use pre-build binary, use the following:

$ git clone https://github.com/OP-TEE/optee_os.git
$ git checkout <hash>

Where <hash> is the OPTEE commit shown in Build Information.


3.14.2. Setup Cross Compile Environment

The cross compile version supported in this release can be found in the release notes for the kernel release.

Before compiling any of the sources referenced in this document, set the cross compiler paths to the toolchains packaged in the Processor SDK [Recommended] as shown below. Refer to Yocto-built SDK Toolchains section for more details on usage.

host# export CROSS_COMPILE_64="${SDK_INSTALL_DIR}/linux-devkit/sysroots/x86_64-arago-linux/usr/bin/aarch64-oe-linux/aarch64-oe-linux-"
host# export SYSROOT_64="${SDK_INSTALL_DIR}/linux-devkit/sysroots/aarch64-oe-linux"
host# export CC_64="${CROSS_COMPILE_64}gcc --sysroot=${SYSROOT_64}"
host# export CFLAGS64="--sysroot=${SYSROOT_64}"
host# export KCFLAGS="--sysroot=${SYSROOT_64}"
host# export LDFLAGS="--sysroot=${SYSROOT_64}"
host# export CROSS_COMPILE_32="${SDK_INSTALL_DIR}/k3r5-devkit/sysroots/x86_64-arago-linux/usr/bin/arm-oe-eabi/arm-oe-eabi-"
host# export SYSROOT_32="${SDK_INSTALL_DIR}/k3r5-devkit/sysroots/armv7at2hf-vfp-oe-eabi"
host# export CFLAGS32="--sysroot=${SYSROOT_32}"

If the Processor SDK is not installed, the Arm GNU toolchains can be downloaded and setup. Refer to ARM toolchains section for more details on usage.

3.14.3. Building OP-TEE OS

3.14.3.1. Building the OP-TEE image

$ make CROSS_COMPILE="$CROSS_COMPILE_32" CROSS_COMPILE64="$CROSS_COMPILE_64" PLATFORM=k3-am62x CFG_ARM64_core=y

Warning

If building OP-TEE on AM62SIP, add the following argument to the above make command: CFG_TZDRAM_START=0x80080000

3.14.3.2. Building the OP-TEE image with debug parameters

$ make CROSS_COMPILE="$CROSS_COMPILE_32" CROSS_COMPILE64="$CROSS_COMPILE_64" PLATFORM=k3-am62x CFG_ARM64_core=y CFG_TEE_CORE_LOG_LEVEL=2 CFG_TEE_CORE_DEBUG=y

3.14.3.3. Building OP-TEE with Pseudo RNG drivers

In certain highly specific use-cases the true RNG drivers could have a detrimental effect to the overall system latency. Using the CFG_WITH_SOFTWARE_PRNG flag to use OP-TEE’s Pseudo RNG drivers as a source of entropy can work around these issues.

$ make CROSS_COMPILE="$CROSS_COMPILE_32" CROSS_COMPILE64="$CROSS_COMPILE_64" PLATFORM=k3-am62x CFG_ARM64_core=y CFG_WITH_SOFTWARE_PRNG=y

3.14.3.4. OP-TEE Secure Storage

OP-TEE provides secure storage functionality through two mechanisms: Rich Execution Environment Filesystem (REE FS) and Replay Protected Memory Block (RPMB).

TI SDK enables REE FS by-default, and configures OP-TEE to store encrypted binary blobs created by REE FS in /var/lib/tee/.

RPMB works in TI SoCs with HS configuration. These embed a Key Encryption Key (KEK) that programs across OP-TEE instances in a derived manner. Each HS device has its own Hardware Unique Key (HUK) signing key Derived Key Encryption Key (DKEK), which is different from other HS devices. TI SDK disables RPMB by-default. To enable it, re-compiling OP-TEE with CFG_RPMB_FS=y flag.

For learning more about secure storage in OP-TEE, and instructions to enable RPMB, refer: https://optee.readthedocs.io/en/latest/architecture/secure_storage.html

There is a hybrid mode, which enables both CFG_REE_FS=y and CFG_RPMB_FS=y. This mode stores the state of the Secure Storage directory in RPMB partition to check for the integrity of the data present in it. It is the recommended way.

E.g. For enabling hybrid mode of RPMB along with REE_FS

$ make CROSS_COMPILE64="$CROSS_COMPILE_64" PLATFORM=k3-am62x CFG_ARM64_core=y CFG_REE_FS=y CFG_RPMB_FS=y

Also update optee-client to enable the use of real eMMC instead of the virtual eMMC, which is the default option.

As an example to show the usage of secure storage, the filesystem provides a binary /usr/bin/optee_examples_secure_storage.

optee_examples_secure_storage

For more details, see optee_examples: https://github.com/linaro-swg/optee_examples

3.14.4. Getting OP-TEE Client source code

To get optee_client source code, do:

Getting OP-TEE Client source code

$ git clone https://github.com/OP-TEE/optee_client

Building OP-TEE Client with RPMB support

To use emulated RPMB, set RPMB_EMU=1. Otherwise, set RPMB_EMU=0.

For example, the following command builds optee_client to use the real RPMB, instead of the emulated one.

$ make CROSS_COMPILE="$CROSS_COMPILE_64" PLATFORM=k3 CFG_TEE_SUPP_LOG_LEVEL=2 RPMB_EMU=0 CFG_ARM64_core=y

Now update optee-client binary and libraries on your SD card with the generated ones in out/export/usr folder


3.14.5. Building u-boot with OP-TEE OS

As of Processor SDK 9.0, the signing functionality earlier provided by the TI Security Development Package, has been integrated within U-Boot itself. This means tee-pager_v2.bin does not need to be signed before being packaged in tispl.bin in U-Boot for HS devices.

Expected binary output

  1. Generated binary: tee-pager_v2.bin

  2. Binary saved saved in: <path-to-optee>/out/arm-plat-k3/core

Integrate binary output into U-boot

  1. Go to u-boot folder <path-to-u-boot>

  2. Re-build U-boot with A72/A53 instructions found under: Build U-Boot, but with the TEE parameter pointing to the newly built tee-pager_v2.bin. i.e. TEE=<path-to-optee>/out/arm-plat-k3/core/tee-pager_v2.bin

Note

tee-pager_v2.bin may be called bl32.bin in other documentation.


PKCS#11

Public Key Cryptography Standard #11 (PKCS#11) is a cryptographic token interface standard that allows applications to access cryptographic services through a platform-independent API.

For userspace integration details, refer: https://optee.readthedocs.io/en/latest/building/userland_integration.html