3.4.4. SELinux - User Guide

3.4.4.1. Introduction

Security-Enhanced Linux (SELinux) is a project to implement mandatory access control under Linux. It is a set of kernel modifications and user-space tools that provide a mechanism for supporting access control security policies. This project was initially developed by the National Security Agency (NSA), as a reference implementation.

SELinux can run in one of three modes: enforcing, permissive, or disabled.

  • Enforcing mode is the recommended mode of operation where SELinux operates normally, enforcing the loaded security policy on the entire system.

  • In permissive mode, the system acts as if SELinux is enforcing the loaded security policy, including labeling objects and emitting access denial entries in the logs, but it does not actually deny any operations. While not recommended for production systems, permissive mode can be helpful for SELinux policy development and debugging.

  • Disabled mode is strongly discouraged; not only does the system avoid enforcing the SELinux policy, it also avoids labeling any persistent objects such as files, making it difficult to enable SELinux in the future.

Note

This guide assumes that the user understands how to build the Linux Kernel and, Yocto or Debian distribution.

3.4.4.2. Filesystem Setup

3.4.4.2.1. Yocto

The following steps describe how to build SELinux user-space tools and configuration on Yocto. Please use Processor SDK - Building the SDK with Yocto as reference.

  1. On a fresh build, update the config file to use configs/arago-scarthgap-selinux-config.txt. This config includes the opensource meta-selinux layer into the build and also adds additional features for the filesystem such as the kernel configs listed below:

    CONFIG_AUDIT=y
    CONFIG_NETWORK_SECMARK=y
    CONFIG_EXT2_FS_SECURITY=y
    CONFIG_EXT3_FS_SECURITY=y
    CONFIG_EXT4_FS_SECURITY=y
    CONFIG_JFS_SECURITY=y
    CONFIG_REISERFS_FS_SECURITY=y
    CONFIG_JFFS2_FS_SECURITY=y
    CONFIG_SECURITY=y
    CONFIG_SECURITYFS=y
    CONFIG_SECURITY_NETWORK=y
    CONFIG_SECURITY_SELINUX=y
    CONFIG_SECURITY_SELINUX_BOOTPARAM=y
    CONFIG_SECURITY_SELINUX_DEVELOP=y
    CONFIG_SECURITY_SELINUX_AVC_STATS=y
    CONFIG_AUDIT_GENERIC=y
    

    Note

    The default policy is targeted. If you want to update it, add the variable PREFERRED_PROVIDER_virtual/refpolicy = "refpolicy-<your_choice>" to the local.conf where <your_choice> is targeted, mls, mcs.

  2. Build the tisdk-default-image. Note that other recipes do not package selinux features for now.

    $ MACHINE=<machine> bitbake -k tisdk-default-image
    
  3. Your newly built wic image will be generated in deploy-ti directory. Use Linux SD Card Creation Guide to flash this generated image onto your SD card. By default, SELinux functionality is in the disabled state.

3.4.4.2.2. Debian

The following steps describe how to install and configure SELinux together with the default policy which enables SELinux for the most important parts of your Debian filesystem. This guide does not describe how to build the filesystem using Debian.

  1. The default Debian image provided by TI (tisdk-debian-trixie-<machine>-<version>.wic.xz) packages necessary kernel configs to enable SELinux. If you are not using the standard linux kernel provided by debian with an ext2/3/4/xfs/btrfs filesystem, you have to make sure that you are using a SELinux capable kernel and filesystem. For ext2/3/4 there is nothing special to be aware of, but for other filesystems there are still some quirks.

  2. On the target machine, get the default policy and the basic set of SELinux utilities by running

    $ sudo apt-get install selinux-basics selinux-policy-default auditd
    

3.4.4.3. Permissive mode Setup

It is intended to go into Permissive mode, log the accesses, create the access policy and only then jump to Enforcing mode. Skipping this step would lead to a login failure due to lack of access.

  1. Boot the target (in disabled state), Run

    root@<machine>:~# fixfiles -F onboot
    

    or

    root@<machine>:~# touch /.autorelabel
    

    to ensure that files are relabeled upon next reboot.

    Warning

    When systems run SELinux in permissive mode, users and processes might label various file-system objects incorrectly. File-system objects created while SELinux is disabled are not labeled at all. This behavior causes problems when changing to enforcing mode because SELinux relies on correct labels of file-system objects.

    To prevent incorrectly labeled and unlabeled files from causing problems, SELinux automatically relabels file systems when changing from the disabled state to permissive or enforcing mode.

  2. Open /etc/selinux/config and edit it to SELINUX=permissive and the policy type you are using.

  3. Restart the system. If using U-Boot, add security=selinux to the boot parameters by stopping at the U-Boot prompt and adding,

    => setenv optargs "security=selinux"
    
  4. If the previous steps were executed correctly, it will take a while to label the filesystems on boot and then it will automatically reboot a second time when that is complete.

    Warning

    If you are using the optargs step, every boot will require you to stop at U-Boot prompt, set optargs and proceed. Not doing so will force SELinux to go back to disabled state and you will have to restart the setup.

  5. You should now have a working SELinux system, which is in permissive mode. This means that the selinux policy is not enforced, but denials are logged. You can see all would-be denials since the last reboot with a small explanation for each with audit2why -al.

  6. Verify your status by running sestatus or getenforce.

    root@<machine>:~# sestatus
    SELinux status:                 enabled
    SELinuxfs mount:                /sys/fs/selinux
    SELinux root directory:         /etc/selinux
    Loaded policy name:             targeted
    Current mode:                   permissive
    Mode from config file:          permissive
    Policy MLS status:              disabled
    Policy deny_unknown status:     allowed
    Memory protection checking:     actual (secure)
    Max kernel policy version:      31
    

3.4.4.4. Enforcing mode Setup

This guide serves as a reference implementation and will not be diving into custom policy writing or analysing and fixing SELinux denial details.

  1. Assuming you are now in permissive mode, use audit2why -al to list all the policy violations that occured since booting up.

  2. We will be using the audit2allow tool to generate a local policy and resolve all the violations seen. Run:

    root@<machine>:~# audit2allow -a -M myPolicy
    

    Follow the instructions generated by the tool to activate the policy.

    Warning

    It is not recommended to use audit2allow to generate a local policy module as your first option when you see an SELinux denial. Troubleshooting should start with a check if there is a labeling problem. The second most often case is that you have changed a process configuration, and you forgot to tell SELinux about it

  3. Update /etc/selinux/config to SELINUX=enforcing, save and reboot.

    Note

    Remember that boot parameter security=selinux must always be present otherwise you will have to begin anew.

  4. Verify your status by using sestatus or getenforce.

    root@<machine>:~# sestatus
    SELinux status:                 enabled
    SELinuxfs mount:                /sys/fs/selinux
    SELinux root directory:         /etc/selinux
    Loaded policy name:             targeted
    Current mode:                   enforcing
    Mode from config file:          enforcing
    Policy MLS status:              enabled
    Policy deny_unknown status:     allowed
    Memory protection checking:     actual (secure)
    Max kernel policy version:      31
    

3.4.4.5. Integrating into Yocto for production

The above steps are useful during development but unusable in a production environment. The following are pointers to help build a final image which does not require the above steps.

  1. security=selinux can be added into sources/meta-arago/meta-arago-distro/recipes-tisdk/tisdk-uenv/tisdk-uenv/uEnv.txt to make it default.

  2. To relabel on first boot, add FIRST_BOOT_RELABEL="1" in local.conf

  3. To set the default selinux mode, add DEFAULT_ENFORCING="<mode>" in local.conf, where <mode> is disabled/permissive/enforcing.

  4. Once the policy has been created, there are multiple ways to install it. This post_install section can be added into your recipe, myPolicy.pp is the policy that is placed in the meta-selinux directory:

    SRC_URI += "file://myPolicy.pp"
    
    do_install:append() {
       install -d ${D}/etc/selinux/targeted/modules/active/modules
       install -m 0644 ${WORKDIR}/myPolicy.pp ${D}/etc/selinux/targeted/modules/active/modules/
    }
    
    pkg_postinst_ontarget:${PN}() {
       #!/bin/bash
       /usr/sbin/semodule -i /etc/selinux/targeted/modules/active/modules/myPolicy.pp
    }