1.2. Building the SDK with Yocto

1.2.1. Introduction

This page provides the steps to build the Processor SDK and individual components from source. The Processor SDK build is based on the Arago Project which provides a set of layers for OpenEmbedded and the Yocto Project targeting TI platforms.

This page will provide the basic steps required to recreate the Processor SDK along with a reference of Processor SDK specific configurations, build targets, and target devices. Also, tips and suggestions are provided along with links for more in-depth information.

1.2.2. Steps to Run Yocto Builds inside Container

TI provides a Ubuntu 22.04 based docker image with all the packages that are required to start a Yocto Build.

The Docker Image is hosted on ghcr.io/texasinstruments.

Refer Steps to Run Yocto builds inside a Container for a comprehensive guide.

Follow Processor SDK Build Reference for Layer Configuration and Build Options.

Attention

Before starting the container, ensure that you have completed all the Pre-Requisites as mentioned here.

1.2.3. Steps to Run Yocto Builds on Host

1.2.3.1. Prerequisites (One-time setup)

The recommended Linux distribution is Ubuntu 22.04.

The following build host packages are required for Ubuntu. The following command will install the required tools on the Ubuntu Linux distribution.

For Ubuntu 22.04, please run the following:

$ sudo apt-get update
$ # Install packages required for builds
$ sudo apt-get -f -y install \
  git build-essential diffstat texinfo gawk chrpath socat doxygen \
  dos2unix python3 bison flex libssl-dev u-boot-tools mono-devel \
  mono-complete curl python3-distutils repo pseudo python3-sphinx \
  g++-multilib libc6-dev-i386 jq git-lfs pigz zstd liblz4-tool \
  cpio file lz4 debianutils iputils-ping python3-git python3-jinja2 \
  python3-subunit locales libacl1 unzip gcc python3-pip python3-pexpect \
  xz-utils wget \
$ sudo locale-gen en_US.UTF-8

By default Ubuntu uses “dash” as the default shell for /bin/sh. You must reconfigure to use bash by running the following command:

$ sudo dpkg-reconfigure dash

Important

Be sure to select “No” when you are asked to use dash as the default system shell.

Large Swap File

Building large packages, especially several at a time, requires a lot of working memory for a computer. For computers with 32 GB of RAM or more, this should not be a problem. For computers with less RAM, a swap file of ~16GB may be needed to build large packages. Creating a large swap file, or resizing a small swap file to be larger will help avoid build errors for large packages.

Proxy Setup

If working behind a proxy, please see Working Behind a Network Proxy.

1.2.3.2. Build Steps

Please refer to here for the layer configuration oeconfig-file for a particular release of Processor SDK Linux AM62x. The MACHINE can be set to am62xx-evm, for example.

The final command below will build the tisdk-default-image, which is the Processor SDK image with arago filesystem. See Build Options for a list of additional targets.

$ git clone https://git.ti.com/git/arago-project/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/<oeconfig-file>
$ cd build
$ . conf/setenv
$ MACHINE=<machine> bitbake -k tisdk-default-image
  • The final command below will build the tisdk-jailhouse-image, which is the Processor SDK image with arago filesystem and Jailhouse support.

  • tisdk-jailhouse-image is not applicable for am62xxsip-evm and beagleplay-ti.

$ git clone https://git.ti.com/git/arago-project/oe-layersetup.git tisdk
$ cd tisdk
$ ./oe-layertool-setup.sh -f configs/processor-sdk/<oeconfig-file>
$ cd build
$ . conf/setenv
$ echo 'TI_EXTRAS="tie-jailhouse"' >> conf/local.conf
$ MACHINE=<machine> bitbake -k tisdk-jailhouse-image

Your newly built wic image will be generated in deploy-ti directory. Use Linux SD Card Creation Guide to flash this image on the SD-Card.

Important

The Yocto build will need ~750GB of hard disk space for building the tisdk-default-image which includes Chromium.

Tip

The tisdk-default-image now includes Chromium by default, which may increase the build time. If you prefer not to build Chromium, you can remove the meta-browser layer from the oeconfig-file before running oe-layertool-setup.sh

However, if you are building the tisdk-default-image specifically to try out the TI Apps Launcher out-of-the-box (OOB), it is not recommended to remove the meta-browser layer. The TI Apps Launcher relies on Chromium and removing the layer may impact its functionality. Keep the meta-browser layer intact for the best OOB experience.

Tip

If your computer is frequently crashing while running the bitbake command, edit the conf/local.conf file under build directory and set the variables: BB_NUMBER_THREADS and PARALLEL_MAKE to cap the number of threads bitbake can create at a time. By default bitbake tries to automatically figure out and set the maximum values for these variables on your system which may lead to errors.

Caution

While building images via Yocto, if you are facing locale.Error: unsupported locale setting error, it means your system is trying to use a locale setting which was not there. Run the following commands which will setup the locale and try building your target image again.

export LC_ALL="en_US.UTF-8"
export LC_CTYPE="en_US.UTF-8"
export LC_NUMERIC="en_US.UTF-8"
export LANG=en_US.UTF-8
export LANGUAGE=en_US.UTF-8
ulimit -n 4096

1.2.4. Processor SDK Build Reference

The following sections provide information for configuration, build options, and supported platforms of the Processor SDK.

1.2.4.1. Layer Configuration

Please refer to here for the layer configuration for a particular release of Processor SDK Linux.

1.2.4.2. Build Options

Images

In addition to individual components packages, the following table provides a list of build targets supported. These are the <target> used in the command:

MACHINE=<machine> bitbake <target>

The build system places the “Build Output” relative to deploy-ti

Target

Build Output

Description

tisdk-default-image

images/<machine>/tisdk-default-image-<machine>.rootfs.tar.xz

Target Filesystem

tisdk-jailhouse-image

images/<machine>/tisdk-jailhouse-image-<machine>.rootfs.tar.xz

Jailhouse Filesystem

tisdk-base-image

images/<machine>/tisdk-base-image-<machine>.rootfs.tar.xz

Minimal Target Filesytem

tisdk-thinlinux-image

images/<machine>/tisdk-thinlinux-image-<machine>.rootfs.tar.xz

Minimal Target Filesytem with docker enabled

meta-toolchain-arago-tisdk

sdk/arago-<arago-version>-<architecture>.sh

Devkit

mc:k3r5:meta-toolchain-arago

sdk/arago-<arago-version>-<architecture>.sh

K3R5 baremetal toolchain

Platforms

The following platforms are supported in Processor SDK. These are the <machine> in the command:

MACHINE=<machine> bitbake <target>

MACHINE

Supported EVMs

am62xx-evm

AM62x Starter Kit (SK) - GP, HS-FS, HS-SE

am62xx-lp-evm

AM62x LP Starter Kit (SK) - HS-FS, HS-SE

beagleplay-ti

BEAGL-PLAY-SBC - GP

MACHINE

Supported EVMs

am62xx-evm

AM62x Starter Kit (SK) - GP, HS-FS, HS-SE

am62xx-lp-evm

AM62x LP Starter Kit (SK) - HS-FS, HS-SE

beagleplay-ti

BEAGL-PLAY-SBC - GP

1.2.4.3. Recipes

Recipe Basics

One or more recipes can be specified for the <target> for greater granularity of recipe development and debug. Specifying a recipe name, minus the version (if the version is appended to the name), will build the recipe and all its dependencies.

For example, the following command builds only the zlib recipe and all the dependencies it defines.

MACHINE=<machine> bitbake zlib

After the preceding bitbake command completes successfully, the arago-tmp-default-glibc/work/aarch64-oe-linux/zlib directory gets created. It has the original source code, shared objects (.so files) in the packages-split folder and IPK packages in the deploy-ipks folder.

Note

Please note that the output of a recipe can be in another folder under arago-tmp-[toolchain]/work directory, depending on the defines of the recipe. You can call the following command from yocto’s build directory to get the path to the workdir of your recipe.

MACHINE=<machine> bitbake-getvar -r <recipe-name> WORKDIR --value

Forced Re-compilation

When needed, source code under the work directory (e.g., arago-tmp-default-glibc/work/aarch64-oe-linux/zlib/<version>/zlib-<version>) can be modified. After the modification is done, run the following commands to force recompilation with the new code and rebuilding of the recipe, For example,

MACHINE=<machine> bitbake zlib --force -c compile
MACHINE=<machine> bitbake zlib

Installing Package

To install a modified and rebuilt package, copy the new IPKs from the deploy-ipks folder (e.g., arago-tmp-default-glibc/work/aarch64-oe-linux/zlib/<version>/deploy-ipks) to the target system and then run the following command to install the IPKs:

opkg install [package_ipk].ipk

Cleaning a Built Recipe

A built recipe can be entirely cleaned using:

MACHINE=<machine> bitbake <target> -c cleanall

The cleanall task removes all output files, shared state (sstate) cache and downloaded source files for a target (i.e. the contents of DL_DIR)

1.2.5. See also

General information on Yocto, OpenEmbedded and Arago projects can be found at: