3.2.2.3. MCAN

Introduction

The Controller Area Network is a serial communications protocol which efficiently supports distributed real-time control with a high level of security. The MCAN module supports bitrates up to 5 Mbit/s and is compliant to the ISO 11898-1:2015. The core IP within M_CAN is provided by Bosch.

This wiki page provides usage information of M_CAN Linux driver.

Setup Details

TI board List

SoC

Board

Number of Instances

Connection Type

Enabled by default

Dra76x

EVM

1

Header

Yes

AM654x

IDK

2

DB9

Yes

AM64x

EVM

2

Header

Yes

AM62x

SK

3

Header

No

AM68

SK

4

Header

Yes

AM69

SK

4

Header

Yes

J721E

SK

4

Header

Yes

J721E

EVM

4

Header

Yes

J7200

EVM

4

Header

Yes

J721S2

EVM

5

Header

Yes

J784S4

EVM

6

Header

Yes

J722S

EVM

3

Header

Yes

Table: Boards M_CAN Driver is Validated on

Connection Configuration

../../../../_images/mcan-diagram-evm-to-evm.png ../../../../_images/Dcan_header_to_db9.png

Header to Header

Header to DB9

Table: Various MCAN EVM Connection Configuration

Equipment

Female DB9 Cable

For boards exposing M_CAN using male DB9 connectors, a female connector is required. The other side can be male or female depending on the other CAN device the user connects to.

../../../../_images/DB9_cable.jpg

Jumper Wires

For boards where the CAN pins are broken out via a header, female jumper cables will be ideal for connection. The CAN pins will be CAN H (typically pin 1 of the header), GND (middle pin of the header) and CAN L (lowest pin on the header). The pinout in the header might vary across different boards and users must consult the board’s schematic to verify this.

../../../../_images/Female_to_female_jumper.png

Custom DB9 to Header Cable

Typically CAN devices use a DB9 connection therefore for boards whose CAN pins are broken out via a header it is helpful to create a header to DB9 connector cable. This custom cable is simple to make. Either a male or female DB9 connector (not cable) must be obtained along with three female jumper wires.

Snip one end of each of the jumper wires and expose some of the wiring. Now solder each of the exposed wires to pin 7 (CAN H), pin 2 (CAN L) and pin 3 (GND). Make sure your soldering on the side of the DB9 that has the metal lip meant to push some of the exposed wire into and soldering to the correct pins correctly. Use the below diagram as a reference.

../../../../_images/DCAN_custom_cable_diagram.png ../../../../_images/Custom_cable.png

Wiring Diagram

Example of completed cable.

CAN Utilities

There may be other userspace applications that can be used to interact with the CAN bus but the SDK supports using Canutils which is already included in the sdk filesystem.

Note

These instructions are for mcu_mcan0. If the board has multiple CAN instances enabled then they can be referenced by their CAN dts node names just like mcu_mcan0 here. For example, 2nd instance of CAN in the main domain ( ie main_mcan2 as referenced in the dts ) will be visible as main_mcan2 to the users.

Quick Steps

Initialize CAN Bus

  • Set bitrate

$ ip link set mcu_mcan0 type can bitrate 1000000
  • CAN-FD mode with bitrate switching

$ ip link set mcu_mcan0 type can bitrate 1000000 dbitrate 4000000 fd on

Start CAN Bus

  • Device bring up

Bring up the device using the command:

$ ip link set mcu_mcan0 up

Transfer Packets

Cansend

Used to generate a specific can frame. The syntax for cansend is as follows:

<can_id>#{R|data}          for CAN 2.0 frames
<can_id>##<flags>{data}    for CAN FD frames

Some examples:

  1. Send CAN 2.0 frame

$ cansend mcu_mcan0 123#F00DCAFE
  1. Send CAN FD frame

$ cansend mcu_mcan0 113##2AAAAAAAA
  1. Send CAN FD frame with BRS

$ cansend mcu_mcan0 143##1AAAAAAAAA

Cangen

Used to generate frames at equal intervals. The syntax for cangen is as follows:

cangen [options] <CAN interface>

Some examples:

  1. Full load test with polling, 10 ms timeout

$ cangen mcu_mcan0 -g 0 -p 10 -x

b. fixed CAN ID and length, inc. data, canfd frames with bitrate switching

$ cangen mcu_mcan0 -g 4 -I 42A -L 1 -D i -v -v -f -b

Candump

Candump is used to display received frames.

candump [options] <CAN interface>

Example:

$ candump mcu_mcan0

Note: Use Ctrl-C to terminate candump

Further options for all canutils commands are available at https://git.pengutronix.de/cgit/tools/canutils

Stop CAN Bus

Stop the can bus by:

$ ip link set mcu_mcan0 down

Note

The earlier CAN naming convention had can0 referring to the first probed CAN instance and can1, can2.. and so on, to the other CAN instances in the order in which they are probed. For example, 2 CAN instances will have names as can0 and can1 assigned to them in the linux kernel, based on the order in which they are probed and irrespective of their CAN instance number. If the earlier CAN naming convention is needed, you can revert 2d2df9f8058a3aa323daa01a64fcef59176500e3 commit in meta-arago repository.