4. How to Guides
- 4.1. Host
- 4.2. Target
- 4.2.1. SDK File System Optimization/Customization
- 4.2.2. Real-Time Linux on TI SoCs
- 4.3. Developer Notes
- 4.1.1. Moving Files to the Target System
- 4.2.1. SDK File System Optimization/Customization
- 4.3.1. How to flash eMMC and boot with eMMC Boot
- 4.3.2. How to flash eMMC and boot from eMMC UDA
- 4.2.2. Real-Time Linux on TI SoCs
- 4.3.3. How to verify IPC between Linux and MCU R5 in Keystone devices?
- 4.3.4. How to check some device tree information from user-space of Linux?
- 4.3.5. How do I integrate a different version of open source software than what is packaged in Processor SDK AM64x?
- 4.1.2. K3 resource partitioning tool
- 4.1.3. How to Setup and Debug using Lauterbach
- 4.1.4. Enabling and Parsing SYSFW Trace
- 4.1.5. Program MMC boot media
- 4.4. Hardware EVM Setup
- 4.5. Frequently Asked Questions