Processor SDK Linux for AM64X Logo
12_01_00_05_03
  • 1. Overview
  • 2. Release Specific
  • 3. Foundational Components
  • 4. How to Guides
    • 4.1. Host
    • 4.2. Target
      • 4.2.1. SDK File System Optimization/Customization
      • 4.2.2. Real-Time Linux on TI SoCs
    • 4.3. Developer Notes
    • 4.4. Hardware EVM Setup
    • 4.5. Frequently Asked Questions
  • 5. RTOS/NO-RTOS [MCU+ SDK]
  • 6. Demo Applications
  • 7. Documentation Tarball
Processor SDK Linux for AM64X
  • 4. How to Guides
  • 4.2. Target
  • Edit on GitHub

4.2. Target

  • 4.2.1. SDK File System Optimization/Customization
    • 4.2.1.1. The Basics of OPKG
      • 4.2.1.1.1. List all available options of opkg
      • 4.2.1.1.2. Show all installed packages
      • 4.2.1.1.3. Show package contents
      • 4.2.1.1.4. Find a file owner
      • 4.2.1.1.5. Show packages which require the package as dependency
      • 4.2.1.1.6. Removing Packages or Deinstallation
      • 4.2.1.1.7. Install local packages
  • 4.2.2. Real-Time Linux on TI SoCs
    • 4.2.2.1. What Is The Real-Time Linux Kernel?
    • 4.2.2.2. Validating We Are Using A Real-Time Capable Kernel
    • 4.2.2.3. Testing Kernel Performance
      • 4.2.2.3.1. Timer Based Applications
      • 4.2.2.3.2. Driver (Ethernet) Based Interrupts
    • 4.2.2.4. Tips For Tuning The Real-Time Kernel
      • 4.2.2.4.1. Technique to Tuning (Slow is Fast)
      • 4.2.2.4.2. Technique to Testing
      • 4.2.2.4.3. Disable Unnecessary Applications
      • 4.2.2.4.4. Disable Unnecessary Drivers
    • 4.2.2.5. Wrapping Up
Previous Next

© Copyright 1995-2026 Texas Instruments Incorporated, CC-BY-SA-4.0. Revision e73340f1. Last updated on Sep 18, 2026.