6.11. DMA

6.11.1. Modules

Name

APIs for EDMA

APIs for SOC Xbars

6.11.2. Types

Base type

Type Name

Brief

enum

CddDma_StatusType

This type defines a range of specific status for Complex driver.

typedef Cdd_Edma_EventCallback

CddDma_CallBackType

Callback type.

6.11.2.1. enum CddDma_StatusType

Enumerator

Value

Description

CDD_DMA_UNINIT

0U

The Complex Driver is not initialized or not usable.

CDD_DMA_IDLE

1U

The Complex Driver is not currently transferring.

CDD_DMA_ALLOW_ACCESS

2U

The Complex Driver is currently open.

CDD_DMA_BUSY

3U

The Complex Driver is performing a write operation.

CDD_DMA_CLOSE

4U

The Complex Driver is currently closed.

Brief: This type defines a range of specific status for Complex driver.

6.11.2.2. typedef CddDma_CallBackType

typedef Cdd_Edma_EventCallback CddDma_CallBackType;

Brief: Callback type.

6.11.3. Structures

Name

Brief

Cdd_Dma_ParamEntry

Param entry.

6.11.4. Defines

Name

Brief

CDD_DMA_SW_MAJOR_VERSION

Driver Implementation Major Version.

CDD_DMA_SW_MINOR_VERSION

Driver Implementation Minor Version.

CDD_DMA_SW_PATCH_VERSION

Driver Implementation Patch Version.

CDD_DMA_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CDD_DMA Driver.

CDD_DMA_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CDD_DMA Driver.

CDD_DMA_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CDD_DMA Driver.

CDD_DMA_VENDOR_ID

Texas Instruments Vendor ID.

CDD_DMA_MODULE_ID

CDD_DMA Driver Module ID.

CDD_DMA_INSTANCE_ID

CDD_DMA Driver Instance ID.

CDD_DMA_ISR_VOID

void ISR type

CDD_DMA_ISR_CAT1

Category 1 ISR type.

CDD_DMA_ISR_CAT2

Category 2 ISR type.

CDD_DMA_INIT_SERVICE_ID

API Service ID for initialization.

CDD_DMA_DEINIT_SERVICE_ID

API Service ID for deinitialization.

CDD_DMA_CBKREGISTER_SERVICE_ID

API Service ID for IntrRegistration.

CDD_DMA_PARAMSET_SERVICE_ID

API Service ID for ParamSet.

CDD_DMA_LINKCHANNEL_SERVICE_ID

API Service ID for Param linking.

CDD_DMA_CHAINCHANNEL_SERVICE_ID

API Service ID for Channel chaining.

CDD_DMA_ENABLETRANSFERREGION_SERVICE_ID

API Service ID for enable a trigger.

CDD_DMA_GETSTATUS_SERVICE_ID

API Service ID for reading TCC status.

CDD_DMA_GETVERSIONINFO_SERVICE_ID

API Service ID for get version info.

Cdd_Dma_GETINITSTATUS_SERVICE_ID

API Service ID for get INIT status.

CDD_DMA_GETPARAM_SERVICE_ID

API Service ID for GetParam.

CDD_DMA_DISABLETRANSFERREGION_SERVICE_ID

API Service ID for disable the transfer region.

CDD_DMA_REGISTER_READBACK_SERVICE_ID

API Service ID for Register Read Back.

CDD_DMA_E_UNINIT

Error code indicating the DMA is uninitialized.

CDD_DMA_E_ALREADY_INITIALIZED

Error code indicating DMA already initialized.

CDD_DMA_E_PARAM_VALUE

Error code indicating Service called with wrong param.

CDD_DMA_E_PARAM_POINTER

Error code indicating invalid parameter.

CDD_DMA_E_ALREADY_REGISTERED

Error code indicating callback is already registered.

CDD_DMA_E_ALREADY_IN_PROGRESS

Error code indicating DMA handle already in use.

CDD_DMA_TRIG_XBAR_EDMA_MODULE_0_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_1_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_2_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_3_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_4_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_5_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_6_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_7_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_8_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_9_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_10_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_11_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_12_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_13_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_14_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_20_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_21_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_22_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_23_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_24_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_25_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_26_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_27_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_28_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_29_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_30_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_31_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_32_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_33_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_34_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_35_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_36_INPUT

CDD_DMA_TRIG_XBAR_EDMA_MODULE_37_INPUT

CddDmaConf_CddDmaDriverHandler_0_Uart_Tx

CddDmaConf_CddDmaDriverHandler_0_Uart_Rx

CddDmaConf_CddDmaDriverHandler_1_Uart_Tx

CddDmaConf_CddDmaDriverHandler_1_Uart_Rx

CddDmaConf_CddDmaDriverHandler_2_Uart_Tx

CddDmaConf_CddDmaDriverHandler_2_Uart_Rx

CddDmaConf_CddDmaDriverHandler_3_Uart_Tx

CddDmaConf_CddDmaDriverHandler_3_Uart_Rx

CddDmaConf_CddDmaDriverHandler_4_Uart_Tx

CddDmaConf_CddDmaDriverHandler_4_Uart_Rx

CddDmaConf_CddDmaDriverHandler_0_Adc

CddDmaConf_CddDmaDriverHandler_1_Adc

CddDmaConf_CddDmaDriverHandler_2_Adc

CddDmaConf_CddDmaDriverHandler_3_Adc

CddDmaConf_CddDmaDriverHandler_4_Adc

CddDmaConf_CddDmaDriverHandler_MemoryTransfer_Interrupt

CddDmaConf_CddDmaDriverHandler_MemoryTransfer_Linking

CddDmaConf_CddDmaDriverHandler_MemoryTransfer_Polling

CddDmaConf_CddDmaDriverHandler_MemoryTransfer_Chaining

CddDmaConf_CddDmaDriverHandler_Spi_0_Tx

CddDmaConf_CddDmaDriverHandler_Spi_0_Rx

CddDmaConf_CddDmaDriverHandler_Spi_1_Tx

CddDmaConf_CddDmaDriverHandler_Spi_1_Rx

CddDmaConf_CddDmaDriverHandler_Spi_2_Tx

CddDmaConf_CddDmaDriverHandler_Spi_2_Rx

CddDmaConf_CddDmaDriverHandler_Spi_3_Tx

CddDmaConf_CddDmaDriverHandler_Spi_3_Rx

CddDmaConf_CddDmaDriverHandler_Spi_4_Tx

CddDmaConf_CddDmaDriverHandler_Spi_4_Rx

CddDmaConf_CddDmaDriverHandler_0_FsiTx

CddDmaConf_CddDmaDriverHandler_1_FsiTx

CddDmaConf_CddDmaDriverHandler_2_FsiTx

CddDmaConf_CddDmaDriverHandler_3_FsiTx

CddDmaConf_CddDmaDriverHandler_0_FsiRx

CddDmaConf_CddDmaDriverHandler_1_FsiRx

CddDmaConf_CddDmaDriverHandler_2_FsiRx

CddDmaConf_CddDmaDriverHandler_3_FsiRx

CddDmaConf_CddDmaDriverHandler_0_Fls

6.11.5. Functions

Return type

Function Name

Brief

void

Cdd_Dma_Init(Cdd_Dma_ConfigType * ConfigPtr)

Service for CDD_DMA initialization.

void

Cdd_Dma_DeInit(void )

Service for CDD_DMA de-initialization Function to de-initialize the Cdd_Dma Module.With this call all the handler regsitered for Cdd-Dma module is de-initialized.

boolean

Cdd_Dma_GetInitStatus(void )

Service for CDD_DMA GetInitStatus. Function to provide the initialization status of the Module.

uint32

Cdd_Dma_CbkRegister(uint32 handleId, void * appdata, Cdd_Edma_EventCallback callback)

Service for CDD_DMA Callback Register. Function to register callback function for a TCC.

void

Cdd_Dma_ParamSet(uint32 handleId, uint32 channelIdx, uint32 paramIndex, Cdd_Dma_ParamEntry paramEntry)

Service for CDD_DMA Param Setting. Function to Set the paramSet values with the param value associated with the channel of a particular handle.

void

Cdd_Dma_LinkChannel(uint32 handleId, uint32 paramIndex0, uint32 paramIndex1)

Service for CDD_DMA Linking params. Function to Link the param. Often used to link different params within the channel.

void

Cdd_Dma_ChainChannel(uint32 handleId, uint32 channelIdx0, uint32 paramIndex0, uint32 channelIdx1, uint32 opt)

Service for CDD_DMA Chaining Channels Function to Chain multiple channel and can be used in transmission only with one trigger.

boolean

Cdd_Dma_EnableTransferRegion(uint32 handleId, uint32 trigMode)

Service for CDD_DMA Enable transfer region Function to Enable the trigger for transmission.

boolean

Cdd_Dma_GetStatus(uint32 handleId)

Service for CDD_DMA Get status Function to Read the status of the transfer. Used in case of polling mode.

void

Cdd_Dma_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr)

Service for CDD_DMA Get version info. Function to Get Version information.

void

Cdd_Dma_GetParam(uint32 handleId, uint32 channelIdx, uint32 paramIndex, CDD_EDMACCEDMACCPaRAMEntry * edmaParam)

Service for CDD_DMA Param Getting Function to Get the paramSet values with the param value associated with the channel of a particular handle.

boolean

Cdd_Dma_DisableTransferRegion(uint32 handleId, uint32 trigMode)

Service for CDD_DMA Disable transfer region. Function to Disable the trigger for transmission.

Std_ReturnType

Cdd_Dma_RegisterReadback(uint32 handleId, Cdd_Dma_RegisterReadbackType * RegPtr)

This function reads the important registers of the hardware unit and returns the value in the structure.

6.11.5.1. function Cdd_Dma_Init

void Cdd_Dma_Init(
    Cdd_Dma_ConfigType * ConfigPtr
)

Brief: Service for CDD_DMA initialization.

Service ID[hex] : 0x01

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • configPtr - Pointer to configuration set

Returns:

  • None

Return: None

6.11.5.2. function Cdd_Dma_DeInit

void Cdd_Dma_DeInit(
    void 
)

Brief: Service for CDD_DMA de-initialization Function to de-initialize the Cdd_Dma Module.With this call all the handler regsitered for Cdd-Dma module is de-initialized.

Service ID[hex] : 0x02

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.11.5.3. function Cdd_Dma_GetInitStatus

boolean Cdd_Dma_GetInitStatus(
    void 
)

Brief: Service for CDD_DMA GetInitStatus. Function to provide the initialization status of the Module.

Service ID[hex] : 0x0A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • True or False

Return: boolean

6.11.5.4. function Cdd_Dma_CbkRegister

uint32 Cdd_Dma_CbkRegister(
    uint32 handleId,
    void * appdata,
    Cdd_Edma_EventCallback callback
)

Brief: Service for CDD_DMA Callback Register. Function to register callback function for a TCC.

Service ID[hex] : 0x03

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to register callback

  • appdata - data associated with it

  • callback - registered callback which will be called on interrupt

Returns:

  • E_OK Status Ok

  • E_NOT_OK Status Not Ok

Return: uint32

6.11.5.5. function Cdd_Dma_ParamSet

void Cdd_Dma_ParamSet(
    uint32 handleId,
    uint32 channelIdx,
    uint32 paramIndex,
    Cdd_Dma_ParamEntry paramEntry
)

Brief: Service for CDD_DMA Param Setting. Function to Set the paramSet values with the param value associated with the channel of a particular handle.

Service ID[hex] : 0x04

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to set the param set value

  • channelIdx - Index of the channel for that particular handle

  • paramIndex - Index of the param for which we want to set the param values

  • paramEntry - Structure which contains the required paramSet fields to be used for the particular param value.

Returns:

  • None

Return: None

6.11.5.6. function Cdd_Dma_LinkChannel

void Cdd_Dma_LinkChannel(
    uint32 handleId,
    uint32 paramIndex0,
    uint32 paramIndex1
)

Brief: Service for CDD_DMA Linking params. Function to Link the param. Often used to link different params within the channel.

Service ID[hex] : 0x05

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to used linking

  • paramIndex0 - Index of the param which should be linked to another param

  • paramIndex1 - Index of the param which is supposed to be linked to the first one

Returns:

  • None

Return: None

6.11.5.7. function Cdd_Dma_ChainChannel

void Cdd_Dma_ChainChannel(
    uint32 handleId,
    uint32 channelIdx0,
    uint32 paramIndex0,
    uint32 channelIdx1,
    uint32 opt
)

Brief: Service for CDD_DMA Chaining Channels Function to Chain multiple channel and can be used in transmission only with one trigger.

Service ID[hex] : 0x06

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to used Chaining

  • channelIdx0 - Index of the first channel which is used for Chaining

  • paramIndex0 - Index of the param which is supposed to be linked to the first one

  • channelIdx1 - Index of the second channel which is used for Chaining

  • opt - Chain Option to be used while Chaining

Returns:

  • None

Return: None

6.11.5.8. function Cdd_Dma_EnableTransferRegion

boolean Cdd_Dma_EnableTransferRegion(
    uint32 handleId,
    uint32 trigMode
)

Brief: Service for CDD_DMA Enable transfer region Function to Enable the trigger for transmission.

Service ID[hex] : 0x07

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to enable the transfer

  • trigMode - Trigger mode which is used to enable the transmission

Returns:

  • Indicate successfully enabled transfer or not with value True or False

Return: boolean

6.11.5.9. function Cdd_Dma_GetStatus

boolean Cdd_Dma_GetStatus(
    uint32 handleId
)

Brief: Service for CDD_DMA Get status Function to Read the status of the transfer. Used in case of polling mode.

Service ID[hex] : 0x08

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to get the status of the TCC

Returns:

  • Returns status as True or False

Return: boolean

6.11.5.10. function Cdd_Dma_GetVersionInfo

void Cdd_Dma_GetVersionInfo(
    Std_VersionInfoType * VersionInfoPtr
)

Brief: Service for CDD_DMA Get version info. Function to Get Version information.

Service ID[hex] : 0x09

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • VersionInfoPtr - pointer to the structure for which data should be stored

Returns:

  • None

Return: None

6.11.5.11. function Cdd_Dma_GetParam

void Cdd_Dma_GetParam(
    uint32 handleId,
    uint32 channelIdx,
    uint32 paramIndex,
    CDD_EDMACCEDMACCPaRAMEntry * edmaParam
)

Brief: Service for CDD_DMA Param Getting Function to Get the paramSet values with the param value associated with the channel of a particular handle.

Service ID[hex] : 0x0B

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to get the param value

  • channelIdx - Index of the channel for that particular handle

  • paramIndex - Index of the param for which we want to get the param values

  • edmaParam - EDMA Parameter RAM struct

Returns:

  • None

Return: None

6.11.5.12. function Cdd_Dma_DisableTransferRegion

boolean Cdd_Dma_DisableTransferRegion(
    uint32 handleId,
    uint32 trigMode
)

Brief: Service for CDD_DMA Disable transfer region. Function to Disable the trigger for transmission.

Service ID[hex] : 0x0C

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to disable the transfer

  • trigMode - Trigger mode which is used to disable the transmission

Returns:

  • Indicate successfully disabled transfer or not with value as True or False

Return: boolean

6.11.5.13. function Cdd_Dma_RegisterReadback

Std_ReturnType Cdd_Dma_RegisterReadback(
    uint32 handleId,
    Cdd_Dma_RegisterReadbackType * RegPtr
)

Brief: This function reads the important registers of the hardware unit and returns the value in the structure.

Service ID[hex] : 0x0D

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • handleId - Cdd_Dma handle is passed for which we want to read the register value

  • RegPtr - Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.

Returns:

  • E_OK Register read back has been done

  • E_NOT_OK Register read back failed

Return: Std_ReturnType