6.21. WDG

6.21.1. Types

Base type

Type Name

Brief

enum

Wdg_StatusType

WDG Status enum.

enum

Wdg_Reaction

DWWD Reaction on violation.

enum

Wdg_WindowSize

DWWD Window size.

6.21.1.1. enum Wdg_StatusType

Enumerator

Value

Description

WDG_UNINIT

Watchdog driver is uninitialized. State on power on before invoking Wdg_Init()

WDG_IDLE

Watchdog driver is in idle state. Default state when WDG timer regs are not being programmed.

WDG_BUSY

Watchdog driver is reprogramming the WD to trigger the watchdog.

Brief: WDG Status enum.

6.21.1.2. enum Wdg_Reaction

Enumerator

Value

Description

WDG_GENERATE_RESET

0x00000005U

Generate Reset.

WDG_GENERATE_NMI

0x0000000AU

Generate NMI.

Brief: DWWD Reaction on violation.

6.21.1.3. enum Wdg_WindowSize

Enumerator

Value

Description

WDG_WINDOW_SIZE_100_PERCENT

0x00000005U

Window size 100 percent.

WDG_WINDOW_SIZE_50_PERCENT

0x00000050U

Window size 50 percent.

WDG_WINDOW_SIZE_25_PERCENT

0x00000500U

Window size 25 percent.

WDG_WINDOW_SIZE_12_5_PERCENT

0x00005000U

Window size 12_5 percent.

WDG_WINDOW_SIZE_6_25_PERCENT

0x00050000U

Window size 6_25 percent.

WDG_WINDOW_SIZE_3_125_PERCENT

0x00500000U

Window size 3_125 percent.

Brief: DWWD Window size.

6.21.2. Structures

Name

Brief

Wdg_ModeInfoType

Mode info type.

Wdg_ConfigType

WDG config structure.

Wdg_RegisterReadbackType

WDG configuration register readback data structure.

6.21.3. Defines

Name

Brief

WDG_SW_MAJOR_VERSION

Driver Implementation Major Version.

WDG_SW_MINOR_VERSION

Driver Implementation Minor Version.

WDG_SW_PATCH_VERSION

Driver Implementation Patch Version.

WDG_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by WDG Driver.

WDG_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by WDG Driver.

WDG_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by WDG Driver.

WDG_VENDOR_ID

Texas Instruments Vendor ID.

WDG_MODULE_ID

WDG Driver Module ID.

WDG_INSTANCE_ID

WDG Driver Instance ID.

WDG_E_DRIVER_STATE

ERROR:Invalid driver state.

WDG_E_PARAM_MODE

ERROR:Invalid mode param.

WDG_E_PARAM_CONFIG

ERROR:Invalid config param.

WDG_E_PARAM_TIMEOUT

ERROR:Invalid timeout value.

WDG_E_PARAM_POINTER

ERROR:Invalid NULL ptr param.

WDG_E_INIT_FAILED

ERROR:Invalid Configuration set selection.

WDG_E_INVALID_EXEC_MODE

ERROR:Invalid ARM execution mode.

WDG_API_INIT

Wdg_Init()

WDG_API_SET_MODE

Wdg_SetMode()

WDG_SET_TRIGGER_CONDITION

Wdg_SetTriggerCondition()

WDG_API_GET_VERSION_INFO

Wdg_GetVersionInfo()

WDG_API_TRIGGER

Wdg_Trigger()

WDG_API_REGISTER_READBACK

Wdg_RegisterReadback()

6.21.4. Functions

Return type

Function Name

Brief

void

Wdg_GetVersionInfo(Std_VersionInfoType * versioninfo)

This service returns the version information of this module.

void

Wdg_Init(const Wdg_ConfigType * ConfigPtr)

This service initializes the WDG driver.

Std_ReturnType

Wdg_SetMode(WdgIf_ModeType Mode)

Switches the watchdog into the mode Mode.

void

Wdg_SetTriggerCondition(uint16 timeout)

Sets the timeout value for the trigger counter.

void

Wdg_Trigger(void )

This function triggers the servicing of the watchdog.

Std_ReturnType

Wdg_RegisterReadback(Wdg_RegisterReadbackType * RegisterReadbackPtr)

This method is Wdg_RegisterReadback Api.

6.21.4.1. function Wdg_GetVersionInfo

void Wdg_GetVersionInfo(
    Std_VersionInfoType * versioninfo
)

Brief: This service returns the version information of this module.

Service ID[hex] : 0x04U

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • versioninfo - Pointer to where to store the version information of this module.

Returns:

  • None

Return: None

6.21.4.2. function Wdg_Init

void Wdg_Init(
    const Wdg_ConfigType * ConfigPtr
)

Brief: This service initializes the WDG driver.

Service ID[hex] : 0x0

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • ConfigPtr - Pointer to WDG driver configuration set.

Returns:

  • None

Return: None

6.21.4.3. function Wdg_SetMode

Std_ReturnType Wdg_SetMode(
    WdgIf_ModeType Mode
)

Brief: Switches the watchdog into the mode Mode.

Service ID[hex] : 0x01

Sync/Async : Synchronous

Reentrancy : Non Reentrant

This Api resets the watchdog to update the set mode configuration.

Parameters:

  • Mode - One of the following statically configured modes

  • WDGIF_OFF_MODE

  • WDGIF_SLOW_MODE

  • WDGIF_FAST_MODE

Returns:

  • E_OK - Set Mode success

  • E_NOT_OK - Set Mode failed

Return: Std_ReturnType

6.21.4.4. function Wdg_SetTriggerCondition

void Wdg_SetTriggerCondition(
    uint16 timeout
)

Brief: Sets the timeout value for the trigger counter.

Service ID[hex] : 0x03

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • timeout - Timeout value (milliseconds) for setting the trigger counter

Returns:

  • None

Return: None

6.21.4.5. function Wdg_Trigger

void Wdg_Trigger(
    void 
)

Brief: This function triggers the servicing of the watchdog.

This function is the watchdog trigger and is invoked from WdgIsr

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.21.4.6. function Wdg_RegisterReadback

Std_ReturnType Wdg_RegisterReadback(
    Wdg_RegisterReadbackType * RegisterReadbackPtr
)

Brief: This method is Wdg_RegisterReadback Api.

Function could be called from from task level

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • RegisterReadbackPtr - Register readback pointer

Returns:

  • E_OK - Register readback success

  • E_NOT_OK - Register readback failed

Return: Std_ReturnType