6.18. PWM
6.18.1. Modules
Name |
|---|
6.18.2. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Possible edge notification. |
|
enum |
Output state type. |
|
enum |
Channel class type. |
|
enum |
EPWM outputs in a single epwm channel. |
|
typedef void(*)(void) |
Notification callback function pointer. |
6.18.2.1. enum Pwm_EdgeNotificationType
Enumerator |
Value |
Description |
|---|---|---|
PWM_RISING_EDGE |
1U |
Rising edges issue notification. |
PWM_FALLING_EDGE |
2U |
Falling edges issue notification. |
PWM_BOTH_EDGES |
3U |
Both edges issue notification. |
Brief: Possible edge notification.
6.18.2.2. enum Pwm_OutputStateType
Enumerator |
Value |
Description |
|---|---|---|
PWM_LOW |
0U |
LOW state. |
PWM_HIGH |
HIGH state. |
Brief: Output state type.
6.18.2.3. enum Pwm_ChannelClassType
Enumerator |
Value |
Description |
|---|---|---|
PWM_FIXED_PERIOD |
0U |
Period is immutable. |
PWM_FIXED_PERIOD_SHIFTED |
Period is immutable with phase shift. |
|
PWM_VARIABLE_PERIOD |
Period is variable. |
Brief: Channel class type.
6.18.2.4. enum Pwm_epwmOutputCh_t
Enumerator |
Value |
Description |
|---|---|---|
PWM_OUTPUT_CH_A |
0U |
Output channel A. |
PWM_OUTPUT_CH_B |
1U |
Output channel B. |
PWM_OUTPUT_CH_BOTH_A_AND_B |
2U |
Both Output channel A and B. |
Brief: EPWM outputs in a single epwm channel.
6.18.2.5. typedef Pwm_NotifyFuncType
typedef void(* Pwm_NotifyFuncType) (void);
Brief: Notification callback function pointer.
6.18.3. Structures
Name |
Brief |
|---|---|
Pwm channel configuration. |
|
Pwm configuration structure. |
|
Pwm channel configuration. |
|
Pwm configuration structure. |
|
PWM register readback structure. |
6.18.4. Defines
Name |
Brief |
|---|---|
PWM_START_SEC_VAR_INIT_8 |
Possible edge notification. |
PWM_STOP_SEC_VAR_INIT_8 |
Possible edge notification. |
PWM_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
PWM_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
PWM_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
PWM_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by PWM Driver. |
PWM_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by PWM Driver. |
PWM_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by PWM Driver. |
PWM_VENDOR_ID |
Texas Instruments Vendor ID. |
PWM_MODULE_ID |
PWM Driver Module ID. |
PWM_INSTANCE_ID |
PWM Driver Instance ID. |
PWM_E_INIT_FAILED |
PWM driver configuration parameter error. |
PWM_E_UNINIT |
PWM driver Not initialized error. |
PWM_E_PARAM_CHANNEL |
PWM driver Invalid param. |
PWM_E_PERIOD_UNCHANGEABLE |
PWM driver Fixed period channel. |
PWM_E_ALREADY_INITIALIZED |
PWM driver Already initialized. |
PWM_E_PARAM_POINTER |
PWM driver pointer parameter error. |
PWM_E_NOT_DISENGAGED |
RunTime Error: API Pwm_SetPowerState is called while the PWM module is still in use. |
PWM_SID_INIT |
PWM driver service ID for Initialization API. |
PWM_SID_DEINIT |
PWM driver service ID for De-Initialization API. |
PWM_SID_SET_DUTY_CYCLE |
PWM driver service ID for set duty cycle API. |
PWM_SID_SET_PERIOD_AND_DUTY |
PWM driver service ID for set duty cycle and period API. |
PWM_SID_SET_OUTPUT_TO_IDLE |
PWM driver service ID for set output state to idle API. |
PWM_SID_GET_OUTPUT_STATE |
PWM driver service ID for get output state API. |
PWM_SID_DISABLE_NOTIFICATION |
PWM driver service ID for disable notification API. |
PWM_SID_ENABLE_NOTIFICATION |
PWM driver service ID for Enable notification API. |
PWM_SID_GET_VERSION_INFO |
PWM driver service ID for Get version info API. |
PWM_SID_REGISTER_READBACK |
PWM driver service ID for Critical register read back API. |
PWM_STATUS_UNINIT |
PWM driver Status uninitialized. |
PWM_STATUS_INIT |
PWM driver Status Initialized. |
PWM_ISR_VOID |
void ISR type |
PWM_ISR_CAT1 |
Category 1 ISR type. |
PWM_ISR_CAT2 |
Category 2 ISR type. |
PWM_DUTY_100_PERCENT |
16 bit value representing 100% of a period value |
PWM_DUTY_0_PERCENT |
16bit value representing 0% of a period value |
PWM_USE_EPWM |
6.18.5. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Pwm_Init(const Pwm_ConfigType * CfgPtr) |
Service for PWM initialization. Initializes internal variables and the PWM unit of the micro controller. The function can be called on task level. |
void |
Pwm_DeInit(void ) |
Service for PWM de-initialization. After DeInit output states should be in idle level (it is configurable whether reset state is restored or if channel output states are really set to idle). The function can be called on task level. |
void |
Pwm_SetDutyCycle(Pwm_ChannelType ChannelNumber, uint16 DutyCycle) |
Service for setting Duty Cycle This service sets the duty cycle for a channel if DutyCycle is 0%, set output to inverse of polarity if DutyCycle is >= 100%, set output to polarity if 0% < DutyCycle < 100%, set output accordingly The function can be called on task level. |
void |
Pwm_SetPeriodAndDuty(Pwm_ChannelType ChannelNumber, Pwm_PeriodType Period, uint16 DutyCycle) |
Service for setting Period and Duty Cycle This service sets period and duty cycle for a channel if DutyCycle is 0%, set output to inverse of polarity if DutyCycle is >= 100%, set output to polarity if 0% < DutyCycle < 100%, set output accordingly The function can be called on task level. |
void |
Pwm_SetOutputToIdle(Pwm_ChannelType ChannelNumber) |
Service to set the output of a channel immediately to idle. This service sets the output of a channel immediately to idle. The idle output level is configured in driver configuration. The function can be called on task level. |
void |
Pwm_DisableNotification(Pwm_ChannelType ChannelNumber) |
Service to disable the Edge Notification Disables the Edge Notification This service deactivates the Edge Notification for the pwm channel specified by the ChannelNumber Parameter. The function can be called on task level. |
void |
Pwm_EnableNotification(Pwm_ChannelType ChannelNumber, Pwm_EdgeNotificationType Notification) |
Service to enable the Edge Notification Enables the Edge Notification This service enables the notification of the chosen edges for the Pwm channel specified by the ChannelNumber.The function can be called on task level. |
void |
Pwm_GetVersionInfo(Std_VersionInfoType * VersionInfoPtr) |
This service returns the version information of this module. Returns the version information of this module. The function can be called on task level. |
Std_ReturnType |
Pwm_RegisterReadback(Pwm_ChannelType PwmChannel, Pwm_RegisterReadbackType * RegRbPtr) |
This function reads the important registers of the hardware unit and returns the value in the structure. This API is used to check the status of critical registers which do not change during program execution. |
Pwm_GetOutputState(Pwm_ChannelType ChannelNumber) |
This function read the internal state of the PWM output signal. |
6.18.5.1. function Pwm_Init
void Pwm_Init(
const Pwm_ConfigType * CfgPtr
)
Brief: Service for PWM initialization. Initializes internal variables and the PWM unit of the micro controller. The function can be called on task level.
Possible output states of a PWM channel
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x00
Sync/Async : Synchronous
Reentrancy : Non Reentrant
Parameters:
CfgPtr - Pointer to the configuration
Returns:
None
Return: None
6.18.5.2. function Pwm_DeInit
void Pwm_DeInit(
void
)
Brief: Service for PWM de-initialization. After DeInit output states should be in idle level (it is configurable whether reset state is restored or if channel output states are really set to idle). The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x01
Sync/Async : Synchronous
Reentrancy : Non Reentrant
Parameters:
None
Returns:
None
Return: None
6.18.5.3. function Pwm_SetDutyCycle
void Pwm_SetDutyCycle(
Pwm_ChannelType ChannelNumber,
uint16 DutyCycle
)
Brief: Service for setting Duty Cycle This service sets the duty cycle for a channel if DutyCycle is 0%, set output to inverse of polarity if DutyCycle is >= 100%, set output to polarity if 0% < DutyCycle < 100%, set output accordingly The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x02
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel number
DutyCycle - Duty cycle
Returns:
None
Return: None
6.18.5.4. function Pwm_SetPeriodAndDuty
void Pwm_SetPeriodAndDuty(
Pwm_ChannelType ChannelNumber,
Pwm_PeriodType Period,
uint16 DutyCycle
)
Brief: Service for setting Period and Duty Cycle This service sets period and duty cycle for a channel if DutyCycle is 0%, set output to inverse of polarity if DutyCycle is >= 100%, set output to polarity if 0% < DutyCycle < 100%, set output accordingly The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x03
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel number
Period - Period
DutyCycle - Duty cycle
Returns:
None
Return: None
6.18.5.5. function Pwm_SetOutputToIdle
void Pwm_SetOutputToIdle(
Pwm_ChannelType ChannelNumber
)
Brief: Service to set the output of a channel immediately to idle. This service sets the output of a channel immediately to idle. The idle output level is configured in driver configuration. The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x04
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel number
Returns:
None
Return: None
6.18.5.6. function Pwm_DisableNotification
void Pwm_DisableNotification(
Pwm_ChannelType ChannelNumber
)
Brief: Service to disable the Edge Notification Disables the Edge Notification This service deactivates the Edge Notification for the pwm channel specified by the ChannelNumber Parameter. The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x06
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel number
Returns:
None
Return: None
6.18.5.7. function Pwm_EnableNotification
void Pwm_EnableNotification(
Pwm_ChannelType ChannelNumber,
Pwm_EdgeNotificationType Notification
)
Brief: Service to enable the Edge Notification Enables the Edge Notification This service enables the notification of the chosen edges for the Pwm channel specified by the ChannelNumber.The function can be called on task level.
Mode : Supervisor Mode (Privileged Mode)
Service ID[hex] : 0x07
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel number
Notification - Notification
Returns:
None
Return: None
6.18.5.8. function Pwm_GetVersionInfo
void Pwm_GetVersionInfo(
Std_VersionInfoType * VersionInfoPtr
)
Brief: This service returns the version information of this module. Returns the version information of this module. The function can be called on task level.
Mode : User Mode (Non-Privileged Mode)
Service ID[hex] : 0x08
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
VersionInfoPtr - version info
Returns:
None
Return: None
6.18.5.9. function Pwm_RegisterReadback
Std_ReturnType Pwm_RegisterReadback(
Pwm_ChannelType PwmChannel,
Pwm_RegisterReadbackType * RegRbPtr
)
Brief: This function reads the important registers of the hardware unit and returns the value in the structure. This API is used to check the status of critical registers which do not change during program execution.
Service ID[hex] : 0x0D
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
PwmChannel - Channel number
RegRbPtr - Pointer to where to store the readback values. If this pointer is NULL, then the API will return E_NOT_OK.
Returns:
E_OK Register read back has been done successfully
E_NOT_OK Register read back failed
Return: Std_ReturnType
6.18.5.10. function Pwm_GetOutputState
Pwm_OutputStateType Pwm_GetOutputState(
Pwm_ChannelType ChannelNumber
)
Brief: This function read the internal state of the PWM output signal.
Service ID[hex] : 0x05
Sync/Async : Synchronous
Reentrancy : Reentrant
Parameters:
ChannelNumber - Channel Number
Returns:
PWM_HIGH The PWM output state is high
PWM_LOW The PWM output state is low
Return: Pwm_OutputStateType