6.1. ADC
6.1.1. Modules
Name |
|---|
6.1.2. Types
Base type |
Type Name |
Brief |
|---|---|---|
enum |
Values that can be passed to ADC_setPrescaler() as the clkPrescale parameter. |
|
enum |
Values that can be passed to ADC_setMode() as the resolution parameter. |
|
enum |
Values that can be passed to ADC_setMode() as the signalMode parameter. |
|
enum |
Values that can be passed to ADC_setupSOC() as the trigger parameter to specify the event that will trigger a conversion to start. |
|
enum |
Values that can be passed to ADC_setupSOC() as the channel parameter. This is the input pin on which the signal to be converted is located. |
|
enum |
Values that can be passed to ADC_enableInterrupt(), ADC_disableInterrupt(), ADC_clearInterruptStatus(), ADC_getInterruptOverflowStatus(), ADC_clearInterruptOverflowStatus(), ADC_setInterruptSource(), ADC_enableContinuousMode(), ADC_disableContinuousMode() and ADC_getInterruptStatus() as the adcIntNum parameter. |
|
enum |
Values that can be passed in as the ppbNumber parameter for several functions. |
|
enum |
Values that can be passed in as the socNumber parameter for several functions. This value identifies the start-of-conversion (SOC) that a function is configuring or accessing. Note that in some cases (for example, ADC_setInterruptSource()) socNumber is used to refer to the corresponding end-of-conversion (EOC). |
|
enum |
Values that can be passed in as the trigger parameter for the ADC_setInterruptSOCTrigger() function. |
|
enum |
Values that can be passed to ADC_setSOCPriority() as the priMode parameter. |
|
enum |
Current status of the conversion of the requested ADC Channel group. |
|
enum |
Type for configuring the trigger source for an ADC Channel group. |
|
enum |
Type for configuring the conversion mode of an ADC Channel group. |
|
enum |
Type for configuring the streaming access mode buffer type. |
|
enum |
Type for configuring the access mode to group conversion results. |
|
enum |
Type for configuring on which edge of the hardware trigger signal the driver should react, i.e. start the conversion. |
|
enum |
Replacement mechanism, which is used on ADC group level, if a group conversion is interrupted by a group which has a higher priority. |
|
enum |
In case of active limit checking: defines which conversion values are taken into account related to the boardes defined with AdcChannelLowLimit and AdcChannelHighLimit. |
|
enum |
Type of ADC Data access method. |
|
enum |
Power state currently active or set as target power state. |
|
enum |
Result of the requests related to power state transitions. |
|
enum |
Enum to number of samplings to average. ADC allows user to program the number of samplings to average. |
|
typedef uint8 |
Numeric ID of an ADC channel. |
|
typedef uint8 |
Numeric ID of an ADC channel group. |
|
typedef uint16 |
Type for reading the converted values of a channel group (raw, without further scaling, right aligned). |
|
typedef uint32 |
Type of clock prescaler factor. |
|
typedef uint16 |
Type of conversion time, i.e. the time during which the sampled analogue value is converted into digital representation. |
|
typedef uint16 |
Type of sampling time, i.e. the time during which the value is sampled (in clockcycles). |
|
typedef uint8 |
Type of channel resolution in number of bits. |
|
typedef uint8 |
Priority level of the channel. Lowest priority is 0. |
|
typedef uint32 |
Type of assignment of channels to a channel group. |
|
typedef uint16 |
Type for configuring the number of group conversions in streaming access mode (in single access mode, parameter is 1). |
|
typedef Adc_mcalTrigger_t |
Type for the value of the ADC module embedded timer. |
|
typedef uint8 |
Specifies the identification (ID) for a ADC Hardware microcontroller peripheral (unit) |
|
typedef void(*)(void) |
Typedef for group end notification function pointer. |
|
typedef Cdd_Edma_EventCallback |
Typedef for group end notification function pointer. |
6.1.2.1. enum Adc_mcalClkPrescale_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_CLK_DIV_1_0 |
0 |
ADCCLK = (input clock) / 1.0. |
ADC_CLK_DIV_2_0 |
2 |
ADCCLK = (input clock) / 2.0. |
ADC_CLK_DIV_2_5 |
3 |
ADCCLK = (input clock) / 2.5. |
ADC_CLK_DIV_3_0 |
4 |
ADCCLK = (input clock) / 3.0. |
ADC_CLK_DIV_3_5 |
5 |
ADCCLK = (input clock) / 3.5. |
ADC_CLK_DIV_4_0 |
6 |
ADCCLK = (input clock) / 4.0. |
ADC_CLK_DIV_4_5 |
7 |
ADCCLK = (input clock) / 4.5. |
ADC_CLK_DIV_5_0 |
8 |
ADCCLK = (input clock) / 5.0. |
ADC_CLK_DIV_5_5 |
9 |
ADCCLK = (input clock) / 5.5. |
ADC_CLK_DIV_6_0 |
10 |
ADCCLK = (input clock) / 6.0. |
ADC_CLK_DIV_6_5 |
11 |
ADCCLK = (input clock) / 6.5. |
ADC_CLK_DIV_7_0 |
12 |
ADCCLK = (input clock) / 7.0. |
ADC_CLK_DIV_7_5 |
13 |
ADCCLK = (input clock) / 7.5. |
ADC_CLK_DIV_8_0 |
14 |
ADCCLK = (input clock) / 8.0. |
ADC_CLK_DIV_8_5 |
15 |
ADCCLK = (input clock) / 8.5. |
Brief: Values that can be passed to ADC_setPrescaler() as the clkPrescale parameter.
6.1.2.2. enum Adc_mcalResolution_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_RESOLUTION_12BIT |
0 |
12-bit conversion resolution |
Brief: Values that can be passed to ADC_setMode() as the resolution parameter.
6.1.2.3. enum Adc_mcalSignalMode_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_MODE_SINGLE_ENDED |
0 |
Sample on single pin with VREFLO. |
ADC_MODE_DIFFERENTIAL |
1 |
Sample on pair of pins. |
Brief: Values that can be passed to ADC_setMode() as the signalMode parameter.
6.1.2.4. enum Adc_mcalTrigger_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_TRIGGER_SW_ONLY |
0x00 |
Software only. |
ADC_TRIGGER_RTI0 |
0x01 |
RTI Timer 0. |
ADC_TRIGGER_RTI1 |
0x02 |
RTI Timer 1. |
ADC_TRIGGER_RTI2 |
0x03 |
RTI Timer 2. |
ADC_TRIGGER_RTI3 |
0x04 |
RTI Timer 3. |
ADC_TRIGGER_INPUT_XBAR_OUT5 |
0x05 |
InputXBar.Out[5]. |
ADC_TRIGGER_EPWM0_SOCA |
0x08 |
ePWM0, ADCSOCA |
ADC_TRIGGER_EPWM0_SOCB |
0x09 |
ePWM0, ADCSOCB |
ADC_TRIGGER_EPWM1_SOCA |
0x0A |
ePWM1, ADCSOCA |
ADC_TRIGGER_EPWM1_SOCB |
0x0B |
ePWM1, ADCSOCB |
ADC_TRIGGER_EPWM2_SOCA |
0x0C |
ePWM2, ADCSOCA |
ADC_TRIGGER_EPWM2_SOCB |
0x0D |
ePWM2, ADCSOCB |
ADC_TRIGGER_EPWM3_SOCA |
0x0E |
ePWM3, ADCSOCA |
ADC_TRIGGER_EPWM3_SOCB |
0x0F |
ePWM3, ADCSOCB |
ADC_TRIGGER_EPWM4_SOCA |
0x10 |
ePWM4, ADCSOCA |
ADC_TRIGGER_EPWM4_SOCB |
0x11 |
ePWM4, ADCSOCB |
ADC_TRIGGER_EPWM5_SOCA |
0x12 |
ePWM5, ADCSOCA |
ADC_TRIGGER_EPWM5_SOCB |
0x13 |
ePWM5, ADCSOCB |
ADC_TRIGGER_EPWM6_SOCA |
0x14 |
ePWM6, ADCSOCA |
ADC_TRIGGER_EPWM6_SOCB |
0x15 |
ePWM6, ADCSOCB |
ADC_TRIGGER_EPWM7_SOCA |
0x16 |
ePWM7, ADCSOCA |
ADC_TRIGGER_EPWM7_SOCB |
0x17 |
ePWM7, ADCSOCB |
ADC_TRIGGER_EPWM8_SOCA |
0x18 |
ePWM8, ADCSOCA |
ADC_TRIGGER_EPWM8_SOCB |
0x19 |
ePWM8, ADCSOCB |
ADC_TRIGGER_EPWM9_SOCA |
0x1A |
ePWM9, ADCSOCA |
ADC_TRIGGER_EPWM9_SOCB |
0x1B |
ePWM9, ADCSOCB |
ADC_TRIGGER_EPWM10_SOCA |
0x1C |
ePWM10, ADCSOCA |
ADC_TRIGGER_EPWM10_SOCB |
0x1D |
ePWM10, ADCSOCB |
ADC_TRIGGER_EPWM11_SOCA |
0x1E |
ePWM11, ADCSOCA |
ADC_TRIGGER_EPWM11_SOCB |
0x1F |
ePWM11, ADCSOCB |
ADC_TRIGGER_EPWM12_SOCA |
0x20 |
ePWM12, ADCSOCA |
ADC_TRIGGER_EPWM12_SOCB |
0x21 |
ePWM12, ADCSOCB |
ADC_TRIGGER_EPWM13_SOCA |
0x22 |
ePWM13, ADCSOCA |
ADC_TRIGGER_EPWM13_SOCB |
0x23 |
ePWM13, ADCSOCB |
ADC_TRIGGER_EPWM14_SOCA |
0x24 |
ePWM14, ADCSOCA |
ADC_TRIGGER_EPWM14_SOCB |
0x25 |
ePWM14, ADCSOCB |
ADC_TRIGGER_EPWM15_SOCA |
0x26 |
ePWM15, ADCSOCA |
ADC_TRIGGER_EPWM15_SOCB |
0x27 |
ePWM15, ADCSOCB |
ADC_TRIGGER_EPWM16_SOCA |
0x28 |
ePWM16, ADCSOCA |
ADC_TRIGGER_EPWM16_SOCB |
0x29 |
ePWM16, ADCSOCB |
ADC_TRIGGER_EPWM17_SOCA |
0x2A |
ePWM17, ADCSOCA |
ADC_TRIGGER_EPWM17_SOCB |
0x2B |
ePWM17, ADCSOCB |
ADC_TRIGGER_EPWM18_SOCA |
0x2C |
ePWM18, ADCSOCA |
ADC_TRIGGER_EPWM18_SOCB |
0x2D |
ePWM18, ADCSOCB |
ADC_TRIGGER_EPWM19_SOCA |
0x2E |
ePWM19, ADCSOCA |
ADC_TRIGGER_EPWM19_SOCB |
0x2F |
ePWM19, ADCSOCB |
ADC_TRIGGER_EPWM20_SOCA |
0x30 |
ePWM20, ADCSOCA |
ADC_TRIGGER_EPWM20_SOCB |
0x31 |
ePWM20, ADCSOCB |
ADC_TRIGGER_EPWM21_SOCA |
0x32 |
ePWM21, ADCSOCA |
ADC_TRIGGER_EPWM21_SOCB |
0x33 |
ePWM21, ADCSOCB |
ADC_TRIGGER_EPWM22_SOCA |
0x34 |
ePWM22, ADCSOCA |
ADC_TRIGGER_EPWM22_SOCB |
0x35 |
ePWM22, ADCSOCB |
ADC_TRIGGER_EPWM23_SOCA |
0x36 |
ePWM23, ADCSOCA |
ADC_TRIGGER_EPWM23_SOCB |
0x37 |
ePWM23, ADCSOCB |
ADC_TRIGGER_EPWM24_SOCA |
0x38 |
ePWM24, ADCSOCA |
ADC_TRIGGER_EPWM24_SOCB |
0x39 |
ePWM24, ADCSOCB |
ADC_TRIGGER_EPWM25_SOCA |
0x3A |
ePWM25, ADCSOCA |
ADC_TRIGGER_EPWM25_SOCB |
0x3B |
ePWM25, ADCSOCB |
ADC_TRIGGER_EPWM26_SOCA |
0x3C |
ePWM26, ADCSOCA |
ADC_TRIGGER_EPWM26_SOCB |
0x3D |
ePWM26, ADCSOCB |
ADC_TRIGGER_EPWM27_SOCA |
0x3E |
ePWM27, ADCSOCA |
ADC_TRIGGER_EPWM27_SOCB |
0x3F |
ePWM27, ADCSOCB |
ADC_TRIGGER_EPWM28_SOCA |
0x40 |
ePWM28, ADCSOCA |
ADC_TRIGGER_EPWM28_SOCB |
0x41 |
ePWM28, ADCSOCB |
ADC_TRIGGER_EPWM29_SOCA |
0x42 |
ePWM29, ADCSOCA |
ADC_TRIGGER_EPWM29_SOCB |
0x43 |
ePWM29, ADCSOCB |
ADC_TRIGGER_EPWM30_SOCA |
0x44 |
ePWM30, ADCSOCA |
ADC_TRIGGER_EPWM30_SOCB |
0x45 |
ePWM30, ADCSOCB |
ADC_TRIGGER_EPWM31_SOCA |
0x46 |
ePWM31, ADCSOCA |
ADC_TRIGGER_EPWM31_SOCB |
0x47 |
ePWM31, ADCSOCB |
ADC_TRIGGER_ECAP0 |
0x48 |
ECAP0. |
ADC_TRIGGER_ECAP1 |
0x49 |
ECAP1. |
ADC_TRIGGER_ECAP2 |
0x4A |
ECAP2. |
ADC_TRIGGER_ECAP3 |
0x4B |
ECAP3. |
ADC_TRIGGER_ECAP4 |
0x4C |
ECAP4. |
ADC_TRIGGER_ECAP5 |
0x4D |
ECAP5. |
ADC_TRIGGER_ECAP6 |
0x4E |
ECAP6. |
ADC_TRIGGER_ECAP7 |
0x4F |
ECAP7. |
ADC_TRIGGER_ECAP8 |
0x50 |
ECAP8. |
ADC_TRIGGER_ECAP9 |
0x51 |
ECAP9. |
ADC_TRIGGER_NONE |
0x7F |
Spare. |
Brief: Values that can be passed to ADC_setupSOC() as the trigger parameter to specify the event that will trigger a conversion to start.
6.1.2.5. enum Adc_mcalChannel_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_CH_ADCIN0 |
0 |
single-ended, ADCIN0 |
ADC_CH_ADCIN1 |
1 |
single-ended, ADCIN1 |
ADC_CH_ADCIN2 |
2 |
single-ended, ADCIN2 |
ADC_CH_ADCIN3 |
3 |
single-ended, ADCIN3 |
ADC_CH_ADCIN4 |
4 |
single-ended, ADCIN4 |
ADC_CH_ADCIN5 |
5 |
single-ended, ADCIN5 |
ADC_CH_CAL0 |
6 |
single-ended, CAL0 |
ADC_CH_CAL1 |
7 |
single-ended, CAL1 |
ADC_CH_ADCIN0_ADCIN1 |
0 |
differential, ADCIN0 and ADCIN1 |
ADC_CH_ADCIN1_ADCIN0 |
1 |
differential, ADCIN1 and ADCIN0 |
ADC_CH_ADCIN2_ADCIN3 |
2 |
differential, ADCIN2 and ADCIN3 |
ADC_CH_ADCIN3_ADCIN2 |
3 |
differential, ADCIN3 and ADCIN2 |
ADC_CH_ADCIN4_ADCIN5 |
4 |
differential, ADCIN4 and ADCIN5 |
ADC_CH_ADCIN5_ADCIN4 |
5 |
differential, ADCIN5 and ADCIN4 |
ADC_CH_CAL0_CAL1 |
6 |
differential, CAL0 and CAL1 |
Brief: Values that can be passed to ADC_setupSOC() as the channel parameter. This is the input pin on which the signal to be converted is located.
6.1.2.6. enum Adc_mcalIntNumber_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_INT_NUMBER1 |
0 |
ADCINT1 Interrupt. |
ADC_INT_NUMBER2 |
1 |
ADCINT2 Interrupt. |
ADC_INT_NUMBER3 |
2 |
ADCINT3 Interrupt. |
ADC_INT_NUMBER4 |
3 |
ADCINT4 Interrupt. |
Brief: Values that can be passed to ADC_enableInterrupt(), ADC_disableInterrupt(), ADC_clearInterruptStatus(), ADC_getInterruptOverflowStatus(), ADC_clearInterruptOverflowStatus(), ADC_setInterruptSource(), ADC_enableContinuousMode(), ADC_disableContinuousMode() and ADC_getInterruptStatus() as the adcIntNum parameter.
6.1.2.7. enum Adc_mcalPPBNumber_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_PPB_NUMBER1 |
0 |
Post-processing block 1. |
ADC_PPB_NUMBER2 |
1 |
Post-processing block 2. |
ADC_PPB_NUMBER3 |
2 |
Post-processing block 3. |
ADC_PPB_NUMBER4 |
3 |
Post-processing block 4. |
Brief: Values that can be passed in as the ppbNumber parameter for several functions.
6.1.2.8. enum Adc_mcalSOCNumber_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_SOC_NUMBER0 |
0 |
SOC/EOC number 0. |
ADC_SOC_NUMBER1 |
1 |
SOC/EOC number 1. |
ADC_SOC_NUMBER2 |
2 |
SOC/EOC number 2. |
ADC_SOC_NUMBER3 |
3 |
SOC/EOC number 3. |
ADC_SOC_NUMBER4 |
4 |
SOC/EOC number 4. |
ADC_SOC_NUMBER5 |
5 |
SOC/EOC number 5. |
ADC_SOC_NUMBER6 |
6 |
SOC/EOC number 6. |
ADC_SOC_NUMBER7 |
7 |
SOC/EOC number 7. |
ADC_SOC_NUMBER8 |
8 |
SOC/EOC number 8. |
ADC_SOC_NUMBER9 |
9 |
SOC/EOC number 9. |
ADC_SOC_NUMBER10 |
10 |
SOC/EOC number 10. |
ADC_SOC_NUMBER11 |
11 |
SOC/EOC number 11. |
ADC_SOC_NUMBER12 |
12 |
SOC/EOC number 12. |
ADC_SOC_NUMBER13 |
13 |
SOC/EOC number 13. |
ADC_SOC_NUMBER14 |
14 |
SOC/EOC number 14. |
ADC_SOC_NUMBER15 |
15 |
SOC/EOC number 15. |
ADC_INVALID_HW_SOC |
16 |
SOC/EOC number 16. |
Brief: Values that can be passed in as the socNumber parameter for several functions. This value identifies the start-of-conversion (SOC) that a function is configuring or accessing. Note that in some cases (for example, ADC_setInterruptSource()) socNumber is used to refer to the corresponding end-of-conversion (EOC).
6.1.2.9. enum Adc_mcalIntSOCTrigger_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_INT_SOC_TRIGGER_NONE |
0 |
No ADCINT will trigger the SOC. |
ADC_INT_SOC_TRIGGER_ADCINT1 |
1 |
ADCINT1 will trigger the SOC. |
ADC_INT_SOC_TRIGGER_ADCINT2 |
2 |
ADCINT2 will trigger the SOC. |
Brief: Values that can be passed in as the trigger parameter for the ADC_setInterruptSOCTrigger() function.
6.1.2.10. enum Adc_mcalPriorityMode_t
Enumerator |
Value |
Description |
|---|---|---|
ADC_PRI_ALL_ROUND_ROBIN |
0 |
Round robin mode is used for all. |
ADC_PRI_SOC0_HIPRI |
1 |
SOC 0 hi pri, others in round robin. |
ADC_PRI_THRU_SOC1_HIPRI |
2 |
SOC 0-1 hi pri, others in round robin. |
ADC_PRI_THRU_SOC2_HIPRI |
3 |
SOC 0-2 hi pri, others in round robin. |
ADC_PRI_THRU_SOC3_HIPRI |
4 |
SOC 0-3 hi pri, others in round robin. |
ADC_PRI_THRU_SOC4_HIPRI |
5 |
SOC 0-4 hi pri, others in round robin. |
ADC_PRI_THRU_SOC5_HIPRI |
6 |
SOC 0-5 hi pri, others in round robin. |
ADC_PRI_THRU_SOC6_HIPRI |
7 |
SOC 0-6 hi pri, others in round robin. |
ADC_PRI_THRU_SOC7_HIPRI |
8 |
SOC 0-7 hi pri, others in round robin. |
ADC_PRI_THRU_SOC8_HIPRI |
9 |
SOC 0-8 hi pri, others in round robin. |
ADC_PRI_THRU_SOC9_HIPRI |
10 |
SOC 0-9 hi pri, others in round robin. |
ADC_PRI_THRU_SOC10_HIPRI |
11 |
SOC 0-10 hi pri, others in round robin. |
ADC_PRI_THRU_SOC11_HIPRI |
12 |
SOC 0-11 hi pri, others in round robin. |
ADC_PRI_THRU_SOC12_HIPRI |
13 |
SOC 0-12 hi pri, others in round robin. |
ADC_PRI_THRU_SOC13_HIPRI |
14 |
SOC 0-13 hi pri, others in round robin. |
ADC_PRI_THRU_SOC14_HIPRI |
15 |
SOC 0-14 hi pri, others in round robin. |
ADC_PRI_ALL_HIPRI |
16 |
All priorities based on SOC number. |
Brief: Values that can be passed to ADC_setSOCPriority() as the priMode parameter.
6.1.2.11. enum Adc_StatusType
Enumerator |
Value |
Description |
|---|---|---|
ADC_IDLE |
The conversion of the specified group has not been started. No result is available. |
|
ADC_BUSY |
The conversion of the specified group has been started and is still going on. So far no result is available. |
|
ADC_COMPLETED |
A conversion round (which is not the final one) of the specified group has been finished. A result is available for all channels of the group. |
|
ADC_STREAM_COMPLETED |
The result buffer is completely filled. For each channel of the selected group the number of samples to be acquired is available. |
Brief: Current status of the conversion of the requested ADC Channel group.
6.1.2.12. enum Adc_TriggerSourceType
Enumerator |
Value |
Description |
|---|---|---|
ADC_TRIGG_SRC_SW |
Group is triggered by a software API call. |
|
ADC_TRIGG_SRC_HW |
Group is triggered by a hardware event Note: This feature is not supported in this driver. |
Brief: Type for configuring the trigger source for an ADC Channel group.
6.1.2.13. enum Adc_GroupConvModeType
Enumerator |
Value |
Description |
|---|---|---|
ADC_CONV_MODE_ONESHOT |
Exactly one conversion of each channel in an ADC channel group is performed after the configured trigger event. |
|
ADC_CONV_MODE_CONTINUOUS |
Repeated conversions of each ADC channel in an ADC channel group are performed. |
Brief: Type for configuring the conversion mode of an ADC Channel group.
6.1.2.14. enum Adc_StreamBufferModeType
Enumerator |
Value |
Description |
|---|---|---|
ADC_STREAM_BUFFER_LINEAR |
he ADC Driver stops the conversion as soon as the stream buffer is full (number of samples reached) |
|
ADC_STREAM_BUFFER_CIRCULAR |
The ADC Driver continues the conversion even if the stream buffer is full (number of samples reached) by wrapping around the stream buffer itself. |
Brief: Type for configuring the streaming access mode buffer type.
6.1.2.15. enum Adc_GroupAccessModeType
Enumerator |
Value |
Description |
|---|---|---|
ADC_ACCESS_MODE_SINGLE |
Single value access mode. |
|
ADC_ACCESS_MODE_STREAMING |
Streaming access mode. |
Brief: Type for configuring the access mode to group conversion results.
6.1.2.16. enum Adc_HwTriggerSignalType
Enumerator |
Value |
Description |
|---|---|---|
ADC_HW_TRIG_RISING_EDGE |
React on the rising edge of the hardware trigger signal. |
|
ADC_HW_TRIG_FALLING_EDGE |
React on the falling edge of the hardware trigger signal. |
|
ADC_HW_TRIG_BOTH_EDGES |
React on both edges of the hardware trigger signal. |
Brief: Type for configuring on which edge of the hardware trigger signal the driver should react, i.e. start the conversion.
Note: This feature is not supported in this driver
6.1.2.17. enum Adc_GroupReplacementType
Enumerator |
Value |
Description |
|---|---|---|
ADC_GROUP_REPL_ABORT_RESTART |
Abort/Restart mechanism is used on group level, if a group is interrupted by a higher priority group. |
|
ADC_GROUP_REPL_SUSPEND_RESUME |
Suspend/Resume mechanism is used on group level, if a group is interrupted by a higher priority group. Note: The implementation is same as abort/restart i.e. when a group is started again, previous intermediate results are discarded and the driver always starts from first channel of the group. |
Brief: Replacement mechanism, which is used on ADC group level, if a group conversion is interrupted by a group which has a higher priority.
6.1.2.18. enum Adc_ChannelRangeSelectType
Enumerator |
Value |
Description |
|---|---|---|
ADC_RANGE_UNDER_LOW |
Range below low limit - low limit value included. |
|
ADC_RANGE_BETWEEN |
Range between low limit and high limit - high limit value included. |
|
ADC_RANGE_OVER_HIGH |
Range above high limit. |
|
ADC_RANGE_ALWAYS |
Complete range - independent from channel limit settings. |
|
ADC_RANGE_NOT_UNDER_LOW |
Range above low limit. |
|
ADC_RANGE_NOT_BETWEEN |
Range above high limit or below low limit - low limit value included. |
|
ADC_RANGE_NOT_OVER_HIGH |
Range below high limit - high limit value included. |
Brief: In case of active limit checking: defines which conversion values are taken into account related to the boardes defined with AdcChannelLowLimit and AdcChannelHighLimit.
Note: This feature is not supported yet.
6.1.2.19. enum Adc_GroupDataAccessType
Enumerator |
Value |
Description |
|---|---|---|
ADC_GROUP_INTERRUPT_ACCESS |
Interrupt Provides the data. |
|
ADC_GROUP_POLLING_ACCESS |
Polling method to get the data. |
|
ADC_GROUP_DMA_ACCESS |
DMA method to get the data. |
Brief: Type of ADC Data access method.
6.1.2.20. enum Adc_PowerStateType
Enumerator |
Value |
Description |
|---|---|---|
ADC_FULL_POWER |
Full Power (0) |
|
ADC_ZERO_POWER |
Power modes with decreasing power consumptions. |
Brief: Power state currently active or set as target power state.
6.1.2.21. enum Adc_PowerStateRequestResultType
Enumerator |
Value |
Description |
|---|---|---|
ADC_SERVICE_ACCEPTED |
Power state change executed. |
|
ADC_NOT_INIT |
ADC Module not initialized. |
|
ADC_SEQUENCE_ERROR |
Wrong API call sequence. |
|
ADC_HW_FAILURE |
The HW module has a failure which prevents it to enter the required power state. |
|
ADC_POWER_STATE_NOT_SUPP |
ADC Module does not support the requested power state. |
|
ADC_TRANS_NOT_POSSIBLE |
ADC Module cannot transition directly from the current power state to the requested power state or the HW peripheral is still busy. |
Brief: Result of the requests related to power state transitions.
6.1.2.22. enum Adc_AveragingMode
Enumerator |
Value |
Description |
|---|---|---|
ADC_AVERAGING_MODE_NONE |
Disable averaging. |
|
ADC_AVERAGING_MODE_2_SAMPLES |
Set number of samplings to average to 2. |
|
ADC_AVERAGING_MODE_4_SAMPLES |
Set number of samplings to average to 4. |
|
ADC_AVERAGING_MODE_8_SAMPLES |
Set number of samplings to average to 8. |
|
ADC_AVERAGING_MODE_16_SAMPLES |
Set number of samplings to average to 16. |
Brief: Enum to number of samplings to average. ADC allows user to program the number of samplings to average.
6.1.2.23. typedef Adc_ChannelType
typedef uint8 Adc_ChannelType;
Brief: Numeric ID of an ADC channel.
6.1.2.24. typedef Adc_GroupType
typedef uint8 Adc_GroupType;
Brief: Numeric ID of an ADC channel group.
6.1.2.25. typedef Adc_ValueGroupType
typedef uint16 Adc_ValueGroupType;
Brief: Type for reading the converted values of a channel group (raw, without further scaling, right aligned).
Note: Even though the resolution for this ADC HW is 10-bit, we set this to 32-bit integer as the register read access is 32-bit.
6.1.2.26. typedef Adc_PrescaleType
typedef uint32 Adc_PrescaleType;
Brief: Type of clock prescaler factor.
6.1.2.27. typedef Adc_ConversionTimeType
typedef uint16 Adc_ConversionTimeType;
Brief: Type of conversion time, i.e. the time during which the sampled analogue value is converted into digital representation.
6.1.2.28. typedef Adc_SamplingTimeType
typedef uint16 Adc_SamplingTimeType;
Brief: Type of sampling time, i.e. the time during which the value is sampled (in clockcycles).
6.1.2.29. typedef Adc_ResolutionType
typedef uint8 Adc_ResolutionType;
Brief: Type of channel resolution in number of bits.
6.1.2.30. typedef Adc_GroupPriorityType
typedef uint8 Adc_GroupPriorityType;
Brief: Priority level of the channel. Lowest priority is 0.
6.1.2.31. typedef Adc_GroupDefType
typedef uint32 Adc_GroupDefType;
Brief: Type of assignment of channels to a channel group.
6.1.2.32. typedef Adc_StreamNumSampleType
typedef uint16 Adc_StreamNumSampleType;
Brief: Type for configuring the number of group conversions in streaming access mode (in single access mode, parameter is 1).
6.1.2.33. typedef Adc_HwTriggerTimerType
typedef Adc_mcalTrigger_t Adc_HwTriggerTimerType;
Brief: Type for the value of the ADC module embedded timer.
6.1.2.34. typedef Adc_HWUnitType
typedef uint8 Adc_HWUnitType;
Brief: Specifies the identification (ID) for a ADC Hardware microcontroller peripheral (unit)
6.1.2.35. typedef Adc_GroupEndNotifyType
typedef void(* Adc_GroupEndNotifyType) (void);
Brief: Typedef for group end notification function pointer.
6.1.2.36. typedef Adc_DmaCallBackFunctionType
typedef Cdd_Edma_EventCallback Adc_DmaCallBackFunctionType;
Brief: Typedef for group end notification function pointer.
6.1.3. Structures
Name |
Brief |
|---|---|
ADC log structure per group entry. |
|
ADC group log structure. |
|
ADC log structure per FIFO error entry. |
|
ADC FIFO error log structure. |
|
Structure containing parameters for ADC MCAL channel configuration. In term of ADC hardware, this represents the step configuration. There are ADC_NUM_CHANNEL steps in the ADC hardware and each step could be mapped to an actual hardware input channel. |
|
ADC Group configuration structure. |
|
ADC Hardware unit configuration structure. |
|
ADC register readback structure. |
|
ADC config structure. |
|
Self referential structure for double link list. |
|
Structure to the link list object information. |
6.1.4. Defines
Name |
Brief |
|---|---|
ADC_SW_MAJOR_VERSION |
Driver Implementation Major Version. |
ADC_SW_MINOR_VERSION |
Driver Implementation Minor Version. |
ADC_SW_PATCH_VERSION |
Driver Implementation Patch Version. |
ADC_AR_RELEASE_MAJOR_VERSION |
AUTOSAR Major version specification implemented by ADC Driver. |
ADC_AR_RELEASE_MINOR_VERSION |
AUTOSAR Minor version specification implemented by ADC Driver. |
ADC_AR_RELEASE_REVISION_VERSION |
AUTOSAR Patch version specification implemented by ADC Driver. |
ADC_VENDOR_ID |
Texas Instruments Vendor ID. |
ADC_MODULE_ID |
ADC Driver Module ID. |
ADC_INSTANCE_ID |
ADC Driver Instance ID. |
ADC_TRUE |
Boolean Macros for ADC module. |
ADC_FALSE |
Boolean Macros for ADC module. |
ADC_ISR_VOID |
void ISR type |
ADC_ISR_CAT1 |
Category 1 ISR type. |
ADC_ISR_CAT2 |
Category 2 ISR type. |
ADC_E_UNINIT |
API service used without module initialization. |
ADC_E_BUSY |
API service called during ongoing process. |
ADC_E_IDLE |
API service called while no conversion is ongoing. |
ADC_E_ALREADY_INITIALIZED |
API Adc_Init service called while the ADC driver has already been initialized. |
ADC_E_PARAM_CONFIG |
API service called with incorrect configuration parameter. |
ADC_E_PARAM_POINTER |
API servcie called with invalid data buffer pointer. |
ADC_E_PARAM_GROUP |
API servcie called with invalid group ID. |
ADC_E_WRONG_CONV_MODE |
API service called on a group with conversion mode configured as continuous. |
ADC_E_WRONG_TRIGG_SRC |
API servcie called for group with wrong trigger source. |
ADC_E_NOTIF_CAPABILITY |
Enable/disable notification function for a group whose configuration set has no notification available. |
ADC_E_BUFFER_UNINIT |
Conversion started and result buffer pointer is not initialized. |
ADC_E_NOT_DISENGAGED |
One or more ADC group/channel not in IDLE state. |
ADC_E_POWER_STATE_NOT_SUPPORTED |
Unsupported power state request. |
ADC_E_TRANSITION_NOT_POSSIBLE |
Requested power state can not be reached directly. |
ADC_E_PERIPHERAL_NOT_PREPARED |
ADC not prepared for target power state. |
ADC_SID_INIT |
Adc_Init() API Service ID. |
ADC_SID_DEINIT |
Adc_DeInit() API Service ID. |
ADC_SID_START_GROUP_CONVERSION |
Adc_StartGroupConversion() API Service ID. |
ADC_SID_STOP_GROUP_CONVERSION |
Adc_StopGroupConversion() API Service ID. |
ADC_SID_READ_GROUP |
Adc_ReadGroup() API Service ID. |
ADC_SID_ENABLE_HARDWARE_TRIGGER |
Adc_EnableHardwareTrigger() API Service ID. |
ADC_SID_DISABLE_HARDWARE_TRIGGER |
Adc_DisableHardwareTrigger() API Service ID. |
ADC_SID_ENABLE_GROUP_NOTIFICATION |
Adc_EnableGroupNotification() API Service ID. |
ADC_SID_DISABLE_GROUP_NOTIFICATION |
Adc_DisableGroupNotification() API Service ID. |
ADC_SID_GET_GROUP_STATUS |
Adc_GetGroupStatus() API Service ID. |
ADC_SID_GET_VERSION_INFO |
Adc_GetVersionInfo() API Service ID. |
ADC_SID_GET_STREAM_LAST_POINTER |
Adc_GetStreamLastPointer() API Service ID. |
ADC_SID_SETUP_RESULT_BUFFER |
Adc_SetupResultBuffer() API Service ID. |
ADC_SID_SET_POWER_STATE |
Adc_SetPowerState() API Service ID. |
ADC_SID_GET_CURRENT_POWER_STATE |
Adc_GetCurrentPowerState() API Service ID. |
ADC_SID_GET_TARGET_POWER_STATE |
Adc_GetTargetPowerState() API Service ID. |
ADC_SID_PREPARE_POWER_STATE |
Adc_PreparePowerState() API Service ID. |
ADC_SID_MAIN_POWER_TRANSITION_MANAGER |
Adc_Main_PowerTransitionManager() API Service ID. |
ADC_SID_IOHWAB_NOTIFICATION |
IoHwAb_AdcNotification() API Service ID. |
ADC_SID_IOHWAB_NOTIFY_READY_FOR_POWER_STATE |
IoHwAb_Adc_NotifyReadyForPowerState() API Service ID. |
ADC_SID_READ_TEMPERATURE |
IoHwAb_Adc_NotifyReadyForPowerState() API Service ID. |
ADC_SID_READ_TEMPERATURE_RESULT |
IoHwAb_Adc_NotifyReadyForPowerState() API Service ID. |
ADC_SID_POLLING_MAINFUNCTION |
Adc_PollingMainFunction() API Service ID. |
ADC_SID_REGISTER_READBACK |
Adc_RegisterReadback() API Service ID. |
ADC_SID_GET_READ_RESULT_BASE_ADDRESS |
Adc_GetReadResultBaseAddress() API Service ID. |
ADC_SID_SET_INTERRUPT_CONTINUOUS_MODE |
Adc_SetInterruptContinuousMode() API Service ID. |
ADC_START_SEC_CODE |
Start Memory section tag. |
ADC_START_SEC_CODE |
Start Memory section tag. |
ADC_STOP_SEC_CODE |
End Memory section tag. |
ADC_STOP_SEC_CODE |
End Memory section tag. |
ADC_FORCE_SOC0 |
SW trigger ADC SOC 0. |
ADC_FORCE_SOC1 |
SW trigger ADC SOC 1. |
ADC_FORCE_SOC2 |
SW trigger ADC SOC 2. |
ADC_FORCE_SOC3 |
SW trigger ADC SOC 3. |
ADC_FORCE_SOC4 |
SW trigger ADC SOC 4. |
ADC_FORCE_SOC5 |
SW trigger ADC SOC 5. |
ADC_FORCE_SOC6 |
SW trigger ADC SOC 6. |
ADC_FORCE_SOC7 |
SW trigger ADC SOC 7. |
ADC_FORCE_SOC8 |
SW trigger ADC SOC 8. |
ADC_FORCE_SOC9 |
SW trigger ADC SOC 9. |
ADC_FORCE_SOC10 |
SW trigger ADC SOC 10. |
ADC_FORCE_SOC11 |
SW trigger ADC SOC 11. |
ADC_FORCE_SOC12 |
SW trigger ADC SOC 12. |
ADC_FORCE_SOC13 |
SW trigger ADC SOC 13. |
ADC_FORCE_SOC14 |
SW trigger ADC SOC 14. |
ADC_FORCE_SOC15 |
SW trigger ADC SOC 15. |
MCAL_ADC_ADCSOCxCTL_STEP |
Register offset difference between 2 ADCSOCxCTL registers. |
MCAL_ADC_ADCINTSELxNy_STEP |
Register offset difference between 2 ADCINTSELxNy registers. |
MCAL_ADC_ADCPPBx_STEP |
Register offset difference between 2 ADCPPBxCONFIG registers. |
MCAL_ADC_ADCPPBTRIP_MASK |
ADC PPB Trip Mask. |
MCAL_ADC_RESULT_ADCPPBxRESULT_STEP |
Register offset difference between 2 ADCPPBxRESULT registers. |
MCAL_ADC_RESULT_ADCRESULTx_STEP |
Register offset difference between 2 ADCRESULTx registers. |
ADC_NUM_CHANNEL |
Number of MCAL channels - in terms of ADC HW, this represents the number of hardware steps. Note: In terms of ADC IP number of steps is 16. Due to AUTOSAR specification, the channel ID’s should be unique i.e each channel Id and actual HW channel should have one to one mapping. So ADC_NUM_CHANNEL is fixed to 9 as number of actual HW channels available is also 9. |
ADC_MIN_CHANNEL_ID |
Minimum value of channel ID. |
ADC_MAX_CHANNEL_ID |
Maximum value of channel ID. |
6.1.5. Functions
Return type |
Function Name |
Brief |
|---|---|---|
void |
Adc_Init(const Adc_ConfigType * CfgPtr) |
Service for ADC initialization. |
void |
Adc_DeInit(void ) |
This service sets all ADC HW Units to a state comparable to their power on reset state. |
Std_ReturnType |
Adc_SetupResultBuffer(Adc_GroupType Group, const Adc_ValueGroupType * DataBufferPtr) |
This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored. |
Adc_GetGroupStatus(Adc_GroupType Group) |
Returns the conversion status of the requested ADC Channel group. |
|
Adc_GetStreamLastPointer(Adc_GroupType Group, Adc_ValueGroupType ** PtrToSamplePtr) |
Returns the number of valid samples per channel, stored in the result buffer. |
|
void |
Starts the conversion of all channels of the requested ADC Channel group. |
|
void |
Stops the conversion of the requested ADC Channel group. |
|
Std_ReturnType |
Adc_ReadGroup(Adc_GroupType Group, Adc_ValueGroupType * DataBufferPtr) |
Reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the DataBufferPtr address. |
void |
Enables the notification mechanism for the requested ADC Channel group. |
|
void |
Disables the notification mechanism for the requested ADC Channel group. |
|
void |
Adc_GetVersionInfo(Std_VersionInfoType * versioninfo) |
This service returns the version information of this module. |
Std_ReturnType |
Adc_RegisterReadback(Adc_HWUnitType HWUnit, Adc_RegisterReadbackType * RegRbPtr) |
This function reads the important registers of the hardware unit and returns the value in the structure. |
void |
Enables the hardware trigger for the requested ADC Channel group. |
|
void |
Disables the hardware trigger for the requested ADC Channel group. |
|
void |
Adc_InitTemperatureRead(void ) |
This service initializes the efuse parameters for temperature calculation. This is a non-autosar, TI defined API This API is not applicable for AM263x. |
void |
Adc_ReadTemperature(Adc_GroupType Group, uint8 NumAverages, Adc_TempSensValueType * TempValuesPtr) |
This service starts temperature conversion, waits for completion and reads the temperature sensors group configured as part of Adc_Init and returns the temperature values. This is a non-autosar, TI defined API. This API is not applicable for AM263x. |
void |
Adc_ReadTemperatureResult(Adc_GroupType Group, Adc_TempSensValueType * TempValuesPtr) |
This service reads only the results of the temperature sensors group configured as part of Adc_Init, Adc_StartGroupConversion and returns the temperature values. This is a non-autosar, TI defined API. This API is not applicable for AM263x. |
void |
Adc_PollingMainFunction(void ) |
This service is used for Polling Group data. |
uint32 |
Returns the HW result register base address. |
|
Std_ReturnType |
Sets the continue to interrupt mode of ADC. |
|
void |
ADC_setPrescaler(uint32 base, Adc_mcalClkPrescale_t clkPrescale) |
Configures the analog-to-digital converter module prescaler. |
void |
ADC_setupSOC(uint32 base, uint32 socNumber, Adc_mcalTrigger_t trigger, uint32 channel, uint32 sampleWindow) |
Configures a start-of-conversion (SOC) in the ADC. |
void |
ADC_setInterruptSOCTrigger(uint32 base, uint16 socNumber, Adc_mcalIntSOCTrigger_t trigger) |
Configures the interrupt SOC trigger of an SOC. |
void |
ADC_enableConverter(uint32 base) |
Powers up the analog-to-digital converter core. |
void |
ADC_disableConverter(uint32 base) |
Powers down the analog-to-digital converter module. |
void |
ADC_forceMultipleSOC(uint32 base, uint16 socMask) |
Forces multiple SOC flags to 1 in the analog-to-digital converter. |
boolean |
ADC_getInterruptStatus(uint32 base, uint16 adcIntNum) |
Gets the current ADC interrupt status. |
void |
ADC_clearInterruptStatus(uint32 base, uint16 adcIntNum) |
Clears ADC interrupt sources. |
boolean |
ADC_getInterruptOverflowStatus(uint32 base, uint16 adcIntNum) |
Gets the current ADC interrupt overflow status. |
void |
ADC_clearInterruptOverflowStatus(uint32 base, uint16 adcIntNum) |
Clears ADC interrupt overflow sources. |
uint16 |
ADC_readResult(uint32 resultBase, uint32 socNumber) |
Reads the conversion result. |
uint32 |
ADC_readResultbaseaddr(uint32 resultBase, uint16 socNumber) |
Reads the address of the conversion result register. |
void |
ADC_setSOCPriority(uint32 base, uint16 priMode) |
Sets the priority mode of the SOCs. |
void |
ADC_setupPPB(uint32 base, Adc_mcalPPBNumber_t ppbNumber, uint16 socNumber) |
Configures a post-processing block (PPB) in the ADC. |
void |
ADC_enableInterrupt(uint32 base, uint16 adcIntNum) |
Enables an ADC interrupt source. |
void |
ADC_disableInterrupt(uint32 base, uint16 adcIntNum) |
Disables an ADC interrupt source. |
void |
ADC_setInterruptSource(uint32 base, uint16 adcIntNum, uint16 socNumber) |
Sets the source EOC for an analog-to-digital converter interrupt. |
void |
ADC_enableContinuousMode(uint32 base, uint16 adcIntNum) |
Enables continuous mode for an ADC interrupt. |
void |
ADC_disableContinuousMode(uint32 base, uint32 adcIntNum) |
Disables continuous mode for an ADC interrupt. |
void |
ADC_setMode(uint32 base, Adc_mcalResolution_t resolution, Adc_mcalSignalMode_t signalMode) |
Configures the analog-to-digital converter resolution and signal mode. |
void |
ADC_setPPBTripLimits(uint32 base, Adc_mcalPPBNumber_t ppbNumber, sint32 tripHiLimit, sint32 tripLoLimit) |
Sets the windowed trip limits for a PPB. |
void |
Init a link list object. |
|
void |
De-init a link list object. |
|
void |
Adc_utilsLinkNodePri(Adc_UtilsLinkListObj * llobj, Adc_UtilsNode * node, void * data, Adc_GroupPriorityType priority, uint32 isPaused) |
Links a node to the linked list. |
void |
Adc_utilsUnLinkNodePri(Adc_UtilsLinkListObj * llobj, Adc_UtilsNode * node) |
Unlinks the node from the list. Used for the priority link lists. |
void |
Adc_utilsInitNodeObject(Adc_UtilsNode * node) |
Initialize the node object with default value. |
Adc_UtilsNode * |
Adc_utilsGetHeadNode(const Adc_UtilsLinkListObj * llobj) |
Returns the reference to the head node. This does not remove the node from the head. |
6.1.5.1. function Adc_Init
void Adc_Init(
const Adc_ConfigType * CfgPtr
)
Brief: Service for ADC initialization.
Initializes the ADC hardware units and driver
Service ID[hex] - 0x00
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Parameters:
CfgPtr Pointer to configuration set in Variant PB (Variant PC requires a NULL_PTR).
Returns:
None
Return: None
6.1.5.2. function Adc_DeInit
void Adc_DeInit(
void
)
Brief: This service sets all ADC HW Units to a state comparable to their power on reset state.
Returns all ADC HW Units to a state comparable to their power on reset state
Service ID[hex] - 0x01
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Returns:
None
Return: None
6.1.5.3. function Adc_SetupResultBuffer
Std_ReturnType Adc_SetupResultBuffer(
Adc_GroupType Group,
const Adc_ValueGroupType * DataBufferPtr
)
Brief: This service initializes ADC driver with the group specific result buffer start address where the conversion results will be stored.
Initializes ADC driver with the group specific result buffer start address where the conversion results will be stored. The application has to ensure that the application buffer, where DataBufferPtr points to, can hold all the conversion results of the specified group. The initialization with Adc_SetupResultBuffer is required after reset, before a group conversion can be started.
Service ID[hex] - 0x0C
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
DataBufferPtr pointer to result data buffer
Returns:
E_OK - result buffer pointer initialized correctly
E_NOT_OK - operation failed or development error occurred
Return: Std_ReturnType
6.1.5.4. function Adc_GetGroupStatus
Adc_StatusType Adc_GetGroupStatus(
Adc_GroupType Group
)
Brief: Returns the conversion status of the requested ADC Channel group.
Returns the conversion status of the requested ADC Channel group.
Service ID[hex] - 0x09
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Returns:
ADC_IDLE The conversion of the specified group has not been started
ADC_BUSY The conversion of the specified group has been started and is still going on.
ADC_COMPLETED The conversion of the specified group has been finished.
ADC_STREAM_COMPLETED The result buffer is completely filled.
Return: Adc_StatusType - Conversion status for the requested group.
6.1.5.5. function Adc_GetStreamLastPointer
Adc_StreamNumSampleType Adc_GetStreamLastPointer(
Adc_GroupType Group,
Adc_ValueGroupType ** PtrToSamplePtr
)
Brief: Returns the number of valid samples per channel, stored in the result buffer.
Returns the number of valid samples per channel, stored in the result buffer. Reads a pointer, pointing to a position in the group result buffer. With the pointer position, the results of all group channels of the last completed conversion round can be accessed. With the pointer and the return value, all valid group conversion results can be accessed (the user has to take the layout of the result buffer into account).
Service ID[hex] - 0x0B
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
PtrToSamplePtr Pointer to result buffer pointer.
Returns:
Number of valid samples per channel
Return: Adc_StreamNumSampleType
6.1.5.6. function Adc_StartGroupConversion
void Adc_StartGroupConversion(
Adc_GroupType Group
)
Brief: Starts the conversion of all channels of the requested ADC Channel group.
Starts the conversion of all channels of the requested ADC Channel group.
Service ID[hex] - 0x02
Sync/Async - Asynchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Returns:
None
Return: None
6.1.5.7. function Adc_StopGroupConversion
void Adc_StopGroupConversion(
Adc_GroupType Group
)
Brief: Stops the conversion of the requested ADC Channel group.
Stops the conversion of the requested ADC Channel group.
Service ID[hex] - 0x03
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Returns:
None
Return: None
6.1.5.8. function Adc_ReadGroup
Std_ReturnType Adc_ReadGroup(
Adc_GroupType Group,
Adc_ValueGroupType * DataBufferPtr
)
Brief: Reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the DataBufferPtr address.
Reads the group conversion result of the last completed conversion round of the requested group and stores the channel values starting at the DataBufferPtr address. The group channel values are stored in ascending channel number order (in contrast to the storage layout of the result buffer if streaming access is configured).
Service ID[hex] - 0x04
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
DataBufferPtr ADC results of all channels of the selected group are stored in the data buffer addressed with the pointer
Returns:
E_OK - results are available and written to the data buffer
E_NOT_OK - no results are available or development error occurred
Return: Std_ReturnType
6.1.5.9. function Adc_EnableGroupNotification
void Adc_EnableGroupNotification(
Adc_GroupType Group
)
Brief: Enables the notification mechanism for the requested ADC Channel group.
Enables the notification mechanism for the requested ADC Channel group.
Service ID[hex] - 0x07
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Returns:
None
Return: None
6.1.5.10. function Adc_DisableGroupNotification
void Adc_DisableGroupNotification(
Adc_GroupType Group
)
Brief: Disables the notification mechanism for the requested ADC Channel group.
Disables the notification mechanism for the requested ADC Channel group.
Service ID[hex] - 0x08
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Returns:
None
Return: None
6.1.5.11. function Adc_GetVersionInfo
void Adc_GetVersionInfo(
Std_VersionInfoType * versioninfo
)
Brief: This service returns the version information of this module.
Returns the version information of this module
Service ID[hex] - 0x0A
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
versioninfo Pointer to where to store the version information of this module
Returns:
None
Return: None
6.1.5.12. function Adc_RegisterReadback
Std_ReturnType Adc_RegisterReadback(
Adc_HWUnitType HWUnit,
Adc_RegisterReadbackType * RegRbPtr
)
Brief: This function reads the important registers of the hardware unit and returns the value in the structure.
This API should be called after Adc_Init is called. Otherwise this API will return E_NOT_OK. This API could be used to readback the register contents after Adc_Init and then the readback value could be compared during ADC execution to check the correctness of the HW unit. Since this API is used for this purpose, the register returned are the ones which doesn’t change after init based on conv or channel config.
Service ID[hex] - 0x16
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
HWUnit ADC Hardware microcontroller peripheral unit ID If this is invalid, then the API will return E_NOT_OK.
RegRbPtr Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.
Returns:
E_OK - Register read back has been done
E_NOT_OK - Register read back failed
Return: Std_ReturnType
6.1.5.13. function Adc_EnableHardwareTrigger
void Adc_EnableHardwareTrigger(
Adc_GroupType Group
)
Brief: Enables the hardware trigger for the requested ADC Channel group.
This function will enable the HW trigger source for the requested ADC channel group.
Service ID[hex] - 0x05
Sync/Async - Asynchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC Channel group.
Returns:
None
Return: None
6.1.5.14. function Adc_DisableHardwareTrigger
void Adc_DisableHardwareTrigger(
Adc_GroupType Group
)
Brief: Disables the hardware trigger for the requested ADC Channel group.
This function will disable the HW trigger source for the requested ADC channel group.
Service ID[hex] - 0x06
Sync/Async - Asynchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC Channel group.
Returns:
None
Return: None
6.1.5.15. function Adc_InitTemperatureRead
void Adc_InitTemperatureRead(
void
)
Brief: This service initializes the efuse parameters for temperature calculation. This is a non-autosar, TI defined API This API is not applicable for AM263x.
Initializes the Driver to read temperature sensors and do the conversion.
Service ID[hex] - None
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Returns:
None
Return: None
6.1.5.16. function Adc_ReadTemperature
void Adc_ReadTemperature(
Adc_GroupType Group,
uint8 NumAverages,
Adc_TempSensValueType * TempValuesPtr
)
Brief: This service starts temperature conversion, waits for completion and reads the temperature sensors group configured as part of Adc_Init and returns the temperature values. This is a non-autosar, TI defined API. This API is not applicable for AM263x.
Returns the temperature sensor values for three digital temperature sensors.
Service ID[hex] - 0x0D
Sync/Async - Synchronous
Reentrancy - Non Reentrant
Parameters:
Group Numeric ID of requested ADC Channel group.
NumAverages Number of samples for averaging the temp value
TempValuesPtr Temperature values for three available digital sensors are stored in this structure
Returns:
None
Return: None
6.1.5.17. function Adc_ReadTemperatureResult
void Adc_ReadTemperatureResult(
Adc_GroupType Group,
Adc_TempSensValueType * TempValuesPtr
)
Brief: This service reads only the results of the temperature sensors group configured as part of Adc_Init, Adc_StartGroupConversion and returns the temperature values. This is a non-autosar, TI defined API. This API is not applicable for AM263x.
Returns the temperature sensor values for three digital temperature sensors.
Service ID[hex] - 0x0E
Sync/Async - Synchronous
Reentrancy - Non Reentrant
This service reads only the results of the temperature sensors group configured as part of Adc_Init, Adc_StartGroupConversion and returns the temperature values. This is a non-autosar, TI defined API. This API is not applicable for AM263x.
Parameters:
Group Numeric ID of requested ADC Channel group.
TempValuesPtr Temperature values for three available digital sensors are stored in this structure
Returns:
None
Return: None
6.1.5.18. function Adc_PollingMainFunction
void Adc_PollingMainFunction(
void
)
Brief: This service is used for Polling Group data.
This service is used for Polling Group data.
Service ID[hex] - 0x15
Sync/Async - Asynchronous
Reentrancy - Non Reentrant
Parameters:
Group Numeric ID of requested ADC Channel group.
Returns:
None
Return: None
6.1.5.19. function Adc_GetReadResultBaseAddress
uint32 Adc_GetReadResultBaseAddress(
Adc_GroupType Group
)
Brief: Returns the HW result register base address.
This service returns the Hardware result register address of the first channel of the ADC group. Hardware result registers of consecutive channels are contiguous. If there are multiple (n) channels in a group, read ‘n’ contiguous values from this base address
Service ID[hex] - 0x17
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Return: uint32 Result base address
6.1.5.20. function Adc_SetInterruptContinuousMode
Std_ReturnType Adc_SetInterruptContinuousMode(
Adc_GroupType Group
)
Brief: Sets the continue to interrupt mode of ADC.
By enabling this function, Interrupt pulses are generated whenever an EOC pulse is generated irrespective of whether the flag bit is cleared or not.
Service ID[hex] - 0x18
Sync/Async - Synchronous
Reentrancy - Reentrant
Parameters:
Group Numeric ID of requested ADC channel group.
Return: Std_ReturnType. E_OK - success, E_NOT_OK - operation failed
6.1.5.21. function ADC_setPrescaler
void ADC_setPrescaler(
uint32 base,
Adc_mcalClkPrescale_t clkPrescale
)
Brief: Configures the analog-to-digital converter module prescaler.
This function configures the ADC module’s ADCCLK.
Parameters:
base base address of the ADC module.
clkPrescale specifies the value by which the input clock is divided to make the ADCCLK. The clkPrescale value can be specified with any of the following variables: ADC_CLK_DIV_1_0, ADC_CLK_DIV_2_0, ADC_CLK_DIV_2_5, …, ADC_CLK_DIV_7_5, ADC_CLK_DIV_8_0, or ADC_CLK_DIV_8_5.
Returns:
None
Return: None
6.1.5.22. function ADC_setupSOC
void ADC_setupSOC(
uint32 base,
uint32 socNumber,
Adc_mcalTrigger_t trigger,
uint32 channel,
uint32 sampleWindow
)
Brief: Configures a start-of-conversion (SOC) in the ADC.
This function configures the a start-of-conversion (SOC) in the ADC module.
Parameters:
base - base address of the ADC module.
socNumber - number of the start-of-conversion. The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which SOC is to be configured on the ADC module specified by base.
trigger - the source that will cause the SOC. The trigger specifies the event that causes the SOC such as software, a timer interrupt, an ePWM event, or an ADC interrupt. It should be a value in the format of ADC_TRIGGER_XXXX where XXXX is the event such as ADC_TRIGGER_SW_ONLY, ADC_TRIGGER_EPWM1_SOCA, and so on.
channel - number associated with the input signal. The channel parameter specifies the channel to be converted. In single-ended mode this is a single pin given by ADC_CH_ADCINx where x is the number identifying the pin between 0 and 5 inclusive. In differential mode, two pins are used as inputs and are passed in the channel parameter as ADC_CH_ADCIN0_ADCIN1, ADC_CH_ADCIN2_ADCIN3, …, or ADC_CH_ADCIN14_ADCIN5.
sampleWindow - acquisition window duration. The sampleWindow parameter is the acquisition window duration in SYSCLK cycles. It should be a value between 1 and 512 cycles inclusive. The selected duration must be at least as long as one ADCCLK cycle. Also, the datasheet will specify a minimum window duration requirement in nanoseconds.
Returns:
None
Return: None
6.1.5.23. function ADC_setInterruptSOCTrigger
void ADC_setInterruptSOCTrigger(
uint32 base,
uint16 socNumber,
Adc_mcalIntSOCTrigger_t trigger
)
Brief: Configures the interrupt SOC trigger of an SOC.
This function configures the interrupt start-of-conversion trigger in the ADC module. This functionality is useful for creating continuous conversions.
Parameters:
base - base address of the ADC module.
socNumber - number of the start-of-conversion. The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which SOC is to be configured on the ADC module specified by base.
trigger - the interrupt source that will cause the SOC. The trigger specifies the interrupt that causes a start of conversion or none. It should be one of the following values.
ADC_INT_SOC_TRIGGER_NONE
ADC_INT_SOC_TRIGGER_ADCINT1
ADC_INT_SOC_TRIGGER_ADCINT2
Returns:
None
Return: None
6.1.5.24. function ADC_enableConverter
void ADC_enableConverter(
uint32 base
)
Brief: Powers up the analog-to-digital converter core.
This function powers up the analog circuitry inside the analog core.
Parameters:
base - base address of the ADC module.
Returns:
None
Return: None
Note: Allow at least a 500us delay before sampling after calling this API. If you enable multiple ADCs, you can delay after they all have begun powering up.
6.1.5.25. function ADC_disableConverter
void ADC_disableConverter(
uint32 base
)
Brief: Powers down the analog-to-digital converter module.
This function powers down the analog circuitry inside the analog core..
Parameters:
base - base address of the ADC module.
Returns:
None
Return: None
6.1.5.26. function ADC_forceMultipleSOC
void ADC_forceMultipleSOC(
uint32 base,
uint16 socMask
)
Brief: Forces multiple SOC flags to 1 in the analog-to-digital converter.
This function forces the SOCFRC1 flags associated with the SOCs specified by socMask. This initiates a conversion once the desired SOCs are given priority. This software trigger can be used whether or not the SOC has been configured to accept some other specific trigger. Valid values for socMask parameter can be any of the individual ADC_FORCE_SOCx values or any of their OR’d combination to trigger multiple SOCs.
Parameters:
base - base address of the ADC module.
socMask - SOCs to be forced through software
Returns:
None
Return: None
Note: To trigger SOC0, SOC1 and SOC2, value (ADC_FORCE_SOC0 | ADC_FORCE_SOC1 | ADC_FORCE_SOC2) should be passed as socMask.
6.1.5.27. function ADC_getInterruptStatus
boolean ADC_getInterruptStatus(
uint32 base,
uint16 adcIntNum
)
Brief: Gets the current ADC interrupt status.
This function returns the interrupt status for the analog-to-digital converter.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum takes a one of the values ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be cleared.
Returns:
ADC_TRUE - if the interrupt flag for the specified interrupt number is set
ADC_FALSE - if the interrupt flag for the specified interrupt number is not set
Return: boolean
6.1.5.28. function ADC_clearInterruptStatus
void ADC_clearInterruptStatus(
uint32 base,
uint16 adcIntNum
)
Brief: Clears ADC interrupt sources.
This function clears the specified ADC interrupt sources so that they no longer assert. If not in continuous mode, this function must be called before any further interrupt pulses may occur.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum takes a one of the values ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be cleared.
Returns:
None
Return: None
6.1.5.29. function ADC_getInterruptOverflowStatus
boolean ADC_getInterruptOverflowStatus(
uint32 base,
uint16 adcIntNum
)
Brief: Gets the current ADC interrupt overflow status.
This function returns the interrupt overflow status for the analog-to-digital converter. An overflow condition is generated irrespective of the continuous mode.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum takes a one of the values ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be cleared.
Returns:
ADC_TRUE - if the interrupt overflow flag for the specified interrupt number is set
ADC_FALSE - if the interrupt overflow flag for the specified interrupt number is not set
Return: boolean
6.1.5.30. function ADC_clearInterruptOverflowStatus
void ADC_clearInterruptOverflowStatus(
uint32 base,
uint16 adcIntNum
)
Brief: Clears ADC interrupt overflow sources.
This function clears the specified ADC interrupt overflow sources so that they no longer assert. If software tries to clear the overflow in the same cycle that hardware tries to set the overflow, then hardware has priority.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum takes a one of the values ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be cleared.
Returns:
None
Return: None
6.1.5.31. function ADC_readResult
uint16 ADC_readResult(
uint32 resultBase,
uint32 socNumber
)
Brief: Reads the conversion result.
This function returns the conversion result that corresponds to the base address passed into resultBase and the SOC passed into socNumber.
Parameters:
resultBase - base address of the ADC results.
socNumber - number of the start-of-conversion The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which SOC’s result is to be read.
Returns:
Returns the conversion result.
Return: uint16
Note: Take care that you are using a base address for the result registers (ADCxRESULT_BASE) and not a base address for the control registers.
6.1.5.32. function ADC_readResultbaseaddr
uint32 ADC_readResultbaseaddr(
uint32 resultBase,
uint16 socNumber
)
Brief: Reads the address of the conversion result register.
This function returns the conversion result that corresponds to the base address passed into resultBase and the SOC passed into socNumber.
Parameters:
resultBase - base address of the ADC results.
socNumber - number of the start-of-conversion The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which SOC’s result is to be read.
Returns:
Returns the conversion result.
Return: uint32
Note: Take care that you are using a base address for the result registers (ADCxRESULT_BASE) and not a base address for the control registers.
6.1.5.33. function ADC_setSOCPriority
void ADC_setSOCPriority(
uint32 base,
uint16 priMode
)
Brief: Sets the priority mode of the SOCs.
This function sets the priority mode of the SOCs. There are three main modes that can be passed in the priMode parameter
All SOCs are in round-robin mode. This means no SOC has an inherent higher priority over another. This is selected by passing in the value ADC_PRI_ALL_ROUND_ROBIN.
All priorities are in high priority mode. This means that the priority of the SOC is determined by its SOC number. This option is selected by passing in the value ADC_PRI_ALL_HIPRI.
A range of SOCs are assigned high priority, with all others in round robin mode. High priority mode means that an SOC with high priority will interrupt the round robin wheel and insert itself as the next conversion. Passing in the value ADC_PRI_SOC0_HIPRI will make SOC0 highest priority, ADC_PRI_THRU_SOC1_HIPRI will put SOC0 and SOC 1 in high priority, and so on up to ADC_PRI_THRU_SOC14_HIPRI where SOCs 0 through 14 are in high priority.
Parameters:
base - base address of the ADC.
priMode - priority mode of the SOCs.
Returns:
None
Return: None
6.1.5.34. function ADC_setupPPB
void ADC_setupPPB(
uint32 base,
Adc_mcalPPBNumber_t ppbNumber,
uint16 socNumber
)
Brief: Configures a post-processing block (PPB) in the ADC.
This function associates a post-processing block with a SOC.
Parameters:
base - base address of the ADC.
ppbNumber - number of the post-processing block. The ppbNumber is a value ADC_PPB_NUMBERX where X is a value from 1 to 4 inclusive that identifies a PPB to be configured.
socNumber - number of the start-of-conversion. The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which SOC is to be configured on the ADC module specified by base.
Returns:
None
Return: None
Note: You can have more that one PPB associated with the same SOC, but a PPB can only be configured to correspond to one SOC at a time. Also note that when you have multiple PPBs for the same SOC, the calibration offset that actually gets applied will be that of the PPB with the highest number. Since SOC0 is the default for all PPBs, look out for unintentional overwriting of a lower numbered PPB’s offset.
6.1.5.35. function ADC_enableInterrupt
void ADC_enableInterrupt(
uint32 base,
uint16 adcIntNum
)
Brief: Enables an ADC interrupt source.
This function enables the indicated ADC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt. Disabled sources have no effect on the processor.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum can take the value ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be enabled.
Returns:
None
Return: None
6.1.5.36. function ADC_disableInterrupt
void ADC_disableInterrupt(
uint32 base,
uint16 adcIntNum
)
Brief: Disables an ADC interrupt source.
This function disables the indicated ADC interrupt source. Only the sources that are enabled can be reflected to the processor interrupt. Disabled sources have no effect on the processor.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum can take the value ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module should be disabled.
Returns:
None
Return: None
6.1.5.37. function ADC_setInterruptSource
void ADC_setInterruptSource(
uint32 base,
uint16 adcIntNum,
uint16 socNumber
)
Brief: Sets the source EOC for an analog-to-digital converter interrupt.
This function sets which conversion is the source of an ADC interrupt.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum can take the value ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module is being configured.
socNumber - number of the start-of-conversion. The socNumber number is a value ADC_SOC_NUMBERX where X is a number from 0 to 15 specifying which EOC is to be configured on the ADC module specified by base.
Returns:
None
Return: None
6.1.5.38. function ADC_enableContinuousMode
void ADC_enableContinuousMode(
uint32 base,
uint16 adcIntNum
)
Brief: Enables continuous mode for an ADC interrupt.
This function enables continuous mode for the ADC interrupt passed into adcIntNum. This means that pulses will be generated for the specified ADC interrupt whenever an EOC pulse is generated irrespective of whether or not the flag bit is set.
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum can take the value ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module is being configured.
Returns:
None
Return: None
6.1.5.39. function ADC_disableContinuousMode
void ADC_disableContinuousMode(
uint32 base,
uint32 adcIntNum
)
Brief: Disables continuous mode for an ADC interrupt.
This function disables continuous mode for the ADC interrupt passed into adcIntNum. This means that pulses will not be generated for the specified ADC interrupt until the corresponding interrupt flag for the previous interrupt occurrence has been cleared using ADC_clearInterruptStatus().
Parameters:
base - base address of the ADC module.
adcIntNum - interrupt number within the ADC wrapper. adcIntNum can take the value ADC_INT_NUMBER1, ADC_INT_NUMBER2, ADC_INT_NUMBER3, or ADC_INT_NUMBER4 to express which of the four interrupts of the ADC module is being configured.
Returns:
None
Return: None
6.1.5.40. function ADC_setMode
void ADC_setMode(
uint32 base,
Adc_mcalResolution_t resolution,
Adc_mcalSignalMode_t signalMode
)
Brief: Configures the analog-to-digital converter resolution and signal mode.
This function configures the ADC module’s conversion resolution and input signal mode and ensures that the corresponding trims are loaded.
Parameters:
base - base address of the ADC module.
resolution - resolution of the converter (12 bits). The resolution parameter specifies the resolution of the conversion. It can be 12-bit specified by ADC_RESOLUTION_12BIT
signalMode - input signal mode of the converter. The signalMode parameter specifies the signal mode. In single-ended mode, which is indicated by ADC_MODE_SINGLE_ENDED, the input voltage is sampled on a single pin referenced to VREFLO. In differential mode, which is indicated by ADC_MODE_DIFFERENTIAL, the input voltage to the converter is sampled on a pair of input pins, a positive and a negative.
Returns:
None
Return: None
6.1.5.41. function ADC_setPPBTripLimits
void ADC_setPPBTripLimits(
uint32 base,
Adc_mcalPPBNumber_t ppbNumber,
sint32 tripHiLimit,
sint32 tripLoLimit
)
Brief: Sets the windowed trip limits for a PPB.
This function sets the windowed trip limits for a PPB. These values set the digital comparator so that when one of the values is exceeded, either a high or low trip event will occur. In 12-bit mode, only bits 12:0 will be compared against bits 12:0 of the PPB result.
Parameters:
base - base address of the ADC module.
ppbNumber - number of the post-processing block. The ppbNumber is a value ADC_PPB_NUMBERX where X is a value from 1 to 4 inclusive that identifies a PPB to be configured.
tripHiLimit - value is the digital comparator trip high limit.
tripLoLimit - value is the digital comparator trip low limit.
Returns:
None
Return: None
6.1.5.42. function Adc_utilsInitLinkList
void Adc_utilsInitLinkList(
Adc_UtilsLinkListObj * llobj
)
Brief: Init a link list object.
Parameters:
llobj Link list object.
Returns:
None
Return: None
6.1.5.43. function Adc_utilsDeInitLinkList
void Adc_utilsDeInitLinkList(
Adc_UtilsLinkListObj * llobj
)
Brief: De-init a link list object.
Parameters:
llobj Link list object.
Returns:
None
Return: None
6.1.5.44. function Adc_utilsLinkNodePri
void Adc_utilsLinkNodePri(
Adc_UtilsLinkListObj * llobj,
Adc_UtilsNode * node,
void * data,
Adc_GroupPriorityType priority,
uint32 isPaused
)
Brief: Links a node to the linked list.
The memory to the node object should be allocated by the caller. This is used for link list with priority.
Parameters:
llobj Link list object.
node Node object pointer used for linking.
data Data pointer to add to node.
priority Priority of the node used for priority based addition of nodes. Priority is in ascending order of the value. So 0 is the lowest priority and is added to the bottom of the node. Nodes with the same priority are always added to the bottom of the existing nodes with same priority. For non-priority based modes, this parameter is ignored and could be set to 0.
isPaused Flag to indiate if this group is paused mid way and is queued back. This is required to put this group ahead of the groups with the same priority as this group so that this group is given precedence to restart ahead of other groups of same priority
Returns:
None
Return: None
6.1.5.45. function Adc_utilsUnLinkNodePri
void Adc_utilsUnLinkNodePri(
Adc_UtilsLinkListObj * llobj,
Adc_UtilsNode * node
)
Brief: Unlinks the node from the list. Used for the priority link lists.
Parameters:
llobj Link list object.
node Node pointer to be unlinked from the list.
Returns:
None
Return: None
6.1.5.46. function Adc_utilsInitNodeObject
void Adc_utilsInitNodeObject(
Adc_UtilsNode * node
)
Brief: Initialize the node object with default value.
Parameters:
node Node pointer to be unlinked from the list.
Returns:
None
Return: None
6.1.5.47. function Adc_utilsGetHeadNode
Adc_UtilsNode * Adc_utilsGetHeadNode(
const Adc_UtilsLinkListObj * llobj
)
Brief: Returns the reference to the head node. This does not remove the node from the head.
Parameters:
llobj Link list object.
Returns:
None
Return: None