6.2. CAN

6.2.1. Modules

Name

CAN Driver Interrupt Handlers

CAN MCAN Driver Implementation

6.2.2. Types

Base type

Type Name

Brief

enum

Can_MailBoxDirectionType

Can Mailbox direction enum.

enum

Can_HandleType

Can Handle Type enum.

enum

Can_TxRxProcessingType

Can Tx/Rx processing enum.

enum

Can_ECCErrorType

Can Controller Error Types.

enum

Can_ControllerInstance

Can Controller instance enum.

typedef void(*)(uint32 canErrorType)

Can_ErrNotifyType

Typedef for error notification function pointer.

typedef uint8

CanControllerState_Type

Can Controller State enum type.

typedef uint32

Can_InterruptMask_Type

Can Interrupt Mask type.

6.2.2.1. enum Can_MailBoxDirectionType

Enumerator

Value

Description

CAN_MAILBOX_DIRECTION_RX

0x0U

Mailbox is for receive.

CAN_MAILBOX_DIRECTION_TX

0x1U

Mailbox is for transmit.

Brief: Can Mailbox direction enum.

6.2.2.2. enum Can_HandleType

Enumerator

Value

Description

CAN_FULL

0x0U

For only one L-PDU (identifier) is handled by the hardware object.

CAN_BASIC

0x1U

For several L-PDUs are handled by the hardware object.

Brief: Can Handle Type enum.

6.2.2.3. enum Can_TxRxProcessingType

Enumerator

Value

Description

CAN_TX_RX_PROCESSING_INTERRUPT

0x0U

Interrupt Mode of operation.

CAN_TX_RX_PROCESSING_MIXED

0x1U

Mixed Mode of operation.

CAN_TX_RX_PROCESSING_POLLING

0x2U

Polling Mode of operation.

Brief: Can Tx/Rx processing enum.

6.2.2.4. enum Can_ECCErrorType

Enumerator

Value

Description

CAN_ECC_ERROR_TYPE_PARITY

0x0U

Parity Error.

CAN_ECC_ERROR_TYPE_SEC

0x1U

Single Bit Error Detected and corrected.

CAN_ECC_ERROR_TYPE_DED

0x2U

Double Bit Error Detected.

Brief: Can Controller Error Types.

6.2.2.5. enum Can_ControllerInstance

Enumerator

Value

Description

CAN_CONTROLLER_INSTANCE_MCAN0

0x0U

MCAN0 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN1

0x1U

MCAN1 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN2

0x2U

MCAN2 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN3

0x3U

MCAN3 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN4

0x4U

MCAN4 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN5

0x5U

MCAN5 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN6

0x6U

MCAN6 Controller Instance.

CAN_CONTROLLER_INSTANCE_MCAN7

0x7U

MCAN7 Controller Instance.

Brief: Can Controller instance enum.

6.2.2.6. typedef Can_ErrNotifyType

typedef void(* Can_ErrNotifyType) (uint32 canErrorType);

Brief: Typedef for error notification function pointer.

6.2.2.7. typedef CanControllerState_Type

typedef uint8 CanControllerState_Type;

Brief: Can Controller State enum type.

6.2.2.8. typedef Can_InterruptMask_Type

typedef uint32 Can_InterruptMask_Type;

Brief: Can Interrupt Mask type.

6.2.3. Structures

Name

Brief

Can_MaskType

Structure defining the filter mask to be used.

Can_HwFilterType

Structure defining the HW filter to be used.

Can_FdBaudConfigType

Structure defining the CAN FD data phase baud rate configuration.

Can_BaudConfigType

Structure defining the CAN baud rate configuration.

Can_ControllerType

Can Controller Configuration definition.

Can_ControllerType_PC

Can Controller Pre Compile Configuration definition.

Can_MailboxType

Can mailbox configuration definition.

Can_MailboxType_PC

Can mailox Pre compile configuration definition.

Can_ConfigType

Can MCAL root configuration structure.

Can_RegisterReadbackType

Register Readback Structure The Safety API to readback CAN register vales will populate this structure.

6.2.4. Defines

Name

Brief

CAN_SW_MAJOR_VERSION

Driver Implementation Major Version.

CAN_SW_MINOR_VERSION

Driver Implementation Minor Version.

CAN_SW_PATCH_VERSION

Driver Implementation Patch Version.

CAN_AR_RELEASE_MAJOR_VERSION

AUTOSAR Major version specification implemented by CanDriver.

CAN_AR_RELEASE_MINOR_VERSION

AUTOSAR Minor version specification implemented by CanDriver.

CAN_AR_RELEASE_REVISION_VERSION

AUTOSAR Patch version specification implemented by CanDriver.

CAN_VENDOR_ID

Texas Instruments Vendor ID.

CAN_MODULE_ID

Can Driver Module ID.

CAN_INSTANCE_ID

CAN Driver Instance ID.

CAN_UNINIT

CAN Driver is NOT initialized.

CAN_READY

CAN Driver is initialized.

CAN_INIT_ID

Can_Init()

CAN_MAINFCT_WRITE_ID

Can_MainFunction_Write()

CAN_SETCTR_ID

Can_SetControllerMode()

CAN_DIINT_ID

Can_DisableControllerInterrupts()

CAN_ENINT_ID

Can_EnableControllerInterrupts()

CAN_WRITE_ID

Can_Write()

CAN_VERSION_ID

Can_GetVersionInfo()

CAN_MAINFCT_READ_ID

Can_MainFunction_Read()

CAN_MAINFCT_BO_ID

Can_MainFunction_BusOff()

CAN_MAINFCT_WU_ID

Can_MainFunction_Wakeup()

CAN_CKWAKEUP_ID

Can_CheckWakeup()

CAN_MAINFCT_MODE_ID

Can_MainFunction_Mode()

CAN_SETBAUDRATE_ID

Can_SetBaudrate()

CAN_DEINIT_ID

Can_DeInit()

CAN_GETCTRERRST_ID

Can_GetControllerErrorState()

CAN_GETCTRMODE_ID

Can_GetControllerMode()

CAN_RXPROCESS_ID_INTERRUPT

Can_RxProcess_Interrupt()

CAN_RXPROCESS_ID_POLLING

Can_RxProcess_Polling()

CAN_REGISTER_READBACK_ID

Can_RegisterReadback()

CAN_LOOPBACK_ENABLE_ID

Can_TestLoopBackModeEnable()

CAN_LOOPBACK_DISABLE_ID

Can_TestLoopBackModeDisable()

CAN_ZERO

Numerical value.

CAN_E_PARAM_POINTER

ERROR:NULL_PTR passed as parameter.

CAN_E_PARAM_HANDLE

ERROR:Invalid Controller Handle.

CAN_E_PARAM_DATA_LENGTH

ERROR:Invalid length of msg.

CAN_E_PARAM_CONTROLLER

ERROR:Invalid controller id.

CAN_E_UNINIT

ERROR:Error due to API invoked without performing Can_Init()

CAN_E_TRANSITION

ERROR:Error during Controller state transition.

CAN_E_PARAM_BAUDRATE

ERROR:Invalid Baudrate configuration.

CAN_E_ICOM_CONFIG_INVALID

ERROR:Invalid config ID.

CAN_E_DATALOST

ERROR:Data lost/dropped . Runtime Error.

6.2.5. Functions

Return type

Function Name

Brief

void

Can_GetVersionInfo(Std_VersionInfoType * Can_VersionInfo)

Function returns the version information of this module.

void

Can_Init(const Can_ConfigType * CfgPtr)

This function initializes the module. All the required initialization for the CAN driver and hardware is performed in this function.

Std_ReturnType

Can_SetControllerMode(uint8 Controller, Can_ControllerStateType Transition)

This function performs software triggered state transitions of the CAN controller State machine.

Std_ReturnType

Can_Write(Can_HwHandleType Hth, const Can_PduType * PduInfo)

This function is called by CanIf to pass a CAN message to CanDrv for transmission.

Std_ReturnType

Can_CheckWakeup(uint8 Controller)

This function checks if a wakeup has occurred for the given controller.

void

Can_DisableControllerInterrupts(uint8 Controller)

This function disables all interrupts for this CAN controller Basically it will Disable the CAN interrupts(reset bit 1 in CTL reg(IE0=0)).

void

Can_EnableControllerInterrupts(uint8 Controller)

This function will Enable the interrupts for the Controller desired. It will restore the interrupts that were defined in the configuration. Basically it will enable the CAN interrupts.

void

Can_MainFunction_Write(void )

This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

void

Can_MainFunction_BusOff(void )

This function performs the polling of bus-off events that are configured statically as ‘to be polled’.

void

Can_MainFunction_Read(void )

This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

void

Can_MainFunction_Wakeup(void )

This function performs the polling of wake-up events that are configured statically as ‘to be polled.

void

Can_MainFunction_Mode(void )

This function performs the polling of CAN controller mode transitions This will indicate only the CanController SW state and cannot indicate any HW state as there is no HW state exposed from the Can Controller.

Std_ReturnType

Can_TestLoopBackModeEnable(uint8 controller, uint8 mode)

This service will enable CAN loopback mode.

Std_ReturnType

Can_TestLoopBackModeDisable(uint8 controller, uint8 mode)

This service will disable CAN loopback mode.

void

Can_0_Int0ISR_Fun(void )

This function is the ISR for CAN controller 0/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_0_Int1ISR_Fun(void )

This function is the ISR for CAN controller 0/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_1_Int0ISR_Fun(void )

This function is the ISR for CAN controller 1/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_1_Int1ISR_Fun(void )

This function is the ISR for CAN controller 1/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_2_Int0ISR_Fun(void )

This function is the ISR for CAN controller 2/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_2_Int1ISR_Fun(void )

This function is the ISR for CAN controller 2/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_3_Int0ISR_Fun(void )

This function is the ISR for CAN controller 3/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

void

Can_3_Int1ISR_Fun(void )

This function is the ISR for CAN controller 3/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

Std_ReturnType

Can_SetBaudrate(uint8 Controller, uint16 BaudRateConfigID)

This function Sets Can controller baud rate selected by BaudRateConfigID.

Std_ReturnType

Can_RegisterReadback(uint8 Controller, Can_RegisterReadbackType * RegRbPtr)

This service will readback CAN registers This is the function for checking the configuration registers. This API can be called by higher layers to check if configuration is correct.

Std_ReturnType

Can_EccParityEnable(uint8 controller, uint8 flag, uint8 ramInitEnable)

This function Enables/Disables Parity This function used to test ECC/Parity error. ramInitEnable should be set to TRUE if ECC enabled for normal operations otherwise pass false if it is diagnostic purpose.

Std_ReturnType

Can_EccDiagnosticGetErrMsgBoxNum(uint8 controller, uint8 * msgBox)

This function returns corrupted mailbox number This function returns mailbox number whose RAM is Corrupted.

Std_ReturnType

Can_EccDiagnosticModeEnable(uint8 controller, uint8 flag)

This function Sets ECC diagnostic mode This function used to test Single bit ECC correction.

Std_ReturnType

Can_EccGetErrStatus(uint8 controller, uint32 * ecccErrStatus)

This API will read the ECC error status information of MCAN controller This function used to test Double bit error detection.

Std_ReturnType

Can_EccClrErrStatus(uint8 controller)

This API clears the ECC error status register.

void

Can_DeInit(void )

This service is only used for UT testing and not for app use. This API is not standard AUTOSAR API. This service sets the internal Can Controller state to UNINIT state so that Can_Init can be invoked again. This is required for UT test cases with diff Config.

Std_ReturnType

Can_GetControllerErrorState(uint8 ControllerId, Can_ErrorStateType * ErrorStatePtr)

This function get the error state of the controller.

Std_ReturnType

Can_GetControllerMode(uint8 Controller, Can_ControllerStateType * ControllerModePtr)

This service reports about the current status of the requested CAN controller.

6.2.5.1. function Can_GetVersionInfo

void Can_GetVersionInfo(
    Std_VersionInfoType * Can_VersionInfo
)

Brief: Function returns the version information of this module.

Service ID[hex] : 0x07

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • versioninfo Pointer to where to store the version information of this module.

Returns:

  • None

Return: None

6.2.5.2. function Can_Init

void Can_Init(
    const Can_ConfigType * CfgPtr
)

Brief: This function initializes the module. All the required initialization for the CAN driver and hardware is performed in this function.

Service ID[hex] : 0x00

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • CfgPtr Pointer to driver configuration.

Returns:

  • None

Return: None

6.2.5.3. function Can_SetControllerMode

Std_ReturnType Can_SetControllerMode(
    uint8 Controller,
    Can_ControllerStateType Transition
)

Brief: This function performs software triggered state transitions of the CAN controller State machine.

Service ID[hex] : 0x03

Sync/Async : Asynchronous

Reentrancy : Non Reentrant

Parameters:

  • Controller - CAN controller for which the status shall be changed

  • Transition - Transition value to request new CAN controller state

Returns:

  • E_OK request accepted

  • E_NOT_OK request not accepted, a development error occurred

Return: Std_ReturnType

6.2.5.4. function Can_Write

Std_ReturnType Can_Write(
    Can_HwHandleType Hth,
    const Can_PduType * PduInfo
)

Brief: This function is called by CanIf to pass a CAN message to CanDrv for transmission.

Service ID[hex] : 0x06

Sync/Async : Synchronous

Reentrancy : Reentrant (thread-safe)

Parameters:

  • Hth - Information which HW-transmit handle shall be used for transmit. Implicitly this is also the information about the controller to use because the Hth numbers are unique inside one hardware unit.

  • PduInfo - Pointer to SDU user memory, DLC and Identifier.

Returns:

  • E_OK Write command has been accepted

  • E_NOT_OK development error occurred

  • CAN_BUSY No TX hardware buffer available or pre-emptive call of Can_Write that can’t be implemented re-entrant

Return: Std_ReturnType

6.2.5.5. function Can_CheckWakeup

Std_ReturnType Can_CheckWakeup(
    uint8 Controller
)

Brief: This function checks if a wakeup has occurred for the given controller.

Service ID[hex] : 0x0b

Sync/Async : Synchronous

Reentrancy : Non Reentrant

Parameters:

  • Controller - Controller to be checked for a wakeup.

Returns:

  • E_OK if wakeup is detected.

  • E_NOT_OK if Wakeup is not detected

Return: Std_ReturnType

6.2.5.6. function Can_DisableControllerInterrupts

void Can_DisableControllerInterrupts(
    uint8 Controller
)

Brief: This function disables all interrupts for this CAN controller Basically it will Disable the CAN interrupts(reset bit 1 in CTL reg(IE0=0)).

Service ID[hex] : 0x04

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.7. function Can_EnableControllerInterrupts

void Can_EnableControllerInterrupts(
    uint8 Controller
)

Brief: This function will Enable the interrupts for the Controller desired. It will restore the interrupts that were defined in the configuration. Basically it will enable the CAN interrupts.

Service ID[hex] : 0x05

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • Controller - CAN controller for which interrupts shall be enabled.

Returns:

  • None

Return: None

6.2.5.8. function Can_MainFunction_Write

void Can_MainFunction_Write(
    void 
)

Brief: This function performs the polling of TX confirmation when CAN_TX_PROCESSING is set to POLLING.

Service ID[hex] : 0x01

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.9. function Can_MainFunction_BusOff

void Can_MainFunction_BusOff(
    void 
)

Brief: This function performs the polling of bus-off events that are configured statically as ‘to be polled’.

Service ID[hex] : 0x09

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.10. function Can_MainFunction_Read

void Can_MainFunction_Read(
    void 
)

Brief: This function performs the polling of RX indications when CAN_RX_PROCESSING is set to POLLING.

Service ID[hex] : 0x08

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.11. function Can_MainFunction_Wakeup

void Can_MainFunction_Wakeup(
    void 
)

Brief: This function performs the polling of wake-up events that are configured statically as ‘to be polled.

Service ID[hex] : 0x0A

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.12. function Can_MainFunction_Mode

void Can_MainFunction_Mode(
    void 
)

Brief: This function performs the polling of CAN controller mode transitions This will indicate only the CanController SW state and cannot indicate any HW state as there is no HW state exposed from the Can Controller.

Service ID[hex] : 0x0C

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.13. function Can_TestLoopBackModeEnable

Std_ReturnType Can_TestLoopBackModeEnable(
    uint8 controller,
    uint8 mode
)

Brief: This service will enable CAN loopback mode.

Service ID[hex] : 0x0f

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • Controller - CAN Controller to enable loopback mode

  • Loopback mode - # 0 - Digital Loopback, # 1 - Analog Loopback

Returns:

  • E_OK Loopback mode enabled in the CAN Controller

  • E_NOT_OK Loopback mode enable failed

Return: Std_ReturnType

6.2.5.14. function Can_TestLoopBackModeDisable

Std_ReturnType Can_TestLoopBackModeDisable(
    uint8 controller,
    uint8 mode
)

Brief: This service will disable CAN loopback mode.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • Controller - CAN Controller to disable loopback mode

  • Loopback mode - # 0 - Digital Loopback, # 1 - Analog Loopback

Returns:

  • E_OK Loopback mode disabled in the CAN Controller

  • E_NOT_OK Loopback mode disable failed

Return: Std_ReturnType

6.2.5.15. function Can_0_Int0ISR_Fun

void Can_0_Int0ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 0/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 0. All the Interrupts are hooked to MCAN0INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.16. function Can_0_Int1ISR_Fun

void Can_0_Int1ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 0/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 0 ECC Error. This ISR will clear and report the ECC Error through call back function.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.17. function Can_1_Int0ISR_Fun

void Can_1_Int0ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 1/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 1. All the Interrupts are hooked to MCAN1INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.18. function Can_1_Int1ISR_Fun

void Can_1_Int1ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 1/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 1 ECC Error. This ISR will clear and report the ECC Error through call back function.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.19. function Can_2_Int0ISR_Fun

void Can_2_Int0ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 2/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 2. All the Interrupts are hooked to MCAN2INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.20. function Can_2_Int1ISR_Fun

void Can_2_Int1ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 2/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 2 ECC Error. This ISR will clear and report the ECC Error through call back function.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.21. function Can_3_Int0ISR_Fun

void Can_3_Int0ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 3/INT 0 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 3. All the Interrupts are hooked to MCAN3INT. This ISR sends the TX confirmation for the successful tx msg. This ISR will call the RX processing function for the received message. This ISR will call the Error processing function in case of any error interrupts.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.22. function Can_3_Int1ISR_Fun

void Can_3_Int1ISR_Fun(
    void 
)

Brief: This function is the ISR for CAN controller 3/INT 1 This function should be invoked either by OS Interrupt frame handler CAN Interrupt frame handler for Category 1 ISR.

This is the ISR function for the MCAN controller 4 ECC Error. This ISR will clear and report the ECC Error through call back function.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.23. function Can_SetBaudrate

Std_ReturnType Can_SetBaudrate(
    uint8 Controller,
    uint16 BaudRateConfigID
)

Brief: This function Sets Can controller baud rate selected by BaudRateConfigID.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • Controller - Controller whose Baud Rate is being set

  • BaudRateConfigID - ID number corresponding to a Baud Rate Configuration

Returns:

  • E_OK Service request accepted, setting of (new) baud rate started

  • E_NOT_OK Service request not accepted

Return: Std_ReturnType

6.2.5.24. function Can_RegisterReadback

Std_ReturnType Can_RegisterReadback(
    uint8 Controller,
    Can_RegisterReadbackType * RegRbPtr
)

Brief: This service will readback CAN registers This is the function for checking the configuration registers. This API can be called by higher layers to check if configuration is correct.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Reentrant

Parameters:

  • Controller - CAN Controller to readback registers

  • RegRbPtr - Pointer to where to store the readback values. If this pointer is NULL_PTR, then the API will return E_NOT_OK.

Returns:

  • E_OK Register readback successful

  • E_NOT_OK Register readback failed

Return: Std_ReturnType

6.2.5.25. function Can_EccParityEnable

Std_ReturnType Can_EccParityEnable(
    uint8 controller,
    uint8 flag,
    uint8 ramInitEnable
)

Brief: This function Enables/Disables Parity This function used to test ECC/Parity error. ramInitEnable should be set to TRUE if ECC enabled for normal operations otherwise pass false if it is diagnostic purpose.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • Controller - Controller Id

  • flag - Enable/Disable Parity

  • ramInitEnable - Enable/Disable Ram Init

Returns:

  • E_OK Parity enabled

  • E_NOT_OK Parity enable failed

Return: Std_ReturnType

6.2.5.26. function Can_EccDiagnosticGetErrMsgBoxNum

Std_ReturnType Can_EccDiagnosticGetErrMsgBoxNum(
    uint8 controller,
    uint8 * msgBox
)

Brief: This function returns corrupted mailbox number This function returns mailbox number whose RAM is Corrupted.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • controller - Controller Id

  • msgBox - Message number which caused ECC error.

Returns:

  • E_OK Request successful

  • E_NOT_OK Request failed

Return: Std_ReturnType

6.2.5.27. function Can_EccDiagnosticModeEnable

Std_ReturnType Can_EccDiagnosticModeEnable(
    uint8 controller,
    uint8 flag
)

Brief: This function Sets ECC diagnostic mode This function used to test Single bit ECC correction.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • controller - Controller Id

  • flag - Enable/Disable Parity

Returns:

  • E_OK ECC diagnostic mode enabled

  • E_NOT_OK ECC diagnostic mode failed

Return: Std_ReturnType

6.2.5.28. function Can_EccGetErrStatus

Std_ReturnType Can_EccGetErrStatus(
    uint8 controller,
    uint32 * ecccErrStatus
)

Brief: This API will read the ECC error status information of MCAN controller This function used to test Double bit error detection.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • controller - Controller Id

  • ecccErrStatus - ECC error status

Returns:

  • E_OK Get ECC error status successful

  • E_NOT_OK Get ECC error status failed

Return: Std_ReturnType

6.2.5.29. function Can_EccClrErrStatus

Std_ReturnType Can_EccClrErrStatus(
    uint8 controller
)

Brief: This API clears the ECC error status register.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • controller - Controller Id

Returns:

  • E_OK Clear ECC error status successful

  • E_NOT_OK Clear ECC error status failed

Return: Std_ReturnType

6.2.5.30. function Can_DeInit

void Can_DeInit(
    void 
)

Brief: This service is only used for UT testing and not for app use. This API is not standard AUTOSAR API. This service sets the internal Can Controller state to UNINIT state so that Can_Init can be invoked again. This is required for UT test cases with diff Config.

Service ID[hex] : N/A

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • None

Returns:

  • None

Return: None

6.2.5.31. function Can_GetControllerErrorState

Std_ReturnType Can_GetControllerErrorState(
    uint8 ControllerId,
    Can_ErrorStateType * ErrorStatePtr
)

Brief: This function get the error state of the controller.

Service ID[hex] : 0x11

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • ControllerId - ID of the CAN controller whose error state is requested.

  • ErrorStatePtr - Pointer where the error state is updated.

Returns:

  • E_OK Error state request accepted

  • E_NOT_OK Error state request not accepted

Return: Std_ReturnType

6.2.5.32. function Can_GetControllerMode

Std_ReturnType Can_GetControllerMode(
    uint8 Controller,
    Can_ControllerStateType * ControllerModePtr
)

Brief: This service reports about the current status of the requested CAN controller.

Service ID[hex] : 0x12

Sync/Async : Synchronous

Reentrancy : Non-Reentrant

Parameters:

  • Controller - CAN controller for which the status shall be changed

  • ControllerModePtr - Pointer to a memory location where the current mode of the CAN controller will be stored.

Returns:

  • E_OK request accepted

  • E_NOT_OK request not accepted

Return: Std_ReturnType