title: Cdd_Dma_ParamEntry summary: Param entry.
Cdd_Dma_ParamEntry
Param entry.
#include <Cdd_Dma.h>
Structure Members
Member Type |
Member name |
Brief |
|---|---|---|
uint32 |
opt |
OPT field of PaRAM Set. |
void * |
srcPtr |
Starting byte address of Source. |
uint16 |
aCnt |
Number of bytes in each Array (ACNT) |
uint16 |
bCnt |
Number of Arrays in each Frame (BCNT) |
void * |
destPtr |
Starting byte address of destination i.e. 5 LSBs should be 0. |
sint16 |
srcBIdx |
Index between consec. arrays of a Source Frame (SRCBIDX) |
sint16 |
destBIdx |
Index between consec. arrays of a Destination Frame (DSTBIDX) |
uint16 |
bCntReload |
Reload value of the numArrInFrame (BCNT). Relevant only for A-sync transfers. |
sint16 |
srcCIdx |
Index between consecutive frames of a Source Block (SRCCIDX) |
sint16 |
destCIdx |
Index between consecutive frames of a Dest Block (DSTCIDX) |
uint16 |
cCnt |
Number of Frames in a block (CCNT) |