AM261x MCU+ SDK  26.00.00

Introduction

This file contains the structures, constants, and interfaces for the Perpherial Contoller Driver (PCD).

The Peripheral Controller Driver (PCD) for Linux will implement the Gadget API, so that the existing Gadget drivers can be used. For the Mass Storage function, the File-backed USB Storage Gadget (FBS) driver will be used. The FBS driver supports the Control-Bulk (CB), Control-Bulk-Interrupt (CBI), and Bulk-Only transports.

Go to the source code of this file.

Data Structures

struct  dwc_req_t
 Structure representing a USB transfer request. More...
 
struct  dwc_usb3_pcd_req_t
 DWC_usb3 request structure. More...
 
struct  dwc_ep_t
 The dwc_ep structure represents the state of a single EP when acting in device mode. It contains the data items needed for an EP to be activated and transfer packets. More...
 
union  dwc_setup_pkt_t
 Buffer used to store the SETUP packet for EP0. More...
 
struct  dwc_usb3_pcd_ep_t
 PCD Endpoint structure. This structure represents an endpoint (EP) in the Peripheral Controller Driver (PCD). More...
 
struct  dwc_hiber_scratchpad_array
 Structure representing an array of hibernation scratchpad DMA addresses. More...
 
struct  dwc_usb3_pcd_t
 DWC_usb3 PCD Structure. This structure encapsulates the data for the dwc_usb3 PCD. More...
 

Macros

#define DWC_MAX_TX_FIFOS   16
 Maximum number of Tx FIFOs. Depends on the RTL configuration. No way to probe the value at runtime. More...
 
#define DWC_MAX_PHYS_EP   32
 Maximum number of physical EPs. Depends on the RTL configuration. No way to probe the value at runtime. More...
 
#define DWC_MAX_DATA_BUFS   13
 Maximum number of data buffers per TRB. OS/application specific. More...
 
#define DWC_MAX_EPS   5U
 Maximum number of EPs, defined by USB spec. More...
 
#define DWC_MAX_EP0_SIZE   512
 Maxpacket size for EP0, defined by USB3 spec. More...
 
#define DWC_MAX_PACKET_SIZE   1024
 Maxpacket size for any EP, defined by USB3 spec. More...
 
#define DWC_PCD_REQ_ZERO   0x001U
 
#define DWC_PCD_REQ_STARTED   0x002U
 
#define DWC_PCD_REQ_MAP_DMA   0x100
 
#define DWC_PCD_REQ_IN   0x200
 
#define dwc_usb3_pcd_ep_to_pcd(pcd_ep)   ((pcd_ep)->dwc_ep.pcd)
 Macro to retrieve the PCD structure from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_num(pcd_ep)   ((pcd_ep)->dwc_ep.num)
 Macro to retrieve the endpoint number from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_type(pcd_ep)   ((pcd_ep)->dwc_ep.type)
 Macro to retrieve the endpoint type from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_is_in(pcd_ep)   ((pcd_ep)->dwc_ep.is_in)
 Macro to check if the endpoint direction is IN. More...
 
#define DWC_STATUS_BUF_SIZE   512U
 
#define dwc_usb3_ep0_setup_desc(pcd)   (pcd)->ep0_setup_desc
 Macro to retrieve the descriptor for SETUP packets for EP0. More...
 
#define dwc_usb3_ep0_setup_desc_dma(pcd)   (pcd)->ep0_setup_desc_dma
 Macro to retrieve the DMA address of the SETUP packet descriptor for EP0. More...
 
#define dwc_usb3_ep0_out_desc(pcd)   (pcd)->ep0_out_desc
 Macro to retrieve the descriptor for Data Out or Status Out phases for EP0. More...
 
#define dwc_usb3_ep0_out_desc_dma(pcd)   (pcd)->ep0_out_desc_dma
 Macro to retrieve the DMA address of the Data Out or Status Out descriptor for EP0. More...
 
#define dwc_usb3_ep0_in_desc(pcd)   (pcd)->ep0_in_desc
 Macro to retrieve the descriptor for Data In or Status In phases for EP0. More...
 
#define dwc_usb3_ep0_in_desc_dma(pcd)   (pcd)->ep0_in_desc_dma
 Macro to retrieve the DMA address of the Data In or Status In descriptor for EP0. More...
 
#define dwc_usb3_ep0_setup_pkt(pcd)   (pcd)->ep0_setup_pkt
 Macro to retrieve the SETUP packet buffer for EP0. More...
 
#define dwc_usb3_ep0_setup_pkt_dma(pcd)   (pcd)->ep0_setup_pkt_dma
 Macro to retrieve the DMA address of the SETUP packet buffer for EP0. More...
 

Enumerations

enum  ep0state_e {
  EP0_IDLE, EP0_IN_DATA_PHASE, EP0_OUT_DATA_PHASE, EP0_IN_WAIT_GADGET,
  EP0_OUT_WAIT_GADGET, EP0_IN_WAIT_NRDY, EP0_OUT_WAIT_NRDY, EP0_IN_STATUS_PHASE,
  EP0_OUT_STATUS_PHASE, EP0_STALL
}
 Enumeration representing the various states of Endpoint 0 (EP0). More...
 
enum  pcdstate_e { DWC_STATE_UNCONNECTED, DWC_STATE_DEFAULT, DWC_STATE_ADDRESSED, DWC_STATE_CONFIGURED }
 Enumeration representing the various states of the PCD. More...
 

Functions

void dwc_usb3_stop_all_xfers (dwc_usb3_pcd_t *pcd)
 Stop any active xfers on the non-EP0 endpoints. More...
 
void dwc_usb3_complete_request (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, u32 event)
 This routine handles non-EP0 transfers. More...
 
dwc_usb3_pcd_ep_t * dwc_usb3_get_out_ep (dwc_usb3_pcd_t *pcd, u32 ep_num)
 This routine returns a pointer to Out EP struct with number ep_num. More...
 
dwc_usb3_pcd_ep_t * dwc_usb3_get_in_ep (dwc_usb3_pcd_t *pcd, u32 ep_num)
 This routine returns a pointer to In EP struct with number ep_num. More...
 
void dwc_usb3_handle_ep_intr (dwc_usb3_pcd_t *pcd, u32 physep, u32 event)
 This interrupt indicates that an EP has a pending interrupt. More...
 
int dwc_usb3_handle_dev_intr (dwc_usb3_pcd_t *pcd, u32 event)
 PCD interrupt handler. More...
 
void dwc_usb3_handle_connect_done_intr (dwc_usb3_pcd_t *pcd)
 This interrupt occurs when a Connect Done is detected. Read the device status register and set the device speed in the data structure. Set up EP0 to receive SETUP packets. More...
 
void dwc_enter_hibernation (dwc_usb3_pcd_t *pcd, int save_state)
 This routine sends the core into hibernation, saving the core's runtime state if requested. More...
 
void dwc_exit_hibernation_after_connect (dwc_usb3_pcd_t *pcd, int connected)
 This routine finishes exiting from hibernation once the device is connected. More...
 
int dwc_exit_hibernation (dwc_usb3_pcd_t *pcd, int restore_state)
 This routine wakes the core from hibernation. More...
 
int dwc_usb3_handle_pme_intr (struct dwc_usb3_device *dev)
 
void dwc_usb3_power_ctl (struct dwc_usb3_device *dev, int on)
 
int dwc_usb3_pcd_init (struct dwc_usb3_device *dev)
 
void dwc_usb3_pcd_remove (struct dwc_usb3_device *dev)
 
dwc_usb3_dma_desc_t * dwc_usb3_pcd_trb_alloc (dwc_usb3_pcd_ep_t *ep, int num_trbs, uByte trb_type, int iso_intvl, int link, dwc_dma_t *trbs_dma_ret)
 This routine allocates the TRBs for an EP. More...
 
void dwc_usb3_pcd_trb_free (dwc_usb3_pcd_ep_t *ep)
 This routine frees the TRBs allocated by dwc_usb3_pcd_trb_alloc(). More...
 
void dwc_usb3_pcd_fill_trbs (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *req)
 This routine assigns and fills in the TRBs for a request. More...
 
void dwc_usb3_ep_activate (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, int restore)
 This routine activates an EP. The Device EP control registers for the EP are configured as defined in the EP structure. More...
 
int dwc_usb3_pcd_ep_enable (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, const usb_endpoint_descriptor_t *ep_desc, const ss_endpoint_companion_descriptor_t *ep_comp)
 This routine is called by the Function Driver for each EP (except EP0) to be configured for the current configuration (SET_CONFIGURATION). More...
 
int dwc_usb3_pcd_ep_disable (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 This routine is called when an EP (except EP0) is disabled due to disconnect or change in configuration. Any pending requests will terminate with a status of -ESHUTDOWN. More...
 
int dwc_usb3_pcd_ep_submit_req (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *req, u32 req_flags)
 This routine submits an I/O Request to an EP. More...
 
void dwc_usb3_pcd_ep_cancel_req (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *req, u32 stream)
 This routine cancels an I/O request from an EP. More...
 
void dwc_usb3_pcd_request_done (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *req, int status)
 This routine completes a request. It calls the request callback. More...
 
void dwc_usb3_pcd_ep_start_transfer (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *req, u32 event)
 This routine does the setup for a data transfer for an EP and starts the transfer. More...
 
void dwc_usb3_pcd_ep_set_stall (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 Set the EP to STALL. More...
 
void dwc_usb3_pcd_ep_clear_stall (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 Clear the EP STALL. More...
 
void dwc_usb3_pcd_ep_set_halt (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, int value)
 This function sets or clears a stall condition on an endpoint. More...
 
void dwc_usb3_ep0_activate (dwc_usb3_pcd_t *pcd, int restore)
 This routine configures EP0 OUT to receive SETUP packets and configures EP0 IN for transmitting packets. More...
 
void dwc_usb3_pcd_ep0_out_start (dwc_usb3_pcd_t *pcd)
 This routine sets up a SETUP stage transfer for EP0 and starts the transfer. More...
 
void dwc_usb3_pcd_ep0_start_transfer (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_req_t *req)
 This routine sets up a data/status stage transfer for EP0 and starts the transfer. If pcd->ep0->dwc_ep.is_in is 0 it will be an OUT transfer, otherwise it will be an IN transfer. More...
 
void dwc_usb3_pcd_ep0_data_stage (dwc_usb3_pcd_t *pcd, int length)
 This routine starts the data stage of a 3-stage control command. pcd->ep0state must be set to EP0_OUT_DATA_PHASE or EP0_IN_DATA_PHASE, and pcd->ep0->dwc_ep.is_in must be set to 0 or 1 before calling this routine. For IN, the data to be sent must be placed in pcd->ep0_status_buf before the call. More...
 
void dwc_usb3_handle_ep0_xfer (dwc_usb3_pcd_t *pcd, u32 event)
 This routine handles EP0 transfers. More...
 
dwc_usb3_pcd_ep_t * dwc_usb3_pcd_get_ep_by_addr (dwc_usb3_pcd_t *pcd, u16 idx)
 This routine gets a pointer to an EP from the wIndex address value of the control request. More...
 
int dwc_usb3_pcd_get_frame_number (dwc_usb3_pcd_t *pcd)
 Gets the current USB frame number. More...
 
int dwc_usb3_pcd_isoc_ep_hiber_restart (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 After hibernation, this function restarts the transfer using the TRB address that was active before hibernation. The address is stored in the hiber_desc_idx field of the dwc_ep structure during the wakeup process. More...
 
void dwc_usb3_pcd_stop (dwc_usb3_pcd_t *pcd)
 This routine is called when the Device is disconnected. It stops any active requests and informs the Function Driver of the disconnect. More...
 
int dwc_usb3_gadget_connect (dwc_usb3_pcd_t *pcd, int speed)
 This routine receives Connect notifications from the PCD. More...
 
int dwc_usb3_gadget_disconnect (dwc_usb3_pcd_t *pcd)
 This routine receives Disconnect notifications from the PCD. More...
 
int dwc_usb3_gadget_suspend (dwc_usb3_pcd_t *pcd)
 This routine receives Suspend notifications from the PCD. More...
 
int dwc_usb3_gadget_resume (dwc_usb3_pcd_t *pcd)
 This routine receives Resume notifications from the PCD. More...
 
int dwc_usb3_gadget_setup (dwc_usb3_pcd_t *pcd, usb_device_request_t *ctrl)
 This routine receives Setup request notifications from the PCD. More...
 
int dwc_usb3_gadget_complete (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, dwc_usb3_pcd_req_t *pcd_req, int status)
 This routine receives Transfer Complete notifications from the PCD. More...
 
void * dwc_usb3_gadget_alloc_dma (dwc_usb3_pcd_ep_t *ep, int size, dwc_dma_t *mem_dma_ret)
 This routine allocates coherent DMA memory. It is used by the PCD to allocate memory for TRBs. The block of memory returned must have a start address aligned to a 16-byte boundary. More...
 
void dwc_usb3_gadget_free_dma (dwc_usb3_pcd_ep_t *ep, int size, void *mem, dwc_dma_t mem_dma)
 This routine frees DMA memory allocated by dwc_usb3_gadget_alloc_dma(). More...
 
dwc_usb3_pcd_req_t * dwc_usb3_gadget_get_request (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 This routine returns the PCD request corresponding to the current transfer request for an endpoint. The current transfer request is the first request submitted that has not been completed yet. More...
 
void dwc_usb3_gadget_start_next_request (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 This routine checks to see if there is another transfer request waiting on an endpoint that has not been started yet. If so then that transfer is started. More...
 
void dwc_usb3_gadget_isoc_ep_start (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, u32 event)
 This routine starts an Isoc EP running at the proper interval, after receiving the initial XferNrdy event. More...
 
void dwc_usb3_gadget_request_nuke (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 This routine terminates all requests which are pending on an endpoint. More...
 
void dwc_usb3_gadget_set_ep_not_started (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep)
 This routine marks all pending requests for an EP as not started. More...
 
void dwc_usb3_task_schedule (struct tasklet_struct *tasklet)
 OS-specific routines called from core code. More...
 

Macro Definition Documentation

◆ DWC_PCD_REQ_ZERO

#define DWC_PCD_REQ_ZERO   0x001U

Flag indicating zero-length packet.

◆ DWC_PCD_REQ_STARTED

#define DWC_PCD_REQ_STARTED   0x002U

Flag indicating the request has started.

◆ DWC_PCD_REQ_MAP_DMA

#define DWC_PCD_REQ_MAP_DMA   0x100

Flag indicating DMA mapping is required.

◆ DWC_PCD_REQ_IN

#define DWC_PCD_REQ_IN   0x200

Flag indicating an IN transfer.

◆ DWC_STATUS_BUF_SIZE

#define DWC_STATUS_BUF_SIZE   512U