AM261x MCU+ SDK  26.00.00

Introduction

This module has APIs for USB Synopsis IP device driver.

Sub Modules

 Control Endpoint 0 API Routines
 
 Endpoint API Routines
 
 Function Driver callback routines
 
 Function Driver notification routines
 
 Initialization API Routines
 
 Miscellaneous API Routines
 
 TRB API Routines
 

Files

file  pcd.h
 This file contains the structures, constants, and interfaces for the Perpherial Contoller Driver (PCD).
 

Data Structures

struct  dwc_req_t
 Structure representing a USB transfer request. More...
 
struct  dwc_usb3_pcd_req_t
 DWC_usb3 request structure. More...
 
struct  dwc_ep_t
 The dwc_ep structure represents the state of a single EP when acting in device mode. It contains the data items needed for an EP to be activated and transfer packets. More...
 
union  dwc_setup_pkt_t
 Buffer used to store the SETUP packet for EP0. More...
 
struct  dwc_usb3_pcd_ep_t
 PCD Endpoint structure. This structure represents an endpoint (EP) in the Peripheral Controller Driver (PCD). More...
 
struct  dwc_hiber_scratchpad_array
 Structure representing an array of hibernation scratchpad DMA addresses. More...
 
struct  dwc_usb3_pcd_t
 DWC_usb3 PCD Structure. This structure encapsulates the data for the dwc_usb3 PCD. More...
 

Functions

void dwc_usb3_stop_all_xfers (dwc_usb3_pcd_t *pcd)
 Stop any active xfers on the non-EP0 endpoints. More...
 
void dwc_usb3_complete_request (dwc_usb3_pcd_t *pcd, dwc_usb3_pcd_ep_t *ep, u32 event)
 This routine handles non-EP0 transfers. More...
 
dwc_usb3_pcd_ep_t * dwc_usb3_get_out_ep (dwc_usb3_pcd_t *pcd, u32 ep_num)
 This routine returns a pointer to Out EP struct with number ep_num. More...
 
dwc_usb3_pcd_ep_t * dwc_usb3_get_in_ep (dwc_usb3_pcd_t *pcd, u32 ep_num)
 This routine returns a pointer to In EP struct with number ep_num. More...
 
void dwc_usb3_handle_ep_intr (dwc_usb3_pcd_t *pcd, u32 physep, u32 event)
 This interrupt indicates that an EP has a pending interrupt. More...
 
int dwc_usb3_handle_dev_intr (dwc_usb3_pcd_t *pcd, u32 event)
 PCD interrupt handler. More...
 
void dwc_usb3_handle_connect_done_intr (dwc_usb3_pcd_t *pcd)
 This interrupt occurs when a Connect Done is detected. Read the device status register and set the device speed in the data structure. Set up EP0 to receive SETUP packets. More...
 
void dwc_enter_hibernation (dwc_usb3_pcd_t *pcd, int save_state)
 This routine sends the core into hibernation, saving the core's runtime state if requested. More...
 
void dwc_exit_hibernation_after_connect (dwc_usb3_pcd_t *pcd, int connected)
 This routine finishes exiting from hibernation once the device is connected. More...
 
int dwc_exit_hibernation (dwc_usb3_pcd_t *pcd, int restore_state)
 This routine wakes the core from hibernation. More...
 
int dwc_usb3_handle_pme_intr (struct dwc_usb3_device *dev)
 
void dwc_usb3_power_ctl (struct dwc_usb3_device *dev, int on)
 
void dwc_usb3_task_schedule (struct tasklet_struct *tasklet)
 OS-specific routines called from core code. More...
 

Enumerations

enum  ep0state_e {
  EP0_IDLE, EP0_IN_DATA_PHASE, EP0_OUT_DATA_PHASE, EP0_IN_WAIT_GADGET,
  EP0_OUT_WAIT_GADGET, EP0_IN_WAIT_NRDY, EP0_OUT_WAIT_NRDY, EP0_IN_STATUS_PHASE,
  EP0_OUT_STATUS_PHASE, EP0_STALL
}
 Enumeration representing the various states of Endpoint 0 (EP0). More...
 
enum  pcdstate_e { DWC_STATE_UNCONNECTED, DWC_STATE_DEFAULT, DWC_STATE_ADDRESSED, DWC_STATE_CONFIGURED }
 Enumeration representing the various states of the PCD. More...
 

Macros

#define DWC_MAX_TX_FIFOS   16
 Maximum number of Tx FIFOs. Depends on the RTL configuration. No way to probe the value at runtime. More...
 
#define DWC_MAX_PHYS_EP   32
 Maximum number of physical EPs. Depends on the RTL configuration. No way to probe the value at runtime. More...
 
#define DWC_MAX_DATA_BUFS   13
 Maximum number of data buffers per TRB. OS/application specific. More...
 
#define DWC_MAX_EPS   5U
 Maximum number of EPs, defined by USB spec. More...
 
#define DWC_MAX_EP0_SIZE   512
 Maxpacket size for EP0, defined by USB3 spec. More...
 
#define DWC_MAX_PACKET_SIZE   1024
 Maxpacket size for any EP, defined by USB3 spec. More...
 
#define dwc_usb3_pcd_ep_to_pcd(pcd_ep)   ((pcd_ep)->dwc_ep.pcd)
 Macro to retrieve the PCD structure from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_num(pcd_ep)   ((pcd_ep)->dwc_ep.num)
 Macro to retrieve the endpoint number from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_type(pcd_ep)   ((pcd_ep)->dwc_ep.type)
 Macro to retrieve the endpoint type from a PCD endpoint. More...
 
#define dwc_usb3_pcd_ep_is_in(pcd_ep)   ((pcd_ep)->dwc_ep.is_in)
 Macro to check if the endpoint direction is IN. More...
 
#define dwc_usb3_ep0_setup_desc(pcd)   (pcd)->ep0_setup_desc
 Macro to retrieve the descriptor for SETUP packets for EP0. More...
 
#define dwc_usb3_ep0_setup_desc_dma(pcd)   (pcd)->ep0_setup_desc_dma
 Macro to retrieve the DMA address of the SETUP packet descriptor for EP0. More...
 
#define dwc_usb3_ep0_out_desc(pcd)   (pcd)->ep0_out_desc
 Macro to retrieve the descriptor for Data Out or Status Out phases for EP0. More...
 
#define dwc_usb3_ep0_out_desc_dma(pcd)   (pcd)->ep0_out_desc_dma
 Macro to retrieve the DMA address of the Data Out or Status Out descriptor for EP0. More...
 
#define dwc_usb3_ep0_in_desc(pcd)   (pcd)->ep0_in_desc
 Macro to retrieve the descriptor for Data In or Status In phases for EP0. More...
 
#define dwc_usb3_ep0_in_desc_dma(pcd)   (pcd)->ep0_in_desc_dma
 Macro to retrieve the DMA address of the Data In or Status In descriptor for EP0. More...
 
#define dwc_usb3_ep0_setup_pkt(pcd)   (pcd)->ep0_setup_pkt
 Macro to retrieve the SETUP packet buffer for EP0. More...
 
#define dwc_usb3_ep0_setup_pkt_dma(pcd)   (pcd)->ep0_setup_pkt_dma
 Macro to retrieve the DMA address of the SETUP packet buffer for EP0. More...
 

Macro Definition Documentation

◆ DWC_MAX_TX_FIFOS

#define DWC_MAX_TX_FIFOS   16

Maximum number of Tx FIFOs. Depends on the RTL configuration. No way to probe the value at runtime.

◆ DWC_MAX_PHYS_EP

#define DWC_MAX_PHYS_EP   32

Maximum number of physical EPs. Depends on the RTL configuration. No way to probe the value at runtime.

◆ DWC_MAX_DATA_BUFS

#define DWC_MAX_DATA_BUFS   13

Maximum number of data buffers per TRB. OS/application specific.

◆ DWC_MAX_EPS

#define DWC_MAX_EPS   5U

Maximum number of EPs, defined by USB spec.

◆ DWC_MAX_EP0_SIZE

#define DWC_MAX_EP0_SIZE   512

Maxpacket size for EP0, defined by USB3 spec.

◆ DWC_MAX_PACKET_SIZE

#define DWC_MAX_PACKET_SIZE   1024

Maxpacket size for any EP, defined by USB3 spec.

◆ dwc_usb3_pcd_ep_to_pcd

#define dwc_usb3_pcd_ep_to_pcd (   pcd_ep)    ((pcd_ep)->dwc_ep.pcd)

Macro to retrieve the PCD structure from a PCD endpoint.

Parameters
pcd_epPointer to the PCD endpoint structure.
Returns
Pointer to the associated PCD structure.

◆ dwc_usb3_pcd_ep_num

#define dwc_usb3_pcd_ep_num (   pcd_ep)    ((pcd_ep)->dwc_ep.num)

Macro to retrieve the endpoint number from a PCD endpoint.

Parameters
pcd_epPointer to the PCD endpoint structure.
Returns
Endpoint number.

◆ dwc_usb3_pcd_ep_type

#define dwc_usb3_pcd_ep_type (   pcd_ep)    ((pcd_ep)->dwc_ep.type)

Macro to retrieve the endpoint type from a PCD endpoint.

Parameters
pcd_epPointer to the PCD endpoint structure.
Returns
Endpoint type.

◆ dwc_usb3_pcd_ep_is_in

#define dwc_usb3_pcd_ep_is_in (   pcd_ep)    ((pcd_ep)->dwc_ep.is_in)

Macro to check if the endpoint direction is IN.

Parameters
pcd_epPointer to the PCD endpoint structure.
Returns
True if the endpoint direction is IN, false otherwise.

◆ dwc_usb3_ep0_setup_desc

#define dwc_usb3_ep0_setup_desc (   pcd)    (pcd)->ep0_setup_desc

Macro to retrieve the descriptor for SETUP packets for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
Pointer to the SETUP packet descriptor.

◆ dwc_usb3_ep0_setup_desc_dma

#define dwc_usb3_ep0_setup_desc_dma (   pcd)    (pcd)->ep0_setup_desc_dma

Macro to retrieve the DMA address of the SETUP packet descriptor for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
DMA address of the SETUP packet descriptor.

◆ dwc_usb3_ep0_out_desc

#define dwc_usb3_ep0_out_desc (   pcd)    (pcd)->ep0_out_desc

Macro to retrieve the descriptor for Data Out or Status Out phases for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
Pointer to the Data Out or Status Out descriptor.

◆ dwc_usb3_ep0_out_desc_dma

#define dwc_usb3_ep0_out_desc_dma (   pcd)    (pcd)->ep0_out_desc_dma

Macro to retrieve the DMA address of the Data Out or Status Out descriptor for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
DMA address of the Data Out or Status Out descriptor.

◆ dwc_usb3_ep0_in_desc

#define dwc_usb3_ep0_in_desc (   pcd)    (pcd)->ep0_in_desc

Macro to retrieve the descriptor for Data In or Status In phases for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
Pointer to the Data In or Status In descriptor.

◆ dwc_usb3_ep0_in_desc_dma

#define dwc_usb3_ep0_in_desc_dma (   pcd)    (pcd)->ep0_in_desc_dma

Macro to retrieve the DMA address of the Data In or Status In descriptor for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
DMA address of the Data In or Status In descriptor.

◆ dwc_usb3_ep0_setup_pkt

#define dwc_usb3_ep0_setup_pkt (   pcd)    (pcd)->ep0_setup_pkt

Macro to retrieve the SETUP packet buffer for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
Pointer to the SETUP packet buffer.

◆ dwc_usb3_ep0_setup_pkt_dma

#define dwc_usb3_ep0_setup_pkt_dma (   pcd)    (pcd)->ep0_setup_pkt_dma

Macro to retrieve the DMA address of the SETUP packet buffer for EP0.

Parameters
pcdPointer to the PCD structure.
Returns
DMA address of the SETUP packet buffer.

Enumeration Type Documentation

◆ ep0state_e

enum ep0state_e

Enumeration representing the various states of Endpoint 0 (EP0).

Enumerator
EP0_IDLE 

Idle state waiting for host to initiate transfer

EP0_IN_DATA_PHASE 

IN data phase of a control transfer

EP0_OUT_DATA_PHASE 

OUT data phase of a control transfer

EP0_IN_WAIT_GADGET 

Waiting for the gadget to complete the IN transfer

EP0_OUT_WAIT_GADGET 

Waiting for the gadget to complete the OUT transfer

EP0_IN_WAIT_NRDY 

Waiting for the IN not ready event from the core

EP0_OUT_WAIT_NRDY 

Waiting for the OUT not ready event from the core

EP0_IN_STATUS_PHASE 

IN status phase of a control transfer

EP0_OUT_STATUS_PHASE 

OUT status phase of a control transfer

EP0_STALL 

Stall state, waiting for the host to clear the stall

◆ pcdstate_e

enum pcdstate_e

Enumeration representing the various states of the PCD.

Enumerator
DWC_STATE_UNCONNECTED 

Device not connected to Host

DWC_STATE_DEFAULT 

Device in default state

DWC_STATE_ADDRESSED 

Device in addressed state

DWC_STATE_CONFIGURED 

Device in configured state

Function Documentation

◆ dwc_usb3_stop_all_xfers()

void dwc_usb3_stop_all_xfers ( dwc_usb3_pcd_t *  pcd)

Stop any active xfers on the non-EP0 endpoints.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.

◆ dwc_usb3_complete_request()

void dwc_usb3_complete_request ( dwc_usb3_pcd_t *  pcd,
dwc_usb3_pcd_ep_t *  ep,
u32  event 
)

This routine handles non-EP0 transfers.

This routine gets the request corresponding to the completed transfer and then calls the core routine for handling the completion.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
epThe EP to complete the request on.
eventThe event associated with the transfer.

◆ dwc_usb3_get_out_ep()

dwc_usb3_pcd_ep_t* dwc_usb3_get_out_ep ( dwc_usb3_pcd_t *  pcd,
u32  ep_num 
)

This routine returns a pointer to Out EP struct with number ep_num.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
ep_numThe endpoint number.
Returns
Pointer to the Out EP struct.

◆ dwc_usb3_get_in_ep()

dwc_usb3_pcd_ep_t* dwc_usb3_get_in_ep ( dwc_usb3_pcd_t *  pcd,
u32  ep_num 
)

This routine returns a pointer to In EP struct with number ep_num.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
ep_numThe endpoint number.
Returns
Pointer to the In EP struct.

◆ dwc_usb3_handle_ep_intr()

void dwc_usb3_handle_ep_intr ( dwc_usb3_pcd_t *  pcd,
u32  physep,
u32  event 
)

This interrupt indicates that an EP has a pending interrupt.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
physepThe physical endpoint number.
eventThe event associated with the transfer.

◆ dwc_usb3_handle_dev_intr()

int dwc_usb3_handle_dev_intr ( dwc_usb3_pcd_t *  pcd,
u32  event 
)

PCD interrupt handler.

The PCD handles the device interrupts. Many conditions can cause a device interrupt. When an interrupt occurs, the device interrupt service routine determines the cause of the interrupt and dispatches handling to the appropriate routine.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
eventThe event associated with the transfer.
Returns
0 if no further action is needed, 1 if the device should enter

◆ dwc_usb3_handle_connect_done_intr()

void dwc_usb3_handle_connect_done_intr ( dwc_usb3_pcd_t *  pcd)

This interrupt occurs when a Connect Done is detected. Read the device status register and set the device speed in the data structure. Set up EP0 to receive SETUP packets.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.

◆ dwc_enter_hibernation()

void dwc_enter_hibernation ( dwc_usb3_pcd_t *  pcd,
int  save_state 
)

This routine sends the core into hibernation, saving the core's runtime state if requested.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
save_stateIf non-zero, the core's runtime state is saved.

◆ dwc_exit_hibernation_after_connect()

void dwc_exit_hibernation_after_connect ( dwc_usb3_pcd_t *  pcd,
int  connected 
)

This routine finishes exiting from hibernation once the device is connected.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
connectedIf non-zero, the device is already connected to the host.

◆ dwc_exit_hibernation()

int dwc_exit_hibernation ( dwc_usb3_pcd_t *  pcd,
int  restore_state 
)

This routine wakes the core from hibernation.

Parameters
pcdProgramming view of DWC_usb3 peripheral controller.
restore_stateIf non-zero, the core's runtime state is restored.
Returns
0 on success, 1 on failure.

◆ dwc_usb3_handle_pme_intr()

int dwc_usb3_handle_pme_intr ( struct dwc_usb3_device *  dev)

◆ dwc_usb3_power_ctl()

void dwc_usb3_power_ctl ( struct dwc_usb3_device *  dev,
int  on 
)

◆ dwc_usb3_task_schedule()

void dwc_usb3_task_schedule ( struct tasklet_struct *  tasklet)

OS-specific routines called from core code.

Parameters
taskletPointer to the tasklet structure to be scheduled.